OMAP3530 Performance

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

OMAP3530 - DVSDK 3.00 (Linux)

Environment

Results

Table 1: Decoding Performance results. (Click on a footnote to read its content)
DECODING PERFORMANCE STATISTICS [ms/frame]
TEST METHOD(*) DSP ONLY FILE to FILE OOB DEMO GSTREAMER CONDITIONS
CODEC VIDEO SIZE RATE1 MV2 AVG MAX AVG MAX FPS3 AVG MAX AVG MAX Clip Used4 PRESET
H264DEC VGA 5Mbps 4 24.95 28.85 28.26 31.88 N/A 28.58 31.47 N/A N/A foreman Default
H264DEC D1 5Mbps 16 28.09 29.33 30.91 32.32 N/A 32.77 35.39 N/A N/A fire Default
H264DEC D1 1.55Mbps 1 20.09 26.66 22.54 28.76 30 24.56 28.73 22.23 28.35 shields Default
MPEG4DEC VGA 3Mbps N/A 11.61 12.47 14.91 21.89 N/A 14.86 16.44 N/A N/A foreman Default
MPEG4DEC D1 10Mbps N/A 19.61 26.66 23.67 31.45 30 24.67 181.634 N/A N/A HPotter Default


Table 2: Encoding Performance results. (Click on a footnote to read its content)
ENCODING PERFORMANCE STATISTICS [ms/frame]
TEST METHOD(*) DSP ONLY FILE to FILE OOB DEMO GSTREAMER CONDITIONS
CODEC VIDEO SIZE RATE1 MV2 AVG MAX AVG MAX FPS3 AVG MAX AVG MAX Clip Used4 PRESET
H264ENC D1 4Mbps 1 30.55 30.83 32.92 33.84 N/A N/A N/A N/A N/A fire Default
H264ENC D1 4Mbps 4 36.38 36.57 37.64 38.20 N/A N/A N/A N/A N/A fire High Speed

Analysis

Figure 1, depicts the analysis for the different measurement methods used to produce the reports based on the shields_720x480_1MV_1_5Mbps.264 clip.

Figure 1: Analysis of the different applications used for shields_720x480_1MV_1_5Mbps.264.

The orange and cyan lines represent respectively the average and maximum processing frame times when running the analysis to decode a H.264 video clip from the DSP perspective only. These indicators serve as a reference to assess the burden of having a multiprocessor system with shared resources; in this particular case, the File-to-File and GStreamer (in yellow) shows an average increment of 12% in processing time; while the DEMO* adds a 22% increment with respect to the average baseline.


Figure 2, show the analysis made from the Decode Demonstration application only and present the impact of playing an audio clip (AAC-HE @ 62.2Kbps/16 bit resolution/24KHz Sample Rate) concurrently; the purpose in this case is to show the behavior of the decode demonstration application, and the results of using a buffer window.

Figure 2: DEMO analysis for Video, Audio and Average Window for shields_720x480_1MV_1_5Mbps.264.

For this analysis scenario the Blue line represents the results for the processing time for a video frame when running the OOB demo applications. (As in the previous case, only 100 frames are extracted for visual clarity). The pink data represents the effects of decoding audio concurrently from the point of view of the video processing (for the DEMO*). Even though a few of the frames go beyond the limit of the allowed time to present the NTSC standard of 29.97FPS, a queue (window) of 8 frames is used after the decoder to smooth out this occurrences and to take advantages of the easy and fast processed frames, the results of this process is represented by the yellow line.

Conclusions

Notes

Leave a Comment

Comments

Comments on OMAP3530 Performance


A0693620 said ...

Can you pls provide results at 600Mhz/430Mhz ?

--A0693620 06:19, 6 August 2009 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox