OMAP35x To AM37x Software Migration Guide

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

 

Contents

AM37x SDK

AM37x SDK contains the following packages as seperate installers.


AM37x Linux PSP

This section describes software interface level changes for drivers supported as part of the BSP and should serve as an aid for migrating existing applications from OMAP35x to the AM/DM37x SoC.

Supported Boot Modes

OMAP35x and AM/DM 37x support the same set of boot modes. Also they share the same base-board - thereby the list of supported boot modes is exactly the same. The list of software supported boot modes include boot from Nand,OneNAND and MMC (UART mode verified separately)

X-Loader/U-boot

The Boot-up procedure is two-stage involving a preliminary bootloader(x-loader) running out of SRAM and secondary bootloader(u-boot) that runs out of DDR.

The same x-loader/u-boot binary should be able to run on both OMAP35x and AM/DM37x platforms. Specific differences between the two platforms are handled through runtime detection of CPU type.

Notable change includes scaling up SGX clock frequency from 96Mhz to 200Mhz(to enable TV-out clock dividers, SGX clock source now derived from Core Clk DPLL)

Ethernet Driver

The ethernet controller is off-chip and both OMAP35x and AM/DM37x re-use the same SMSC 9220 chip. The driver and supported set of features remain the same.

Since the driver relies on CPU for handling IO (no DMA support), overall through put will see an improvement as AM/DM37x platform is clocked at a higher operating frequency.

Audio Driver

The basic components that make-up the audio subsystem like McBSP,I2C,sDMA are unchanged from OMAP35x. The driver and supported set of features remain the same.

Storage Subsystem - NAND, MMC/SD

OMAP35x and AM/DM37x share the same GPMC(interfacing NAND, NOR)and MMC/SD Host controller implementation. The SW drivers are hence re-used and support the same set of features.


Display Sub-System

The Display controller module is similar in both OMAP35x and AM/DM37x supporting various features like, 3 plane (gfx, video1 and video2), 2 overlay manager (LCD/DVI out and TV out), VRFB rotation engine, alpha blending, and color keying.

The differences are summarized below:

From application interface (Fbdev and V4L2) point of view there is no change between OMAP35x and AM/DM37x.

V4L2 Capture Driver

On Capture side, both OMAP35x and AM/DM37x share the same video capture sub-system with features like previewer, resizer and histogram. The SW implementation for both these platforms supports BT656 interface through TVP5146 decoder.

Stand-Alone Resizer Driver

The capture sub-subsytem includes resizer functionality that can be exported to the user for memory-to-memory resize operation(one-shot mode). This is supported through a char device interface on Linux (WIP for Mem-to-Mem framework under V4L2)

From application interface point of view there is no change between OMAP35x and AM/DM37x.

USB Drivers

MUSB OTG Driver

Mentor OTG core version for AM3/DM7x has been upgraded as compared to OMAP35x - some of the hardware issues applicable to OMAP35x have been addressed with this upgradation

The following sections describe the impact of these changes as applicable to specific uses cases

Mass Storage Class(Host)

On AM/DM37x platform, MSC class Rx throughput would improve due to support for concurrent DMA and Rx DMA Mode-1 fixes.

CDC/RNDIS Class

Mentor DMA requires the buffers to be aligned on a four byte boundary on AM/DM37x while there is no such limitation for OMAP35x. This limitation would affect CDC/RNDIS class of application on AM/DM37x as networking stack allocated buffers typically end up being unaligned on word boundary(ethernet header being 14 Bytes long and the stack aligns IP headers on 4-byte boundary). USB driver mitigates this issue by using system DMA for all unaligned buffers. Using system DMA can impact throughput and cpu loading as compared to using Mentor DMA.

Isochronous Class

On AM/DM37x ability to use Mentor DMA for Rx transfers should result in higher FPS rate for USB video streaming. As compared to OMAP35x, the USB driver should be able to sustain simultaneous audio recording along with video streaming(VGA resolution).

Since applications interface through class/gadget drivers and these are unchanged between OMAP35x and AM35x, there should be no interface level changes from application standpoint.

USBHOST(EHCI) Driver

There is no change in USBHOST interface.

SGX Subsystem

The Graphics subsystem on AM/DM37x is clocked at a much higher frequency of 200Mhz as compared to OMAP35x.


Hardware Migration Guide

Refer to the OMAP35x To AM37x Hardware Migration Guide

E2e.jpg For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article OMAP35x To AM37x Software Migration Guide here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox