OMAP3x DVSDK 3.01.00.10 Release Notes

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

TIBanner.png


Contents

OMAP3x Digital Video Software Development Kit (DVSDK) 3.01.00.10 Release Notes

Release Notes - May 24, 2010
Refer online version of release notes for latest updates.

Introduction

This Linux DVSDK Software release for OMAP3525 and OMAP3530 platforms gives developers the ability to evaluate the hardware and software capabilities on OMAP35x DVEVM platform and to begin development using the DSP and video accelerators available on OMAP35x.

This is an OMAP3x DVSDK v3.01 beta release. This release contains defect fixes for the DVSDK demos, enhancements in DMAI and updates to the Multi-media Framework Package. This release also contains the Mega Codec Server, which has the MP3 decoder and AAC Encoder integrated.


Device Support

This release supports the Texas Instruments OMAP3530 and OMAP3525 SoC as well as the OMAP35x Evaluation Module (EVM)


Host Support

This release supports installation and development on the following host platforms


Features Supported

This DVSDK release includes support for OMAP3x platforms with the following features:


What's not Supported


Change Log

Change since DVSDK 3.01.00.06


Change since DVSDK 3.01.00.03


DVSDK Package Contents

The DVSDK installer contains the following components as part of its package.

Component Version Description
biosutils 1.02.02 BIOS Utilities
ceutils 1.06 RTSC Package Wizards
cg_xml 2.12.00 CG XML Utilities
dsplink_linux 1.65.00.02 Foundation software for the inter-processor communication across the GPP-DSP boundary
edma3_lld 01.11.00.03 EDMA low level driver
linuxutils 2.25.02.08 Contiguous memory allocator for Linux
framework_components 2.25.01.05 Framework Components is a collection of framework-independent utility libraries which other software frameworks can build upon.
local_power_manager_linux 1.24.02.09 Local Power Manager to control the DSP power on/off
codec_engine 2.25.02.11 The Codec Engine provides a framework for creating and interacting with multimedia codecs
dvsdk_demos 3.01.00.13 Demo applications that illustrate usage of Linux drivers and codecs
dmai 2.05.00.12 DaVinci Multimedia Application Interface
dvtb 4.20.05 Digital Video Test Bench (DVTB) is an interactive application for evaluating codec performance
xdais 6.25.02.11 XDAIS
kernel_binaries NA Pre-built Dynalically Loadable Kernel Modules for DVSDK demos
linuxlibs 3.01 Target prebuilt libraries for host side SDK build
bios 5.41.00.06 DSP BIOS - Required for DSP side executables
xdctools 3.16.01.27 Tools for XDC package and build


It is necessary to install the codec server to perform the OMAP3X DVSDK build. The following codec servers are available as part of this release.

Component Version Description
cs1omap3530 1.01.00 TI proprietary TSPA Codec Server
ms1omap3530 1.00.00 TI proprietary Non-TSPA Mega Codec Server


The DVSDK depends on the following components.

Component Version Description
AM35x-OMAP35x-PSP-SDK 3.00.01.06 Linux Platform Support Package.
TI_CGT_C6000 6.1.12 TI C6x CodeGen tools.
Code sourcery tool chain arm-2009q1-203 OMAP3 Linux toolchain


Codec Version Details

Codecs Version
AAC HE Decoder 1.30.02.000
MPEG4 SP Decoder 02.01.00
H264 BP Decoder 2.01.007
MPEG2 MP Decoder 02.00.02
JPEG Decoder 02.00.01
MPEG4 SP Encoder 02.04.00
H264 BP Encoder 2.01.013
JPEG Encoder 02.01.01
G711 Encoder 1.12.00.000
G711 Decoder 1.12.00.000
Deinterlacer (I2P) 1.00.00.07


In addition to the above codecs, the following two codecs are part of the mega combo server

Codecs Version
AAC LC/HE Encoder 1.20.005
MP3 Decoder 01.31.01.001


Documentation


Upgrade and Compatibility Information


Installation and Usage


Dependencies


Known Issues


Limitations


Defects Fixed


Special Notes


Technical Support and Product Updates

Please register your EVM serial number as instructed on the printed Read Me 1st Card in order to download the updated software release as soon as it becomes available.


E2e.jpg For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article OMAP3x DVSDK 3.01.00.10 Release Notes here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox