OMAP and Sitara CCS support
From Texas Instruments Embedded Processors Wiki
Contents |
Introduction
This page contains the GEL and CCS configuration files for all OMAP and Sitara devices. This page still needs to be completed, but will contain files for OMAP35x, AM35x, AM37x, and DM37x devices. Eventually, these will be part of the general CCS package, but until then, they will reside here.
CCS 3.3 support files
OMAP3530 and OMAP3525
GEL Files
Configuration files
OMAP3503 and OMAP3515
GEL Files
GELs for OMAP35x EVM (These are the same GEL files as above for OMAP3530/25, but the DSP specific scripts will not function on OMAP3503/15).
Configuration files
DM3730 and DM3725
GEL Files
Configuration files
AM3703 and AM3715
GEL Files
Configuration files
CCS 4.x and 5.x support files
OMAP3530 and OMAP3525
GEL Files
GELs for OMAP3EVM for CCSv4 and CCSv5
DM3730 and DM3725
GEL Files
GELs for OMAP3EVM with DM3730 for CCSv4 and CCSv5
Configuration files
DM8148
GEL Files
GEL for DM8148 EVM baseboard
The package Diagnostics Software of the DM8148EVM support page at Mistral Solutions has additional GEL files for the EVM and peripheral boards.
DM8168
GEL Files
Gel files for all variants of this board are available at the Spectrum Digital's support page.
AM335x
GEL Files
Beaglebone GEL
AM335x EVM GEL for 13x13 v1.0 (with mDDR)
AM335x EVM GEL v1.2 (with DDR2)
AM335x EVM GEL v1.3 (with DDR3)
AM3358 StarterKit GEL
AM3359 ICE board GEL
Comments
Comments on OMAP and Sitara CCS support
NicholasLee said ...
Dbaughman said ...
Is there a reason why there are no entries for AM3703 and AM3715?
--Dbaughman 09:00, 24 October 2011 (CDT)
Philbattenberg said ...
Is there anything available for the AM3703/AM3715?
--Philbattenberg 08:25, 9 February 2012 (CST)

Dead links to the Blackhawk Emulator USB510 and Texas Instruments XDS560 Configuration files.
--Nicholas Lee 03:17, 30 March 2011 (CDT)