Omapl137/DA830 linux bootup
From Texas Instruments Embedded Processors Wiki
(Redirected from Omapl137 linux bootup)
Translate this page to
This page is intended to describe the OMAPL137/DA830 EVM boot sequence and several additional details required to reflash the built-in SPI Flash memory.
Contents |
Booting the OMAP-L137/DA830 EVM
Boot overview
- On the OMAP-L137/DA830 SoC, the DSP boots first
- ARM remains disabled at reset.
- The device supports booting from various media.
- On the EVM, booting from SPI flash is supported.
- The DSP User Boot Loader (UBL) comes up first.
- resides at start of SPI flash
- is in Application Image Script (AIS) file format
- loads the ARM UBL to internal RAM, sets up ARM reset vector and enables ARM.
- Typically there should be no need to modify this software
- The ARM UBL comes up next
- resides next to DSP UBL in SPI flash
- is in flat-binary file format
- Sets up PLLs, SDRAM and does other basic initialization
- Copies U-Boot to SDRAM and starts it.
- U-Boot
- De-facto boot loader for ARM Linux
- resides in SPI flash after ARM UBL
- is in flat-binary file format
- Supported version is 1.3.3
Obtaining Software
- Need:
- Boot Utils (part of PSP package)
- MontaVista tools
- Code Composer Studio v3.3 (Code Composer Studio v4 for the DA830)
- Obtaining Boot Utils - Use either of:
- Standalone PSP package for DA830/OMAP-L137 from https://www-a.ti.com/downloads/sds_support/targetcontent/psp/mv_lsp_2_20/index.html
- PSP package part of OMAP-L137 Software Development Kit obtainable from: http://focus.ti.com/dsp/docs/dspcontent.tsp?contentId=51607&DCMP=OMAP-LxProcessors+Other&HQS=Other+OT+omapl137sksoftwareea
- Obtaining MontaVista tools
- Demonstration version of tools included with the OMAP-L137 starter kit.
- MontaVista tools obtainable from MVZone support.mvista.com
- Obtaining Code Composer Studio
- CCStudio CD included with OMAP-L137 starter kit.
- Visit: www.ti.com/ccstudio
Flashing the EVM
- Setup CCStudio on Host PC using CCS Config files and GEL files here: http://support.spectrumdigital.com/boards/evmomapl137/revd/
- Setup the EVM in "emulation debug" mode by setting SW2 switch as follows:
| Pin # | 7 | 2 | 1 | 0 | 3 |
|---|---|---|---|---|---|
| Position | 1 | 1 | 1 | 1 | 0 |
On EVM revisions A and B, the SW2 switch for Pin #3 is inverted. That is, OFF = 1 and ON = 0. This problem has been corrected from EVM revision C onwards.
- Power-up the EVM and connect the on-board emulation to the PC using the supplied USB cable
- Start CCStudio, connect to DSP, then to ARM
- From the ARM window, load spiflash_writer.out
- When prompted for filetype, enter dspais =armubl= or u-boot.bin depending on whether you are burning the DSP UBL, the ARM UBL, or U-Boot respectively
- All three files need to be burnt to SPI flash for successful boot-up
- Disconnect CCStudio and Power-off EVM, and setup it to boot from SPI0 Flash
| Pin # | 7 | 2 | 1 | 0 | 3 |
|---|---|---|---|---|---|
| Position | 0 | 1 | 0 | 1 | X |
- Connect NULL modem cable from DB9 connector on EVM to COM port on PC
- Setup the serial terminal for 115200 baud, 8 bit data, no parity, 1 stop-bit and no flow control
- Power up the EVM and you should see the U-Boot prompt on the serial console.
Booting Linux
- Boot from SPI flash
- SPI flash is 4MBytes on EVM board
- Use SPI flash to store kernel, use SDRAM, NFS, MMC/SD etc for storing FS
- Select the serial flash device sf probe 0
- Download uImage and copy it to SPI flash partition
tftp 0xc0700000 uImage sf erase 0x1E0000 0x220000 sf write 0xc0700000 0x1E0000 0x220000
- Download ramdisk.gz to SDRAM. tftp 0xc1180000 ramdisk.gz
- Setup bootargs to boot with this configuration
setenv bootargs 'mem=32M console=ttyS2,115200n8 root=/dev/ram0 rw initrd=0xc1180000,4M ip=dhcp' setenv bootcmd 'sf probe 0;sf read 0xc0700000 0x1E0000 0x220000; bootm 0xc0700000'
Compiling Software
- Optional if using pre-compiled binaries from bin directory of PSP package
- To compile SPI flash writer:
- open board_utils/flash_writers/spi_flash_writer/ccsv3.3/spiflash_writer.pjt in CCStudio v3.3
- Build the Project like any other CCStudio project
- spiflash_writer.out is placed in the Debug directory
- Re-compiling DSP UBL should typically not be needed. If required, refer to "Additional Procedures" section of PSP User's Guide.
- To compile ARM UBL
- open board_utils/armubl/ubl.pjt in CCStudio v3.3
- Build the Project like any other CCStudio project
- ubl-spi.bin file is placed in the board_utils/armubl directory
- To compile U-Boot:
- untar board_utils/u-boot-1.3.3.tar.gz
- Make sure MontaVista tools are in $PATH
- change to u-boot-1.3.3 directory and issue:
make distclean make da830_omapl137_config make
- u-boot.bin in created in top level directory
- To compile Linux:
- install mvl_5_0_0_demo_lsp_setuplinux_02_20_X_X.bin; untar the kernel.
- change to linux-2.6.18_pro500 directory and issue:
make distclean ARCH=arm CROSS_COMPILE=arm_v5t_le make da830_omapl137_defconfig ARCH=arm CROSS_COMPILE=arm_v5t_le make uImage ARCH=arm CROSS_COMPILE=arm_v5t_le-
- uImage in created in arch/arm/boot directory
Recording of the Presentations
Streaming WebEx recording of OMAPL1 Linux Boot Up Driver
Leave a Comment