Optimize Linux Boot Time
From Texas Instruments Embedded Processors Wiki
This work is licensed under a Creative Commons Attribution-ShareAlike 3.0 Unported License.
Introduction
Boot-time i.e. the time taken by the system to show its "availability" since the power button was pushed on; is a becoming a key differentiator in the usability vector.
The definition of availability varies across the devices. For example:
- Appearance of home screen for devices containing a display e.g. cellphone, media player
- An audible tone / LED turning on or changing color for devices without display
- Appearance of shell prompt on development systems with console.
As these examples suggest, there isn't an objective measure that can be used across. This article doesn't attempt to define boot-time. It recognizes the fact that boot-time must be measured in context of the device, its intended usage and associated user expectations.
Objectives
Specific usage of term 'optimizing' - instead of 'reducing' - sets the overall direction for this article. The reduction can be achieved by adding hacks/ quirks/ taking custom shortcuts - that are difficult to maintain across component versions. Optimizations are generic and easily maintainable.
This article describes a typical boot sequence and identifies the opportunities for optimization. It also walks through different techniques that can be used to optimize the boot time. These optimizations are illustrated with specific patches that currently apply against the latest PSP 04.02.00.07 release for OMAP35x and Sitara AM37x devices.
This article is augmented with actual patches across the boot-loader(s) and Linux kernel to illustrate the techniques discussed here. Therefore, discussion is limited to select techniques and changes. The commit messages in the individual patches provide more detailed description. The differences between SDK and an end-product will be visible in these patches as well.
- The SDK tends to generic and inclusive. It is intended to demonstrate maximum features available on the platform and tools to leverage these features.
- An end-product is specific and exclusive. It implements only defined set of use-cases.
To provide a direction to the optimizations, these use-cases are being defined:
Use-case 1: Boot from SDHC Card
- Boot from SDHC card
- Mount the filesystem from SDHC card itself
- Shell on serial console.
- A graphical application on the LCD
Use-case 2: Boot from NAND
- Boot from NAND
- Mount the filesystem from NAND partition.
- Shell on serial console.
- A graphical application on the LCD
Understanding the boot sequence
A typical (and simplified) boot sequence in Linux based systems is illustrated below:
NOTE
- Actual boot sequence depends upon the device used viz. NAND flash, MMC/SD Card, NOR flash etc.
- Two stage bootloading is required when the bootloader cannot fit into the internal memory of the processor.
- There are multiple inter-dependencies between loading modules and starting services. This picture is presenting a simplified view for illustration purpose.
Measuring boot time
Optimization begins with knowing current boot-time, setting the target and defining the boundary conditions. The boundary conditions are derived from the characteristics of the end-product.
Optimization is an iterative process and we need a reliable mechanism for measure the time. Developers have a variety of options ranging from C programs that can be compiled to scripts that time stamp each line appearing on the serial port. (More details here.)
The author used RealTerm for the purpose.
- Supports logging in Unix date format - easy for analysis
- Ability to log directly to a file without displaying on the screen - more accurate measurement
- Ability to stop logging after predefined time
- No need to switch terminal for interactive session just for the measurement
Identify markers
As discussed above, the overall boot process involves boot-loader(s), Linux kernel and the filesystem. We must identify the markers in the boot log that can be used as delimiters for each stage of the boot process. This helps in determining the time spent in each stage.
- x-loader
- First newline character received on the serial console indicates start of x-loader.
- u-boot
- The banner containing the U-Boot version indicates the start of u-boot.
- U-Boot 2010.06 (Apr 16 2011 - 15:22:19)
- Linux kernel
- First line after this indicates the start of Linux kernel:
Uncompressing Linux... done, booting the kernel.
- First line after this indicates the start of Linux kernel:
- File System
- INIT: version 2.86 booting
Developers with intimate knowledge of the source code can point that some of the strings are printed much after the start (e.g. U-boot banner) or much before (e.g. filesystem marker) the actual event. While this is definitely true, these markers serve the purpose well.
Profiling the bootloaders
No built-in infrastructure exists to profile the bootloaders at the moment. Much of profiling is based upon various strings that are printed on the serial console. And it is quite effective!
Looking from the end-product perspective - when all development is complete - the bootloaders are required to perform only these 2 tasks:
- Perform basic initialization
- Load binary for the next stage (x-loader loads u-boot and u-boot loads the kernel)
Profiling should be restricted to these actions only.
Profiling the Linux Kernel
Enable timestamps on kernel prints
A timestamp can be added to each string printed by the kernel. Auditing the timestamps can helps in calculating actual time spent in processing. To enable timestamp, select the option "Show timing information on printks" when configuring the kernel.
This translates to following in the .config:
CONFIG_PRINTK_TIME=y
Instrument kernel initialization
When the Linux kernel boot up, all statically linked drivers and subsystems are initialized. This initialization happens via series of initcalls. These "initcalls" can be instrumented by adding bootarg initcall_debug to the kernel command-line.
Raw data can be extracted by following command at the shell prompt:
$ dmesg | grep initcall
However, sorting the drivers and subsystems by the time time spent in the respective "initcall" is more useful.
- If CONFIG_PRINTK_TIME is enabled:
- $ dmesg | grep initcall | sort -k8 -n
- If CONFIG_PRINTK_TIME is disabled:
- $ dmesg | grep initcall | sort -k6 -n
Same information can be viewed graphically via bootgraph script included in the kernel sources. This requires CONFIG_PRINTK_TIME to be enabled.
$ dmesg | perl scripts/bootgraph.pl > boot.svg
Areas of optimization
Any optimization would fall into either of these categories:
- Size
- Reduce the size of binaries for each successive component loaded.
- Remove features that are not required
- Speed
- Optimize for target processor
- Use faster medium for loading primary, secondary boot loaders and kernel.
- Reduce number of tasks leading to the boot.
- Remove features that are not required
Optimization - in both these areas - must be viewed in full context of the target platform and its use cases.
IMPORTANT
Optimization reduces general applicability due to loss of features. This is true for all components - bootloaders, kernel and filesystem.
Reducing the size does help in increasing overall speed - mainly due to gains in time to load the components. But, beyond a certain point, efficiency of implementation gains prominence.
NOTE
This article doesn't attempt to discuss possibility of optimizing the individual kernel subsystems and modules. However, this may be required in the context of the end-product. For example, code meant for handling out-of-protocol quirks, non-conforming devices etc. can be excluded if devices are known to follow defined specs.
Techniques for optimization
Shedding the bulk
The boot-loaders and the Linux kernel contain a default configuration that decides which components are included in the build. These default configurations become starting point for creating a product specific configuration. These configurations must be tailored to ensure that unnecessary components aren't being included in the final build.
Some of the features may be required only by developers and don't have much use in the end-product. These features can also be removed.
Here are few examples of simple decisions that can result in a tailored configuration for a product.
x-loader
- If NAND support is not required, remove it from the configuration
- #undef CFG_NAND
- If OneNAND support is not required, remove it from the configuration
- #undef CFG_ONENAND
- If MMC/SD support is not required, remove these from the configuration
- #undef CONFIG_MMC
- #undef CFG_CMD_MMC
- #undef CFG_CMD_FAT
- #undef CONFIG_DOS_PARTITION
u-boot
- Avoid long help text for the u-boot commands.
- #undef CONFIG_SYS_LONGHELP
- Use simple parser - instead of hush
- #undef CONFIG_SYS_HUSH_PARSER
- If USB support is not required, remove it from the configuration:
- #undef CONFIG_USB_OMAP3
- #undef CONFIG_MUSB_HCD
- #undef CONFIG_MUSB_UDC
- If ETHERNET support is not required, remove it from the configuration:
- #undef CONFIG_CMD_NET
Linux kernel
The drivers and subsystems that are not required in the product can simply be left out of the kernel configuration. Ones that are not "essential" at the system boot-up can be built as insertable modules. These modules can be inserted into the kernel when they are really needed.
- If the product doesn't support any of MTD devices, the corresponding drivers and support for JFFS2 filesystem can be removed from the kernel configuration.
- Initialization of the capture driver can be delayed until it is really required.
Decision on "What is essential?" and "What is extra?" depends upon the actual product definition.
NOTE
#undef is used here to illustrate the configuration options that can be removed in x-loader and u-boot. To exclude them from product specific configuration, not defining them is sufficient.
Deferred initialization
As discussed above, initcalls for some modules may take quite long delaying the boot process. A short patch had been created (against kernel version 2.6.27) to defer selected initcalls until after the system is booted - without having to explicitly define them as modules.
- Identify the modules that are not essential for the system at boot-up
- Locate the initcall definition of these modules in the source code.
- Change the declaration of the initcalls from module_init() to deferred_module_init()
- Once the system has booted, deferred initcalls can be executed by:
- $ echo 1 >/proc/deferred_initcalls
Refer to this page for details and link to the original patch.
Build for product
The default configuration of u-boot and the Linux kernel is friendly for development systems - not the end products. This includes, building with debug information, additional code for traceability, etc.
Once the development is complete and the individual components have been well tested, much of the debug infrastructure can be removed.
Here are some suggestions:
x-loader
- Remove option -g from the compiler.
u-boot
- Remove option -g from the compiler.
- u-boot is build for armv5 for compatibility reasons. Update compiler flags to build it for armv7-a.
Linux kernel
- Remove option -g from the compiler.
- Disable Kernel debugging
- Disable Debug Filesystem
- Disable Tracers
When choosing the compiler options, a common dilemma is to optimize for speed or 'size. Here are few data points that should help make the decision faster:
- Unless executing-in-place, the executable images have to be loaded into the memory from the storage media e.g. while booting from MMC/SD. Bigger means longer time to load the image... which impacts the boot time.
- When optimizing for size, the image would be smaller but the execution would is expected to be little slower.
It is common to see the balance shift on either side during the optimization cycles.
Filesystem
A heavy filesystem can negate all the efforts in optimizing the components. Most of the filesystems are derived from the desktop based systems that may not apply to embedded systems.
IMPORTANT
Initialization scripts need to be reviewed to ensure that only necessary initializations are done.
It is quite common for the filesystems to be built for generic architectures. This may not provide best performance.
For example, ARMv7 based system using filesystem built for ARMv5.
Be quiet
In the default configuration, boot-loaders and the Linux kernel print many verbose messages on the serial console. Though quite useful in the development stages, these messages are not required in the end product. Depending upon the number of prints, turning off these messages can save 1 - 2 seconds on the overall boot process.
x-loader
- Add the following line to board specific configuration:
- #undef CFG_PRINTF
u-boot
Turning the prints off is a 2 step process:
- Add the following line to board specific configuration:
- #define CONFIG_SILENT_CONSOLE 1
- Set the environment variable silent to 1.
- OMAP3_EVM # set silent 1
- OMAP3_EVM # saveenv
Linux kernel
The prints in the Linux kernel can be turned off by adding bootarg quiet to the kernel command-line.
IMPORTANT
As we have seen above, most of the data used for optimizations is available via these prints. This should, therefore, be delayed till the last iteration. If the desired boot time isn't achieved, enable the prints again and look for more opportunities.
Avoid duplication
Boot-loader(s) and the Linux kernel are independent systems. As generic products, they cannot make assumptions about the state of the devices before using them. This could lead to same device getting initialized - to same settings - across both. Product development happens in a controlled environment, where the responsibilities of each layer can be fixed upfront. This would help avoid unnecessary duplication of initialization code.
As an example, IVA was being initialized in the x-loader, u-boot and later in the Linux kernel for DM37x devices.
- IVA is not being used in either of the boot-loaders - x-loader and u-boot.
- IVA needs to be initialized only for the SoC variants containing IVA e.g. OMAP3530, DM3730.
For devices like OMAP3503 and AM3703, this initialization is just a waste of time!
There could be similar instances for other drivers...
Leverage the SoC speed
Running the SoC - processor and other peripherals - at maximum rated performance is easiest way to reduce the boot time. Since, this is too obvious and doesn't involve any optimization, it is being discussed at the end.
Don't forget to remove instrumentation
In initial sections of the this article, additional instrumentation was added/ enabled to get objective measure to time spent in each software layer. One we are satisfied with the progress made, this instrumentation can be turned off. After a certain stage, amount of time spent in instrumentation becomes proportionally sizable.
Doing it yourself
Starting with the stock PSP release, a series of patches are available for each of x-loader, u-boot and Linux kernel - that indicate the changes done to optimize the boot time.
To illustrate the optimization steps, new configurations - specific to the use cases - were created. Key considerations behind this decision were:
- The default configuration remains untouched for developers to try both configurations without changing branch/ reverting patches.
- This mimics the development flow customers would be taking to create product specific configuration - starting with a known base.
Each patch contains detailed description of the change being done.
Getting sources
x-loader
- Branch qb_v1.51_OMAPPSP_04.02.00.07
U-Boot
Linux Kernel
NOTE
- Current set of patches are applicable for the OMAP3EVM.
- In the process of optimizations few generic issues (not related to optimization) were found and fixed on the same branch. Since, these changes apply over a code freeze sources, they will be rolled into base PSP package in next cycle.
- Patches for use-case 2 shall be available soon
Building sources
Build x-loader
$ make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- omap3_evm_mmc_config $ make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi-
Build u-boot
$ make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- omap3_evm_quick_mmc_config $ make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi-
Build Linux kernel
$ make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- omap3_evm_quick_defconfig $ make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- uImage
Build Linux kernel modules
$ make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- modules
Install Linux kernel modules
$ make ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi- INSTALL_MOD_PATH=<fs-path> modules_install
- If same host machine is being used for building the Linux kernel and the filesystem, then <fs-path> should point to base of the target filesystem directory.
- If using a pre-built filesystem:
- Set <fs-path> to a local path e.g. ./_install
- Create a tarball of the ./_install directory
- $ cd _install
- $ tar cvfz ../modules.tgz .
- Copy this tarball to root of the installed filesystem and extract the contents.
- $ tar xvfz modules.tgz
- Now modules can be installed individually / via scripts e.g.
- $ modprobe snd
NOTE
Steps to prepare the MMC card and NAND flash are not covered in this article. These steps are described in the User Guide corresponding to each release.
Pre-built binaries
TODO : Links to download pre-built binaries to be added
What is current status?
As described in initial sections, AM37x EVM was chosen as the first target for the optimization.
Comparing size of binaries
This table compares the size of binaries generated with optimized configurations against default configurations.
| Component/ File | Default Config (in bytes) | Opt for MMC (in bytes) | Opt for NAND (in bytes) |
|---|---|---|---|
| x-loader.bin | 18,932 | 12,460 | 7,712 |
| u-boot.bin | 219,280 | 64,808 | 88,908 |
NOTE
Depending upon the compiler version used, there may be minor differences in the size of binaries generated. These numbers correspond to Codesourcery Lite v2009q1-203.
Comparing boot times
| Usage scenario | Before (in secs) | Opt for MMC (in secs) | Opt for NAND (in secs) |
|---|---|---|---|
| Time to console prompt | TBD | TBD | TBD |
| Time to graphical app | TBD | TBD | TBD |
TODO : Fill the table with actual values
IMPORTANT
Being a wiki these tables are open for editing. Request users to change add notes/comments and additional links bottom of the page. All values here will be backed up by actual patches. Please do not link individual website from the core article.
Before and After Demo
TODO : Will be added soon...
What next?
As discussed earlier in the article, optimizations must be viewed in the context of the end use of product. In the continuum, it would be unfair to suggest/ believe that no further optimizations are possible.
This section describes additional steps that are planned in near future. It also lists alternatives that can be tried out.
Short term
- Specific patches shall be added soon to:
- Implement the use-case 2 described above
- Boost the MPU frequency early in the boot process
Long term
- Support for other platforms
More things to try
- Developers would also notice that U-Boot sources in this PSP release are based-off 2010.06 release. Cache support was added to ARM architectures in 2010.09. Migration to this U-Boot version can speed up the U-Boot execution and kernel decompression.
- Barebox is another bootloader that can be used instead of U-Boot.
- UBIFS is a new filesystem that may be considered instead of JFFS2. Since it doesn't need to scan the media while mounting, filesystem can be mounted in few milliseconds.
- Use LZO compression instead of default GZIP for the Linux kernel. It is expected to speed-up kernel decompression.
- If NOR flash is used then kernel compression isn't required.
IMPORTANT
Developers should identify the right set of patches to (rework and) apply in their products. Then, use the learnings from the discussion above to further optimize the boot time.
Frequently Asked Questions
- Time to load binary from the storage medium
- Actual execution time
This can be a useful mechanism for branding as well. To use / avoid a splash screen is a compromise between these factors.