Optimized Sort Algorithms For DSP

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Implementing an optimized sort algorithm on a DSP requires giving some thought to the algorithm used, just like on any CPU architecture, but it also requires paying careful attention to how it is possible to leverage some advantages of the Texas Instruments c64x+ DSP architecture such as:

The result of this study is a set of data points that will hopefully guide you in making an informed decision when picking and/or implementing your algorithm, and give you an order of magnitude of the performance you can expect to see in your real-time application, as well as code-size and memory requirements.

Contents

Sort Algorithms

In the scope of this algorithm and implementation review we have considered the Quicksort and Merge Sort algorithms, and we are only considering the problem of sorting unsigned 32-bits integers.

Much of these results do apply if we were to sort signed integers, but would likely vary if we were sorting 16-bits or 8-bits values as the optimization techniques used would likely vary.

Quick Sort Algorithm

The Quicksort algorithm has the following performance caracteristics:

For a good discussion on this algorithm please refer to description of the Quick Sort algorithm on Wikipedia, or to the book The Art of Computer Programming by Donald Knuth which is an excellent reference on the subject.

Merge Sort Algorithm

The Merge Sort algorithm has the following performance caracteristics:

A typical implementation of the Merge Sort algorithm involves:

When implementing this algorithm you need to choose at what level the division into subsets will stop.

For a good discussion on this algorithm please refer to description of the Merge Sort algorithm on Wikipedia, or to the book The Art of Computer Programming by Donald Knuth which is an excellent reference on the subject.

Variations on a Theme

When considering the uses a DSP application might do of a sort function it quickly becomes obvious that sorting alone will often not be the complete solution to the problem the application is trying to solve.

Index Ordering

For quite a few applications it will be interesting for the application to not only get as a result a sorted list, but also get an array that will give the original position of each item in the sorted list.

This is what is called here "Index Ordering", and as part of this study implementations with and without "Index Ordering" have been created.

Finding the Top K entries from an array

In some cases the real problem to be solved requires only finding the top K entries from an array of N values, rather than sorting the whole array.

If that is the case of your application then this opens the door for some additional optimizations, as quite some CPU cycles can be saved by only partially sorting the content of the array.

A good starting point to learn more about this type of algorithms is the Wikipedia page on Selection Algorithm.

We have decided in this article to implement an optimized version of the Quickselect algorithm described on Wikipedia. It is basically a modified version of the Quicksort algorithm.

Keeping a list always sorted

Will be documented later.

Rather than sorting an array of values at periodic intervals or even just when needed it might be interesting to keep the list of sorted at all times.

This means that the list has to be re-ordered every time a value is updated.

Benchmark Results

Here are benchmark results of the run of three implementations of sort. These benchmarks were run in the following configuration:

CPU Cyles

The results are CPU cycles for the execution of the sort algorithm, with index ordering enabled.

Please note that in our benchmarking the index ordering does not noticeably degrades the performance of algorithm. This can be explained by the fact that Texas Instruments DSPs have the ability to execute up to 8 instructions in parallel, and that the cost of index ordering is absorbed or hidden that way.

Merge sort vs qsort 1 to 256.png

From this graph we can draw the following conclusions on our implementations:

Code Size

To be documented later

Memory Requirements

Here is a summary of the extra memory these various algorithms require to work. We call here N the number of 32 bit unsigned words to be sorted:

Implementations

We are providing here the software implementations of the algorithms we have evaluated in this study. Feel free to use these functions as a starting point for your own implementation.

Quicksort from <stdlib.h>

The qsort() function provided with the Texas Instruments runtime support library (interface defined in <stdlib.h>) gives you the ability to sort an array of elements of any type and size. However the genericity of this quicksort implementation has an impact on its performance which is clearly demonstrated by the results of our benchmarks.

If the performance of your sort function is likely to be on the critical path of your real-time application using the qsort() function is probably a good first step to get a functional application, but implementing your own sort function might be required at some point.

In the benchmark results our custom implementation Quick Sort algorithm is consistently outperforming the <stdlib.h> qsort() implementation. The reasons for that are simple:

Standard Quicksort Implementation

#include <stdlib.h>
int qsort_cmp(const void *e1, const void *e2) {
  unsigned int v1 = *(unsigned int *)e1;
  unsigned int v2 = *(unsigned int *)e2;
 
  if (v1 < v2) return -1;
  else if (v1 > v2) return 1;
  else return 0;
}
void Sort_stdlib32(unsigned int * restrict array, int size) {
 
  /* This is a simple implementation of the QuickSort algorithm.  */
  qsort((void *)array, size, 4, &qsort_cmp);
}

Quicksort

Quicksort Implementation

The following Quicksort implementation is very heavily based on the pseudo code found the Wikipedia entry for the Quicksort Algorithm.

inline int partition(unsigned int * restrict array, int left, int right, int pivotIndex) {
  int pivotValue = array[pivotIndex];
  int storeIndex, i;
  unsigned int temp;
 
  temp = array[pivotIndex];
  array[pivotIndex] = array[right]; // Move pivot to end
  array[right] = temp;
  storeIndex = left;
  for (i=left; i<right; i++) { // left <= i < right 
    if (array[i] <= pivotValue) {
      temp = array[i];
      array[i] = array[storeIndex];
      array[storeIndex++] = temp;
    }
  }
  temp = array[right];
  array[right] = array[storeIndex]; // Move pivot to its final place
  array[storeIndex] = temp;
  return storeIndex;
}
 
static void quicksort(unsigned int * restrict array, int left, int right) {
  int pivotIndex, pivotNewIndex;
 
  if (right > left) {
    /* select a pivot index (e.g. pivotIndex := (left+right)/2) */
    pivotIndex = (left+right)/2;
    pivotNewIndex = partition(array, left, right, pivotIndex);
    quicksort(array, left, pivotNewIndex - 1);
    quicksort(array, pivotNewIndex + 1, right);
  }
}
 
void Sort_qsort32(unsigned int * restrict array, int size) {
 
  /* This is simple implementation of the QuickSort algorithm.  */
  quicksort(array, 0, size-1);
}

Quicksort Implementation with Index Ordering

The index ordering requires that the index be updated as the array is sorted. Because the Texas Instruments DSPs are able to execute multiple instructions in parallel the overhead introduced by the maintenance of the index is very limited.

static int ipartition(unsigned int * restrict array, unsigned int * restrict order, int left, int right, int pivotIndex) {
  int pivotValue = array[pivotIndex];
  int storeIndex, i;
  unsigned int temp;
  unsigned int itemp;

  temp = array[pivotIndex]; itemp = order[pivotIndex];
  array[pivotIndex] = array[right]; // Move pivot to end
  order[pivotIndex] = order[right];
  array[right] = temp;
  order[right] = itemp;
  storeIndex = left;
  for (i=left; i<right; i++) { // left <= i < right 
    if (array[i] <= pivotValue) {
      temp = array[i];
      itemp = order[i];
      array[i] = array[storeIndex];
      order[i] = order[storeIndex];
      order[storeIndex] = itemp;
      array[storeIndex++] = temp;
    }
  }
  temp = array[right];
  itemp = order[right];
  array[right] = array[storeIndex]; // Move pivot to its final place
  order[right] = order[storeIndex];
  array[storeIndex] = temp;
  order[storeIndex] = itemp;
  return storeIndex;
}

static void quicksort(unsigned int * restrict array, unsigned int * restrict order, int left, int right) {
  int pivotIndex, pivotNewIndex;

  if (right > left) {
    /* select a pivot index (e.g. pivotIndex := (left+right)/2) */
    pivotIndex = (left+right)/2;
    pivotNewIndex = partition(array, order, left, right, pivotIndex);
    quicksort(array, order, left, pivotNewIndex - 1);
    quicksort(array, order, pivotNewIndex + 1, right);
  }
}

void SortIndex_qsort32(unsigned int * restrict array, int size, unsigned int * restrict index) {

	quicksort(array, index, 0, size-1);
}

Optimized Quicksort

It is possible to make a quite simple optimization of our base Quicksort implementation by using some scratch memory and a slight rewrite of the inner-loop of the Quicksort algorithm (found in the partition() function).

This change allows the compiler to generate code that is much more efficient and leverage the Texas Instruments C64x+ DSP features for the optimization of loops.

Optimized Quicksort Implementation

static int partition(unsigned int * restrict ping, unsigned int * restrict pong, int left, int right, int pivotIndex) {
  int pivotValue = ping[pivotIndex];
  int storeIndex, i, rightIndex;
  unsigned int temp;

  temp = ping[pivotIndex];
  ping[pivotIndex] = ping[right]; // Move pivot to end
  ping[right] = temp;
  storeIndex = left;
  rightIndex = right;
  /* This loop is optimized by the Texas Instruments compiler.  */
  for(i=left;i<right;i++) {
    if (ping[i] <= pivotValue) {
      pong[storeIndex++] = ping[i];
    } else {
      pong[rightIndex--] = ping[i];
    }
  }
  pong[storeIndex] = ping[right];
  /* Copy pivotValue back into the ping buffer.  */
  ping[storeIndex] = pong[storeIndex];
  return storeIndex;
}

static void quicksort(unsigned int * restrict ping, unsigned int * restrict pong, int left, int right, int depth, int idx) {
  int pivotIndex, pivotNewIndex;

  if (right <= left && (depth & 1)) {
    /* Copy array value back into the pong buffer.  */
    pong[idx] = ping[idx];
  }
  if (right > left) {
    /* select a pivot index (e.g. pivotIndex := (left+right)/2) */
    pivotIndex = (left+right)/2;
    pivotNewIndex = partition(ping, pong, left, right, pivotIndex);
    quicksort(pong, ping, left, pivotNewIndex - 1, depth+1, left);
    quicksort(pong, ping, pivotNewIndex + 1, right, depth+1, right);
  }
}

void Sort_qsort32(unsigned int * restrict array, int size, unsigned int * restrict scratch) {
	
  /* This implementation is using scratch memory to enable an optimization
     of the inner loop of the quicksort algorithm.  */
  quicksort(array, scratch, 0, size-1, 0, 0);
}

Optimized Quicksort Implementation with Index Ordering

One interesting thing to note is that the implementation with Index Ordering is only introducing a very small degradation in performance (we have observed it to be consistently under XXX %).

static int partition(unsigned int * restrict ping, unsigned int * restrict pong,
                     unsigned int * restrict iping, unsigned int * restrict ipong,
                     int left, int right, int pivotIndex) {
  int pivotValue = ping[pivotIndex];
  int storeIndex, i, rightIndex;
  unsigned int temp, itemp;

  temp = ping[pivotIndex]; itemp = iping[pivotIndex];
  ping[pivotIndex] = ping[right]; // Move pivot to end
  iping[pivotIndex] = iping[right]; // Move pivot to end
  ping[right] = temp; iping[right] = itemp;
  storeIndex = left;
  rightIndex = right;
  /* This loop is optimized by the Texas Instruments compiler.  */
  for(i=left;i<right;i++) {
    if (ping[i] <= pivotValue) {
      pong[storeIndex] = ping[i];
      ipong[storeIndex++] = iping[i];
    } else {
      pong[rightIndex] = ping[i];
      ipong[rightIndex--] = iping[i];
    }
  }
  pong[storeIndex] = ping[right];
  ipong[storeIndex] = iping[right];
  /* Copy pivotValue back into the ping buffer.  */
  ping[storeIndex] = pong[storeIndex];
  iping[storeIndex] = ipong[storeIndex];
  return storeIndex;
}

static void quicksort(unsigned int * restrict ping, unsigned int * restrict pong,
                      unsigned int * restrict iping, unsigned int * restrict ipong,
                      int left, int right, int depth, int idx) {
  int pivotIndex, pivotNewIndex;

  if (right <= left && (depth & 1)) {
    /* Copy array value back into the pong buffer.  */
    pong[idx] = ping[idx];
    ipong[idx] = iping[idx];
  }
  if (right > left) {
    /* select a pivot index (e.g. pivotIndex := (left+right)/2) */
    pivotIndex = (left+right)/2;
    pivotNewIndex = partition(ping, pong, iping, ipong, left, right, pivotIndex);
    quicksort(pong, ping, ipong, iping, left, pivotNewIndex - 1, depth+1, left);
    quicksort(pong, ping, ipong, iping, pivotNewIndex + 1, right, depth+1, right);
  }
}

void SortIndex_qsort32(unsigned int * restrict array, int size, unsigned int * restrict index, unsigned int * restrict scratch) {
	
  /* This is simple implementation of the QuickSort algorithm.  */
  quicksort(array, scratch, index, scratch+size, 0, size-1, 0, 0);
}

Merge Sort

The Merge Sort implementation presented here works as follows:

As you can see we have decided to opt for an implementation that is using an iterative approach rather than a recursive approach. This iterative approach in our experiments has proven to be much more optimization-friendly.

Merge Sort Implementation

The full implementation of our Optimized Merge Sort For DSP is documented separately.

Merge Sort Function

void Sort_merge32(unsigned int * restrict array, int size, unsigned int * restrict output, unsigned int * restrict scratch);

Two-Ways Merge

void Merge_twoWays32 (unsigned int **inputs, int *sizes,
		      unsigned int * restrict out, unsigned int * restrict scratch);

Three-Ways Merge

void Merge_threeWays32(unsigned int **inputs, int *sizes, unsigned int * restrict out, unsigned int * restrict scratch);

Four-Ways Merge

void Merge_fourWays32(unsigned int **inputs, int *sizes, unsigned int * restrict out, unsigned int * restrict scratch);

Merge Sort Implementation with Index Ordering

The full implementation of our Optimized Merge Sort For DSP With Index Ordering is documented separately.

Merge Sort Function with Index Ordering

void SortIndex_merge32(unsigned int * restrict array, int size, unsigned int * restrict index,
                       unsigned int * restrict output, unsigned int * restrict order, unsigned int * restrict scratch);

Two-Ways Merge With Index Ordering

void MergeIndex_twoWays32 (unsigned int **inputs, int *sizes,
		      unsigned int * restrict out, unsigned int * restrict scratch);

Three-Ways Merge With Index Ordering

void MergeIndex_threeWays32(unsigned int **inputs, int *sizes, unsigned int * restrict out, unsigned int * restrict scratch);

Four-Ways Merge With Index Ordering

void MergeIndex_fourWays32(unsigned int **inputs, int *sizes, unsigned int * restrict out, unsigned int * restrict scratch);

Top K Elements from an Array of N Elements

Based on the Quickselect algorithm described in the Selection Algorithm page from Wikipedia we have made an implementation optimized for Texas Instruments c64x+ DSPs. This implementation does perform #Index_Ordering as described in the

A number of optimizations have been built in the implementation of this algorithm among which:

Software Implementation

The software implementation of this algorithm can be found here: Top K Elements Sort For DSP With Index Ordering.


Benchmark Results

Here is a visualization of the results of a benchmark of the function in a case where we sort the top 20 elements of an array of up 600 elements.

Our Quickselect algorithm is compared to repeating 20 times the search for the maximum in the array. The maximum search function is an optimized one and is also provided with our example code.

Quick select vs max.png

References

Leave a Comment

Comments

Comments on Optimized Sort Algorithms For DSP


Contents

A0393857 said ...

I work for the Automotive Vision team and one of my customers is looking for a sorting algorithm optimized for C64x+ DSP. Could you please share the source code used in the above experimentats? Thanks.

--A0393857 06:08, 5 April 2011 (CDT)

A0393857 said ...

I work for the Automotive Vision team and one of my customers is looking for a sorting algorithm optimized for C64x+ DSP. Could you please share the source code used in the above experiments? Thanks.

--A0393857 06:08, 5 April 2011 (CDT)

Gerardo rosiles said ...

Can you provide a better figure for the second graphic? one that displays the x-axis scale?

--Gerardo rosiles 20:56, 11 April 2011 (CDT)

Laurent gauthier said ...

The source code is all available on the wiki page.

About the graph question I am currently working on revising the article content and will improve that. The scale on that graph goes from 1 to 600.

--Laurent gauthier 09:57, 19 May 2011 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox