PASM Tool
From Texas Instruments Embedded Processors Wiki
^ Up to main Programmable Realtime Unit Software Development Table of Contents
This arcticle is part of a collection of articles describing software development on the PRU subsystem included in OMAP-L1x8/C674m/AM18xx devices (where m is an even number). To navigate to the main PRU software development page click on the link above.
Contents |
Assembler Use and Overview
PASM is a command line driven assembler for the Programmable Real-time execution unit (PRU) of the Programmable Real-time Unit Subsystem (PRUSS). It is designed to build single executable images using a flexible source code syntax and a variety of output options. PASM is available for Windows and Linux.
Calling Syntax
The command line syntax to PASM is:
pasm [-bBcmldexz] SourceFile [OutFileBasename] [-Dname=value] [-CArrayName]
Note that only the source file SourceFile is required on the command line. The assembler will default to output option "-c" which generates a C array containing the binary opcode data. The majority of the option flags select a variety of output formats.
The output file OutFileBasename is a base name only. It defaults to the same name as the source file (for example "myprog.p" would have a default base name of "myprog". Standard filename extensions are applied to the base name to create the final output filename(s), depending on the output option(s) selected.
When specifying PASM options, options can be specified individually or as a group. For example, either of the two invocations below is valid:
pasm –cdl myprog.p
pasm –c –d -l myprog.p
Also filenames and options can be mixed for example:
pasm myprog.p -cdl
pasm –cd myprog.p –DMYVAL=1 -l
Output Formats
All program images start at Programmable Realtime Unit (PRU) address 0. For example, if a program has an internal origin of 8, the first eight 32 bit words of the program image output will be zero.
The following output options are supported. The output file name shown in the table is generated assuming a base name of "myprog":
| Command Line Option | Output Format | Output Filename | |
|---|---|---|---|
| -b | Little endian binary file | myprog.bin | |
| -c | C include file containing unsigned long array called PDSPcode[]* | myprog_bin.h | |
| -m | Image file containing one 32 bit hex opcode per line | myprog.img | |
| -l | Listing file containing the source code and generated opcodes | myprog.lst | |
| -d | pView debugger output file (opcodes with source and label info) | myprog.dbg | |
| *The name "PDSPcode[]" can be redefined using the –C option. | |||
Additional Options
PASM supports some additional command line options that are not associated with output file format:
| Command Line Option | Function |
|---|---|
| -C | Rename the code array declared when using the –c option |
| -D | Constant definition |
| -x | Force legacy behavior |
| -z | Enable debug output |
Rename the Code Array for the –c Option
By default, the –c option will create an output file with a name ending in "_bin.h". Inside this created include file, the output code is defined as a C array of 32 bit values. The default name of the array is "PDSPcode[]". The –C option allows the user to redefine this name to something more appropriate. For example the following command line will create an output file named "myprog_bin.h", and the C array inside the created file will be called "MyProg_Release_003a[]".
pasm –c myprog.p –CMyProg_Release_003a
Constant Definitions
When the "-D" option is specified, the remaining command line argument is interpreted as a constant assignment. For example, to add an assignment "1" to the constant "MYVAL", any of the following is valid:
pasm –cdl myprog.p –DMYVAL=1 pasm –c –d -l –DMYVAL=1 myprog.p pasm myprog.p –cdlDMYVAL=1
Since the default value assigned to a constant is "1", the following is also equivalent:
pasm –c –d -l –DMYVAL myprog.p
Note that constants defined on the command line do not override constants defined in the source code.