Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

PRU-ICSS Ethernet

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:


Introduction

As of version 3.1.0.6 of the Linux Processor SDK, the evaluation modules listed below support additional 100 Mbps Ethernet ports through the PRU-ICSS while running Linux as your host operating system.

This page DOES NOT cover any of the industrial protocols that are supported by the PRU-ICSS while running other host operating systems (bare metal, StarterWare, TI RTOS, third party, etc).

For previous versions of the Linux Processor SDK, please see the Archives section at the bottom of this page.

Boards Supported

Am335x ice.jpg

AM3359 Industrial Communications Engine (ICE)

The AM3359 Industrial Communications Engine (ICE) is a development platform targeted for systems that specifically focus on the industrial communications capabilities of the Sitara AM335x ARM® Cortex™-A8 Processors

The AM335x ARM Cortex-A8 Processors integrate the Programmable Real-time Unit (PRU) that has been architected to implement the real-time communication technologies used in a broad range of industrial automation equipment. It enables low foot print designs with minimal external components and with best in class low power performance.


Am437x idk 500x300.jpg

AM437x Industrial Development Kit (IDK)

The AM437x Industrial Development Kit (IDK) is an application development platform for evaluating the industrial communication and control capabilities of Sitara™ AM4379 and AM4377 processors for industrial applications.

The AM4379 and AM4377 processors are ideal for industrial communications, industrial control, and industrial drives applications. The AM437x processors integrate a quad-core Programmable Real-time Unit (PRU) that has been architected to implement the real-time communication technologies used in a broad range of industrial automation equipment. It enables low foot print designs with minimal external components and with best in class low power performance.


Am571x idk.JPG

AM571x Industrial Development Kit (IDK)

The AM571x IDK is a standalone test, development, and evaluation module that enables developers to write software and develop hardware for industrial control and industrial communications applications. It has been equipped with a TI AM5718 processor and a defined set of features to allow you to experience industrial communication solutions using various serial or Ethernet based interfaces. Using standard interfaces, the AM571x IDK may interface to other processors or systems and act as a communication gateway or controller. In addition, it can directly operate as a standard remote I/O system or a sensor connected to an industrial communication network.

NOTE

Due to pin muxing between the optional LCD and the PRUSS1 Ethernet ports, the AM571x IDK supports two configurations. The first configuration is 4-port Ethernet + LCD. In this configuration, two Ethernet ports are provided by the CPSW, two Ethernet ports are provided by PRUSS2, and the LCD is enabled. To use this configuration, place a jumper across J51 on the board. The second configuration is 6-port Ethernet. In this configuration, two Ethernet ports are provided by the CPSW, two Ethernet ports are provided by PRUSS1, two Ethernet ports are provided by PRUSS2, and the LCD is disabled. To use this configuration, leave J51 open.


Am572x idk.PNG

AM572x Industrial Development Kit (IDK)

The AM572x Industrial Development Kit (IDK) is a development platform for evaluating the industrial communication and control capabilities of Sitara AM572x processors for applications in factory automation, drives, robotics, grid infrastructure, and more. AM572x processors include dual PRU-ICSS (Programmable Real-time Unit for Industrial Communications) sub-systems which can be used for industrial Ethernet protocols such as Profinet, EtherCAT, Ethernet/IP, and others. The TMDXIDK5728 breaks out six ports of Ethernet, four of which can be used concurrently: 2x Gb Ethernet ports and 2x 10/100 Ethernet ports from the PRU-ICSS subsystems.

NOTE

Due to changes in the PRU-ICSS between silicon revisions, the PRU Ethernet firmwares provided for the AM5728 device are only meant to be used on silicon revision SR 2.0.


K2g ice.PNG

K2G Industrial Communication Engine (ICE)

The K2G Industrial Communications Engine (ICE) enables 66AK2Gx processor developers to immediately start development, demonstration and test of industrial communication protocols for products such as PLC, bus controllers, motion control and other real-time industrial networked applications. The evaluation module is supported by Processor SDK for RT Linux and TI-RTOS operating systems and is supplied with an SD micro card for easy boot up and out of box experience. The two PRU-ICSS subystems can be used for industrial Ethernet protocols such as Profinet, EtherCAT, Ethernet/IP, and others.



What You Get

With the PRU-ICSS Ethernet support, you get two (or four, on the AM571x IDK and K2G ICE) additional 100 Mbps Ethernet interfaces that show up just like any other Ethernet interface in Linux. These interfaces are there 'out-of-the-box' in the latest Linux Processor SDK when ran on any of the boards shown above. All you need to do is plug in an Ethernet cable and bring the interface up from the console (discussed below).

The current implementation does not support Ethernet switching within the PRU-ICSS. The provided PRU firmwares only support 'dual emac' mode in this release of the Linux Processor SDK.



How It Works

Texas Instruments provides all of the necessary software and firmware in the Linux Processor SDK to enable the PRU-ICSS Ethernet ports. The PRU firmware binaries can be found in the /lib/firmware/ti-pruss/ folder in the filesystem. A Linux kernel networking driver is provided that can be found at <%LINUX_PROC_SDK_X_X_X_X%>/board-support/linux-x.y.z..../drivers/net/ethernet/ti/prueth.c. The required device tree modifications are also given in the dts files of the supported boards from above.

As the boards boot, the prussN_eth device tree node causes the ti-prueth driver to be probed. This probe function does several things to prepare the PRU-ICSS Ethernet ports:

  • Configures the mux mode of the PRU pins for MII mode
  • Requests ownership of the PRUSS memory regions from the pruss driver
  • Allocates a pool of memory in OCMC SRAM for the Ethernet buffers to be passed from the PRU to Linux
  • Initializes a netdev devices
  • Registers the network device with Linux

At this point the Linux driver is ready for the new Ethernet interface to be started. Once the user issues the interface up command ('ifup eth2' for example), the emac_ndo_open function is called in the ti-prueth driver which uses the remoteproc interface to boot the PRU cores with the firmware provided in the /lib/firmware/ti-pruss/ folder of the EVM filesystem. The PRUs running this firmware, coupled with the ti-prueth Linux driver, allows up to 2 (or 4, on the AM571x IDK) additional 100 Mbps Ethernet interfaces to be exposed to the user.


Block Diagram

This is a high level block diagram to show how everything fits together. For more information see the schematics for the boards as well as the Linux driver source code.
Pru eth block diagram 3 0 0 4.PNG


Try It Out

Here are the steps needed to test out the new Ethernet interfaces:

  • Get your hands on one of the industrial boards
  • Download the Linux Processor SDK (v3.1.0.6 or higher)
  • Run the 'create SD card' script provided in the SDK to create a bootable SD card
    • Plug your SD card into your Ubuntu development machine with a USB card reader
    • cd <%LINUX_PROC_SDK_X_X_X_X%>/bin/
    • sudo ./create-sdcard.sh
    • follow the script directions to format your SD card and then install the pre-built binaries from the SDK
    • for more information on creating an SD card: Processor_SDK_Linux_create_SD_card_script
  • Boot from the newly created SD card
    • Put the SD card into your board, power it on, and wait for the login prompt then type root to log in.
      NOTE

      You'll need to clear the SPI flash on the AM3359 ICE board before you can boot from an SD card: AM3359 ICE clear SPI flash
  • Plug an Ethernet cable into the ports supported by the PRU-ICSS
    • On the AM3359 ICE there are only two Ethernet ports on the board
      • In order to use the PRU-ICSS with these ports (instead of the CPSW) you need to correctly configure both of the jumpers that are located right next to the RJ45 jacks
        • Jumpers J18 and J19 both need to be set to MII to use PRU-ICSS on the ports, you need to reboot the device for jumper changes to take effect
        • If you set both of these jumpers to RMII then the CPSW will drive the ports, not the PRU-ICSS
        • It is not supported to set the two jumpers to different values. Both need to be MII (PRU-ICSS) or both need to be RMII (CPSW).
    • On the AM437x IDK the silkscreen says PRUETH0 and PRUETH1 for the supported PRU ports
    • On the AM571x IDK the silkscreen says PRU1 ETH0, PRU1 ETH1, PRU2 ETH0, and PRU2 ETH1 for the supported PRU ports
      NOTE

      On the AM571x IDK board, the pins used for PRU1 ETH0 and PRU1 ETH1 are shared with pins used for the optional LCD touchscreen. U-Boot uses jumper J51 to determine if the LCD touchscreen should be enabled or not. If J51 is closed (jumper is present across the two pins), then U-Boot will load a device tree that enables the LCD touchscreen and disables PRUSS1 Ethernet ports. This means that only PRU2 ETH0 and PRU2 ETH1 will be supported if jumper J51 is closed. If J51 is open (jumper is not present across the two pins), then U-Boot will load a device tree that enables all four PRUSS Ethernet ports, two from PRUSS1 and two from PRUSS2. In this mode, the LCD touchscreen is disabled.
    • On the AM572x IDK the silkscreen says PRU2 ETH0 and PRU2 ETH1 for the supported PRU ports
    • On the K2G ICE the supported PRU ports are the two stacked RJ45 connectors
  • Bring up the PRU Ethernet interface in Linux
    • Depending on your board and the contents of your /etc/networking/interfaces file, the PRU-ICSS Ethernet ports may already be brought up. If not:
    • On the AM3359 ICE type ifup eth0 to bring up Ethernet_0 and type ifup eth1 to bring up Ethernet_1
    • On the AM437x IDK type ifup eth1 to bring up PRUETH0 and type ifup eth2 to bring up PRUETH1
    • On the AM571x IDK type ifup eth2 to bring up PRU1 ETH0, type ifup eth3 to bring up PRU1 ETH1, type ifup eth4 to bring up PRU2 ETH0, and type ifup eth5 to bring up PRU2 ETH1
      NOTE

      As mentioned in the note above, jumper J51 on the board determines if two or four PRUSS Ethernet ports are supported. If J51 is closed then only two of the four interfaces listed here will be available for use.
    • On the AM572x IDK type ifup eth2 to bring up PRU2 ETH0 and type ifup eth3 to bring up PRU2 ETH1
    • On the K2G ICE type ifup eth1, ifup eth2, ifup eth3, and ifup eth4 to bring up the PRU Ethernet interfaces
  • If all goes well you should see the PRU-ICSS ports in the output of the ifconfig command



Network Topologies

The following network topologies are possible with the PRU-ICSS Ethernet ports.

Single Port Mode

In this mode only one of the PRU-ICSS Ethernet ports are used. This is the simplest mode and works as you would expect it to.
Pru eth block single port 3 0 0 4.PNG


Dual MAC Mode (Gateway)

One use case made possible with two ports on the same device is to allow your device to act as a gateway between two different subnets. In this use case you just need to bring up both ports and then plug them into the two subnets as shown below.

NOTE

It is not a normal use case to plug both PRU-ICSS Ethernet ports into the same switch (same subnet) out-of-the-box. While it may appear to work at first, it will lead to unexpected behavior including (but not limited to) packets entering/exiting the device on the opposite port that you would expect due to ARP broadcasts and other topics that are outside the scope of this wiki page. If you would like to use both ports on the same subnet, keep scrolling to the Bonding section below.


Pru eth block gateway 3 0 0 4.PNG



Dual MAC Mode (Bonding)

Bonding, also called link aggregation or port trunking, is a networking feature that uses multiple Ethernet ports to provide link redundancy or an increase in throughput.

The next section shows how to use the two PRU-ICSS Ethernet ports to provide link redundancy by using the 'active-backup' bonding mode. If one of the cables is unplugged the Ethernet traffic will fail over to the other port and continue. To learn more about the other types bonding available check out the Linux bonding documentation.
Pru eth block bonding 3 0 0 4.PNG

To learn even more about bonding see the Wikipedia Link aggregation page.



Steps to enable 'active-backup' bonding mode

While testing the below steps, I plugged both PRU-ICSS Ethernet ports into the same switch that has access to a DHCP server. During boot and bonding setup I left the cables connected. I only started unplugging cables when I was testing the bond0 interface for redundancy in the last step.

On your Linux development machine

  1. Enable Bonding driver support using menuconfig, rebuild Linux, and boot your board
    • The menuconfig option can be found under Device Drivers -> Network device support -> Bonding driver support'
    • You can either configure the driver as built-in to the kernel (*) or as a module (M). Keep in mind that if you build the driver into the kernel that you will not be able to pass any parameters to it as it is loaded. For the example shown here, we will be using the sysfs interface to configure the bonding so it doesn't matter which method you choose (we used the module (M) method though).
    • Once Bonding driver support is enabled, rebuild your Linux kernel and modules
    • Now boot your board with the new kernel and bonding driver built above

On your development board console

  1. Insert the bonding module (unless you built it into the kernel above, then it's already there)
    • modprobe bonding
  2. Get the IP address and netmask of one of your PRU-ICSS Ethernet ports (we will need it in a second)
    • If the ports are already up
      • ifconfig
    • If the ports are not up yet
      • ifup eth2 where 2 is the interface number for one of your PRU-ICSS Ethernet ports (this is board dependent)
      • ifconfig
        NoteNote: AM3359ICE: eth0 and eth1 are the PRU-ICSS Ethernet ports
        AM437x IDK: eth1 and eth2 are the PRU-ICSS Ethernet ports
        AM572x IDK: eth2 and eth3 are the PRU-ICSS Ethernet ports
  3. Take down your PRU-ICSS Ethernet ports (this is necesary for bonding)
    • ifconfig eth2 down
    • ifconfig eth3 down
  4. Configure bonding to use mode 1: active-backup mode
    • echo 1 > /sys/class/net/bond0/bonding/mode
  5. Configure the MII link monitoring frequency in milliseconds
    • echo 100 > /sys/class/net/bond0/bonding/miimon
  6. Bring up the bond0 interface using the IP address and netmask that you noted down from above
    • ifconfig bond0 192.168.0.100 netmask 255.255.254.0 up
  7. Bind your two PRU-ICSS Ethernet ports to the bond0 interface
    • echo +eth2 > /sys/class/net/bond0/bonding/slaves
    • echo +eth3 > /sys/class/net/bond0/bonding/slaves
  8. Test out the link redundancy of the bond0 interface
    • Start a ping test between your board and your development machine
    • Watch the board's console and unplug one of the Ethernet cables
    • Now plug that cable back in and unplug the other Ethernet cable
    • You should observe the ping program continuously receiving responses despite the cables being plugged and unplugged
    • The console output will show when an interface goes does down as well as if the active interface changes

Frequently Asked Questions

Are the HSR or PRP protocols supported?

Yes! The HSR and PRP protocols are currently supported on the AM572x IDK board. To learn more about the HSR and PRP PRU firmware implementation click here. To learn more about running the protocols/firmwares while using the Linux Processor SDK click here.

HSR stands for High Availability Seamless Redundancy. This is a protocol used to support redundant networks needed for industrial applications such as factory automation, substation automation etc. The standard is defined in IEC 62439-3 clause 5.

PRP stands for Parallel Redundancy Protocol which is another redundancy protocol defined by IEC 62439-3 clause 4.

I am using the AM571x IDK, why do I only see 4 Ethernet interfaces instead of 6?

Due to pin sharing between the optional LCD and the PRUSS1 Ethernet pins, the AM571x IDK supports two different configurations: 4-port Ethernet + LCD or 6-port Ethernet with no LCD. Jumper J51 controls which configuration is selected. If J51 is closed then the 4-port + LCD configuration is selected and if J51 is open then the 6-port Ethernet configuration is selected and the LCD is disabled.

What if I want the PRU-ICSS to run a custom firmware (not Ethernet) on one of these industrial boards?

The pru_rproc driver uses the of_machine_is_compatible() function to check if the device that it is running on is compatible with one of the boards above. If it is compatible, then the pru_rproc driver loads the Texas Instruments provided PRU-ICSS Ethernet firmwares. If you would like to run your own PRU firmwares on one of the IDKs or the ICE board then you will need to modify the device tree file to remove the IDK or ICE compatibility declaration:

  • AM3359 ICE board
    • Remove the "ti,am3359-icev2" compatible declaration at the top of the arch/arm/boot/dts/am335x-icev2.dts file
  • AM437x IDK board
    • Remove the "ti,am437x-idk-evm" compatible declaration at the top of the arch/arm/boot/dts/am437x-idk-evm.dts file
  • AM572x IDK board
    • Remove the "ti,am5718-idk" compatible declaration at the top of the arch/arm/boot/dts/am571x-idk.dts file
  • AM572x IDK board
    • Remove the "ti,am5728-idk" compatible declaration at the top of the arch/arm/boot/dts/am572x-idk.dts file

Once these compatibility declarations are removed you will need to rebuild your .dtb file and place it wherever it needs to be when you reboot your board (filesystem, nfs directory, tftp directory, etc.)

Keep in mind that the PRU pin muxing on these boards is configured to bring the MII pins out of the device. Changing the pin muxing to accommodate your custom PRU firmware will be left as an exercise for the user.

What is the expected PRU-ICSS Ethernet throughput? How can I test the throughput on my setup?

The maximum bandwidth of the PRU-ICSS Ethernet ports is 100 Mbps. The observed throughput that I have achieved consistently is around 94 Mbps using TCP or UDP and testing with iperf. Here are the commands needed to test for yourself (this assumes you've followed the steps on this page to get your PRU-ICSS interface up and running already):

  • Make sure that your board and your Linux development machine can 'see' each other on the network (I connect both to the same switch and allow them to use DHCP to acquire IP addresses on the same network)
  • Use ifconfig on both your Linux development machine and your board and note down each IP address
    • For the purposes of this example I will use 192.168.0.105 as the Linux host IP and 192.168.1.110 as the board's IP
  • Testing TCP transmit throughput
    • Start an iperf server on your Linux development machine (sudo apt-get install iperf if you don't already have iperf installed)
      • iperf -s
    • Run the iperf client from your board to connect to the iperf server you just started
      • iperf -c 192.168.0.105
    • You should see your board connect to the server and a few seconds later both the server and the client will output the Bandwidth achieved
      • For me this is output is around 94 Mbits/sec
    • Quit the iperf server that is running on your Linux development machine
      • Ctrl + c
  • Testing TCP receive throughput
    • Use the same procedure as provided for testing TCP transmit throughput except swap the commands on the two devices (iperf -s from the board and iperf -c 192.168.1.110 from the Linux development machine)
  • Testing UDP transmit throughput
    • Start a UDP iperf server on your Linux development machine
      • iperf -s -u
    • Run a UDP iperf client from your board and specify the bandwidth you'd like to achieve
      • iperf -c 192.168.0.105 -u -b 100M
    • Once again my results are around 94 Mbit/sec
    • Quit the iperf server that is running on your Linux development machine
      • Ctrl + c
  • Testing UDP receive throughput
    • Use the same procedure as provided for testing UDP transmit throughput except swap the commands on the two devices (iperf -s -u from the board and iperf -c 192.168.0.110 -u -b 100M from the Linux development machine)

Is flow control supported in the PRU-ICSS Ethernet ports?

Flow control is not currently supported in this version of the PRU-ICSS Ethernet firware that is provided by Texas Instruments.

How do I check the link status and hardware statistics of my PRU-ICSS Ethernet ports?

You can use the ethtool utility:

  • ethtool eth2 (for link status)
  • ethtool -S eth2 (for hardware statistics)



Archives