PRU-ICSS Remoteproc and RPMsg

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:


Introduction

Overview.PNG

The host processor on TI's Sitara family of devices is an ARM Cortex-A processor. Typically the ARM core is running Linux based on the Processor SDK. TI has developed custom pruss and pru_rproc (PRU Subsystem Remote Processor) drivers which will plug into this kernel. This provides an interface for the kernel to load firmware into the PRU core(s) and provides basic control such as start and halt. A message passing driver, named rpmsg_pru (remote processor message), has also been developed that allows the PRU and ARM cores to pass messages and buffers back and forth.

What do we need Linux to do?

The following is a list of services that Linux needs to provide in order to enable the PRU cores:

  • Load firmware into the PRU cores
  • Control PRU execution (start, stop, etc.)
  • Manage resources (memory, interrupt mappings, etc.)
  • Provide a method to send/receive messages

All of these services are provided through a combination of the pruss, pru_rproc, and rpmsg_pru Linux drivers that TI provides in the Processor SDK.



Remoteproc

Overview

Remoteproc is a framework that allows the ARM host processor(s) to load firmware into PRU cores, start the PRU cores, stop the PRU cores, and configure resources that the PRUs might need during their execution (such as configuring the PRUSS INTC module and providing shared buffers in DDR memory for message passing). The next section will discuss the process that happens when the remoteproc module loads the PRU cores with a firmware. Most of this happens transparently to the user when the pruss and pru_rproc modules are inserted but an understanding of the concepts below should help users to better understand how to debug problems with remoteproc should they arise.

Load Procedure

This section will walk through each step that the drivers takes as they load firmwares into the PRU cores and then run them.

Step 0

Step0 2 0 2 11.PNG

The four blocks in the image to right represent: The ARM core running Linux, the Linux filesystem where the PRU firmware binaries are initially stored, the PRU subsystem, and DDR memory. This image shows the initial state of the system before the pruss_remoteproc module is inserted.

  • Remoteproc driver is included as a kernel driver. This is a core remoteproc driver that provides the load/run/halt/etc API to other more specific remoteproc drivers.
  • A sysfs interface is also exposed to User Space to start/stop the PRU cores as well as specify the firmware file to load.
    • The sysfs interface is found at /sys/class/remoteproc/remoteprocN/ (e.g. remoteproc1 is PRU0 and remoteproc2 is PRU1 on the AM335x device (remoteproc0 is the M3 core used for power management functions)).
  • PRU firmware binaries exist in the filesystem in the /lib/firmware/ directory.



Step 1

Step1 2 0 2 11.PNG

In this step, the sysfs interface (mentioned above in step 0) is used to specify the name of the firmware to be loaded as well as to signal that the user wants to load and start the PRU cores
echo 'am335x-pru0-fw' > /sys/class/remoteproc/remoteproc1/firmware
echo 'am335x-pru1-fw' > /sys/class/remoteproc/remoteproc2/firmware
echo 'start' > /sys/class/remoteproc/remoteproc1/state
echo 'start' > /sys/class/remoteproc/remoteproc2/state



Step 2

Step2 2 0 2 11.PNG

The pru_rproc module verifies two things before it proceeds with the firmware loading process.

  • The pru_rproc modules checks for the existence of PRU firmware binaries in the filesystem (as specified by the firmware entry in the sysfs in step 1 above)
    • These binaries must be located in the /lib/firmware/ directory
    • am335x-pru0-fw and am335x-pru1-fw are the default names used for the AM335x device but any name can be used as long as the firmware exists in /lib/firmware/
  • The pru_rproc module also parses the firmware binaries looking for a section named .resource_table
    • This .resource_table section of the firmware specifies the system resources that the PRUs will need during their program execution




Step 3

Step3 2 0 2 11.PNG
  • The pru_rproc module configures all of the resources that are being requested by the firmwares
  • In this case, that includes creating vrings in DDR memory for communication as well as setting up the interrupt mapping in the PRU subsystem INTC module



Step 4

Step4 2 0 2 11.PNG

The pru_rproc module then loads the binary into the instruction RAM of the PRUs and also copies the resource table into the PRUs data RAM space

Note: Configuration details can be shared from the ARM to the PRUs through the resource table that gets copied into the data RAM of each PRU




Step 5

Step5 2 0 2 11.PNG

Now that everything is configured and the application code is in place, the pru_rproc module instructs the PRU cores to begin execution.

Notice that the PRU state was previously set to 'Halted' but now it is 'Run'


RPMsg

RPMsg is a message passing mechanism that requests resources through remoteproc and builds on top of the virtio framework. Shared buffers are requested through the resource_table and provided by the remoteproc module during PRU firmware loading (as shown in the remoteproc procedure above). The shared buffers are contained inside a vring data structure in DDR memory. There are two vrings provided per PRU core, one vring is used for messages passed to the ARM and the other vring is used for messages received from the ARM. System level mailboxes are used to notify cores (ARM or PRU) when new messages are waiting in the shared buffers.

There are two RPMsg software implementations provided in the Linux Processor SDK. On the ARM Linux side, RPMsg communication is received in kernel space. An interface module is provided (rpmsg_pru) that creates a character device in user space so that users can write/read to/from a character device in the file system to send/receive messages to/from the PRUs. On the PRU side, an RPMsg library is provided in the PRU Software Support Package that aims to abstract the communication to a point where a user's code can just call the pru_rpmsg_receive and pru_rpmsg_send functions in order to communicate with the ARM core. Source code for the PRU RPMsg library is provided in the support package along with the ability to rebuild the library if changes are desired.

Rpmsg diagram 2 0 2 11.PNG


ARM to PRU

Arm-to-pru.PNG

The diagram to the right shows the process that occurs when the ARM sends a message to the PRU. These steps are shown for illustrative purposes as the provided software in the SDK hides them in an abstraction layer.

  • ARM Host Steps
    • Step 1a: Allocate a new buffer
      -or-
    • Step 1b: Get a Used buffer from the slave Vring
    • Step 2: Copy data to be transferred into the buffer from Step 1
    • Step 3: Add the newly filled buffer to the Available list in the slave Vring
    • Step 4: Kick the slave Vring by writing its index (1) into a message in Mailbox 2
  • PRU Steps
    • Step 5: A Kick is discovered in Mailbox 2 with the index of the Kicked Vring (1). This indicates to the PRU that data is available for receive
    • Step 6: Get the Available buffer from the slave Vring
    • Step 7: Copy data to be received out of the buffer from Step 2
    • Step 8: Add the now empty buffer to the Used list in the slave Vring
    • Step 9: Kick the slave Vring by writing its index (1) into a message in Mailbox 3


PRU to ARM

Pru-to-arm.PNG

The diagram to the right shows the process that occurs when the PRU sends a message to the ARM. These steps are shown for illustrative purposes as the provided software in the SDK hides them in an abstraction layer.

  • PRU Steps
    • Step 1: Get an Available buffer from the host Vring
    • Step 2: Copy data to be transferred into the buffer from Step 1
    • Step 3: Add the newly filled buffer to the Used list in the host Vring
    • Step 4: Kick the host Vring by writing its index (0) into a message in Mailbox 3
  • ARM Host Steps
    • Step 5: An interrupt signals that Mailbox 3 was kicked with the index of Vring (0). This indicates to the ARM Host that data is available for receive
    • Step 6: Get the Used buffer from the host Vring
    • Step 7: Copy data to be received out of the buffer from Step 2
    • Step 8: Add the now empty buffer to the Available list in the host Vring
    • Step 9: Kick the host Vring by writing its index (0) into a message in Mailbox 2


RPMsg PRU Code Example

The RPMsg library provided for the PRU cores attempts to abstract the underlying implementation (Vring transport layer, mailboxes, etc.) to make programming as simple as possible. See the code below for an example PRU firmware the that can receive, and then echo back, messages from the ARM core. This code is provided as an example in the PRU Software Support Package that is include in the Linux Processor SDK.
Rpmsg code.PNG


Next Steps

To get started quickly with remoteproc and RPMsg you can use the RPMsg Quick Start Guide.

For Hands-on Labs that work with the BeagleBone Black and a PRU Cape start here.

Archived Versions