PRU Assembly Instructions

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

^ Up to main Programmable Realtime Unit Software Development Table of Contents

This arcticle is part of a collection of articles describing software development on the PRU subsystem included in OMAP-L1x8/C674m/AM18xx devices (where m is an even number).  To navigate to the main PRU software development page click on the link above.

Contents

Instruction Set Syntax Terminology

Table 1 provides terminology needed to understand the syntax for the instruction set.

Table 1: Instruction Set syntax Terminology
Parameter Name Meaning Examples
REG, REG1, REG2, ... Any register field from 8 to 32 bits r0, r1.w0, r3.b2
Rn, Rn1, Rn2, ... Any 32 bit register field (r0 through r31) r0, r1
Rn.tx Any 1 bit register field (x dentoes the bit position) r0.t23, r1.b2.t5
Cn, Cn1, Cn2, ... Any 32 bit constant table entry (c0 through c31) c0,c1
bn Specifies a field that must be b0, b1, b2, or b3 – denoting r0.b0, r0.b1, r0.b2, and r0.b3 respectively. b0,b1
LABEL Any valid label, specified with or without parenthesis. An immediate value denoting an instruction address is also acceptable. loop1, (loop1), 0x0000
IM(n) An immediate value from 0 to n. Immediate values can be specified with or without a leading hash "\#".Immediate values, labels, and register addresses are all acceptable. #23, 0b0110, 0xF2, 2+2, &r3.w2
OP(n) The union of REG and IM(n) r0, r1.w0, #0x7F, 1<<3, loop1, &r1.w0


Instruction set

Arithmetic and Logical

All operations are 32 bits wide (with a 33 bit result in the case of arithmetic’s). The source values are zero extended prior to the operation. If the destination is too small to accept the result, the result is truncated.

On arithmetic operations, the first bit to the left of the destination width becomes the carry value. Thus if the destination register is an 8 bit field, bit 8 of the result becomes the carry. For 16 and 32 bit destinations, bit 16 and bit 32 are used as the carry bit respectively.


Unsigned Integer Add (ADD)

Performs 32-bit add on two 32 bit zero extended source values.

Syntax:

   ADD REG1, REG2, OP(255)

Operation:

   REG1 = REG2 + OP(255) 
   carry = (( REG2 + OP(255) ) >> bitwidth(REG1)) & 1

Example:

    add    r3, r1, r2
    add    r3, r1.b0, r2.w2
    add    r3, r3, 10


Unsigned Integer Add with Carry (ADC)

Performs 32-bit add on two 32 bit zero extended source values, plus a stored carry bit.

Definition:

   ADC REG1, REG2, OP(255)

Operation:

   REG1 = REG2 + OP(255) + carry
   carry = (( REG2 + OP(255) + carry ) >> bitwidth(REG1)) & 1

Example:

    adc     r3, r1, r2
    adc     r3, r1.b0, r2.w2
    adc     r3, r3, 10


Unsigned Integer Subtract (SUB)

Performs 32-bit subtract on two 32 bit zero extended source values

Definition:

   SUB REG1, REG2, OP(255)

Operation:

   REG1 = REG2 - OP(255) 
   carry = (( REG2 - OP(255) ) >> bitwidth(REG1)) & 1

Example:

    sub     r3, r1, r2
    sub     r3, r1.b0, r2.w2
    sub     r3, r3, 10


Unsigned Integer Subtract with Carry (SUC)

Performs 32-bit subtract on two 32 bit zero extended source values with carry (borrow)

Definition:

   SUC REG1, REG2, OP(255)

Operation:

   REG1 = REG2 - OP(255) - carry
   carry = (( REG2 - OP(255) - carry ) >> bitwidth(REG1)) & 1

Example:

    suc     r3, r1, r2
    suc     r3, r1.b0, r2.w2
    suc     r3, r3, 10


Reverse Unsigned Integer Subtract (RSB)

Performs 32-bit subtract on two 32 bit zero extended source values. Source values reversed.

Definition:

   RSB REG1, REG2, OP(255)

Operation:

   REG1 = OP(255) - REG2
   carry = (( OP(255) - REG2 ) >> bitwidth(REG1)) & 1

Example:

    rsb     r3, r1, r2
    rsb     r3, r1.b0, r2.w2
    rsb     r3, r3, 10


Reverse Unsigned Integer Subtract with Carry (RSC)

Performs 32-bit subtract on two 32 bit zero extended source values with carry (borrow). Source values reversed.

Definition:

   RSC REG1, REG2, OP(255)

Operation:

   REG1 = OP(255) - REG2 - carry
   carry   = (( OP(255) - REG2 - carry ) >> bitwidth(REG1)) & 1

Example:

    rsc     r3, r1, r2
    rsc     r3, r1.b0, r2.w2
    rsc     r3, r3, 10


Logical shift left (LSL)

Performs 32-bit shift left of the zero extended source value

Definition:

   LSL REG1, REG2, OP(31)

Operation:

   REG1 = REG2 << ( OP(31) & 0x1f )

Example:

    lsl     r3, r3, 2
    lsl     r3, r3, r1.b0 
    lsl     r3, r3.b0, 10


Logical Shift Right (LSR)

Performs 32-bit shift right of the zero extended source value

Definition:

   LSR REG1, REG2, OP(31)

Operation:

   REG1 = REG2 >> ( OP(31) & 0x1f )

Example:

    lsr     r3, r3, 2
    lsr     r3, r3, r1.b0 
    lsr     r3, r3.b0, 10


Bitwise AND (AND)

Performs 32-bit logical AND on two 32 bit zero extended source values.

Definition:

   AND REG1, REG2, OP(255)

Operation:

   REG1 = REG2 & OP(255)

Example:

    and     r3, r1, r2
    and     r3, r1.b0, r2.w2
    and     r3.b0, r3.b0, ~(1<<3)    // Clear bit 3


Bitwise OR (OR)

Performs 32-bit logical OR on two 32 bit zero extended source values.

Definition:

   OR REG1, REG2, OP(255)

Operation:

   REG1 = REG2 | OP(255)

Example:

    or      r3, r1, r2
    or      r3, r1.b0, r2.w2
    or      r3.b0, r3.b0, 1<<3     // Set bit 3


Bitwise Exclusive OR (XOR)

Performs 32-bit logical XOR on two 32 bit zero extended source values.

Definition:

   XOR REG1, REG2, OP(255)

Operation:

   REG1 = REG2 ^ OP(255)

Example:

    xor      r3, r1, r2
    xor      r3, r1.b0, r2.w2
    xor      r3.b0, r3.b0, 1<<3   // Toggle bit 3


Bitwise NOT (NOT)

Performs 32-bit logical NOT on the 32 bit zero extended source value.

Definition:

   NOT REG1, REG2

Operation:

   REG1 = ~REG2

Example:

    not      r3, r3
    not      r1.w0, r1.b0


Copy Minimum (MIN)

Compares two 32 bit zero extended source values and copies the minimum value to the destination register.

Definition:

   MIN REG1, REG2, OP(255)

Operation:

   if( OP(255) > REG2 )
       REG1 = REG2;
   else
       REG1 = OP(255);

Example:

    min      r3, r1, r2
    min      r1.w2, r1.b0, 127


Copy Maximum (MAX)

Compares two 32 bit zero extended source values and copies the maximum value to the destination register.

Definition:

   MAX REG1, REG2, OP(255)

Operation:

   if( OP(255) > REG2 )
       REG1 = OP(255);
   else
       REG1 = REG2;

Example:

    max      r3, r1, r2
    max      r1.w2, r1.b0, 127


Clear Bit (CLR)

Clears the specified bit in the source and copies the result to the destination. Various calling formats are supported:

Format 1

Definition:

   CLR REG1, REG2, OP(31)

Operation:

   REG1 = REG2 & ~( 1 << (OP(31) & 0x1f) )

Example:

    clr      r3, r1, r2          // r3 = r1 & ~(1<<r2)
    clr      r1.b1, r1.b0, 5     // r1.b1 = r1.b0 & ~(1<<5)
Format 2 (same source and destination)

Definition:

   CLR REG1, OP(31)

Operation:

   REG1 = REG1 & ~( 1 << (OP(31) & 0x1f) )

Example:

    clr      r3, r1             // r3 = r3 & ~(1<<r1)
    clr      r1.b1, 5           // r1.b1 = r1.b1 & ~(1<<5)
Format 3 (source abbreviated)

Definition:

   CLR REG1, Rn.tx

Operation:

   REG1 = Rn & ~(1<<x)

Example:

    clr      r3, r1.t2         // r3 = r1 & ~(1<<2)
    clr      r1.b1, r1.b0.t5   // r1.b1 = r1.b0 & ~(1<<5)
Format 4 (same source and destination – abbreviated)

Definition:

   CLR Rn.tx

Operation:

   Rn = Rn & ~(1<<x)

Example:

    clr      r3.t2             // r3 = r3 & ~(1<<2)

Set Bit (SET)

Sets the specified bit in the source and copies the result to the destination. Various calling formats are supported.

NOTE: Whenever R31 is selected as the source operand to a SET, the resulting source bits will be NULL, and not reflect the current input event flags that are normally obtained by reading R31.

Format 1

Definition:

   SET REG1, REG2, OP(31)

Operation:

   REG1 = REG2 | ( 1 << (OP(31) & 0x1f) )

Example:

    set      r3, r1, r2          // r3 = r1 | (1<<r2)
    set      r1.b1, r1.b0, 5     // r1.b1 = r1.b0 | (1<<5)
Format 2 (same source and destination)

Definition:

   SET REG1, OP(31)

Operation:

   REG1 = REG1 | ( 1 << (OP(31) & 0x1f) )

Example:

    set      r3, r1             // r3 = r3 | (1<<r1)
    set      r1.b1, 5           // r1.b1 = r1.b1 | 1<<5)
Format 3 (source abbreviated)

Definition:

   SET REG1, Rn.tx

Operation:

   REG1 = Rn | (1<<x)

Example:

    set      r3, r1.t2         // r3 = r1 | (1<<2)
    set      r1.b1, r1.b0.t5   // r1.b1 = r1.b0 | (1<<5)
Format 4 (same source and destination – abbreviated)

Definition:

   SET Rn.tx

Operation:

   Rn = Rn | (1<<x)

Example:

    set      r3.t2             // r3 = r3 | (1<<2)

Register Field Scan (SCAN)

The SCAN instruction scans the register file for a particular value. It includes a configurable field width and stride. The width of the field to match can be set to 1, 2, or 4 bytes. The span between fields in bytes is programmable from 1 to 4 bytes. (Having a stride independent of width allows the programmer to scan for non-byte values on byte boundaries. For example, scan for "7F03" on a byte by byte basis). This instruction is deprecated and not available on all PRU cores.

Definition:

   SCAN Rn, OP(255)

Operation:

   The register "Rn" serves as both the source and results register. It is coded as follows:
Rn.b0 Byte offset from the start of the register file to begin the scan

(see section 3.3 for details on register addressing)

Rn.b1 Number of fields to scan
Rn.b2 Byte width of field to scan for (1, 2, 4)
Rn.b3 Byte stride of consecutive fields (1 to 4)

The instruction scans for the value specified in OP(255). On completion, the Rn register holds the results of the scan. It is coded as follows:

Rn.b0 Byte offset from R0.b0 to the matching field (or 0xFF if no match)
Rn.b1 Number of fields left to scan (including the matched field if any)
Rn.b2 Not altered
Rn.b3 Not altered

To continue a scan after a match, the programmer can write:

    ADD     R1.w0, R1.w0, #0xFF01 // Inc byte offset, dec count
    SCAN    R1, OP(255)

Example: Scan the register file for the sequence "0x7F 0x03" starting at R2.b1 and extending for 18 bytes. Do not assume the sequence is word aligned.

    LDI     R1.w0, 0x7F | 0x03<<8  // 0x7F 0x03 in little endian
    LDI     R30.w2, 2 | 1<<8       // Field width of 2, stride of 1
    LDI     R30.w0, &r2.b1 | 18<<8 // Start at R2.b1, scan 18 bytes
    SCAN    R30, R1.w0             // Scan for byte sequence
    QBEQ    NOT_FOUND, R30.b1, 0   // Jump if sequence not found


Left-Most Bit Detect (LMBD)

Scans REG2 from its left-most bit for a bit value matching bit 0 of OP(255), and writes the bit number in REG1 (writes 32 to REG1 if the bit is not found).

Definition:

   LMBD REG1, REG2, OP(255)

Operation:

   for( i=(bitwidth(REG2)-1); i>=0; i-- )
   if( !((( REG2>>i) ^ OP(255))&1) )
       break;
   if( i<0 )
       REG1 = 32;
   else
       REG1 = i;

Example:

    lmbd     r3, r1, r2
    lmbd     r3, r1, 1
    lmbd     r3.b3, r3.w0, 0

Register Load and Store

Copy Value (MOV)

The MOV instruction moves the value from OP(65535), zero extends it, and stores it into REG1. The instruction is a pseudo op, and is coded with different PRU instructions, depending on how it is used.

Definition:

   MOV REG1, OP(65535)

Operation:

   REG1 = OP(65535)

Example:

    mov     r3, r1
    mov     r3, r1.b0        // Zero extend r1.b0 into r3
    mov     r1, 10           // Move 10 into r1
    mov     r1, #10          // Move 10 into r1
    mov     r1, 0b10 + 020/2 // Move 10 into r1
    mov     r30.b0, &r2      // Move the offset of r2 into r30.b0


Load Immediate (LDI)

The LDI instruction moves the value from IM(65535), zero extends it, and stores it into REG1. The instruction is one form of MOV (the MOV pseudo op uses LDI when the source data is an immediate value).

Definition:

   LDI REG1, IM(65535)

Operation:

   REG1 = IM(65535)

Example:

    ldi     r1, 10           // Load 10 into r1
    ldi     r1, #10          // Load 10 into r1
    ldi     r1, 0b10 + 020/2 // Load 10 into r1
    ldi     r30.b0, &r2      // Load the offset of r2 into r30.b0


Move Register File Indirect (MVIx)

The MVIx instruction family moves an 8 bit, 16 bit, or 32 bit value from the source to the destination. The size of the value is determined by the exact instruction used; MVIB, MVIW, and MVID, for 8 bit, 16 bit, and 32 bit values respectively. The source, destination, or both can be register pointers. There is an option for auto-increment and auto-decrement on register pointers, and a count register can be supplied to auto-loop the operation multiple times.

Definition:

    MVIB	[*][&][--]REG1[++], [*][&][--]REG2[++]  [, bn]
    MVIW	[*][&][--]REG1[++], [*][&][--]REG2[++]  [, bn]
    MVID	[*][&][--]REG1[++], [*][&][--]REG2[++]  [, bn]

Operation:


Standard PRU Core Support

On the standard PRU code, this instruction is implemented as a pseudo-op. The only forms of the instruction supported in this environment are the following:

    MVIB    [*&]REG1, [*&]REG2
    MVIW    [*&]REG1, [*&]REG2
    MVID    [*&]REG1, [*&]REG2

Since writing ’*&R1’ appears to be the same as writing ’R1’, this operation may seem to simplify into a MOV pseudo-op. However, when writing the expression as ’*&R1’, the size of the move is determined by the instruction, as opposed to when writing ’R1’, where the size of the move is determined by the register field. To illustrate this more fully, consider the following example:

Example:

    // Define a simple structure
    .struct test_struct
        .u8 Byte0
        .u8 Byte1
        .u16 Word0
    .ends

    // This stucture assignment maps the structure "test"
    // (of type "test_struct") to the register "R29".
    .assign test_struct, R29, R29, test

In our source code, we only want to refer to the structure by its name (’test’). The structure mapping (to R29) is abstracted from the source so that we are free to alter the mapping later without affecting the source code.

The statement below reads the value of the ’Byte0’ field in ’test’, and zero extends the 8 bit value into R0. This is equivalent to writing "mov R0, test.Byte0".

    mvid R0, test.Byte0

Instead of just reading the single field, assume we want to read all 32 bits of the structure into R0. This can not be done using a MOV pseudo-op, but the statement below reads the values of the Byte0, Byte1, and Word0 fields in ’test’, and packs them into R0 (arrangement is endian dependent).

    mvid R0, *&test.Byte0


Load Byte Burst (LBBO)

The LBBO instruction is used to read a block of data from memory into the register file. The memory address to read from is specified by a 32 bit register (Rn2), using an optional offset. The destination in the register file can be specified as a direct register, or indirectly through a register pointer.

NOTE: Either the traditional direct register syntax or the more recent register address offset syntax can be used for the first parameter.

Format 1 (immediate count)

Definition:

   LBBO REG1, Rn2, OP(255), IM(124) 

Operation:

   memcpy( offset(REG1), Rn2+OP(255), IM(124) );

Example:

    lbbo     r2, r1, 5, 8      // Copy 8 bytes into r2/r3 from the
                               // memory address r1+5
    lbbo     &r2, r1, 5, 8     // Copy 8 bytes into r2/r3 from the
                               // memory address r1+5
Format 2 (register count)

Definition:

   LBBO REG1, Rn2, OP(255), bn

Operation:

   memcpy( offset(REG1), Rn2+OP(255), bn );

Example:

    lbbo     r3, r1, r2.w0, b0  // Copy "r0.b0" bytes into r3 from the
                                // memory address r1+r2.w0
    lbbo     &r3, r1, r2.w0, b0 // Copy "r0.b0" bytes into r3 from the
                                // memory address r1+r2.w0
Important Usage Note

For Format 2, do not use a byte count of 0 provided in R0.bn. It could cause the PRU to hang.


Store Byte Burst (SBBO)

The SBBO instruction is used to write a block of data from the register file into memory. The memory address to write to is specified by a 32 bit register (Rn2), using an optional offset. The source in the register file can be specified as a direct register, or indirectly through a register pointer.

NOTE: Either the traditional direct register syntax or the more recent register address offset syntax can be used for the first parameter.

Format 1 (immediate count)

Definition:

   SBBO REG1, Rn2, OP(255), IM(124)

Operation:

   memcpy( Rn2+OP(255), offset(REG1), IM(124) );

Example:

    sbbo     r2, r1, 5, 8      // Copy 8 bytes from r2/r3 to the
                               // memory address r1+5
    sbbo     &r2, r1, 5, 8     // Copy 8 bytes from r2/r3 to the
                               // memory address r1+5
Format 2 (register count)

Definition:

   SBBO REG1, Rn2, OP(255), bn

Operation:

   memcpy( Rn2+OP(255), offset(REG1), bn );

Example:

    sbbo     r3, r1, r2.w0, b0  // Copy "r0.b0" bytes from r3 to the
                                // memory address r1+r2.w0
    sbbo     &r3, r1, r2.w0, b0 // Copy "r0.b0" bytes from r3 to the
                                // memory address r1+r2.w0
Important Usage Note

For Format 2, do not use a byte count of 0 provided in R0.bn. It could cause the PRU to hang.


Load Byte Burst with Constant Table Offset (LBCO)

The LBCO instruction is used to read a block of data from memory into the register file. The memory address to read from is specified by a 32 bit constant register (Cn2), using an optional offset from an immediate or register value. The destination in the register file is specified as a direct register.

NOTE: Either the traditional direct register syntax or the more recent register address offset syntax can be used for the first parameter.

Format 1 (immediate count)

Definition:

   LBCO REG1, Cn2, OP(255), IM(124)

Operation:

   memcpy( offset(REG1), Cn2+OP(255), IM(124) );

Example:

    lbco     r2, c1, 5, 8      // Copy 8 bytes into r2/r3 from the
                               // memory address c1+5
    lbco     &r2, c1, 5, 8     // Copy 8 bytes into r2/r3 from the
                               // memory address c1+5
Format 2 (register count)

Definition:

   LBCO REG1, Cn2, OP(255), bn

Operation:

   memcpy( offset(REG1), Cn2+OP(255), bn );

Example:

    lbco     r3, c1, r2.w0, b0  // Copy "r0.b0" bytes into r3 from the
                                // memory address c1+r2.w0
    lbco     &r3, c1, r2.w0, b0 // Copy "r0.b0" bytes into r3 from the
                                // memory address c1+r2.w0
Important Usage Note

For Format 2, do not use a byte count of 0 provided in R0.bn. It could cause the PRU to hang.


Store Byte Burst with Constant Table Offset (SBCO)

The SBCO instruction is used to write a block of data from the register file into memory. The memory address to write to is specified by a 32 bit constant register (Cn2), using an optional offset from an immediate or register value. The source in the register file is specified as a direct register.

NOTE: Either the traditional direct register syntax or the more recent register address offset syntax can be used for the first parameter.

Format 1 (immediate count)

Definition:

   SBCO REG1, Cn2, OP(255), IM(124)

Operation:

   memcpy( Cn2+OP(255), offset(REG1), IM(124) );

Example:

    sbco     r2, c1, 5, 8      // Copy 8 bytes from r2/r3 to the
                               // memory address c1+5
    sbco     &r2, c1, 5, 8     // Copy 8 bytes from r2/r3 to the
                               // memory address c1+5
Format 2 (register count)

Definition:

   SBCO REG1, Cn2, OP(255), bn

Operation:

   memcpy( Cn2+OP(255), offset(REG1), bn );

Example:

    sbco     r3, c1, r2.w0, b0  // Copy "r0.b0" bytes from r3 to the
                                // memory address c1+r2.w0
    sbco     &r3, c1, r2.w0, b0 // Copy "r0.b0" bytes from r3 to the
                                // memory address c1+r2.w0
Important Usage Note

For Format 2, do not use a byte count of 0 provided in R0.bn. It could cause the PRU to hang.


Load from Coprocessor (LFC)

The LFC instruction is used to load data from an external "coprocessor register" using an 8 bit coprocessor register address. This instruction is deprecated and not available on all PRU cores.

Definition:

   LFC REG1, IM(255)

Operation:

   REG1 = Coprocessor Register IM(255)

Example:

   lfc     r2, 5      // Read coprocessor register 5


Store to Coprocessor (STC)

The STC instruction is used to write data to an external "coprocessor register" using an 8 bit coprocessor register address. Optionally, bits 31:24 can be specified from a third parameter OP(255) . This instruction is deprecated and not available on all PRU cores.

Format 1

Definition:

   STC REG1, IM(255)

Operation:

   Coprocessor Register IM(255) = (unsigned32) REG1

Example:

   stc     r2, 5        // Write coprocessor register 5
Format 2

Definition:

   STC REG1, IM(255), OP(255)

Operation:

   Coprocessor Register IM(255) = ((unsigned32) REG1 & 0x00FFFFFF) | (OP(255)<<24)

Example:

   stc     r2, 5, 0xFF  // Write coprocessor register 5
                        // (force the MS byte to 0xFF)
   stc     r2, 5, r3.b0 // Write coprocessor register 5, with
                        // bits 31:24 coming from r3.b0


Clear Register Space (ZERO)

This pseudo-op is used to clear space in the register file (set to zero).

Definition:

    ZERO IM(123), IM(124)
    ZERO &REG1, IM(124)

Operation:

   The register file data starting at offset IM(123) (or &REG1) with a length of IM(124) is cleared to zero.

Example:

    zero    0, 8     // Set R0 and R1 to zero
    zero    &r0, 8   // Set R0 and R1 to zero
    // Set all elements in myStruct zero
    zero    &myStruct, SIZE(myStruct)

This pseudo-op will generate the necessary LDI instructions to clear the specified register range to zero. The instructions generated are optimized based on the starting register alignment and length.


Transfer Bus Hardware Connection

The transfer bus coming out of the PRU consists of 124 bytes of data and a sufficient number of control lines to control the transfer. Any given transfer will consist of a direction (in or out of the PRU), a peripheral ID, a starting byte offset, and a length. These can be represented in hardware as register and byte enable signals as needed for a proper implementation (which is beyond the scope of this description).

How the bus transfer is used is entirely up to the peripherals that connect to it. The number of registers that are implemented on the peripheral and how they align to the PRU register file is determined by the peripheral connection. For example, the system below connects PRU registers R1::R3 to "peripheral A" registers A0::A2, and connects PRU registers R2::R4 to "peripheral B" registers B0::B2.

Flow Control

Unconditional Jump (JMP)

Unconditional jump to a 16 bit instruction address, specified by register or immediate value.

Definition:

   JMP OP(65535)

Operation:

   PRU Instruction Pointer = OP(65535)

Example:

    jmp     r2.w0    // Jump to the address stored in r2.w0
    jmp     myLabel  // Jump to the supplied code label


Unconditional Jump and Link (JAL)

Unconditional jump to a 16 bit instruction address, specified by register or immediate value. The address following the JAL instruction is stored into REG1, so that REG1 can later be used as a "return" address.

Definition:

   JAL REG1, OP(65535)

Operation:

   REG1 = Current PRU Instruction Pointer + 1
   PRU Instruction Pointer = OP(65535)

Example:

    jal     r2.w2, r2.w0      // Jump to the address stored in r2.w0
                              // put return location in r2.w2
    jal     r30.w0, myLabel   // Jump to the supplied code label and
                              // put the return location in r30.w0


Call Procedure (CALL)

The CALL instruction is a pseudo op designed to emulate a subroutine call on a stack based processor. Here, the JAL instruction is used with a specific call/ret register being the location to save the return pointer. The default register is R30.w0, but this can be changed by using the .setcallreg dot command. This instruction works in conjunction with the ".ret" dot command (deprecated) or the RET pseudo op instruction.

Definition:

   CALL OP(65535)

Operation:

   JAL call register, OP(65535)   (where call register defaults to r30.w0)

Example:

    call    r2.w0    // Call to the address stored in r2.w0
    call    myLabel  // Call to the supplied code label


Return from Procedure (RET)

The RET instruction is a pseudo op designed to emulate a subroutine return on a stack based processor. Here, the JMP instruction is used with a specific call/ret register being the location of the return pointer. The default register is R30.w0, but this can be changed by using the .setcallreg dot command. This instruction works in conjunction with the CALL pseudo op instruction.

Definition:

   RET

Operation:

   JMP call register   (where call register defaults to r30.w0)

Example:

    ret    // Return address stored in our call register


Quick Branch if Greater Than (QBGT)

Jumps if the value of OP(255) is greater than REG1.

Definition:

   QBGT LABEL, REG1, OP(255)

Operation:

   Branch to LABEL if OP(255) > REG1

Example:

    qbgt    myLabel, r2.w0, 5  // Branch if 5 > r2.w0
    qbgt    myLabel, r3, r4    // Branch if r4 > r3


Quick Branch if Greater Than or Equal (QBGE)

Jumps if the value of OP(255) is greater than or equal to REG1.

Definition:

   QBGE LABEL, REG1, OP(255)

Operation:

   Branch to LABEL if OP(255) >= REG1

Example:

    qbge    myLabel, r2.w0, 5  // Branch if 5 >= r2.w0
    qbge    myLabel, r3, r4    // Branch if r4 >= r3


Quick Branch if Less Than (QBLT)

Jumps if the value of OP(255) is less than REG1.

Definition:

   QBLT LABEL, REG1, OP(255)

Operation:

   Branch to LABEL if OP(255) < REG1

Example:

    qblt    myLabel, r2.w0, 5  // Branch if 5 < r2.w0
    qblt    myLabel, r3, r4    // Branch if r4 < r3


Quick Branch if Less Than or Equal (QBLE)

Jumps if the value of OP(255) is less than or equal to REG1.

Definition:

   QBLE LABEL, REG1, OP(255)

Operation:

   Branch to LABEL if OP(255) <= REG1

Example:

    qble    myLabel, r2.w0, 5  // Branch if 5 <= r2.w0
    qble    myLabel, r3, r4    // Branch if r4 <= r3


Quick Branch if Equal (QBEQ)

Jumps if the value of OP(255) is equal to REG1.

Definition:

   QBEQ LABEL, REG1, OP(255)

Operation:

   Branch to LABEL if OP(255) == REG1

Example:

    qbeq    myLabel, r2.w0, 5  // Branch if r2.w0==5
    qbeq    myLabel, r3, r4    // Branch if r4==r3


Quick Branch if Not Equal (QBNE)

Jumps if the value of OP(255) is NOT equal to REG1.

Definition:

   QBNE LABEL, REG1, OP(255)

Operation:

   Branch to LABEL if OP(255) != REG1

Example:

    qbne    myLabel, r2.w0, 5  // Branch if r2.w0!=5
    qbne    myLabel, r3, r4    // Branch if r4!=r3

Quick Branch Always (QBA)

Jump always. This is similar to the JMP instruction, only QBA uses an address offset and thus can be relocated in memory.

Definition:

   QBA LABEL

Operation:

   Branch to LABEL

Example:

    qba    myLabel	  // Branch


Quick Branch if Bit is Set (QBBS)

Jumps if the bit OP(31) is set in REG1.

Format 1

Definition:

   QBBS LABEL, REG1, OP(31)

Operation:

   Branch to LABEL if( REG1 & ( 1 <<  (OP(31) & 0x1f) ) )

Example:

    qbbs     myLabel r3, r1     // Branch if( r3&(1<<r1) )
    qbbs     myLabel, r1.b1, 5  // Branch if( r1.b1 & 1<<5 )
Format 2

Definition:

   QBBS LABEL, Rn.tx

Operation:

   Branch to LABEL if( Rn & Rn.tx )

Example:

    qbbs     myLabel, r1.b1.t5  // Branch if( r1.b1 & 1<<5 )
    qbbs     myLabel, r0.t0     // Brach if bit 0 in R0 is set


Quick Branch if Bit is Clear (QBBC)

Jumps if the bit OP(31) is clear in REG1.

Format 1

Definition:

   QBBC LABEL, REG1, OP(31)

Operation:

   Branch to LABEL if( !(REG1 & ( 1 <<  (OP(31) & 0x1f) )) )

Example:

    qbbc     myLabel r3, r1     // Branch if( !(r3&(1<<r1)) )
    qbbc     myLabel, r1.b1, 5  // Branch if( !(r1.b1 & 1<<5) )
Format 2

Definition:

   QBBC LABEL, Rn.tx

Operation:

   Branch to LABEL if( !(Rn & Rn.tx) )

Example:

    qbbc     myLabel, r1.b1.t5	// Branch if( !(r1.b1 & 1<<5) )
    qbbc     myLabel, r0.t0    // Brach if bit 0 in R0 is clear

Wait until Bit Set (WBS)

The WBS instruction is a pseudo op that uses the QBBC instruction. It is used to poll on a status bit, spinning until the bit is set. In this case, REG1 is almost certainly R31, else this instruction could lead to an infinite loop.

Format 1

Definition:

   WBS REG1, OP(31)

Operation:

   QBBC $, REG1, OP(31)

Example:

    wbs     r31, r1     	// Spin here while ( !(r31&(1<<r1)) )
    wbs     r31.b1, 5  	// Spin here while ( !(r31.b1 & 1<<5) )
Format 2

Definition:

   WBS Rn.tx

Operation:

   QBBC $, Rn.tx

Example:

   wbs     r31.b1.t5     // Spin here while ( !(r31.b1 & 1<<5) )
   wbs     r31.t0        // Spin here while bit 0 in R31 is clear

Wait until Bit Clear (WBC)

The WBC instruction is a pseudo op that uses the QBBS instruction. It is used to poll on a status bit, spinning until the bit is clear. In this case, REG1 is almost certainly R31, else this instruction could lead to an infinite loop.

Format 1

Definition:

   WBC REG1, OP(31)

Operation:

   QBBS $, REG1, OP(31)

Example:

   wbc     r31, r1     // Spin here while ( r31&(1<<r1) )
   wbc     r31.b1, 5  	// Spin here while ( r31.b1 & 1<<5 )
Format 2

Definition:

   WBC Rn.tx

Operation:

   QBBS $, Rn.tx

Example:

    wbc     r31.b1.t5    // Spin here while ( r31.b1 & 1<<5 )
    wbc     r31.t0       // Spin here while bit 0 in R31 is set

Halt Operation (HALT)

The HALT instruction disables the PRU. This instruction is used to implement software breakpoints in a debugger. The PRU program counter remains at its current location (the location of the HALT). When the PRU is re-enabled, the instruction is re-fetched from instruction memory.

Definition:

   HALT

Operation:

   Disable PRU

Example:

    halt


Sleep Operation (SLP)

The SLP instruction will sleep the PRU, causing it to disable its clock. This instruction can specify either a permanent sleep (requiring a PRU reset to recover) or a "wake on event". When the wake on event option is set to "1", the PRU will wake on any event that is enabled in the PRU Wakeup Enable register.

Definition:

   SLP IM(1)

Operation:

   Sleep the PRU with optional "wake on event" flag.

Example:

    SLP  0    // Sleep without wake events
    SLP  1    // Sleep until wake event set


Return to Main Page on PRU Software Development

Click here.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox