Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

PRU Projects

From Texas Instruments Wiki
Jump to: navigation, search

Users of TI processors with PRU-ICSS have created application for many different uses. A list of a few are shared below. For additional support resources, software and documentation visit the PRU-ICSS wiki.

Project Description Type Link
LEDscape BeagleBone Black cape and firmware for driving a large number of WS281x LED strips Code Library https://github.com/osresearch/LEDscape
Documentation and example projects http://trmm.net/LEDscape
LDGraphy Laser direct lithography for printing PCBs Code library and example project https://github.com/hzeller/ldgraphy/blob/master/README.md
PRdUino This is a port of the Energia platform based on the Arduino framework allowing you to use Arduino software libraries on PRU. Code Library https://github.com/lucas-ti/PRdUino
DMX Lighting Controlling professional lighting systems
Project http://beagleboard.org/CapeContest/entries/BeagleBone+DMX+Cape/
Tutorial http://blog.boxysean.com/2012/08/12/first-steps-with-the-beaglebone-pru/
Code Library https://github.com/boxysean/beaglebone-DMX
Interacto A cape making BeagleBone interactive with a triple-axis accelerometer, gyroscope and magnetometer plus a 640 x 480/30 fps camera. All sensors are digital and communicate via I²C to the BeagleBone. The camera frames are captured using the PRU-ICSS. The sensors on this cape give hobbyists and students a starting point to easily build robots and flying drones.
Project 1 http://beagleboard.org/CapeContest/entries/Interacto/
Project 2 http://www.hitchhikeree.org/beaglebone_capes/interacto/
code library https://github.com/cclark2/interacto_bbone_cape
Replicape: 3D Printer Replicape is a high end 3D-printer electronics package in the form of a Cape that can be placed on a BeagleBone Black. It has five high power stepper motors with cool running MosFets and it has been designed to fit in small spaces without active cooling. For a Replicape Daemon that processes G-code, see the Redeem Project Project http://www.thing-printer.com/product/replicape/
Code Library https://bitbucket.org/intelligentagent/replicape/
PyPRUSS: Python library PyPRUSS is a Python library for programming the PRUs on BeagleBone (Black) Code Library http://hipstercircuits.com/pypruss-a-simple-pru-python-binding-for-beaglebone/
Geiger The Geiger Cape, created by Matt Ranostay, is a design that measures radiation counts from background and test sources by utilising multiple Geiger tubes. The cape can be used to detect low-level radiation, which is needed in certain industries such as security and medical. Project 1 http://beagleboard.org/CapeContest/entries/Geiger+Cape/
Project 2 http://elinux.org/BeagleBone/GeigerCapePrototype
Code library https://github.com/mranostay/beaglebone-telemetry-presentation
Servo Controller Foosball Table Used for ball tracking and motor control Project http://www.element14.com/community/community/knode/single-board_computers/next-gen_beaglebone/blog/2013/07/17/hackerspace-challenge--leeds-only-pru-can-make-the-leds-bright
Tutorial https://docs.google.com/spreadsheet/pub?key=0AmI_ryMKXUGJdDQ3LXB4X3VBWlpxQTFWbGh6RGJHUEE&output=html
Code library https://github.com/pbrook/pypruss
Imaging with connected camera Low resolution imaging ideal for machine vision use-cases, robotics and movement detection Project http://www.element14.com/community/community/knode/single-board_computers/next-gen_beaglebone/blog/2013/08/18/bbb--imaging-with-a-pru-connected-camera
Code library
Computer Numerical Control (CNC) Translator Smooth stepper motor control; real embedded version of LinuxCNC Tutorial http://www.buildlog.net/blog/2013/09/cnc-translator-for-beaglebone/
Tutorial http://bb-lcnc.blogspot.com/p/machinekit_16.html
Robotic Control Chubby Project http://www.youtube.com/watch?v=dEes9k7-DYY
Code library https://github.com/cagdasc/Chubby1_v1
SpiderBot Project http://www.youtube.com/watch?v=JXyewd98e9Q
Reference http://www.ti.com/lit/wp/spry235/spry235.pdf
Software UART Soft-UART implementation on the PRU of AM335x Code library http://processors.wiki.ti.com/index.php/Soft-UART_Implementation_on_AM335X_PRU_-_Software_Users_Guide
Reference
Deviant LCD PRU bit-banged LCD interface @ 240x320 Project http://www.beagleboard.org/CapeContest/entries/DeviantLCD/
Code library https://github.com/cclark2/deviantlcd_bbone_cape
Nixie tube interface code library https://github.com/mranostay/beagle-nixie
Thermal imaging camera Thermal camera using Beaglebone Black, a small LCD, and a thermal array sensor project https://element14.com/community/community/knode/single-board_computers/next-gen_beaglebone/blog/2013/06/07/bbb--building-a-thermal-imaging-camera
Code library
Sine wave generator using PWMs Simulation of a pulse width modulation Project http://elinux.org/ECE497_BeagleBone_PRU
Reference
Code library https://github.com/millerap/AM335x_PRU_BeagleBone
Emulated memory interface ABX loads amovie into the Beaglebone's memory and then launches the memory emulator on the PRU sub-processor of the Beaglebone's ARM AM335x Project https://github.com/lybrown/abx
6502 memory interface System permitting communication between Linux and 6502 processor Project http://elinux.org/images/a/ac/What's_Old_Is_New-_A_6502-based_Remote_Processor.pdf
Code library https://github.com/lybrown/abx
JTAG/Debug Investigating the fastest way to program using JTAG and provide for debugging facilities built into the Beaglebone Project http://beagleboard.org/project/PRUJTAG/
High Speed Data Acquistion Reading data at high speeds Reference http://www.element14.com/community/community/knode/single-board_computers/next-gen_beaglebone/blog/2013/08/04/bbb--high-speed-data-acquisition-and-web-based-ui
Prufh (PRU Forth) Forth Programming Language and Compiler. It consists of a compiler, the forth system itself, and an

optional program for loading and communicating with the forth code proper.

Compiler https://github.com/biocode3D/prufh
VisualPRU VisualPRU is a minimal browser-based editor and debugger for the Beaglebone PRUs. The app runs from a local server on the Beaglebone. Editor and Debugger https://github.com/mmcdan/visualpru
libpruio Library for easy configuration and data handling at high speeds. This library can configure and control the devices from single source (no need for further overlays or the device tree compiler) Documentation http://users.freebasic-portal.de/tjf/Projekte/libpruio/doc/html/index.html
Library (German) http://www.freebasic-portal.de/downloads/fb-on-arm/libpruio-325.html
BeagleLogic 100MHz 14channel logic analyzer using both PRUs (one to capture and one to transfer the data) Project http://beaglelogic.net
BeaglePilot Uses PRUs as part of code for a BeagleBone based autopilot Code Library https://github.com/BeaglePilot/beaglepilot
PRU Speak Implements BotSpeak, a platform independent interpreter for tools like Labview, on the PRUs Code Library https://github.com/deepakkarki/pruspeak