Pin for Pin Compatibility of DM357 and DM644x
From Texas Instruments Embedded Processors Wiki
Overview
The DM644x family of processors has several pin-for-pin compatible variants: DM6446, DM6443, DM6441. To further enhance the selection of pin-for-pin compatible devices another device was created to be pin-for-pin compatible with these existing parts. That device is the DM357.
Pin-for-pin compatibility has some great advantages:
- A design can easily upgrade, e.g. from DM357 to DM6446 without any hardware changes!
- A "common platform" can be used such that the same board is being used across multiple designs.
- Reduces hardware development time
- Increases driver/software re-use
Comparison of Devices
Key Differences between DM357 and DM644x
- DM357 has 270 MHz ARM rather than 297 MHz on DM6446
- DM357 has H.264/MPEG-4/JPEG accelerator rather than DSP and VICP
- DM357 has 3 DACs, not 4
- DM357 does not have CF/ATA interface
- DM357 does not have VLYNQ
- DM357 requires Ball B17 be pulled down. That would correspond to the DSP being held in reset and booted by the ARM on the DM644x devices, which is typically the way it would be used anyway.
| | DM6446 | DM6443 | DM6441 | DM357 |
| ARM926EJ-S Speed | 297 MHz | 297 MHz | 256 MHz | 270 MHz |
| ARM9 Cache($)/Memory | 16KB I$, 8KB D$, 16KB RAM | 16KB I$, 8KB D$, 16KB RAM | 16KB I$, 8KB D$, 16KB RAM | 16KB I$, 8KB D$, 16KB RAM |
| Coprocessors | DSP, VICP | DSP | DSP, VICP | H.264/MPEG-4/JPEG accel. |
| Video Processing Front End | YES | NO | YES | YES |
| Video Processing Back End | YES, 4 DACs | YES, 4 DACs | YES, 4 DACs | YES, 3 DACs |
| EMAC | 10/100 | 10/100 | 10/100 | 10/100 |
| USB | 2.0 OTG | 2.0 OTG | 2.0 OTG | 2.0 OTG |
| SD/MMC | YES | YES | YES | YES |
| CF/ATA | YES | YES | YES | NO |
| VLYNQ | YES | YES | YES | NO |
| UART | 3 (1 with flow control) | 3 (1 with flow control) | 3 (1 with flow control) | 3 (1 with flow control) |
| GP Timer | 2x 64-bit | 2x 64-bit | 2x 64-bit | 2x 64-bit |
| Watchdog | 1x 64-bit | 1x 64-bit | 1x 64-bit | 1x 64-bit |
| I2C | YES | YES | YES | YES |
| SPI | YES | YES | YES | YES |
| PWM | 3 | 3 | 3 | 3 |
| HPI | 16-bit muxed | 16-bit muxed | 16-bit muxed | 16-bit muxed |
| EDMA3 | 64-channel | 64-channel | 64-channel | 64-channel |
| DDR2 | 32-bit, 125-166.67 MHz | 32-bit, 125-166.67 MHz | 32-bit, 125-166.67 MHz | 32-bit, 125-166.67 MHz |
| EMIFA | 16-bit (NAND/NOR) | 16-bit (NAND/NOR) | 16-bit (NAND/NOR) | 16-bit (NAND/NOR) |
| Audio Serial Port | YES | YES | YES | YES |
| GPIO | 71 | 71 | 71 | 71 |
| Package | 361-pin BGA (0.8mm spacing) | 361-pin BGA (0.8mm spacing) | 361-pin BGA (0.8mm spacing) | 361-pin BGA (0.8mm spacing) |
| Temp Options | 0-85°C, -40-85°C | 0-85°C | 0-85°C | 0-85°C |
| Price (100u as of 4/15/2009) | $39.35 | $33.75 | $34.00 | $20.20 |
Software Compatibility
No software changes should be required when sharing code between DM6446 and DM357. The peripheral layout (memory map) is identical aside from the peripherals that were removed in DM357 (i.e. VLYNQ, a DAC, CF/ATA, DSP). In terms of using the codecs, the Codec Engine framework isolates the end user from changes "under the hood" that result from removing the DSP and adding the HMJCP.
For example, if you had a high-end platform using DM6446 and a lower cost platform using DM357 you could have basic encode/decode functionality on both platforms using the exact same APIs. If you wished to add custom image processing analytics to the DSP you would have that flexibility on the DM6446.
Leave a Comment