Processor SDK Android create SD card script

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:


Return to the Software Developer's Guide

Ti stk 1c rev rgb png.png


Overview

The Android SDK includes a script in the <ANDROID SDK INSTALL DIR>/bin directory named create-sdcard.sh. The purpose of this script is to create SD cards for the following high-level use case:

  1. Create the SD card using default images from the Processor SDK for Android

The script will give you information about each step, but the following sections will go over the details for the use case above and walk you through how to use the script as well.

Common Steps

Invoking the Script

The create-sdcard.sh script can be run from any location but must be run with root permissions. This usually means using the sudo command to start execution of the script. For example:

sudo <ANDROID SDK INSTALL DIR>/bin/create-sdcard.sh

If you fail to execute the script without root permissions you will receive a message that root permissions are required and the script will exit.

Select the SD Card Device

The first step of the script will ask you to select the drive representing the SD card that you want to format. In most cases your host root file system drive has been masked off to prevent damage to the host system. When prompted enter the device number corresponding to the SD card. For example if the output looks like:

Availible Drives to write images to: 
 
#  major   minor    size   name 
1:   8       16    7761920 sdb
 
Enter Device Number: 

You would enter 1 to select the sdb device

NOTE: For most common installations, this script works fine. However, if you are using more advanced disk slicing and volume management, the presented list of device nodes are off by one; in the best case (picking the last item) it will flag a range error, and in the worst case (anything in the middle) the wrong DASD can be destroyed. The problem originates when it attempts to determine the $ROOTDRIVE to "mask" the volume where "/" is mounted from the selection list using a "grep -v $ROOTDRIVE" For the naive partitioning case, its heuristic is fine, yielding something like "sda" --- but for LVM, it grabs some chunk of the device name, e.g. "mapp" (out of "/dev/mapper/kubuntu--vg-root on / type ...")

Re-Partitioning the SD Card

Any partitions of the device that are already mounted will be un-mounted so that the device is ready for partitioning.

If the SD Card already has partition you will see a prompt like the following asking you if you would like to repartition the card. If the card was not already partitioned then this step will be skipped and you can move on to the next step.

Would you like to re-partition the drive anyways [y/n] :
  • Options:
    • y - This will allow you to change the partitioning of the SD card. For example if you have a 3 partition card and want to create a 2 partition card to give additional storage space to the root file system you would select y here.
      NOTE: This operation WILL ERASE the contents of your SD card
    • n - If the SD card already has the desired number of partitions then this will leave the partitioning alone. If you select n here skip on to the Installing SD Card Content section.

Installing SD Card Content

After the SD card is partitioned, you will be prompted whether you want to continue installing the file system or safely exit the script.

  • Options:
    • y - Selecting yes here will begin the process of installing the SD card contents. This operation WILL ERASE any existing data on the SD card. Refer to one of the following sections for additional instructions depending on which use case you are creating an SD card for
    • n - Selecting no here will allow you to have partitioned your card but will leave the partitions empty.


SD Card Using Default Images

The purpose of this section is to cover how to use the create-sdcard.sh script to populate an SD card that can be used to boot the device using the default images that ship with the Processor SDK for Android.

Prerequisites

  1. The Processor SDK for Android is installed on your host system
  2. The SD card you wish to create is inserted into the host system and has a size sufficiently large to hold at least the bootloaders, kernel, and Android file system.
  3. You have started running the script as detailed in the Common Steps section above.

Choose Install Pre-built Images

You should now see a prompt like:

now installing:  ti-processor-sdk-android-am57xx-evm-04.00.00.01

0. BOOTFILEPATH = ....00.00.01//board-support/prebuilt-images
1. MLO          = GP_MLO
2. BOOTIMG      = u-boot-am57xx-evm.img
3. BOOTUENV     = uEnv.txt
4. KERNELIMAGE  = zImage-am57xx-evm.bin
5. DTBDIR       = ....00.00.01//board-support/prebuilt-images
    * am571x-idk-lcd-osd.dtb
    * am571x-idk-lcd-osd101t2587.dtb
    * am571x-idk.dtb
    * am572x-idk-lcd-osd.dtb
    * am572x-idk-lcd-osd101t2587.dtb
    * am572x-idk.dtb
    * am57xx-beagle-x15-revb1.dtb
    * am57xx-beagle-x15.dtb
    * am57xx-evm-reva3.dtb
    * am57xx-evm.dtb
6. RAMDISKIMG   = ...oard-support/prebuilt-images/ramdisk.img
7. SYSTEMIMG    = ...board-support/prebuilt-images/system.img
8. USERDATAIMG  = ...ard-support/prebuilt-images/userdata.img


Would you like to continue? [y/n] :

You should choose option y to create an SD card using the pre-built images from the SDK. If you choose n then the script will exit.

You should execute this script from within the SDK so the script can determine the SDK path automatically. The script will start copying the contents to the SD card. Once the files are copied the script will exit.



Archived Versions