Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK Bare Metal Examples

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide Getting Started with Bare-Metal Examples




Overview

The bare-metal examples gets user started with development of code without an operating system. These are simple examples that does not get into details of software components provided in the SDK. Consequently, make sure there are no SD cards installed on the EVM with an OS prior to exploring the following examples.

If you face any problems with CCS or JTAG, see try these troubleshooting steps.

NOTE

All instructions on this wiki have been created using CCSv6 but should apply to CCSv7. Please report any issues by posting on E2E forums


ARM Cortex-A15

In this article, we take a look at creating bare-metal hello world examples for Cortex A15 core using pre-built templates in CCS. As a sample we will use the AM572x device to describe the steps but the same steps can be used for create hello world examples for Cortex A15 cores in the Keystone 2 family of devices.

NOTE

  • Only major difference between A15 examples for AM572x and Keystone 2 is that the Keystone 2 device contain MSMC memory instead of OCMC memory as the shared memory.
  • For K2G devices, the hello world template will be created with the .lds file that specifies MSMC and DDR memory sections. For K2E and K2H, the CCS template doesn`t populate the .lds file. K2H & K2E users can choose to use 66AK2G02.lds located at ccsv6\ccs_base\arm\include as reference to add .lds file to their hello world projects.


1. Start CCS and create a work space for generating the project.

2. Click on File menu option and select New--> CCS Project.

3. Select Target as AM572x -Cortex A15 and GPEVM_AM572x as shown in the image

4. Select Cortex A setting in the options below and provide name of the project as "hello_world" and use default Advanced settings for the project. If the Default settings uses "TI ARM compiler 5.x.x" switch to GNU Linaro 4.8.4 (or higher) tool chain for A15 and check the build little endian ELF binary for the A15 core. Under Project templates and examples, select Basic Examples-> Hello World

Click Finish after you are done to allow CCS to auto generate the project from the template Basic Examples-> Hello World.

NewCCSProject Hello world.png

5. The generated CCS project contains source file main.c, ARM assembly code startup_ARMCA15.S and a linker command file AM572x.lds. Please modify the main.c file by adding the following highlighted code lines and save main.c file.

  /*
  * hello.c
  */ 
  #include <stdio.h>
 
  int main(void) { 
 
      printf("Hello_world\n");
      return 0; 
 }
NOTE

For Keystone2 users, the startup_ARMCA15.S and .lds file is not auto populated by CCS. To add these file, right click the project and add files and locate the 66AK2Gxx.lds and startup_ARMCA15.S under the file path ccsvX/ccs_base/arm/include and add them to the project

6. Ensure that CCSv6 generated linker command file AM572x.lds contains the following Memory configurations.

 MEMORY
 {
    OCMC_RAM1 :  o = 0x40300000,  l = 0x00080000  /* 512kB L3 OCMC RAM1 */
    OCMC_RAM2 :  o = 0x40400000,  l = 0x00100000  /* 1MB L3 OCMC RAM2 */
    OCMC_RAM3 :  o = 0x40500000,  l = 0x00100000  /* 1MB L3 OCMC RAM3 */
    DDR0 :       o = 0x80000000,  l = 0x40000000  /* 1GB external DDR Bank 0 */
    DDR1 :       o = 0xC0000000,  l = 0x40000000  /* 1GB external DDR Bank 1 */
 }
NOTE

For Keystone 2 devices, replace all the OCMC_RAM# regions in the lds file and replace it with MSMC memory section as shown below. Refer to 66AK2G02.lds file in ccs installation under directory path ccsv6\ccs_base\arm\include
   MSMC  :      o=0x0c000000,    l = 0x00600000  /* 6MB Muticore shared memory */ 
NOTE

The .lds file expects users to provide STACKSIZE and HEAPSIZE from linker settings. To provide these settings got to Build Settings GNU Linker add the following to the Symbols section. Keystone II devices require this to be done explicitly in the linker settings
STACKSIZE=10000
HEAPSIZE=400

7. Right click on the project and select Build Project, to build the project and generate hello_world.out.

8. Launch target configuration using your emulator to connect to AM572X EVM as described in the Getting Started Guide.

9. Right click CortexA15_0 and select connect target.

10. Initialize DDR configuration. On CCS --> Scripts --> DDR configurations --> AM572_DDR3_532MHz_config

11. Load and run hello_world.out example file. You should see Hello_world string displayed on CCS console window.

HelloWorldOutput.jpg

NOTE

  • If the example does not load correctly in the first attempt, reload and ensure ARM core starts at main.
  • If the ARM loads correctly but you don`t see any output then check to see if the GNU linker is linking to Semihosting library (librdimon) in the linker setting. If it is not linked go to GNU linker settings in CCS project and add "rdimon" to the libraries that are linked



ARM Cortex-A9

1. Start CCSv6 and create a work space for generating the project.

NOTE

CCSv6.1.1 doesn`t contain a hello world project template for Cortex A9 core using GNU Linaro 4.8.x tool chain. Due to code compatibility of Cortex A8 and cortex A9 platforms, We recommend that you create a project for Cortex A8 platform like AM335x using the GNU Linaro tool chain and then use the code to test hello world application on the Cortex A9 on the AM437x platform. If you wish to use TI ARM compiler 5.2.x, then you can use the default hello world template in CCSv6 for the Cortex A9 on AM437x

2. Click on File menu option and select New--> CCS Project. Steps assume that user is using GN Linaro tool chain for Cortex A9.

3. Select Target as AM33xx -Cortex A8 and appropriate target Board setting as shown in the image

4. Select Cortex A8 setting in the options below and provide name of the project as "hello_world_a9" and use default Advanced settings for the project. If the Default settings uses "TI ARM compiler 5.x.x" switch to GNU Linaro 4.8.4 (or higher) tool chain for A9 and check the build little endian ELF binary for the A9 core. Click Finish after you are done to allow CCS to auto generate the project from the template Basic Examples-> Hello World.

Bare-Metal A9 templateselect.jpg

5. The generated CCS project contains source file main.c, ARM assembly code startup_ARMCA8.S and a linker command file AM335x.lds. The startup file does some basic setup and there is no difference between A8 and A9, so it can be used directly on A9 target. Ensure the main.c file contains the following code

  /*
  * hello.c
  */ 
  #include <stdio.h>
 
  int main(void) { 
 
      printf("Hello_world\n");
      return 0; 
 }

6. Ensure that CCSv6 generates the linker command file AM335x.lds.

 MEMORY
 {
    SRAM :     o = 0x402F0400,  l = 0x0000FC00  /* 64kB internal SRAM */
    L3OCMC0 :  o = 0x40300000,  l = 0x00010000  /* 64kB L3 OCMC SRAM */
    M3SHUMEM : o = 0x44D00000,  l = 0x00004000  /* 16kB M3 Shared Unified Code Space */
    M3SHDMEM : o = 0x44D80000,  l = 0x00002000  /* 8kB M3 Shared Data Memory */
    DDR0 :     o = 0x80000000,  l = 0x40000000  /* 1GB external DDR Bank 0 */
 }
NOTE

An optional step is to modify the section definition in AM437x.lds file if you wish to introduce more sections or partition the existing sections. If you renamed the startup file from startup_ARMCA8.S to startup_ARMCA9.S in your project, then the linker command file needs to be updated as well for code section placement: from startup_ARMCA8.o (.text) to startup_ARMCA9.o (.text)

7. Now build the project to generate hello_world.out file.

8. Launch target configurations using your emulator to connect to AM335X EVM as described in the Getting Started Guide.

9. Right click CortexA9 and connect target. The on target functionality in the GEL will initialize the clocks and DDR.

10. Load and run hello_world_a9.out file. You should see Hello World! string displayed on CCS console window.

Hello world a9.jpg

NOTE

If the example does not load correctly in the first attempt, reload and ensure ARM core starts at main.


ARM Cortex-A8

1. Start CCSv6 and create a work space for generating the project.

2. Click on File menu option and select New--> CCS Project.

3. Select Target as AM33xx -Cortex A8 and appropriate target Board setting as shown in the image

4. Select Cortex A8 setting in the options below and provide name of the project as "hello_world_a8" and use default Advanced settings for the project. If the Default settings uses "TI ARM compiler 5.x.x" switch to GNU Linaro 4.8.4 (or higher) tool chain for A8 and check the build little endian ELF binary for the A8 core. Click Finish after you are done to allow CCS to auto generate the project from the template Basic Examples-> Hello World.

Bare-Metal A8 templateselect.jpg

5. The generated CCS project contains source file hello.c, ARM assembly code startup_ARMCA8.S and a linker command file AM335x.lds. Ensure the main.c file contains the following code

  /*
  * hello.c
  */ 
  #include <stdio.h>
 
  int main(void) { 
 
      printf("Hello_world\n");
      return 0; 
 }

6. Ensure that CCSv6 generates the linker command file AM335x.lds.

 MEMORY
 {
    SRAM :     o = 0x402F0400,  l = 0x0000FC00  /* 64kB internal SRAM */
    L3OCMC0 :  o = 0x40300000,  l = 0x00010000  /* 64kB L3 OCMC SRAM */
    M3SHUMEM : o = 0x44D00000,  l = 0x00004000  /* 16kB M3 Shared Unified Code Space */
    M3SHDMEM : o = 0x44D80000,  l = 0x00002000  /* 8kB M3 Shared Data Memory */
    DDR0 :     o = 0x80000000,  l = 0x40000000  /* 1GB external DDR Bank 0 */
 }
NOTE

An optional step is to modify the section definition in AM335x.lds file if you wish to introduce more sections or partition the existing sections.

7. Now build the project to generate hello_world_a8.out file.

8. Launch target configurations using your emulator to connect to AM335X EVM as described in the Getting Started Guide.

9. Right click CortexA8 and select connect target. The on target functionality in the GEL will initialize the clocks and DDR.

10. Load and run hello_world_a8.out file. You should see Hello World! string displayed on CCS console window.

Hello world a8.jpg

NOTE

If the example does not load correctly in the first attempt, reload and ensure ARM core starts at main.


ARM Coretex-M4

1. Start CCSv6 and create a work space for generating the project.

2. Click on File menu option and select New--> CCS Project.

3. Select Target as AM572x -Cortex M4 and GPEVM_AM572x as shown in the image

4. Select Cortex M setting in the options below and provide name of the project as "hello_world_m4" and use default Advanced settings for the project. Click Finish after you are done to allow CCS to auto generate the project from the template Basic Examples-> Hello World. The Default settings uses "TI ARM compiler 5.x.x" tool chain for cortex M4 and sets the build for little endian ELF binary for the M4 core.

Bare-Metal M4 templateselect.jpg

5. The generated CCS project contains only one source file hello.c. Ensure the main.c file contains the following code

  /*
  * hello.c
  */ 
  #include <stdio.h>
 
  int main(void) { 
 
      printf("Hello_world\n");
      return 0; 
 }

6. CCSv6 includes a default linker command file(AM57xx_CM4.cmd) for the M4 (IPU) core which will place code into appropriate device memory. The linker command file has the following memory sections.

MEMORY
{
    IRAM:      o = 0x00000000 l = 0x00001000   /* 4kB internal SRAM */
    OCMC_RAM1: o = 0x40300000 l = 0x00080000   /* 512kB L3 OCMC SRAM1 */
    OCMC_RAM2: o = 0x40400000 l = 0x00100000   /* 1MB L3 OCMC SRAM2 */
    OCMC_RAM3: o = 0x40500000 l = 0x00100000   /* 1MB L3 OCMC SRAM3 */
    DDR0:      o = 0x80000000 l = 0x40000000   /* 1GB external DDR Bank 0 */
}

The linker command file is designed to place code in OCMC memory with interrupt vectors and .intc_txt generated by the compiler being place in device internal memory.

NOTE

  • Please note that if the device GEL files are setting up MMU for the core then the code will not load correctly on the core and will cause a CPU exception. We recommend that you modify the linker command file appropriately to match the MMU settings in the GEL file. The linker command file in all CCS releases prior to CCS 6.1.3 don`t account for this MMU Setting in AM57xx GEL files. Please modify the OCMC addresses to the logical address set in the GEL file
  • An optional step is to modify the section definition in AM57xx_CM4.cmd file if you wish to introduce/partition existing sections or place the code in different memory section.

7. Now build the project to generate hello_world_m4.out.

8. Launch target configurations using your emulator to connect to AM572X EVM as described in the Getting Started Guide.

9. In order to wake up the M4 core from A15, Go to Menu option Scripts->AM572x_Multicore_Initialization->IPU1SSClkEnable_API. Refer to the Processor_SDK_RTOS_Setup_CCS.

You should see the following log in the Console

 CortexA15_0: GEL Output: --->>> IPU1SS Initialization is in progress ... <<<---
 CortexA15_0: GEL Output: --->>> IPU1SS Initialization is DONE! <<<---

11. Select and Connect to Cortex_M4_IPU1_C0. Load and run Hello_Example_m4.out file. You should see Hello World string displayed on console window.

Hello world m4.jpg

NOTE

If the example does not load correctly in the first attempt, reload and ensure ARM core starts at main.


DSP C66x

In this article, we take a look at creating bare-metal hello world examples for C66x core using pre-built templates in CCS. As a sample we will use the AM572x device to describe the steps but the same steps can be used for create hello world examples for C66x cores in the Keystone 2 family of devices.

NOTE

Only major difference C66x examples for AM572x and Keystone 2 is that the Keystone 2 device contain MSMC memory instead of OCMC memory as the shared on chip memory.

1. Start CCSv6 and create a work space for generating the project.

2. Click on File menu option and select New--> CCS Project.

3. Select Target as AM572x -C66xx and GPEVM_AM572x as shown in the image

4. Select C66XX [C6000] DSP setting in the options below and provide name of the project as "hello_world_dsp" and use default Advanced settings for the project. Click Finish after you are done to allow CCS to auto generate the project from the template Basic Examples-> Hello World. The Default settings uses "TI CG Tools compiler 8.x.x" tool chain for C66x and sets the build for little endian ELF binary for the C66x core.

Bare-Metal C66x templateselect.jpg

5. The generated CCS project contains only one source file hello.c. Ensure the main.c file contains the following code

  /*
  * hello.c
  */ 
  #include <stdio.h>
 
  int main(void) { 
 
      printf("Hello_world\n");
      return 0; 
 }

6. CCSv6 includes a default linker command file(AM57xx_C66.cmd) for the C66x DSP core which will place code into appropriate device memory. The linker command file has the following memory sections.

MEMORY
{
    IRAM_MEM:  o = 0x00800000 l = 0x00008000   /* 32kB internal SRAM */
    OCMC_RAM1: o = 0x40300000 l = 0x00080000   /* 512kB L3 OCMC SRAM1 */
    OCMC_RAM2: o = 0x40400000 l = 0x00100000   /* 1MB L3 OCMC SRAM2 */
    OCMC_RAM3: o = 0x40500000 l = 0x00100000   /* 1MB L3 OCMC SRAM3 */
    DDR0:      o = 0x80000000 l = 0x40000000   /* 1GB external DDR Bank 0 */
}

The linker command file is designed to place code in OCMC memory.

NOTE

For Keystone 2 devices, replace all the OCMC_RAM# regions in the lds file and replace it with MSMC memory section as shown below.
   MSMC  :      o=0x0c000000,    l = 0x00600000  /* 6MB Muticore shared memory */ 
NOTE

An optional step is to modify the section definition in linker command file if you wish to introduce/partition existing sections or place the code in different memory section.

7. Now build the project to generate hello_world_dsp.out.

8. Launch target configurations using your emulator to connect to AM572X EVM as described in the Getting Started Guide.

9. In order to wake up the DSP1 core from A15, Go to Menu option Scripts->AM572x_Multicore_Initialization->DSP1SSClkEnable_API. Refer to the Processor_SDK_RTOS_Setup_CCS.

You should see the following log in the Console

 CortexA15_0: GEL Output: --->>> DSP1SS Initialization is in progress ... <<<---
 CortexA15_0: GEL Output: DEBUG: Clock is active ... 
 CortexA15_0: GEL Output: DEBUG: Checking for data integrity in DSPSS L2RAM ... 
 CortexA15_0: GEL Output: DEBUG: Data integrity check in GEM L2RAM is sucessful! 
 CortexA15_0: GEL Output: --->>> DSP1SS Initialization is DONE! <<<---

11. Select and Connect to C66x_DSP1. Load and run hello_world_dsp.out file. You should see Hello World string displayed on console window.

Hello world dsp.jpg


DSP C674x

In this article, we take a look at creating bare-metal hello world examples for C674x core using pre-built templates in CCS. As a sample we will use the C6748 LCDK device to describe the steps but the same steps can be used for create hello world examples for C674x cores in the OMAPL13x/C647x/DA8x family of devices.

NOTE

All the C674x DSP cores on in OMAPL13x/C674x/DA8x have the same memory map so modification are limited to selecting the correct platform when generating the project

1. Start CCS and create a work space for generating the project.

2. Click on File menu option and select New--> CCS Project.

3. Select Target as OMAPLx -C674xx and LCDK674x as shown in the image

4. Select C67XX [C6000] DSP setting in the options below and provide name of the project as "hello_world_lcdk674x" and use default Advanced settings for the project. Click Finish after you are done to allow CCS to auto generate the project from the template Basic Examples-> Hello World. The Default settings uses "TI CG Tools compiler 8.x.x" tool chain for C674x and sets the build for little endian ELF binary for the C674x core.

Baremetal helloWorld ProjectCreate step1.png

5. The generated CCS project contains only one source file hello.c. Ensure the main.c file contains the following code

  /*
  * hello.c
  */ 
  #include <stdio.h>
 
  int main(void) { 
 
      printf("Hello_world\n");
      return 0; 
 }

6. CCS includes a default linker command file(C6748.cmd) for the C674x DSP core which will place code into appropriate device memory. The linker command file has the following memory sections.

MEMORY
{
    DSPL2ROM     o = 0x00700000  l = 0x00100000   /* 1MB L2 Internal ROM */
    DSPL2RAM     o = 0x00800000  l = 0x00040000   /* 256kB L2 Internal RAM */
    DSPL1PRAM    o = 0x00E00000  l = 0x00008000   /* 32kB L1 Internal Program RAM */
    DSPL1DRAM    o = 0x00F00000  l = 0x00008000   /* 32kB L1 Internal Data RAM */
    SHDSPL2ROM   o = 0x11700000  l = 0x00100000   /* 1MB L2 Shared Internal ROM */
    SHDSPL2RAM   o = 0x11800000  l = 0x00040000   /* 256kB L2 Shared Internal RAM */
    SHDSPL1PRAM  o = 0x11E00000  l = 0x00008000   /* 32kB L1 Shared Internal Program RAM */
    SHDSPL1DRAM  o = 0x11F00000  l = 0x00008000   /* 32kB L1 Shared Internal Data RAM */
    EMIFACS0     o = 0x40000000  l = 0x20000000   /* 512MB SDRAM Data (CS0) */
    EMIFACS2     o = 0x60000000  l = 0x02000000   /* 32MB Async Data (CS2) */
    EMIFACS3     o = 0x62000000  l = 0x02000000   /* 32MB Async Data (CS3) */
    EMIFACS4     o = 0x64000000  l = 0x02000000   /* 32MB Async Data (CS4) */
    EMIFACS5     o = 0x66000000  l = 0x02000000   /* 32MB Async Data (CS5) */
    SHRAM        o = 0x80000000  l = 0x00020000   /* 128kB Shared RAM */
    DDR2         o = 0xC0000000  l = 0x20000000   /* 512MB DDR2 Data */
}

The linker command file is designed to place code in OCMC memory.

NOTE

For OMAPL13x/C674x devices, the linker command file places code in the SHRAM memory section as shown below.
   SECTIONS                                       
  {                                              
   .text          >  SHRAM                    
   .stack         >  SHRAM                    
   .bss           >  SHRAM      
    .......

}

NOTE

An optional step is to modify the section definition in linker command file if you wish to introduce/partition existing sections or place the code in different memory section.

7. Now build the project by right clicking on the Project and selecting "Build Project" to generate hello_world_lcdk674x.out.

8. Launch target configurations using your emulator to connect to OMAPLx/C674x LCDK as described in the Getting Started Guide.

9. Developers can Connect to the C674x on OMAPL137/C6747/C6748 can connect directly to the DSP. For OMAPL138 device, you will need to connect to the ARM as this is ARM master boot device and ARM needs to power up the DSP You should see the following log in the Console

C674X_0: Output: 	Target Connected.
C674X_0: Output: 	---------------------------------------------
C674X_0: Output: 	Memory Map Cleared.
C674X_0: Output: 	---------------------------------------------
C674X_0: Output: 	Memory Map Setup Complete.
C674X_0: Output: 	---------------------------------------------
C674X_0: Output: 	PSC Enable Complete.
C674X_0: Output: 	---------------------------------------------
C674X_0: Output: 	PLL0 init done for Core:300MHz, EMIFA:25MHz
C674X_0: Output: 	DDR initialization is in progress....
C674X_0: Output: 	PLL1 init done for DDR:150MHz
C674X_0: Output: 	Using DDR2 settings
C674X_0: Output: 	DDR2 init for 150 MHz is done
C674X_0: Output: 	---------------------------------------------


11. Select and Connect to C674x. Load and run hello_world_dsp.out file. You should see Hello World string displayed on console window.

Hello world dsp674x.png