Processor SDK Linux HSR PRP

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:


Overview

In both HSR and PRP protocols, the DAN (Dual Attached Node) sends an identical frame to both the interfaces and uses a sequence number in the tag to allow drop duplicates at the Rx node to achieve redundancy. This section describes the different software components of a Linux based HSR/PRP solution to support redundancy.

Features

  • Enhanced ICSS cut-through switch with HSR capability
  • HSR End Node (DANH) complying to IEC62439-3 Edition 2 Clause 5
  • PRP End Node (DANP) complying to IEC6239-3 Edition 2 Clause 4
  • 10/100 Mbits/s Full Duplex Ethernet Interface
  • Store & forward with data integrity check
  • VLAN over HSR/PRP interface
  • node table size 256
  • Statistics & Node Table MIB support
  • HSR Modes H;N,T,U,M - mode changethrough SNMP SET
  • Duplicate Accept/Reject configuration change through SNMP SET
  • Run time change of Protocol at PRU Ethernet



Software Architecture

The diagram below highlights the software components that are modified or developed specifically for HSR/PRP. These along with other standard Linux OS components are used to implement the Linux HSR/PRP DAN (Dual Attached Node).

  • Linux Kernel drivers
    • HSR/PRP driver
    • Ethernet driver
  • User space
    • Net-SNMP
    • iproute2

Linux-hsr-architecture.png

Linux HSR/PRP Driver

The Linux networking subsystem in upstream kernel has added support for HSR driver starting in v3.12 (HSRv0 - IEC 62439-3:2010) and enhanced the same to support HSRv1 (IEC 62439-3:2012) in v4.6. This driver allows user to create an HSR network device with a pair of slave network interfaces (A and B) that are standard Ethernet interfaces. For example on TI's AM572x IDK EVM, there are two Ethernet interfaces (10/100) per each PRU ICSS. The PRU Emac driver available for ICSS PRU Ethernet h/w supports two Ethernet ports. Using ip link command, user will be able to setup a HSR interface on this EVM that pair the two PRU Ethernet interfaces to create a HSR node or DAN-H.

TI has enhanced the Linux HSR driver and ip link command in iproute2 package to support PRP defined in IEC 62439-3 clause 4. With this change, user will be able to create a Doubly Attached Node with PRP (DAN-P) using standard Ethernet interfaces. As in the case of HSR, using ip link command, user will be able to setup a prp interface using two Ethernet interfaces such as the one provided by PRU EMAC driver.

Linux HSR/PRP driver provides a standard Ethernet interface to application layer and hide the details of the redundancy protocol under the driver layer. Linux HSR/PRP driver implements the Link Redundancy Entity (LRE) that is central to implementing redundancy using respective protocol.

HSR LRE functions and L2 routing can be offloaded to the firmware running on the PRU cores of ICSS. The diagram below shows the architecture of an Offloaded HSR/PRP driver. The upper layer driver is existing Linux HSR/PRP driver described in the previous section. The PRU Ethernet driver exports HSR/PRP capabilities in the NetDev feature flags. The green blocks in the Redundancy layer shows the software blocks that gets offloaded to PRUs in ICSS which is shown green as well. The upper layer HSR/PRP driver uses the feature flags exported by the PRU Ethernet driver to disable corresponding functions in its layer. The firmware is a re-use from the TI RTOS implementation that is discussed above. Re-use means the data structures and API should be re-used across both TI RTOS and Linux driver implementations. A common PRU Ethernet driver is developed to support existing EMAC device as well HSR/PRP device. Hsr-prp-offload.png



Ethernet Driver

Starting from Processor SDK 04.00.00 release, the PRU Ethernet driver supports HSR/PRP firmware offload. More specifically, based on a module parameter configured at boot time, the PRU Ethernet driver loads either a PRU EMAC firmware, PRU HSR firmware or PRU PRP firmware. The first case (EMAC) is the non-offload case, while the latter 2 cases are the firmware offload cases. When a HSR/PRP firmware is loaded, the PRU Ethernet driver will do proper firmware configurations and indicate offload capabilities in the netdev feature flag. The Linux HSR/PRP driver stack use these feature flag to determine if offload is supported or not at the lower level Ethernet driver and disable certain processing at the its layer.

Notice that, from the user point of view, other than providing a module parameter to specify which firmware to load, all of the above mentioned driver behavior is transparent to the user.



PRU Ethernet Driver (EMAC/HSR/PRP)

Starting from Processor SDK 04.00.00 release, the PRU Ethernet driver supports HSR/PRP firmware offload. More specifically, based on a module parameter configured at boot time, the PRU Ethernet driver loads either a PRU EMAC firmware, PRU HSR firmware or PRU PRP firmware. The first case (EMAC) is the non-offload case, while the latter 2 cases are the firmware offload cases. When a HSR/PRP firmware is loaded, the PRU Ethernet driver will do proper firmware configurations and notify the Linux HSR/PRP driver stack that offload has been enabled. From then on, LRE functionality is carried out in firmware.

Notice that, from the user point of view, other than providing a module parameter to specify which firmware to load, all of the above mentioned driver behavior is transparent to the user.

Queue Usage and VLAN PCP to Queue Map

At the Ingress, there are two queues assigned for packets coming from each port or PRU. Here is how the PCP values of incoming packets mapped to the each of the two queues. Firmware maintains a mapping table in the shared memory that is configured by the PRU Ethernet driver for HSR/PRP. For EMAC, the firmware has a similar mapping that is hard coded.

Ingress Host PCP to priority Queue map table in shared memory for HSR/PRP/EMAC

  byte 0 => PRU 0 (eth2), PCP 0-3 => Q1 
  byte 1 => PRU 0 (eth2), PCP 4-7 => Q0
  byte 2 => Unused.
  byte 3 => Unused.
  byte 4 => PRU 1 (eth3), PCP 0-3 => Q3 
  byte 5 => PRU 1 (eth3), PCP 4-7 => Q2 
  byte 6 => Unused
  byte 7 => Unused

The convention is that higher queue value corresponds to lower priority

At the Ingress, two separate irq handlers are assigned to each port to process the packets. Driver handler first process packets from the high priority queue followed by packets from the lower priority queue.

At the Egress, there are 4 queues where driver enqueue the packets for Egress transmission. Following are the PCP to queue map used for Egress that are same across all protocols.

 low  - pcp 0..1 maps to Q3
            2..3 maps to Q2
            4..5 maps to Q1
 high - pcp 6..7 maps to Q0.

Firmware sends the frames first from Q1, and then from the next higher queue (Q2) and so forth.



Changing protocol at PRU Ethernet

PRU Ethernet driver support multiple protocols based on the firmware loaded on ICSS PRU. In Processor SDK 04.00.00, a capability was added to change the protocol running on the PRU at boot time through bootargs. This is described at Processor_SDK_Linux_HSR_PRP#Testing_HSR.2FPRP_Firmware_Offload. Starting Processor SDK 04.01.00, The driver can be configured to switch the protocol while the board is powered up and running Linux kernel. By default, the PRU Ethernet driver is probed to be in the EMAC mode and EMAC firmware is loaded on to the PRU unless user set the pruss2_ethtype to run HSR (1) or PRP (2). Two feature names are added to help offload HSR or PRP in the PRU Ethernet driver :- hsr-rx-offload and prp-rx-offload. PRU Firmware essentially offload the rx side processing of LRE, such as duplicate detection and drop, node table update, stats update etc. To reflect the same, the features are named with a rx-offload suffx to the protocol name. Ethtool command has an option -K to set or clear the feature in a network device. So this flag can be set or reset rx offload feature in the PRU Ethernet device. As the device may be hooked up to a upper HSR/PRP network device, user is expected to delete the hsr or prp interface before changing the flag at the PRU Ethernet device. General procedure to change protocol at PRU Ethernet device is as follows:-

Below assumes that hsr or prp interface using the PRU Ethernet devices is currently deleted. Here are the steps at a high level:-

1. Bring down the two PRU Ethernet interfaces using ifconfig and unassign the ip address using ifconfig. For example

ifconfig eth2 down 0.0.0.0
ifconfig eth3 down 0.0.0.0

2. If the PRU Ethernet device is currently running HSR or PRP offload feature, the same has to be disabled before switching to EMAC or another protocol using ethtool -K option. For example if HSR is currently running, do

   ethtool -K eth2 hsr-rx-offload off
   ethtool -K eth3 hsr-rx-offload off

Similarly if PRP is currently running, do

   ethtool -K eth2 prp-rx-offload off
   ethtool -K eth3 prp-rx-offload off

3. If user would like to offload HSR, enable the feature hsr-rx-offload on both devices.

  ethtool -K eth2 hsr-rx-offload on
  ethtool -K eth3 hsr-rx-offload on

4. Now the PRU Ethernet devices can be paired to create an HSR interface using ip link command. To offload PRP user does following command in step 3

  ethtool -K eth2 prp-rx-offload on
  ethtool -K eth3 prp-rx-offload on

To display the offload feature currently active at the PRU Ethernet, user may type following command for example for eth2

  ethtool -k eth2



Sample commands

Before using these commands, save the MAC address of both interfaces. These sample commands assumes a MAC address of 70:FF:76:1C:0E:8C for both PRU Ethernet interfaces and an IP address of 192.168.2.20 for the hsr/prp interface. Eth3 MAC address is assumed to be 70:FF:76:1C:0E:8E. Also assumes user create hsr0 or prp0 interface using eth2 and eth3 interfaces. Please note that for each DAN, user needs to assign unique MAC address and IP address from the same subnet.

  • To switch from EMAC to HSR
ifconfig eth2 0.0.0.0 down
ifconfig eth3 0.0.0.0 down
ifconfig eth2 hw ether 70:FF:76:1C:0E:8C
ifconfig eth3 hw ether 70:FF:76:1C:0E:8C
ethtool -K eth2 hsr-rx-offload on
ethtool -K eth3 hsr-rx-offload on
ifconfig eth2 up
ifconfig eth3 up
ip link add name hsr0 type hsr slave1 eth2 slave2 eth3 supervision 45 version 1
ifconfig hsr0 192.168.2.20
  • To switch from HSR to PRP
ip link delete hsr0
ifconfig eth2 down
ifconfig eth3 down
ethtool -K eth2 hsr-rx-offload off
ethtool -K eth3 hsr-rx-offload off
ethtool -K eth2 prp-rx-offload on
ethtool -K eth3 prp-rx-offload on
ifconfig eth2 up
ifconfig eth3 up
ip link add name prp0 type prp slave1 eth2 slave2 eth3 supervision 45
ifconfig prp0 192.168.2.20
  • To switch from PRP to HSR
ip link delete prp0
ifconfig eth2 down
ifconfig eth3 down
ethtool -K eth2 prp-rx-offload off
ethtool -K eth3 prp-rx-offload off
ethtool -K eth2 hsr-rx-offload on
ethtool -K eth3 hsr-rx-offload on
ifconfig eth2 up
ifconfig eth3 up
ip link add name hsr0 type hsr slave1 eth2 slave2 eth3 supervision 45 version 1
ifconfig hsr0 192.168.2.20
  • To switch from HSR to EMAC
ip link delete hsr0
ifconfig eth2 down
ifconfig eth3 down
#Restore eth3 MAC address
ifconfig eth3 hw ether 70:FF:76:1C:0E:8E
ethtool -K eth2 hsr-rx-offload off
ethtool -K eth3 hsr-rx-offload off
ifconfig eth2 192.168.2.20
ifconfig eth3 192.168.3.20
  • To switch from PRP to EMAC
ip link delete prp0
ifconfig eth2 down
ifconfig eth3 down
ethtool -K eth2 prp-rx-offload off
ethtool -K eth3 prp-rx-offload off
#Restore eth3 MAC address
ifconfig eth3 hw ether 70:FF:76:1C:0E:8E
ifconfig eth2 192.168.2.20
ifconfig eth3 192.168.3.20



PRP EMAC mode

PRP EMAC mode is a special mode of PRP Ethernet type where the driver configures the PRP firmware to work like EMAC firmware. This is because currently PTP support is available only in PRU PRP firmware. So the current implementation of SAN with PTP requires PRUETH driver to be configured as PRP using bootargs. User needs to configure the PRP Firmware in PRP EMAC mode before bringing up the Ethernet interfaces. It is expected to add the PTP support to EMAC firmware in a future release. Until then this intermediate solution is used. Here are the steps to use PRUETH as SAN with PTP

  • Boot the IDK EVM with prussX_ethtype in bootargs set to PRP as described at #Testing_HSR.2FPRP_Firmware_Offload
  • Once the EVM boots up and user login, first thing to verify is if PRUETH is configured as PRP Ethernet type. See above section for details
  • Configure PRP EMAC mode in the PRP firmware by issuing the following command at the console
 echo 1 > /sys/kernel/debug/prueth-ethX/prp_emac_mode
 where X is 2 or 3 or 4 or 5
  • Now bring up Ethernet interfaces as usual and the device is ready to be used as SAN. PTP support can be enabled at this time. See section on [[1]] for the details.

NOTE: run time protocol switch is not supported for switch to SAN PTP for now and required boot time configuration and above debugfs command once device is boot up in PRP mode



VLAN over PRU Ethernet

Virtual LAN (VLAN) is a standard Linux feature that can be enabled over PRU Ethernet devices. There are many websites that describes how Linux VLAN works. Some of them are at [[2]] or at [[3]] and some configuration details are also discussed at [[4]].

User may use ip link command to setup vlan interface over prueth interfaces. For example, over a hsr interface, if user would like to setup two vlan interfaces say, hsr0.2 and hsr0.3, user execute the following commands assuming the hsr0 interface is already setup:-

Node-1

ifconfig hsr0 0.0.0.0
ip link add link hsr0 name hsr0.2 type vlan id 2
ip link add link hsr0 name hsr0.3 type vlan id 3
ifconfig hsr0.2 192.168.2.40
ifconfig hsr0.3 192.168.3.40
ip link set hsr0.2 type vlan egress 0:0 
ip link set hsr0.3 type vlan egress 0:7

Node-2

ifconfig hsr0 0.0.0.0
ip link add link hsr0 name hsr0.2 type vlan id 2
ip link add link hsr0 name hsr0.3 type vlan id 3
ifconfig hsr0.2 192.168.2.50
ifconfig hsr0.3 192.168.3.50
ip link set hsr0.2 type vlan egress 0:0
ip link set hsr0.3 type vlan egress 0:7

The above assume we have a network with two nodes connected back to back. The procedure is same if more than two nodes are present in the network. Using similar commands, user would be able to overlay multiple virtual LANs over the physical LAN created. The egress option of ip link command allow mapping packet priority to VLAN PCP values. In the example the packets on VLAN ID 2 is mapped to PCP value of 0 and VLAN ID 3 is mapped to PCP value of 7. At the Egress PRU Ethernet device looks at the PCP value and places it into one of the 4 queues. PRU scan the high priority queue first for packets and transmits them before transmitting packets from the lower priority queues. At the ingress, the PRU checks the PCP value of the packet in the VLAN header and places the frame into one of the ingress queues. More details on Queue usage is available at #Queue_Usage_and_VLAN_PCP_to_Queue_Map

In the above example, after passing some UDP traffic over hsr0.2 and hsr0.3, the user may check following statistics to verify if the packets are going over the right VLAN interface

On Node-1

cat /proc/net/vlan/hsr0.3
hsr0.3  VID: 3   REORDER_HDR: 1  dev->priv_flags: 1001
         total frames received        68090
          total bytes received     52598480
      Broadcast/Multicast Rcvd           52
      total frames transmitted        68090
       total bytes transmitted     52598459
Device: hsr0
INGRESS priority mappings: 0:0  1:0  2:0  3:0  4:0  5:0  6:0 7:0
 EGRESS priority mappings: 0:7
root@am57xx-evm:~# cat /proc/net/vlan/hsr0.2
hsr0.2  VID: 2   REORDER_HDR: 1  dev->priv_flags: 1001
        total frames received        68105
         total bytes received     52604702
      Broadcast/Multicast Rcvd           53

      total frames transmitted        68074
       total bytes transmitted     52583138
Device: hsr0
INGRESS priority mappings: 0:0  1:0  2:0  3:0  4:0  5:0  6:0 7:0
 EGRESS priority mappings: 0:0
root@am57xx-evm:~# cat /sys/kernel/debug/prueth-eth2/stats
   TxQ-0    TxQ-1    TxQ-2    TxQ-3    RxQ-0    RxQ-1
=====================================================
   68041        0        0    68908    67809    68925
root@am57xx-evm:~# cat /sys/kernel/debug/prueth-eth3/stats
   TxQ-0    TxQ-1    TxQ-2    TxQ-3    RxQ-2    RxQ-3
=====================================================
   68041        0        0    68912      234      695

Similar procedure can be used for setting up VLAN interfaces over PRU EMAC and HSR Ethernet types.



Net-SNMP

The TI SDK release ships tisdk-rootfs-image-am57xx-evm.tar.xz with Net-SNMP 5.7.3 binaries pre-installed and snmpd is started as part of the user space initialization. TI has developed a Net-SNMP module to support IEC-62439-3 related MIB access at the DAN using snmp commands such as snmpwalk, snmpget etc. NOTE: IEC-62439-3 MIB is supported only in the offloaded case. So user is expected to create HSR/PRP interface with offload. For details on how to setup HSR/PRP interface with offload, please refer HSR-PRP Offload

Command examples

An example snmpwalk command execution is shown below where 192.168.2.20 is the IP address of the remote DAN-P or DAN-H prp/hsr interface.

root@am57xx-evm:/etc/snmp# snmpwalk -v 2c -c public 192.168.2.20 iec62439
IEC-62439-3-MIB::lreManufacturerName.0 = STRING: TI LRE
IEC-62439-3-MIB::lreInterfaceCount.0 = INTEGER: 1
IEC-62439-3-MIB::lreRowStatus.1 = INTEGER: active(1)
IEC-62439-3-MIB::lreNodeType.1 = INTEGER: hsr(2)
IEC-62439-3-MIB::lreNodeName.1 = STRING: hsr0
IEC-62439-3-MIB::lreVersionName.1 = ""
IEC-62439-3-MIB::lreMacAddress.1 = STRING: d2:ef:e6:2a:1f:5b
IEC-62439-3-MIB::lrePortAdminStateA.1 = INTEGER: active(2)
IEC-62439-3-MIB::lrePortAdminStateB.1 = INTEGER: active(2)
IEC-62439-3-MIB::lreLinkStatusA.1 = INTEGER: up(1)
IEC-62439-3-MIB::lreLinkStatusB.1 = INTEGER: up(1)
IEC-62439-3-MIB::lreDuplicateDiscard.1 = INTEGER: discard(2)
IEC-62439-3-MIB::lreTransparentReception.1 = INTEGER: 0
IEC-62439-3-MIB::lreHsrLREMode.1 = INTEGER: modeh(1)
IEC-62439-3-MIB::lreSwitchingEndNode.1 = INTEGER: hsrnode(5)
IEC-62439-3-MIB::lreRedBoxIdentity.1 = INTEGER: id1a(2)
IEC-62439-3-MIB::lreEvaluateSupervision.1 = INTEGER: true(1)
IEC-62439-3-MIB::lreNodesTableClear.1 = INTEGER: noOp(0)
IEC-62439-3-MIB::lreProxyNodeTableClear.1 = INTEGER: noOp(0)
IEC-62439-3-MIB::lreDupListResideMaxTime.1 = INTEGER: 26214 binaryFractionOfSecond
IEC-62439-3-MIB::lreCntTxA.1 = Counter32: 7384
IEC-62439-3-MIB::lreCntTxB.1 = Counter32: 7385
IEC-62439-3-MIB::lreCntTxC.1 = Counter32: 4032
IEC-62439-3-MIB::lreCntErrWrongLanA.1 = Counter32: 0
IEC-62439-3-MIB::lreCntErrWrongLanB.1 = Counter32: 0
IEC-62439-3-MIB::lreCntErrWrongLanC.1 = Counter32: 0
IEC-62439-3-MIB::lreCntRxA.1 = Counter32: 4024
IEC-62439-3-MIB::lreCntRxB.1 = Counter32: 4025
IEC-62439-3-MIB::lreCntRxC.1 = Counter32: 0
IEC-62439-3-MIB::lreCntErrorsA.1 = Counter32: 3351
IEC-62439-3-MIB::lreCntErrorsB.1 = Counter32: 3351
IEC-62439-3-MIB::lreCntErrorsC.1 = Counter32: 0
IEC-62439-3-MIB::lreCntNodes.1 = INTEGER: 1
IEC-62439-3-MIB::lreCntProxyNodes.1 = INTEGER: 0
IEC-62439-3-MIB::lreCntUniqueA.1 = Counter32: 4
IEC-62439-3-MIB::lreCntUniqueB.1 = Counter32: 4
IEC-62439-3-MIB::lreCntUniqueC.1 = Counter32: 0
IEC-62439-3-MIB::lreCntDuplicateA.1 = Counter32: 0
IEC-62439-3-MIB::lreCntDuplicateB.1 = Counter32: 0
IEC-62439-3-MIB::lreCntDuplicateC.1 = Counter32: 3992
IEC-62439-3-MIB::lreCntMultiA.1 = Counter32: 0
IEC-62439-3-MIB::lreCntMultiB.1 = Counter32: 0
IEC-62439-3-MIB::lreCntMultiC.1 = Counter32: 0
IEC-62439-3-MIB::lreCntOwnRxA.1 = Counter32: 0
IEC-62439-3-MIB::lreCntOwnRxB.1 = Counter32: 0
IEC-62439-3-MIB::lreNodesMacAddress.1.1 = STRING: 70:ff:76:1c:f:8d
IEC-62439-3-MIB::lreTimeLastSeenA.1.1 = Timeticks: (0) 0:00:00.00
IEC-62439-3-MIB::lreTimeLastSeenB.1.1 = Timeticks: (1) 0:00:00.01
IEC-62439-3-MIB::lreRemNodeType.1.1 = INTEGER: danh(3)

Individual MIB variable may be queried or set using snmpset or snmpget commands. Below are some examples:- snmpset

snmpset -v 2c -c private 192.168.2.20 IEC-62439-3-MIB::lreHsrLREMode.1 i 3

snmpget

snmpget -v 2c -c public 192.168.2.20 IEC-62439-3-MIB::lreManufacturerName.0



MIB Support

MIB variable Group Actions Specified by Standard Action supported
lreManufacturerName lreConfigurationGeneralGroup get get
lreInterfaceCount lreConfigurationGeneralGroup get get
lreInterfaceConfigTable lreConfigurationInterfaceGroup NA NA
lreInterfaceConfigEntry lreConfigurationInterfaceGroup NA NA
lreInterfaceConfigIndex lreConfigurationInterfaceGroup NA NA
lreRowStatus lreConfigurationInterfaceGroup NA get
lreNodeType lreConfigurationInterfaceGroup get/set get
lreNodeName lreConfigurationInterfaceGroup get/set get
lreVersionName lreConfigurationInterfaceGroup get get
lreMacAddress lreConfigurationInterfaceGroup get/set get
lrePortAdminStateA lreConfigurationInterfaceGroup get/set get
lrePortAdminStateB lreConfigurationInterfaceGroup get/set get
lreLinkStatusA lreConfigurationInterfaceGroup get get
lreLinkStatusB lreConfigurationInterfaceGroup get get
lreDuplicateDiscard lreConfigurationInterfaceGroup get/set get/set
lreTransparentReception lreConfigurationInterfaceGroup get/set get/set
lreHsrLREMode lreConfigurationInterfaceGroup get/set get/set
lreSwitchingEndNode lreConfigurationInterfaceGroup get/set get
lreRedBoxIdentity lreConfigurationInterfaceGroup get/set NS
lreEvaluateSupervision lreConfigurationInterfaceGroup get/set NS
lreNodesTableClear lreConfigurationInterfaceGroup get/set get/set
lreProxyNodeTableClear lreConfigurationInterfaceGroup get/set NS
lreDupListResideMaxTime lreConfigurationInterfaceGroup get/set get
lreInterfaceStatsTable lreStatisticsInterfaceGroup NA NA
lreInterfaceStatsEntry lreStatisticsInterfaceGroup NA NA
lreInterfaceStatsIndex lreStatisticsInterfaceGroup NA Yes
lreCntTxA lreStatisticsInterfaceGroup get get
lreCntTxB lreStatisticsInterfaceGroup get get
lreCntTxC lreStatisticsInterfaceGroup get get
lreCntErrWrongLanA lreStatisticsInterfaceGroup get get
lreCntErrWrongLanB lreStatisticsInterfaceGroup get get
lreCntErrWrongLanC lreStatisticsInterfaceGroup get get
lreCntRxA lreStatisticsInterfaceGroup get get
lreCntRxB lreStatisticsInterfaceGroup get get
lreCntRxC lreStatisticsInterfaceGroup get get
lreCntErrorsA lreStatisticsInterfaceGroup get get
lreCntErrorsB lreStatisticsInterfaceGroup get get
lreCntErrorsC lreStatisticsInterfaceGroup get get
lreCntNodes lreStatisticsInterfaceGroup get get
lreCntProxyNodes lreStatisticsInterfaceGroup get NS
lreCntUniqueA lreStatisticsInterfaceGroup get get
lreCntUniqueB lreStatisticsInterfaceGroup get get
lreCntUniqueC lreStatisticsInterfaceGroup get get
lreCntDuplicateA lreStatisticsInterfaceGroup get get
lreCntDuplicateB lreStatisticsInterfaceGroup get get
lreCntDuplicateC lreStatisticsInterfaceGroup get get
lreCntMultiA lreStatisticsInterfaceGroup get get
lreCntMultiB lreStatisticsInterfaceGroup get get
lreCntMultiC lreStatisticsInterfaceGroup get get
lreCntOwnRxA lreStatisticsInterfaceGroup get get
lreCntOwnRxB lreStatisticsInterfaceGroup get get
lreNodesTable lreStatisticsInterfaceGroup NA Yes
lreNodesIndex lreStatisticsInterfaceGroup NA Yes
lreNodesMacAddress lreStatisticsInterfaceGroup get get
lreTimeLastSeenA lreStatisticsInterfaceGroup get get
lreTimeLastSeenB lreStatisticsInterfaceGroup get get
lreRemNodeType lreStatisticsInterfaceGroup get get
lreProxyNodeTable lreStatisticsInterfaceGroup NS
lreProxyNodeEntry lreStatisticsInterfacesGroup NA NS
lreProxyNodeMacAddress lreStatisticsInterfacesGroup get NS

Note NS: Not supported, NA: Not Applicable



iproute2

iproute2 is enhanced to allow creating a prp interface similar to hsr interface using two slave interfaces.

Linux PTP

Linux PTP documentation is available at [[5]]



Linux HSR/PRP Driver source code and Kconfig option

The driver source code is located under net/hsr-prp folder of the Linux source tree. To build kernel with this driver, set Kconfig option CONFIG_HSR_PRP=y in the dotconfig or enable it from the menu.



Supported Platforms

  • AM571x, AM572x IDK (Only eth2 and eth3)



Test Procedure

Testing HSR/PRP Firmware Offload

The setup of the IDKs for testing HSR/PRP firmware offload and the configuration of the HSR/PRP interfaces after kernel boot up are no different than the case without firmware offload. The differences are, in the case of firmware offload, the correct PRU firmware needs to be loaded and the PRUETH driver needs to be configured to interface with the type of firmware loaded, during boot up.

The module parameter "ti_prueth.pruss1_ethtype" and "ti_prueth.pruss2_ethtype" are used for instructing the PRU Ethernet driver what type of PRU firmware is to be loaded to PRU-ICSS1 and PRU-ICSS2 respectively. These type values are:

ti_prueth.prussX_ethtype, X = 1,2 firmware type
0 EMAC
1 HSR
2 PRP

These ti_prueth.prussX_type values can be set up in the Kernel boot argument in Uboot. For example, to load HSR firmware to PRU-ICSS1 and PRP firmware to PRU-ICSS2, and assuming boot using NFS rootfs, the Kernel boot argument can be configured as follows. Under Uboot prompt,

 => setenv netargs 'setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
ti_prueth.pruss1_ethtype=${pruss1_ethtype} ti_prueth.pruss2_ethtype=${pruss2_ethtype}'
 => setenv pruss1_ethtype 1
 => setenv pruss2_ethtype 2
 => saveenv

NOTE If using mmc rootfs, update args_mmc as below

 => setenv args_mmc 'run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
ti_prueth.pruss1_ethtype=${pruss1_ethtype} ti_prueth.pruss2_ethtype=${pruss2_ethtype}'

Just change the value of pruss1_ethtype or pruss2_ethtype in the above example to switch to a different type of firmware (see the above table). If a ti_prueth.prussX_ethtype is not configured, ie. does not appear in Kernel boot argument, the default EMAC firmware will be loaded to the corresponding PRU-ICSSX. In this case, if user sets up HSR/PRP interface, it will work without offload using the PRU EMAC firmware and driver. So using offload or no offload is controlled via selecting appropriate firmware at boot up and is transparent to user.

Remarks:

  1. Setting ti_prueth.prussX_ethtype to 0 is the same as not using it in the Kernel argument. In either case, default EMAC firmware is loaded.
  2. "ti_prueth.prussX_ethtype=", ie. setting the module parameter but without a value, is incorrect.
  3. On AM572x IDK, only PRU-ICSS2 is supported. Hence only prueth.pruss2_type takes effect.

To verify PRU Ethernet type after boot, do following that display TI PRU ethernet type

dmesg | grep "TI PRU ethernet (type"

For PRU Emac, the string displayed will be

prueth pruss2_eth: TI PRU ethernet (type 0) driver initialized

For PRU HSR, the string displayed will be

prueth pruss2_eth: TI PRU ethernet (type 1) driver initialized

For PRU PRP, the string displayed will be

prueth pruss2_eth: TI PRU ethernet (type 2) driver initialized

Where type is what is set in the bootargs and is listed in the table at the beginning of this section



Node Tables (firmware offload)

In the case of HSR/PRP firmware offload, the Node Table can be displayed as follows. Note: the locations are different from those when there is no firmware offload.

To show the HSR Node Table, under the kernel prompt on the terminal connected to the IDK, do

  • root@am57xx-evm:~# cat /sys/kernel/debug/prueth-hsr/node_table
  • Sample display
 root@am57xx-evm:~# cat /sys/kernel/debug/prueth-hsr/node_table 
 
 Remote nodes in network: 1
 
 Node[1]:
 MAC ADDR: 70:ff:76:1c:0f:99
 state: valid
 DANH
 RxA=2992 SupRxA=148
 RxB=2992 SupRxB=148
 Time Last Seen: Sup=0 RxA=0 RxB=0

To show the PRP Node Table, under the kernel prompt on the terminal connected to the IDK, do

  • root@am57xx-evm:~# cat /sys/kernel/debug/prueth-prp/node_table
  • Sample display
 root@am57xx-evm:~# cat /sys/kernel/debug/prueth-prp/node_table 
 
 Remote nodes in network: 1
 
 Node[1]:
 MAC ADDR: 70:ff:76:1c:0f:99
 state: valid
 DupDiscard (0x80)
 DANP
 RxA=17 SupRxA=17
 RxB=17 SupRxB=17
 Time Last Seen: Sup=0 RxA=0 RxB=0
 PRP LineID Err: A=0 B=0

LRE Statistics (firmware offload)

The LRE statistics is displayed as part the interface statistics using the "ethtool -S DEVNAME" command, where DEVNAME, in the case AM572x IDK, is eth2 or eth3. The fields pertaining to LRE statistics are prefixed with "lre". Since LRE statistics are LRE specific, instead of interface specific, so either "ethtool -S eth2" or "ethtool -S eth3" will show the same LRE statistics.

Sample display:

 root@am57xx-evm:~# ethtool -S eth2     
 NIC statistics:
      txBcast: 1
      txMcast: 11635
      txUcast: 3
      txOctets: 816642
      rxBcast: 0
      rxMcast: 36
      rxUcast: 17
      rxOctets: 4841
      tx64byte: 6
      tx65_127byte: 11633
      tx128_255byte: 0
      tx256_511byte: 0
      tx512_1023byte: 0
      tx1024byte: 0
      rx64byte: 4
      rx65_127byte: 49
      rx128_255byte: 0
      rx256_511byte: 0
      rx512_1023byte: 0
      rx1024byte: 0
      lateColl: 0
      singleColl: 0
      multiColl: 0
      excessColl: 0
      rxMisAlignmentFrames: 0
      stormPrevCounter: 0
      macRxError: 0
      SFDError: 0
      defTx: 0
      macTxError: 0
      rxOverSizedFrames: 0
      rxUnderSizedFrames: 0
      rxCRCFrames: 0
      droppedPackets: 0
      txHWQOverFlow: 0
      txHWQUnderFlow: 0
      lreTxA: 11636
      lreTxB: 11639
      lreTxC: 66
      lreErrWrongLanA: 0
      lreErrWrongLanB: 0
      lreErrWrongLanC: 0
      lreRxA: 40
      lreRxB: 40
      lreRxC: 0
      lreErrorsA: 11560
      lreErrorsB: 11559
      lreErrorsC: 0
      lreNodes: 0
      lreProxyNodes: 0
      lreUniqueRxA: 0
      lreUniqueRxB: 0
      lreUniqueRxC: 0
      lreDuplicateRxA: 0
      lreDuplicateRxB: 0
      lreDuplicateRxC: 0
      lreMultiRxA: 0
      lreMultiRxB: 0
      lreMultiRxC: 0
      lreOwnRxA: 0
      lreOwnRxB: 0
      lreDuplicateDiscard: 2
      lreTransRecept: 1
      lreNtLookupErrA: 0
      lreNtLookupErrB: 0
      lreNodeTableFull: 0

HSR Testing

To test HSR, user would need two AM572x EVMs.

  1. Setup HSR Ring network as per diagram below. Connect the PRU2ETH0 (See the marking on the EVM) Ethernet ports of the two EVMs together (corresponds to Linux interface eth2) as shown below. Similarly, connect the PRU2ETH1 ports (Linux interface eth3) as well.
  2. Configure the bootargs to boot PRU with HSR firmware as described above at Processor_SDK_Linux_HSR_PRP#Testing_HSR.2FPRP_Firmware_Offload
  3. Boot the EVMs using the pre-built images from the Processor SDK release. These images are built with Linux HSR/PRP driver enabled. Login to the console using root user name.
  4. Note the MAC Address of eth2 at DAN-H-1(Say MAC-A) using the ifconfig command. Do ifconfig eth2 at the Linux console of DAN-H-1
  5. Note the MAC Address of eth2 at DAN-H-2(Say MAC-B) using the ifconfig command. Do ifconfig eth2 at the Linux console of DAN-H-2
    1. ifconfig eth2 down
    2. ifconfig eth3 down
    3. ifconfig eth3 hw ether <MAC-A>
    4. ifconfig eth2 up
    5. ifconfig eth3 up
    6. ip link add name hsr0 type hsr slave1 eth2 slave2 eth3 supervision 45 version 1
    7. ifconfig hsr0 <IP Address of hsr interface at DAN-H-1> up
  6. Repeat the above steps for DAN-H-2, but this time use MAC-B in step 4.3 above. And use IP Address from the same subnet as that of DAN-H-1 hsr interface hsr0.

Hsr-network-setup-v2.jpg

For example use Ip Address 192.168.2.20 for DAN-H-1 and 192.168.2.30 for DAN-H-2. Assume CPSW ports at the EVM are on a different Subnet than the HSR interface.

Once both hsr0 interfaces are created, user should be able to do a ping from DAN-H-1 to DAN-H-2 or vice-versa. Disconnect Ethernet cable at eth2 or eth3. The Ping should continue to go through. User could run iperf between the two HSR interfaces and test the iperf is not affected when one of the cable is disconnected. This verifies redundancy.

A Sample script that automates the steps 4.1 to 4.7, say setup.sh, is below



#!/bin/sh
if [ $# -lt 3 ]
then
        echo "setup.sh <hsr/prp> <MAC-Address for both slaves> <ip address for hsr/prp interface>"
        exit
fi
  
if [ "$1" != "hsr" ] && [ "$1" != "prp" ]
then
    echo "use hsr or prp as first argument"
    exit
fi
 
echo "Setting up $10 interface with MAC address $2 for slaves and IP address $3"
 
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth2 hw ether $2
ifconfig eth3 hw ether $2
ifconfig eth2 up
ifconfig eth3 up
 
if [ "$1" == "hsr" ]
then
        ip link add name hsr0 type hsr slave1 eth2 slave2 eth3 supervision 45 version 1
        ifconfig hsr0 $3 up
else
        ip link add name prp0 type prp slave1 eth2 slave2 eth3 supervision 45
        ifconfig prp0 $3 up
fi

Using this script, user can setup hsr interface as

 
/setup.sh hsr <MAC-A> <IP Address of the interface>

where it is assumed that the setup.sh is copied to the root directory of the target file system and is made executable

Below script can be used to teardown the hsr interface (say teardown.sh)


#!/bin/sh
if [ $# -lt 1 ]
then
        echo "teardown.sh <hsr/prp>"
        exit
fi

if [ "$1" != "hsr" ] && [ "$1" != "prp" ]
then
    echo "use hsr or prp as first argument"
    exit
fi

if [ "$1" == "hsr" ]
then
        ip link del hsr0
else
        ip link del prp0
fi

Using the above script, user teardown the hsr interface as


/teardown.sh hsr

Sample logs are shown here DAN-H-1, DAN-H-2



PRP Testing

Prp-network-setup.jpg

For Testing PRP, user is required to use the setup shown in the above diagram. A DAN-P is attached to two independent networks (A and B) each of which is shown as a separate Ethernet switch. Do the following steps to setup the prp interface. Note that in the below example Linux interface eth2 is Link-A (slave1 in ip link command) and eth3 is Link-B (slave2 in ip link command). Link-A is the Ethernet cable that connects DUT to Switch A and Link-B is the Ethernet cable that connects to Switch-B. This is very important for PRP as swapping them is an incorrect connection and can produce undesirable results.

  1. Connect the DAN-P-1 EVM, PRU2ETH0 (marking on EVM) to a port at Ethernet switch A and PRU2ETH1 to a port at Ethernet switch B
  2. Similarly, connect DAN-P-2 EVM, PRU2ETH0 to a port at Ethernet switch A and PRU2ETH1 to a port at Ethernet switch B
  3. Configure the PRU to load PRP firmware by setting env variable as discussed at Processor_SDK_Linux_HSR_PRP#Testing_HSR.2FPRP_Firmware_Offload
  4. Boot the EVMs using the pre-built images from the Processor SDK release. These images are built with Linux HSR/PRP driver enabled. Login to the console using root user name.
  5. This time user may use the script (setup.sh) to create the prp interface. Note the MAC-A and MAC-B as in the case of HSR (MAC address of eth2)
  6. setup the prp interface at DAN-P-1 as follows
    1. /setup.sh prp <MAC-A> <IP Address of prp interface>
  7. setup the prp interface at DAN-P-2 as follows:-
    1. /setup.sh prp <MAC-B> <IP Address of prp interface>

If PRP interface uses IP address 192.168.2.20 and eth2 MAC address is 70:ff:76:1c:0f:8d, following example command may be used at DAN-P-1

/setup.sh prp 70:ff:76:1c:0f:8d 192.168.2.20

If PRP interface uses IP address 192.168.2.30 and eth2 MAC address is 70:ff:76:1c:0f:8e following example command may be use at DAN-P-2

/setup.sh prp 70:ff:76:1c:0f:8e 192.168.2.30

To teardown the prp interface do

/teardown.sh prp

Sample logs are shown here DAN-P-1, DAN-P-2



Performance Test and Logs

Boot up two AM571x/572x EVM to configure PRU Ethernet in HSR or PRP mode as described at Processor_SDK_Linux_HSR_PRP#Testing_HSR.2FPRP_Firmware_Offload. They are connected over eth2 and eth3 as described in Processor_SDK_Linux_HSR_PRP#HSR Test or Processor_SDK_Linux_HSR_PRP#PRP Test

UDP

Sample iperf UDP test showing no packet loss for MTU sized packets. For HSR/PRP, there are 6 bytes of Tag effectively reducing pay load size to 1466 (1500 - 6 - 20 - 8)

Server Side

root@am57xx-evm:~# iperf -s -u
------------------------------------------------------------
Server listening on UDP port 5001
Receiving 1470 byte datagrams
UDP buffer size:  160 KByte (default)
------------------------------------------------------------
[  3] local 192.168.2.20 port 5001 connected with 192.168.2.30 port 34255
[ ID] Interval       Transfer     Bandwidth        Jitter   Lost/Total Datagrams
[  3]  0.0-60.0 sec   630 MBytes  88.1 Mbits/sec   0.002 ms    0/450887 (0%)
[  3]  0.0-60.0 sec  1 datagrams received out-of-order

Client side

root@am57xx-evm:~# iperf -c 192.168.2.20 -u -b88M -l1466 -t60
------------------------------------------------------------
Client connecting to 192.168.2.20, UDP port 5001
Sending 1466 byte datagrams
UDP buffer size:  160 KByte (default)
------------------------------------------------------------
[  3] local 192.168.2.30 port 34255 connected with 192.168.2.20 port 5001
[ ID] Interval       Transfer     Bandwidth
[  3]  0.0-60.0 sec   630 MBytes  88.1 Mbits/sec
[  3] Sent 450888 datagrams
[  3] Server Report:
[  3]  0.0-60.0 sec   630 MBytes  88.1 Mbits/sec   0.002 ms    0/450887 (0%)
[  3]  0.0-60.0 sec  1 datagrams received out-of-order

NOTE: When doing UDP test, user may observe out of order packets sometimes. This is normal as the driver doesn't use NAPI and packets may get queued to backlog queues of each CPU which may get delivered out of sequence to the iperf application. Out of order delivery of UDP packets are normal and kernel doesn't guarantee in sequence delivery of UDP packets to application. So iperf may show some packets lost during the test. User may use some of the tools available to migrate the rx irq threads and iperf server to same CPU, example CPU 0, to mitigate out of order issue and get a no loss iperf stats for udp tests.

For example, here is a snapshot of the test that shows packet lost during the test. The test also shows 106 datagram received out of order.

root@am57xx-evm:~# iperf -s -u
------------------------------------------------------------
Server listening on UDP port 5001
Receiving 1470 byte datagrams
UDP buffer size:  160 KByte (default)
------------------------------------------------------------
[  3] local 192.168.2.30 port 5001 connected with 192.168.2.20 port 41976
[ ID] Interval       Transfer     Bandwidth        Jitter   Lost/Total Datagrams
[  3]  0.0-600.0 sec  6.15 GBytes  88.0 Mbits/sec   0.004 ms    5/4501411 (0.00011%)
[  3]  0.0-600.0 sec  106 datagrams received out-of-order


Here is how to re-run the test by migrating the iperf server and irq threads to CPU 0

Run the iperf -s -u & Do ps command and find the PID of the iperf and migrate the process to CPU 0 as follows

root@am57xx-evm:~# ps
 PID TTY          TIME CMD
 964 ttyS2    00:00:00 login
1063 ttyS2    00:00:00 sh
1135 ttyS2    00:00:00 iperf
1141 ttyS2    00:00:00 ps
root@am57xx-evm:~# taskset -cp 0 1135
pid 1135's current affinity list: 0,1
pid 1135's new affinity list: 0

Now find the irq thread for eth2, eth3 devices using

root@am57xx-evm:~# ps -ef  | grep "eth3"
root      1464     2  0 06:01 ?        00:00:00 [irq/498-eth3]
root      1495  1065  0 06:04 ttyS2    00:00:00 grep irq/498-eth3
root@am57xx-evm:~# ps -ef  | grep "eth2"
root      1462     2  0 06:01 ?        00:00:00 [irq/496-eth2]
root      1497  1065  0 06:04 ttyS2    00:00:00 grep irq/496-eth2

In the above example 1462 is the process id of irq/496-eth2 thread and 1464 is the process ID of irq/498-eth3 . Do following to migrate them to CPU 0.

root@am57xx-evm:~# taskset -cp 0 1464
pid 1464's current affinity list: 0,1
pid 1464's new affinity list: 0
root@am57xx-evm:~# taskset -cp 0 1462
pid 1462's current affinity list: 0,1
pid 1462's new affinity list: 0
root@am57xx-evm:~#
root@am57xx-evm:~#

Now start iperf client on the other side. The server side log below with these tuning shows no packet loss.

[  4] local 192.168.2.30 port 5001 connected with 192.168.2.20 port 36415
[  4]  0.0-600.0 sec  6.15 GBytes  88.0 Mbits/sec   0.007 ms    0/4501355 (0%)
[  4]  0.0-600.0 sec  1 datagrams received out-of-order


UDP Performance for HSR
Packet Size Tput with no packet loss (Mbits/sec)
1466 88
1024 88
512 64
256 45
UDP Performance for PRP
Packet Size Tput with no packet loss (Mbits/sec)
1466 88
1024 88
512 60
256 38


NOTE-1:Test ran for 1 minute with single direction traffic (Client to Server). Reduced the traffic from 88Mbits/sec until there is no out of order or lost packets in the iperf stats

TCP

HSR

Server side

root@am57xx-evm:~# iperf -s   
------------------------------------------------------------
Server listening on TCP port 5001
TCP window size: 85.3 KByte (default)
------------------------------------------------------------
[  4] local 192.168.2.20 port 5001 connected with 192.168.2.30 port 54148
[ ID] Interval       Transfer     Bandwidth
[  4]  0.0-60.0 sec   663 MBytes  92.7 Mbits/sec


Client side

root@am57xx-evm:~# iperf -c 192.168.2.20  -t60
------------------------------------------------------------
Client connecting to 192.168.2.20, TCP port 5001
TCP window size: 43.8 KByte (default)
------------------------------------------------------------
[  3] local 192.168.2.30 port 54148 connected with 192.168.2.20 port 5001
[ ID] Interval       Transfer     Bandwidth
[  3]  0.0-60.0 sec   663 MBytes  92.7 Mbits/sec

PRP

Server side

root@am57xx-evm:~# iperf -s
------------------------------------------------------------
Server listening on TCP port 5001
TCP window size: 85.3 KByte (default)
------------------------------------------------------------
[  4] local 192.168.2.20 port 5001 connected with 192.168.2.30 port 54150
[ ID] Interval       Transfer     Bandwidth
[  4]  0.0-60.0 sec   660 MBytes  92.3 Mbits/sec

Client side

root@am57xx-evm:~# iperf -c 192.168.2.20 -t60               
------------------------------------------------------------
Client connecting to 192.168.2.20, TCP port 5001
TCP window size: 43.8 KByte (default)
------------------------------------------------------------
[  3] local 192.168.2.30 port 54150 connected with 192.168.2.20 port 5001
[ ID] Interval       Transfer     Bandwidth
[  3]  0.0-60.0 sec   660 MBytes  92.3 Mbits/sec

Redundancy Test and Logs

For HSR and PRP redundancy is implemented using duplicate links and sending frame over both links and discarding the duplicate at the receive side. The test requires two DAN-P or DAN-H nodes connected over eth2 and eth3 Ethernet Links. Boot up the EVM with bootargs set to configure PRU Ethernet in HSR or PRP mode as described at Processor_SDK_Linux_HSR_PRP#Testing_HSR.2FPRP_Firmware_Offload Do an iperf UDP test at 88Mbits/sec for MTU sized packets (size = 1466) and then pull out either eth2 or eth3 Ethernet cable. Make sure iperf stats doesn't show packet loss during the test period. Here is the log for HSR that show link failed during the test and there was no packet loss.

eth3 link failed

root@am57xx-evm:~# iperf -c 192.168.2.20 -u -b88M -l1466 -t60
------------------------------------------------------------
Client connecting to 192.168.2.20, UDP port 5001
Sending 1466 byte datagrams
UDP buffer size:  160 KByte (default)
------------------------------------------------------------
[  3] local 192.168.2.30 port 50443 connected with 192.168.2.20 port 5001
[  108.740402] prueth pruss2_eth eth3: Link is Down
[ ID] Interval       Transfer     Bandwidth
[  3]  0.0-60.0 sec   631 MBytes  88.2 Mbits/sec
[  3] Sent 451002 datagrams
[  3] Server Report:
[  3]  0.0-60.0 sec   631 MBytes  88.2 Mbits/sec   0.003 ms    0/451001 (0%)
[  3]  0.0-60.0 sec  1 datagrams received out-of-order
root@am57xx-evm:~# [  181.444988] prueth pruss2_eth eth3: Link is Up - 100Mbps/Full - flow control off

eth2 link failed

root@am57xx-evm:~# iperf -c 192.168.2.20 -u -b88M -l1466 -t60
------------------------------------------------------------
Client connecting to 192.168.2.20, UDP port 5001
Sending 1466 byte datagrams
UDP buffer size:  160 KByte (default)
------------------------------------------------------------
[  3] local 192.168.2.30 port 49260 connected with 192.168.2.20 port 5001
[  204.253286] prueth pruss2_eth eth2: Link is Down
[ ID] Interval       Transfer     Bandwidth
[  3]  0.0-60.0 sec   631 MBytes  88.2 Mbits/sec
[  3] Sent 451028 datagrams
[  3] Server Report:
[  3]  0.0-60.0 sec   631 MBytes  88.2 Mbits/sec   0.005 ms    0/451027 (0%)
[  3]  0.0-60.0 sec  1 datagrams received out-of-order
root@am57xx-evm:~# uname -a
Linux am57xx-evm 4.9.41-rt23-gc038d21a22 #2 SMP PREEMPT RT Wed Sep 27 06:34:09 EDT 2017 armv7l GNU/Linux



Useful Commands

For Non offload case following commands are available. To dump stats

  • cat /sys/kernel/debug/hsr/stats

To dump Node_Table

  • cat /sys/kernel/debug/hsr/node_table

For PRP, replace hsr in the above paths with prp

For Offloaded case following commands are available to change mode To change HSR mode do both commands below.

  • echo 1 > /sys/kernel/debug/hsr/hsr_mode
  • echo 1 > /sys/kernel/debug/prueth-prp/hsr_mode

To see the node table entries for offloaded case, do

  • cat /sys/kernel/debug/prueth-prp/new_nt_bins

or

  • cat /sys/kernel/debug/prueth-hsr/new_nt_bins

where 1 is for Mode-H

Other values are 2 (Mode-N), 3 (Mode-T), 4 (Mode-U), 5 (Mode-M)



FAQ

  1. How to disable udhcpc from sending DHCP request over prueth Ethernet interfaces (eth2-eth3) when it is configured to run HSR/PRP protocol in firmware?

Linux HSR/PRP driver uses the eth2/eth3 interface as slave interfaces to implement the protocol on top of it. Application is expected to send or receive packets over the hsr or prp lre interface also known as C port. However prueth also support plain Ethernet and the file system /etc/systemd/network/10-eth.network has a general rule to enable DHCP over all of the interface matching eth*. Modify the file to match unique name instead of generic name wild cards. For example to do DHCP over only eth0 interface, 10-eth.network may be modified as follows:-

root@am57xx-evm:~# cat /etc/systemd/network/10-eth.network

[Match]
Name=eth0
KernelCommandLine=!root=/dev/nfs

[Network]
DHCP=yes

To do DHCP over hsr0 or prp0 interfaces, user may add additional files to /etc/systemd/network/ one for each prp0 or hsr0 similar to eth0, by using a Match name string of hsr0 or prp0. More details on this is at [[6]]