Processor SDK Linux Migration Guide

From Texas Instruments Wiki
Jump to: navigation, search

Ti stk 1c rev rgb png.png

Last updated: 12/21/2017


Linux Software Developer's Guide Migration Guide




Overview

This page covers migration information for applications built on top of the Processor SDK for Linux.

Processor SDK Linux 04.02.00

Linux

PRUETH Driver

The module parameter syntax has changed from "prueth.pruss1_ethtype" and "prueth.pruss2_ethtype" in older release to "ti_prueth.pruss1_ethtype" and "ti_prueth.pruss2_ethtype".

Processor SDK Linux 04.01.00

IPC

PRUSS remoteproc

  • PRUs are no longer automatically booted (remoteproc 'auto_boot' is set to false) by remoteproc core. A PRU has to be booted either by PRU Client Drivers or a PRU applications in userspace. The kernel-space boot is triggered using the rproc_boot() kernel API, and the user-space applications can use the sysfs to start and stop the corresponding remoteproc. Please see Documentation/ABI/testing/sysfs-class-remoteproc file in kernel for sysfs usage details.
  • PRU remoteproc driver no longer configures the PRU Ethernet firmwares automatically using board-machine compatibles. The needed firmware names are configured by the PRU Ethernet driver now using the rproc_set_firmware() function.
  • Userspace PRU applications have to make sure to unload any existing PRU client drivers using a specific PRU, and set their firmware using sysfs before starting and using a PRU



Processor SDK Linux 04.00.00

  • This is the first release for 2017 LTS (Kernel: 4.9, U-boot: 2017.01, gcc: 6.2.1 and Yocto: 2.2 (morty)), with following major changes.

IPC

remoteproc

  • The debugfs 'state' variable is replaced with a sysfs 'state' variable accepting 'start' and 'stop' to boot and shutdown a remote processor from userspace
  • A new sysfs variable 'firmware' is also added to set a new firmware. remoteprocs need to be in stopped state before a firmware can be set. New firmwares still need to reside in /lib/firmware
  • Booting a remote processor is now triggered by the insertion of the respective remoteproc platform driver. On 4.4, with virtio-rpmsg enabled firmwares, this only happened when both the remoteproc platform driver and virtio_rpmsg_bus module were installed.
  • Upstream 4.9 remoteproc and rpmsg cores are not suitable for TI platforms. A minimum of 4.10-rc4 (or the required remoteproc/rpmsg patches from 4.10-rc4) is needed if porting TI remoteproc drivers onto upstream.

rpmsg

  • virtio_rpmsg_bus module split into a 'rpmsg_core' and virtio-rpmsg transport specific 'virtio_rpmsg_bus' modules.
  • Removal of virtio_rpmsg_bus no longer stops a remote processor and should be avoided if a remote processor is running. * If removed and installed again, the rpmsg communication devices will not be reprobed.

Keystone_remoteproc

  • A new 'label' binding property is now mandatory. It will have the string names for the DSPs in the format "dsp<X>" (eg: dsp0, dsp7 etc)
  • K2G DSP nodes will require a new "ti,sci-id" property, and a different value for "power-domains" property (this is generic to all K2G devices)

PRUSS remoteproc

  • The AM437x specific am437x_pruss_wrapper module has been replaced with a generic pruss_soc_bus module, and is required to be installed on all SoCs.
  • New compatibles on AM335x and AM437x SoCs - The previous 'am3352-xxx' and 'am4372-xxx' have been replaced with a 'am3356-xxx' and 'am4376-xxx' compatibles since PRUSS are not present on AM3352 and AM4372 SoCs. The PRU nodes are also not enabled by default in base 'am33xx.dtsi' and 'am4372.dtsi' files.
  • New device hierarchy structure - The PRUSS node hierarchy from 4.4 is moved one-level down under a new parent pruss_soc_bus node.

CPSW CPDMA Descriptor Usage

There is a notable change in how to place cpsw cpdma descriptors in DDR and configure descs number: TI K4.4 device tree property was used "descs_pool_size" - descs_pool_size : total number of CPDMA CPPI descriptors to be used for both ingress/egress packets processing. if not specified the default value 256 will be used which will allow to place descriptors pool into the internal CPPI RAM.

New approach http://processors.wiki.ti.com/index.php/Linux_Core_CPSW_User%27s_Guide#Configure_number_of_TX.2FRX_descriptors

PCI ENDPOINT

The usage of 'pci-ep' configfs directory to configure PCI Endpoint has been changed in accordance with upstream review comments. Please see http://processors.wiki.ti.com/index.php/Linux_Core_PCIe_EP_User%27s_Guide#4.9_Kernel, for additional details

Display

fbdev is only set up for the primary display, instead of all displays. This results in the secondary displays to be left disabled by the kernel, until an userspace application enables the displays.

U-Boot RNDIS boot

AM335x USB client (RNDIS) boot and Ethernet boot modes are now supported using default defconfig (am335x_evm_defconfig). Similarly AM437x USB client (RNDIS) boot is now supported by am43xx_evm_defconfig. Separate defconfigs for above boot modes no longer exist.

Keystone-2 features

The following features are not ported to 2017 LTS

  • SRIO Kernel driver
  • 10G Uboot
  • IPSec sideband and inflow mode
  • QoS



Processor SDK Linux 03.03.00

  • HDMI-connected monitor no longer takes precedence over built-in LCD as a default graphics display for e.g. Matrix
  • See the Release Notes for full list of modifications.


Processor SDK Linux 03.02.00

  • The QT QPA eglfs_kms, which supports multiple screens, has been enabled and used as the default eglfs platform plugin. For more information, see QT and Graphics Migration
  • bootmonitor now goes thru mkimage and as a result the load address changed. Users should manually execute following commands in their u-boot environment to properly install the secure monitor on k2 platforms:
setenv addr_mon 0xc08000
setenv addr_mon_mkimg 0xc07ffc0
setenv mon_size 0x1210
setenv sec_bm_install 'go ${addr_mon}4 0xc084000 ${mon_size}; mon_install ${addr_mon_mkimg}'
run sec_bm_install
  • HDMI-connected monitor no longer takes precedence over built-in LCD as a default graphics display for e.g. Matrix


Processor SDK Linux 03.01.00

  • defconfig_builder is now used to generate working kernel defconfigs
  • In K2 U-Boot, added multi slave support.
  • In K2 Linux PA driver, added pre-classification support. So explicit lut rules for broadcast and multicast are removed and the same is achieved through this feature in PA
  • 10G Ethernet driver now supports auto configuration using MCU firmware (a.k.a 10G KR firmware). The firmware file name is ks2_xgbe_serdes_mcu_fw.bin which is available at the same location as other serdes firmwares.
  • The current version of the serdes firmware is 03.03.00.02C and the same is not backward compatible with the firmware in the previous SDK release (03.00.00)


Processor SDK Linux 03.00.00

  • First 2016 LTS Release (Linux Kernel: 4.4, U-Boot: 2016.05, GCC 5.3, Yocto 2.1)
  • Unified kernel configuration based on multi_v7_defconfig
  • Migrated from SysVinit to systemd for user space initialization.
  • U-Boot drivers now uses DT, but is transparent to users
  • The content of <evm>-<os>-sdk-arago-src-<ver>.tar.gz on the download page changed from sources to a fetcher script that obtains the sources. This is to efficiently share the sources between different platforms and OSes supported by Processor SDK. See the README inside the tar-ball for instructions
  • This release adds support for RT Linux on AM335x ICE and K2G GPEVM
  • In K2 U-Boot, multi slave support is currently missing. To use multiple interfaces, please disable CONFIG_DM_ET option in u-boot .config and build.
  • See the Release Notes for full list of modifications.
  • For information on migrating from MCSDK (K2x) to Processor SDK, see this migration page.


Processor SDK Linux 02.00.02

  • This release adds RT Linux support on AM335x, K2H/K, K2E, K2L
  • This release supports AM572x IDK and K2G EVM
  • OpenCV now uses OpenCL under the hood, to offload compute tasks to C66x cores. This is transparent to the application
  • The SGX driver for AM335x has been enhanced to support DRM/WAYLAND based Multi-Window Display. For more information, see AM3 Graphics Migration
  • See the Release Notes for full list of modifications.
  • For information on migrating from MCSDK (K2x) to Processor SDK, see this migration page.


Processor SDK Linux 02.00.01

  • This release adds support for devices from the KeyStone architecture: K2E, K2H/K, and K2L
  • This release also supports RT Linux is supported on AM4 and AM5 device
  • The SGX driver for AM4 has been enhanced to support DRM/WAYLAND based Multi-Window Display. For more information, see AM4 Graphics Migration
  • There is no migration impact to customers using AM3, and AM5.
  • See the Release Notes for full list of modifications.
  • For information on migrating from MCSDK (K2x) to Processor SDK, see this migration page.


Processor SDK Linux 02.00.00

  • This release adds support for AM57x
  • First 2015 LTS (Kernel 4.1, U-boot 2015.07) Release
  • Starting this release, Processor SDK Installer is 64-bit, and installs only on 64-bit host machine. Support for 32-bit host is dropped as Linaro toolchain is available only for 64-bit machines
  • For AM3, AM4, Graphics SDK is now obsolete and Graphics stack is integrated into Processor SDK, and supports null DRM based Full Window, with Front and Flip modes. For more information, see Graphics Migration
  • Ethernet performance degraded ~10% on am335x-evm due to move from preempt_voluntary
  • See the Release Notes for full list of modifications.