Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK Posix-SMP Demo

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide Posix-SMP Demo




Introduction

This page describes the SMP/Posix demo provided in the Processor-SDK for RTOS and Linux. This demo uses Posix APIs together with a simple benchmark (Dhrystone) to automatically calculate the effective throughput of all the cores in each SMP cluster. SMP mode is only supported on Coretex-A15 cores.

This demo runs on:

  • AM572x (A15, C66, M4)
  • AM437x (A9)
  • AM335x (A8)
  • K2H (A15, C66)
  • K2E (A15, C66)
  • K2G (A15, C66)
  • K2L (A15, C66)
  • C6678 (C66)
  • C6657 (C66)

The sections below provide details of the application as well as build and run instructions.


Requirements

The following materials are required to run this demonstration:

Hardware

  • TI EVM (see list above)
  • Serial UART cable (provided in EVM kit)

Software

  • Processor-SDK RTOS
  • Code Composer Studio


Software Design

The demo is based on Dhrystone 2.1 from link.

The purpose of the demo is two-fold. First, it is to show easy scaling of throughput across cores in a SMP cluster when running TI-RTOS. Second, it shows easy portability of Posix threads between TI-RTOS and Linux.

The overall requirement is discover all parameters automatically without user input, and to minimize the amount of code that must be customized between TI-RTOS and Linux. This demonstrates that the same Posix threads as well as their setup/control code can be run on either TI-RTOS or Linux with minimal effort.

In order to accomplish this, several major modifications were made to Dhrystone in order to "threadify" it. Some of these changes slightly affect the results compared to an unmodified version. Thus this modified version should be run on all processors where comparisons will be drawn.

  • Removal of most printf() during normal operation. Original code dumped all final values for the user to verify. Changed to programmatic verification. Only printf() for actual results (DMIPS and Dhrystones) preserved.
  • Removal of all global variables. They are accessed through an "inst" pointer instead.
  • Adaptive discovery of iteration count. Original code used a #define. This version doubles iteration count until execution time is about 10M timer ticks.
  • Adaptive discovery of number of cores in SMP cluster. Original code didn't use threads. This version doubled number of threads until cumulative DMIPS flattens out.

POSIX barriers are used inside the timed portion of the code. This is not to time the performance of the barrier, but is instead used to time how long all threads together take to complete. It is assumed the execution times of the threads (> 0.1 second) are orders of magnitude more than the barrier, so the barrier's effect on results is negligible.

Processor SDK uses makefiles for TI-RTOS and Yocto recipes for Linux for the supported EVMs. The makefile can also be used to compile native builds for Linux (both for EVMs and x86).

For more information on TI-RTOS Posix, see POSIX Support.


How to Run the Demo

The processor SDK includes pre-built binaries which may be loaded and run using the SBL with UART or using CCS with UART or ROV (UART display for newer versions and ROV for older versions). To run using UART, hook up to the board using UART and run the .out file.

Figure 1, UART demo result

To run using CCS, use the following steps. Each binary has an associated *.rov.xs file located in the same directory--enabling the CCS ROV tool. Newer versions will display directly to the UART console and any steps involving ROV may be skipped.

<SDK_INSTALL_PATH>/processor_sdk_rtos_<platform>_2_00_xx_xx/demos/posix-smp/bin/<platform>/<core>/debug/dhry.out
<SDK_INSTALL_PATH>/processor_sdk_rtos_<platform>_2_00_xx_xx/demos/posix-smp/bin/<platform>/<core>/debug/dhry_pa15fg.rov.xs

For all platforms and core types, the basic procedure for running the demo will be the same:

  1. Using CCS, launch the target configuration for the EVM CCS-Target Configurations. Please ensure that the target configuration will load the appropriate CCS gel files found in the emupak.
  2. The default ccxml file only loads a gel on connect for some of the cores. Modify the ccxml file to load the gel for all the corresponding cores.
  3. In the CCS debug view, group and then connect to all cores of device that you wish to test on (i.e. - all of the clustered A15 cores).
  4. For each, core load the dhry.out file. The principle core should halt at main while the SMP linked cores will begin auto-running upon load.
  5. Once all cores have been loaded, run all the cores.
  6. The output will be sent to the UART console in real time.
  7. The demo should not take more than a few minutes to run. You must manually halt the cores to end the demo.

If using Processor-SDK 3.0 or later,

  1. Open the ROV window (Tools > RTOS Object View (ROV)) and view the SysMin module to inspect the output of the demo. If you see the below message, please specify the XDC and SYSBIOS versions:

Use rov 1.jpg

Use rov 2.png

Figure 2, ROV of demo result

The output buffer shown in the ROV contains the different stages of the demo's progression:

  1. The demo finds an appropriate number of iterations for the device.
  2. The demo begins to add threads.
  3. The demo concludes when adding additional threads does not further increase the DMIPS.

The output takes the form of: "xxxxxxx iterations *n threads; dhrystones xxxxxxxx, dmips = xxxx". In the screenshot above, moving from two threads to four threads does not appreciably improve the DMIPS, so the demo completes. This behavior is expected because the demo is only running on two cores in this example.

NOTE

  • A15 cores may usually be connected to directly; on the AM572x, the M4 IPUs must first be initialized by the gel scripts (Scripts > AM572x MULTICORE initialization > IPUxSSClkEnable_API)
  • If the K2 demo will not run, try updating to the latest emupack by doing "Help/Check For Updates" and selecting "Keystone2 device support" update (only). There are additional instructions for configuring groups, etc. at SMP Debug.
  • If the primary core of an SMP group will not allow running after loading the demo, try pausing the linked cores and then running all the cores in a group
  • For TI-RTOS documentation for enabling SMP, refer to SMP/BIOS. The POSIX demo in the Processor SDK RTOS packages with C66x does not support SMP. This is a POSIX pthread demo intended to run Dhrystone on one C66x core without SMP.
  • Some of the DMIPS values may not be accurate, but the values will increase proportionally with the number of cores


How to Build the Demo

Processor-SDK RTOS

To build the project manually, first navigate to the top level makefile:

 <SDK_INSTALL_PATH>/processor_sdk_rtos_<platform>_2_00_xx_xx/demos/posix-smp/makefile

Edit the makefile to include the paths to BIOS, XDC, PDK packages, and the toolchains for the cores being used.

#DEPOT = <ROOT_INSTALL_PATH>
#### BIOS-side dependencies ####
#BIOS_INSTALL_PATH ?= $(DEPOT)\bios_n_nn_nn_nn
#XDC_INSTALL_PATH ?= $(DEPOT)\xdctools_n_nn_nn_nn_core
#### BIOS-side toolchains ####
#TOOLCHAIN_PATH_A15 ?= $(DEPOT)\ccsv6\tools\compiler\gcc-arm-none-eabi-n_n-xxxxqn
#TOOLCHAIN_PATH_M4 ?= $(DEPOT)\ccsv6\tools\compiler\ti-cgt-arm_x.x.x

Navigate to the demo directory and run "make". The steps to run the demo will be the same.

Processor-SDK Linux

The Posix-SMP demo has been added to the Linux SDK matrix starting in Processor-SDK 3.0. Simply run the example from the Matrix and the output will be displayed on the console.

For the documentation on the Linux Matrix, please see: link.