Processor SDK RTOS Audio Benchmark Starterkit

From Texas Instruments Wiki
Jump to: navigation, search


RTOS Software Developer Guide Audio Benchmark Starterkit




Introduction

The Audio Benchmark Starterkit is intended to provide an easy and quick way to benchmark key audio functions on C66x and C674x DSP devices. This package is intended for users who are new to the TI DSP development environment and provides an easy path to compare core audio benchmarks to other implementations. For the purposes of benchmarking we have selected the following signal processing functions

  • Complex Fast Fourier transform (FFT)
  • Real Block FIR filters with 128 samples, 16 coefficients
  • Cascaded Biquad (2 channels, 3 stages) IIR filter for 128 Samples

The package is also a great way to get familiar with benchmarking functions on TI DSP with or without TI`s Code Composer Studio environment. It also intends to provide guidance on the compiler options and code/data memory placement that allows developers to obtain optimal performance on TI DSP architecture. The package also demonstrates use of signal processing functions from TI C6000 DSPLIB which contains several kernels optimized for TI DSP architectures.

Software Features

  • Benchmark applications for core signal processing functions
  • Makefile and CCS Project scripts to build applications
  • SD card bootable binaries [Supported on SOCs that support SD boot]

Directory Structure

The audio benchmark starterkit is located in the Processor SDK RTOS release under the directory path

<SDK_INSTALL_PATH>\processor_sdk_rtos_<soc>_x_xx_xx_xx\demos\audio-benchmark-starterkit


The directory structure for the audio benchmark starterkit is shown in the image below.

Detailed description of the directory structure is given below:

Audben dirStructure.png
  • prebuilt-binaries - directory contains prebuilt out files to run the benchmarks.
    • bootimages: SD card boot files to run the benchmarks using SD boot.
  • docs - directory contains ReadMe, Quick start guide and the software manifest for the package.
  • scripts - directory contains .txt script files that is used by BenchmarkProjectCreate script to create CCS projects
  • src
    • common - Contains linker command file and logging functions used by all benchmark tests.
    • singlePrecision_FFT - Source files for benchmark app for FFT
    • singlePrecision_FIR - Source files for benchmark app for FIR
    • singlePrecision_IIR - Source files for benchmark app for IIR

Software Dependencies

NOTE

For correct version of Code Composer Studio to download, please refer to the Release Notes corresponding to the Processor SDK RTOS version that you have installed

Supported Hardware

Platforms supported in Processor SDK RTOS 3.3 and later

Platforms planned in Processor SDK RTOS 4.0

QuickStart with How-To-Video

For an easy and visual experience to build and run the benchmark tests, we have created a short How to video that demonstrates how the Benchmark Starterkit can be built and run on C66x DSP on the K2G EVM which you can check out from the link provided below:

How to Build the Benchmarks

The benchmark starterkit is designed to build with makefiles as well as with Code Composer Studio (CCS) IDE Environment. Both the approaches requires developers to setup the Processor SDK RTOS development environment. Developers can use either approach based on their familiarity with the chosen build environment. Let us take a closer look at both approaches.

Using Makefile

Step1 : Setup Processor SDK RTOS build Environment.

Developers are required to setup the Processor SDK RTOS build environment as described in Processor SDK RTOS Setup environment

  1. set SDK_INSTALL_PATH = C:\ti\<Install directory>
  2. setupenv.bat
NOTE

If developers install CCS or Processor SDK RTOS under Custom path then they need to refer to the setup instructions described under Setup environment when installing to a custom path


Step2 : Invoke Make from root directory

The make file in the root director of the audio-starterkit can be used to build the entire package. To build the benchmark examples:

  1. cd <PROC_SDK_INSTALL_PATH>/demos/audio-benchmark-starterkit
  2. make all
NOTE

The build picks up the SOC information from the SDK setup. Also, in the make environment the benchmark application is built to send benchmark logs to UART console so that there is no dependency on the CCS IDE environment


For Other supported options, please type

For Windows:

gmake help

For Linux :

make help

All available options are provided below:

Make help.png

Using CCS Projects

The audio benchmark starterkit does not provide pre-canned CCS Projects as it is difficult to set up projects to be portable across various developer build environments. To create CCS Projects with the benchmarks, developers are required to run the BenchmarkProjectCreate script provided in the root directory of the starterkit.

Step1 : Setup Processor SDK RTOS build Environment.

  1. set SDK_INSTALL_PATH = C:\ti\<Install directory>
  2. set TOOLS_INSTALL_PATH = C:\ti\<CCS Install directory>
  3. setupenv.bat

Note: CCS by default is installed in the path C:\ti\ccsv7 so TOOLS_INSTALL_PATH=C:\ti

Developers are required to setup the Processor SDK RTOS build environment as described in Processor SDK RTOS Setup environment

NOTE

If developers install CCS or Processor SDK RTOS under a Custom path then they need to refer to the setup instructions described under Setup environment when installing to a custom path


Step 2: Run BenchmarkProjectCreate script to generate CCS Projects

To generate the CCS Projects

  1. cd $PROC_SDK_INSTALL_PATH/demos/audio-benchmark-starterkit
  2. BenchmarkProjectCreate [Options]

The Project create script can be run using the following syntax

 BenchmarkProjectCreate.bat <soc> <board> <all>

Description of arguments:

  • soc - K2G (Default) / K2H/ K2E/ C6678/ C6657/ AM572X/ AM571x/ OMAPL138
  • board - all (Default) / <SOC supported EVMs>
  • module - all / (FFT / FIR / IIR)
Example:
 a) BenchmarkProjectCreate.bat
             - Creates all module projects for the K2G soc for evmK2G platform
 b) BenchmarkProjectCreate.bat AM572x 
             - Creates all module projects for AM572x soc for evmAM572x and idkAM572x platform
 c) BenchmarkProjectCreate.bat C6657 evmC6657 
             - Creates all modules for C6657 DSP for evmC6657 platform
 d) BenchmarkProjectCreate.bat K2H evmK2H FFT
             - Creates FFT module project for K2H soc for evmK2H
NOTE

Known issue with Processor SDK RTOS 3.3

The BenchmarkProjectCreate script uses text files .txt from scripts folder to generate the CCS projects. The name for the demo folder was updated from "audio-benchmark-kit" to "audio-benchmark-starterkit". This will require CCS users to update the name in the .txt file before generating the scripts.

For Example if you are using K2G platform locate file Benchmark_FFT_evmK2G_c66ExampleProject.txt, Benchmark_FIR_evmK2G_c66ExampleProject.txt and Benchmark_IIR_evmK2G_c66ExampleProject.txt and update the demo name in the text files from "audio-benchmark-kit" to "audio-benchmark-starterkit"

Step 3: Import Generated CCS Projects in CCS Workspace

Launch CCS and Import the CCS Project using the Project->Import Existing CCS Project and browse to the audio-benchmark-starterkit folder

Import CCS Project.png CCS Project Browse.png Imported Projectt View.png

Step 4: Build Imported CCS Benchmark Projects

Right click on the Benchmark Project File and Build the project as shown below:

Build Benchmark.png

How to Run the Benchmarks

The benchmark examples can be run by loading the built out files with an emulator using the CCS Debug functionality or the examples can be run on the DSP by creating SD card bootable images using out files. Let us take a look at both these approaches.

Using CCS

Step 1: Connect Emulator and UART to Hardware

  • Refer to the Hardware Setup guide and connect the onboard or external emulator to the Hardware and Host machine with CCS installed.
  • Connect the UART cable from the EVM to the Host machine and configure the Serial console with following settings:
    • Baud Rate: 115200
    • Data Bits: 8
    • Parity: None
    • Flow Control: Off

Step 2: Create Target configuration and connect to the DSP

To connect to the SOC, developers need to create a Target configuration by following the procedure described in wiki Create_Target_Configuration_File_for_EVM


Instructions specific to supported EVMs:

NOTE

Please refer to Hardware User Guide corresponding to each supported EVM so setup the boot switches to No boot if available


Step 3: Loading and Running Benchmark application on the DSP

  • Load the out file using Run -> Load -> Load Program and browse to the output binary.
  • After loading the out file, run the benchmark app by Pressing F8 or Run -> Resume


Output in CCS IO Console : Output in UART Console :
FFTBenchmark CCS Output.png FFTbenchmark UART.png

Using SD card (Supported only on AM57xx and K2G)

Step 1: Run Create SD script to generate SD bootable binaries

The root directory in the audio-benchmark-starterkit contains a create-sd.bat file that will convert the .out files installed int the bin folder into SD bootable images which will be installed in the path bin/sd_card_files/<EVM>

The syntax to run the create-sd script is as follows:

create-sd.bat <EVM>

EVM : refers to evaluation platfom on which the binaries are meant to be run

Eg: create-sd evmK2G - Creates SD bootable images for K2G EVM.

Step 2 : Format and copy the SD card binaries to the SD card

Create an SD card using the procedure described in Creating SD card in Windows and Create SD card in Linux

Copy the "MLO" and "Singleprecision_<Module>_app" to the boot partition on the SD card.

Step 3: Boot the Benchmark app by configuring SD boot on the EVM

  • Configure the boot switches on the evaluation hardware to SD boot.
  • Insert the SD card in the microSD or SD card slot on the board.
  • Connect the UART on the hardware to the Host and configure the host to Baud Rate= 115200, Data Bits= 8 , Parity= None, Flow Control= Off
  • Power on the EVM to view the output on the Serial console on the host

Benchmark App output on UART console :

FFTbenchmark sdBoot.png

Benchmark Starterkit Implementation

Signal Processing functions used in Starterkit

Single Precision FFT: DSPF_sp_fftSPxSP (Mixed Radix Forward FFT )

The audio benchmark kit uses the FFT implementation(DSPF_sp_fftSPxSP) from the TI DSP Library. The DSPF_sp_fftSPxSP kernel calculates the discrete Fourier transform of complex input array ptr_x using a mixed radix FFT algorithm. The result is stored in complex output array ptr_y in normal order. Each complex array contains real and imaginary values at even and odd indices, respectively. DSPF_sp_fftSPxSP kernel is implemented in assembly to maximize performance, but a natural C implementation is also provided. The demonstration app for this kernel includes the required bit reversal coefficients, brev, and additional code to calculate the twiddle factor coefficients, ptr_w.


NOTE

Single Precision FIR: DSPF_sp_fir_cplx (Complex FIR Filter)

The audio benchmark kit uses the FFT implementation(DSPF_sp_fftSPxSP) from the TI DSP Library. The DSPF_sp_fir_cplx kernel performs complex FIR filtering on complex input array x with complex coefficient array h. The result is stored in complex output array y. For each complex array, real and imaginary elements are respectively stored at even and odd index locations.

The API reference and the implementation details can found in the TI DSPLIB documentation included in the Processor SDK.

Single Precision IIR : tisigCascadeBiquadSP_2c_3s_kernel (Cascade Biquad Filter for Multichannel input)

The Cascade biquad filtering function in the audio benchmark starterkit is an improved biquad infinite impulse response filter Patent US20160112033 Pending. The new filter structure modifies the feedback path in the filter, resulting in a significant reduction in execution cycles. One of the most-used digital filter forms is the biquad. A biquad is a second order (two poles and two zeros) Infinite Impulse Response (IIR) filter. It is high enough order to be useful on its own, and because of the coefficient sensitivities in higher order filters the biquad is often used as the basic building block for more complex filters. For instance, a biquad low pass filter has a cutoff slope of 12 dB/octave, useful for tone controls; if a 24 dB/octave filter is needed, you can cascade two biquads and it will have less coefficient sensitivity problems than a single fourth-order design.

For implementation details please check the USTO link

API reference:

int tisigCascadeBiquad32f_2c_3skernel(CascadeBiquad_FilParam *pParam) 

where CascadeBiquad_FilParam is defined as

 CascadeBiquad_FilParam {
      float *restrict pin1;    // Input Data Channel 1 
      float *restrict pin2;    // Input Data Channel 2
      float  *restrict pOut1;  // Output Data Channel 1
      float  *restrict pOut2;  // Output Data Channel 1
      float  *restrict pCoef;  // Filter Coefficients a, b for 3 stages
      float  *restrict pVar0;  // Filter Variables d0, d1 for 3 stages channel 0
      float  *restrict pVar1;  // Filter Variables d0, d1 for 3 stages channel 1
      int      sampleCount;    // Number of samples
 }  CascadeBiquad_FilParam;

Memory placement of Instruction and Data

The best performance of the DSP can be obtained by placing all the data and instructions in L2 SRAM. Please refer to the linker command files include in the src/common folder to see how the instructions and data can be place in DSP internal L2 memory.

NOTE

In application use cases where audio data needs to be place in onchip shared memory (OCMC or MSMC) and DDR memory, we recommend that users move data from external memory to L2 for processing using EDMA or enable DSP cache using CSL to optimize performance.

Compiler Optimization Flags

All the projects in the Audio Benchmark starterkit are built using C6000 compiler with -o3 optimization that allows the source code to be compiled with highest compiler optimization settings. User can refer to the compiler Build settings in the Makefiles or go to Build Settings in CCS Project settings to modify the compiler options.


NOTE

* For more Details on recommended C6000 Compiler options refer C6000_Compiler:_Recommended_Compiler_Options

SOC Integration and Optimization

Configuring device clocks

Every SOC with TI DSP requires users to enable the DSP clocks by setting up the PLL and or enabling the DSP through Power Sleep Controller or Power and Control (PRCM) module. The way the clocks are set up differs depending on the environment setup

  • Development environment with emulator:In this case the SOC clocks are setup using GEL files which are added to the target configuration file. For audio benchmark starterkit, this done using GEL files setup explained in the Hardware Setup section
  • Application Boot from boot mediaIf you are booting application from a boot media like SD/MMC or flash device, the ROM bootloader or a secondary level bootloader performs the clock configuration. For audio starterkit, this initialization is done using board library which is linked to the secondary bootloader and the benchmark tests.
NOTE

If the clocks are not configured the DSP will run at speed of the input clock rather than at the device speed grade. Hence if the clocks are not configured correctly the benchmarks will run much slower than anticipated but the cycle count will show the same.

Benchmarking using DSP TSCH/TSCL registers

For C66x+ and C674x members of the C6000 family, there is a pair of registers, TSCL and TSCH, which together provide a 64-bit clock value. You can create your own clock function to take advantage of these registers. Simply add this function to your program and it will override the clock function from the library.

The Bench mark test application, use the following functions to capture cycle count using the TSCH and TSCL regsiters.

       /* ---------------------------------------------------------------- */
       /* Initialize timer for clock */
       TSCL= 0,TSCH=0;
       /* Compute the overhead of calling _itoll(TSCH, TSCL) twice to get timing info */
       /* ---------------------------------------------------------------- */
       t_start = _itoll(TSCH, TSCL);
       t_stop = _itoll(TSCH, TSCL);
       t_overhead = t_stop - t_start;
       t_start = _itoll(TSCH, TSCL);
       <Algorithm to be bechmarked>
       t_stop = _itoll(TSCH, TSCL);
       t_measured = (t_stop - t_start) - t_overhead;

Benchmark logging

The Audio benchmarks demonstrates two ways to log benchmark numbers. One approach that can be used when code is loaded and run from Code composer studio is to use standard printf messages from the standard IO RTS libraries and the other approach is to use UART based logging that can send the benchmark logs to serial console on the host at the baud rate of 115.2 kbps.

All the benchmark test application include a file Benchmark_log.h and Benchmark_log.c, that are used to log messages based on the definition of macro IO_CONSOLE. If IO_CONSOLE is defined the output will be directed to CCS console. If it is not defined, the logs are sent to the UART console.

Makefiles and scripts that build binaries to boot from SD card will not have IO_CONSOLE defined hence the benchmark logs will be directed to the UART serial console. In the CCS projects, we define the IO_CONSOLE macro so that the output can be observed on the CCS console.

Cache configuration for Code/data sections in SRAM/DDR

The best performance of the DSP can be obtained by placing all the data and instructions in L2 SRAM. If developer application use cases places audio data in onchip shared memory (OCMC or MSMC) and DDR memory then the user will need to enable L1 and L2 cache using CSL API.

To enable and utilize cache in the application, please refer to the csl_cacheAux.h file in the pdk_<soc>_x_x_x/packages/ti/csl folder in the SDK and link the CSL library for the soc into the application code.

Benchmark results

Algorithm\DSP Architecture C66x DSP C674x DSP
Single Precision FFT (256 samples) 1808 cycles 2314 cycles
Single Precision FIR (128 samples, 16 coefficients) 2652 cycles 4465 cycles
Single Precision IIR (1k samples from 2 channel with 3 stage cascade biquad) 8258 cycles 12381 cycles

Notes:

  • All code and data for the benchmark tests is placed in L2 Memory.
  • C6000 compiler version used was CGTools v8.1.3
  • Bench marks were obtained from C66x DSP on K2G and C674x DSP on OMAPL138 LCDK
  • FFT and FIR benchmarks were obtained using the DSPLIB functions.

Support

For questions, feature requests and bug reports, please use the TI E2E Forums provided below:

Additional resources

White papers: