Processor SDK RTOS BOOT AM335x/AM437x

From Texas Instruments Wiki
Jump to: navigation, search



Overview

User Interface

Application

Debug


Overview

Bootloader supports power-on-reset bootstraps for the board. It initializes board, loads application from the memory device to DDR and transfers control to application. Section provides additional details including flashing and booting instructions across different media.

Source Reference

< BASE_DIR = PDK_INSTALL_DIR\packages\ti\starterware>


Bootloader build files for AM335x/AM437x

Source files:

  • BASE_DIR\bootloader\src: Common source files for bootloader functionality
  • BASE_DIR\bootloader\src\<device>: Files specific to device to initialize platform features like PLL, pinmux and DDR

Build Files:

  • BASE_DIR/build/makerules/rules_a8.mk: Common Compiler flags used for A8 cores. Applies to AMIC110 and AM335x
  • BASE_DIR/build/makerules/rules_a8.mk: Common Compiler flags used for A9 cores. Applies to AM437x devices
  • BASE_DIR/build/makerules/platform.mk: Global settings for all components for a particular platform.
  • BASE_DIR/build/makerules/components.mk: Specific settings for components in starterware
  • BASE_DIR/build/makerules/build_cfg.mk: Flags to enable features in the build
  • BASE_DIR/bootloader/Makefile: Makefile for bootloader that provides list of source files and library to create bootloader binary.

Boot and flashing tools:

  • BASE_DIR/tools Contains tools to create boot images and flashing tools to program the boot binary on the boot media.


Bootloader execution sequence

The Processor SDK RTOS boot loader uses a two stage boot process. The different stages of the application boot sequence using Processor SDK RTOS bootloader are shown below:

Boot Sequence

  1. Power on Reset
  2. ROM Bootloader (RBL)
    • Platform configuration and initialization.
      • DPLL and clock settings for MPU, I2C, MMCSD, USB, SPI, QSPI, Ethernet etc.
    • Checks Sysboot pins and choose booting device
      • If no valid bootloader found on booting device, RBL checks for next booting device. The sequence depends on RBL execution flow and Sysboot pins.
    • RBL gets image size and load address by checking TI Image Header appended on bootloader binary(.bin). Check binary formats.
    • Loads the binary to internal OCMC memory at the Load address fetched from TI Image Header
    • Passes control to Secondary Bootloader(SBL)
  3. Secondary Bootloader(SBL)
    • Configure PLL and Initialize DDR
    • Configure PRCM and PinMux  for Boot Peripherals
    • Copies application image to DDR
    • Passes execution control to Application
  4. Application execution

Tools and Binary formats

Binary format

Requirement Details
.bin

QSPI bootloader,

UART bootloader and app

QSPI bootloader binary should in .bin format and Application binary should be in _ti.bin format.

UART bootloader and applications are loaded in .bin format through XMODEM in terminal.

_ti.bin

MMCSD bootloader and app,

NAND bootloader and app,

MCSPI boot loader and app,

QSPI app.

.bin binaries are converted to _ti.bin format by adding Image size(4bytes) and Image load address(4bytes) as image header.
Refer to Image format section in Initialization chapter of AM437x ARM cortex A9 Processors Technical reference manual

MMCSD, NAND and MCSPI boot loaders and application binaries should be appended with ti image header.

Procedure for conversion is here.


TI Boot image


Offset Binary value
0x00000000 Size
0x00000004 Entry Point (Location)
0x00000008 Binary (.bin)
NOTE

* For bootloader Entry point is usually 0x402f0000
  • For the app the entry point is usually 0x80000000.

Binary format conversion procedure

Binary format conversion in Linux

1) To convert from .out -> .bin

TOOLCHAIN_PATH_<A8/A9>/bin/arm-none-eabi-objcopy -O binary <application>.out <application>.bin

2) Build tiimage.out. Go to starterware/tools/ti_image/

gcc tiimage.c –o tiimage.out

3) To convert from .bin -> _ti.bin

tiimage.out <Image Load Address> NONE <application>.bin <application>_ti.bin

Binary format conversion in Windows

1) To convert from .out -> .bin

TOOLCHAIN_PATH_<A8/A9>/bin/arm-none-eabi-objcopy -O binary <application>.out <application>.bin

2) To convert from .bin -> _ti.bin. tiimage.exe is provided as prebuilt binary in starterware/tools/ti_image.

tiimage.exe <Image Load Address> NONE <application>.bin <application>_ti.bin


Boot Modes supported

Following are the Boot Modes supported through AM335x/AM437x bootloader for the various EVMs.


MMCSD NAND McSPI QSPI UART
AM335x GPEVM YES YES YES NO YES
AM335x ICEv2 YES NO YES NO NO
AM335x StarterKit YES NO NO NO YES
AM335x BeagleBoneBlack YES NO NO NO YES
AM437x GPEVM YES NO NO NO YES
AM437x IDK YES NO NO YES NO
AM437x StarterKit YES NO NO NO NO



Building the Bootloader

Pre-requisite: Setup SDK build environment as described in article Setup_Environment

Normal Operation of Bootloader:

Bootloading an application from flash into DDR memory as in case of TI evaluation platforms is described as normal operation mode for the bootloader. This is the default behaviour of the bootloader and can be built using the following command in starterware.

gmake bootloader BUILDCFG=boot BOOTMODE=<BOOT_MODE> PLATFORM=<EVM> PROFILE=<BUILD_PROFILE> -s KW_BUILD=no

  • BOOT_MODE: mcspi, nand, qspi, mmcsd, uart (Check supported boot modes for your evaluation platform)
  • EVM: am335x-evm, am43xx-evm, amic110-ddrless
  • BUILD_PROFILE: debug, release

Additional Build options (currently support only for AMIC110/AM335x ICE Users)

  • DDR less Application boot setup
gmake bootloader BUILDCFG=boot BOOTMODE=mcspi PLATFORM=amic110-ddrless PROFILE=debug -s KW_BUILD=no USE_DDR=no
gmake bootloader BUILDCFG=boot BOOTMODE=mcspi PLATFORM=amic110-ddrless PROFILE=release -s KW_BUILD=no USE_DDR=no

This option builds an ultra light weight (<10 KB) bootloader for cost optimized application that don`t external DDR memory.

  • PRU/ICSS Enable in SBL
gmake bootloader BUILDCFG=boot BOOTMODE=mcspi PLATFORM=am335x-evm PROFILE=debug -s KW_BUILD=no ENABLE_PRU=yes
gmake bootloader BUILDCFG=boot BOOTMODE=mcspi PLATFORM=am335x-evm PROFILE=release -s KW_BUILD=no ENABLE_PRU=yes

This feature is required in application that need to quick wake up of ICSS/PRU cores. The PRU cores can be woken up and loaded from the SBL by combining the ENABLE_PRU and BIN_LOAD arguments.

  • Load additional binaries from flash
gmake bootloader BUILDCFG=boot BOOTMODE=mcspi PLATFORM=am335x-evm PROFILE=debug -s KW_BUILD=no BIN_LOAD=yes
gmake bootloader BUILDCFG=boot BOOTMODE=mcspi PLATFORM=am335x-evm PROFILE=release -s KW_BUILD=no BIN_LOAD=yes

The location of binaries in offset is configured using sbl_flash_offset_cfg.h in the bootloader source. Users are required to use TIIMAGE tool to append an header to the binary so that the bootloader knows the loction and size of the binary to be loaded.

Industrial DDRless Booting

The AMIC110 DDRLESS platform provides a superset flag to enable all the above features and build the bootloader . The superset build is invoked using BUILD_ICSS_DDRLESS_BOOT=yes as shown below:

gmake bootloader BUILDCFG=boot BOOTMODE=mcspi PLATFORM=amic110-ddrless PROFILE=debug -s KW_BUILD=no BUILD_ICSS_DDRLESS_BOOT=yes
gmake bootloader BUILDCFG=boot BOOTMODE=mcspi PLATFORM=amic110-ddrless PROFILE=release -s KW_BUILD=no BUILD_ICSS_DDRLESS_BOOT=yes

Prebuilt binaries inside the Processor SDK RTOS for AMIC110-DDRLESS will be configured using this option to allow for testing of cost optimized industrial use case.


Boot Mode settings

Boot mode settings for all supported AM335x and AM437x boards are here

Boot Modes

Booting Via SD Card

Booting from SD Card involves two steps.

  1. Preparing SD card.
  2. Booting target.

Preparing SD card 

  1. To boot target the SD card should be bootable. Follow the steps at Creating bootable SD card in windows or Creating bootable SD card in Linux.
  2. Delete the "MLO" and "app" in the bootable SD card which are created in the process of making the SD bootable.
  3. Bootloader images with ti header (<mmcsd_bootloader>_ti.bin)should be renamed to "MLO". Bootloader images are located at <PDK_INSTALL_DIR\packages\ti\starterware\starterware\binary\bootloader\bin\<TargetType>
  4. Similarly the converted application binary image has to be renamed to "app" from "<app_name>_ti.bin"
  5. Copy both the boot loader image "MLO" and the application image "app" to the SD card.
  6. The SD card is ready for use on target.

Booting target

  1. Insert SD card to the base board SD slot. Connect a UART cable to a host running a serial terminal application (teraterm/hyperterminal) with 115200 baud, 8bit, No parity and 1 STOP bit configuration.
  2. Configure the board for SD Boot mode
    1. SD instance 0 (on base board) is available in all profiles.
    2. SD instance 0 boot mode needs to appropriately set. For SD boot to be selected first, SD boot should appear first in the boot device list in the boot mode. If any other boot mode is selected, even if a SD boot card is inserted, and does not appear first in the list, the first available sane boot image (like NAND or SPI etc) is booted and SD is not selected. Only if no sane boot image is found in the first devices, SD boot image will be selected.
  3. Once SD boot image is chosen, the MLO is first detected and copied and executed from the OCMC0 RAM. The MLO then copies the application image (app) from the card to the SDRAM and passes the control to the application. If the process is succesful, messages identifying board and SoC will appear on the serial console.

After this the application will take control and execute.

NOTE: If board have BootMode selection pins choose proper Boot Selection pins from hardware reference manuals.

If the boards have no boot mode selection pins and a valid boot image is present on McSPI flash, Booting will happen from McSPI flash. Erase McSPI flash in such cases to boot from SD card McSPI flash erase . The boot sequence depends on ROM bootloader.

Booting Via QSPI

Booting from QSPI flash involves two steps-

  1. Preparing Flash Device
  2. Booting target.

Preparing Flash Device

Procedure relies on contents being copied to SD card. Additional details below:

  1. Copy bootloader image(bootloader_boot_qspi_a9host_debug.bin rename) and app image("<app_name>_ti.bin") into the SD card.
    The file names have to be renamed in such a way that the length of name is less than 9 characters. Any file name less than 9 characters can be used.
    Rename the bootloader file to 'boot' and application image to 'app' with no extensions.
  2. Copy the 'config' file into the SD card which will contain the names of the image to be flashed and the offset.
    A sample config file can be found at <\PDK_INSTALL_DIR\packages\ti\starterware\starterware\tools\qspi\config\> directory. Do not change name of the config file.
    NOTE: "config" file can be used without any modifications if bootloader and application images are renamed to "boot" and "app".
    NOTE: Do not rename bootloader to be copied to SD card as "MLO", as MMCSD bootloader expects "MLO" and "app" to boot.
  3. Now SD card contains 1)boot 2)app 3)config files.
    config file contains the address of boot image as 0x0 and app image as 0x80000.
    Insert it into the SD card slot.
  4. Connect the board with CCS and load the prebuilt qspi flash writer application from <PDK_INSTALL_DIR\packages\ti\starterware\starterware\binary\qspi_app_flash_writer\bin\m43xx-evm>
  5. Run the QSPI flash writer application. Following logs expected on console.
StarterWare QSPI Flash Writer!!
BOARDInit status [0x0]
SoC                   : [AM43XX]
Core                  : [A9]
Board Detected        : [IDKEVM]
Base Board Revision   : [UNKNOWN]
Daughter Card Revision: [UNKNOWN]
Copying boot to QSPI Flash
Copying app to QSPI Flash
Changing read to quad mode
Read mode has been changed to Quad mode
SUCCESS!!!
Flashing completed

Booting the target.

  1. Connect UART cable to a host running serial terminal application (teraterm/hyperterminal) with 115200 baud, 8bit, No parity and 1 STOP bit configuration.
  2. After flashing successfully remove SD card and reboot to see following logs
StarterWare Boot Loader
BOARDInit status [0x0]
SoC                   : [AM43XX]
Core                  : [A9]
Board Detected        : [IDKEVM]
Base Board Revision   : [UNKNOWN]
Daughter Card Revision: [UNKNOWN]
Copying Header of the application image
Copying image from flash to DDR
Jumping to StarterWare Application...
 NOTE: Boot logs will appear approximately after 25 seconds on reset.
 NOTE:If there is no boot mode selection present on board, boot image will be loaded depending on ROM boot sequence
Example: If QSPI flash and MMCSD has valid bootloaders, on reset MMCSD boot image will be loaded following ROM Boot sequence.

Booting Via UART

ROM and Bootloader supports XMODEM protocol with images being binary not requiring any additional headers. Following are steps for boot:

  1. Configure board for UART boot mode :
    UART boot need to be first in the boot device list. Note: In case if any other boot mode is selected, the first available boot image (eg:NAND or MMCSD etc) will override. In case of no valid images, UART boot will be selected.   
    • Select View->Memory Browser through CCS.   
    • Select address 0x44e10040.   
    • Write 0x19 to last 2 bytes of this memory address.(UART boot)   
    • Soft reset the board. This is a volatile bit which gets reset after power on.
  2. ROM code will print "CC.." on UART console expecting Bootloader via XMODEM. File can be sent via xmodem through tera-term File-> Transfer -> XMODEM -> Send.
  3. On transmitting bootloader image, bootloader_boot_uart_a9host_debug.bin via XMODEM, following message will be expected on serial console.
CCCCCCCCCCCCCCCCCCCCCCCCCCCC
StarterWare Boot Loader
BOARDInit status [0x0]
 SoC                   : [AM43XX]
 Core                  : [A9]
 Board Detected        : [IDKEVM]
 Base Board Revision   : [UNKNOWN]
 Daughter Card Revision: [UNKNOWN]
GPIO Instance number: 0
Pin number: 22
Please transfer file:
CCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCCC


  4.  As  a next step application binary (without header) can be sent via XMODEM which will lead to application start executing.

Booting Via McSPI

Booting from McSPI involves two steps.

  1. Preparing Flash Device
  2. Booting the target.

Preparing Flash Device

  • Set the appropriate bootmode if applicable for EVM.Refer Boot mode settings. Note: Most of the boards may not have switch settings.
  • Add a required target configuration in CCS depending on emulator and board connected.
  • Connect target to required core. Ex: A8.
  • Load the flash writer from <PDK_INSTALL_DIR\packages\ti\starterware\starterware\tools\flash_writer\spi_flash_writer_AM335X.out onto the EVM.
  • Run the application and observe the logs on CCS console.
Starting SPIWriter.
Choose Operation:
Enter 1 ----> To FLASH an Image
Enter 2 ----> To ERASE Flash
Enter 3 ----> To EXIT 
  • When Flash option is chosen program prompts to enter file name.
Enter the File Name
  • Provide the complete path of file bootloader_boot_mcspi_a8host_release_ti.bin at directory "binary/bootloader/bin/<PLATFORM>/<gcc/ccs>/" and hit Enter.
Enter the Offset in bytes (in HEX)
  • Provide 0x00000 to flash bootloader.
  • To flash application binary image <app_name>_a8host_ti.bin, provide 0x20000.
  • Wait for few miniuits as flashing is a slower process.
Erasing flash at byte offset: xx, byte length: xxxx
SF: Successfully erased xxxx bytes @ xxxx
Writing flash at page offset: x, number of pages: xxxx
Flashing is in progress...
Verifying... Success. 
  • Once SPI flash writing completes disconnect target.

Booting the target

  1. Connect a serial cable to a host running a serial terminal application (teraterm/hyperterminal) with 115200 baud, 8bit, No parity and 1 STOP bit configuration.
  2. Configure the board for SPI boot mode.
  3. On reset, ROM bootloder copies the bootloader from flash to internal memory. The bootloader then copies the application image from flash to DDR and passes the control to the application.


Booting Via NAND

Booting from NAND involves two steps.

  1. Preparing Flash Device
  2. Booting the target.

Preparing Flash Device

  • Configure BOOT pins for NAND Boot mode settings
  • Connect target with CCS.
  • Load the <PDK_INSTALL_DIR\packages\ti\starterware\starterware\tools\flash_writer\nand_flash_writer_AM335X.out> to target and Run. Flash writer will output messages to CCS console. When it prompts for inputs, proper inputs shall be given via CCS console.
  • When prompted for binary file name, update file with proper path.
  • Select option for flashing.
Choose your operation
Enter 1 ---> To Flash an Image
Enter 2 ---> To ERASE the whole NAND
Enter 3 ---> To EXIT
  • If Option 1 is selected, enter image path to flash when prompted as shown below.
Enter image file path

    Provide the complete path (e.g. <PDK_INSTALL_DIR\packages\ti\starterware\starterware\binary\bootloader\bin\<am335x/am437x-evm>\<compiler>\bootloader_boot_nand_a8host_<debug/release>_ti.bin)

  • Enter offset when prompted as shown below.
Enter offset (in hex):

    This offset is start location from where the image should be flashed.
NOTE:

  1. Use hex format
  2. If bootloader is to be flashed, provide 0x00000. For application binary, provide 0x80000.
  • Select ECC for flashing.
Choose the ECC scheme from given options
Enter 1 ---> BCH 8 bit
Enter 2 ---> HAM
Enter 3 ---> T0 EXIT
Please enter ECC scheme type:

    Always select BCH8 for bootloader and application as ROM code and bootloader uses the BCH8 ECC scheme.

  • Ensure that flash info displayed by tool matches NAND flash in EVM.
  • After this tool should first erase the required region in flash and then start flashing new image.
  • If flashing procedure is complete following message should be displayed.
Application is successfully flashed
NAND flashing successful!
  • Once NAND flash writing completes, disconnect from CCS.

Booting the target

  • Connect a UART cable to a host running a serial terminal application (teraterm/hyperterminal) with 115200 baud, 8bit, No parity and 1 STOP bit configuration.
  • Configure the board for NAND boot mode. Refer  Boot mode settings
  • On reset, ROM detects bootloader from NAND and copies it to internal memory. Bootloader then copies application image from the NAND to DDR and passes control to application. If the process is succesful, following messages appear in serial console.
   StarterWare Boot Loader
BOARDInit status [0x0]
SoC                   : [AM335X]
Core                  : [A8]
Board Detected        : [GPEVM]
Base Board Revision   : [1.5]
Daughter Card Revision: [UNKNOWN]
NAND flash is connected to GPMC on this board
Jumping to StarterWare Application...

After this application should take control and execute.

Test Application

The section explains steps for building and booting a sample pdk application for am335x or am437x using MMCSD bootloader.

Test Application Image Creation

Follow below steps to generate the bootable application image.

  1. Generate .out files using steps for Rebuilding PDK. Locate .out file in directory <PDK_INSTALL_PATH/MyExampleProjects/<ExampleProjectDirectory>/Debug>
  2. Convert files to support MMCSD boot using steps as per Binary format conversion procedure.
  3. Rename generated <Application>_ti.bin to "app".

Loading Test application

Follow procedure to use "app" file as per section Booting Via SD Card.

Usage Notes

  • Bootloader Memory map

The bootloader code runs from internal OCMC memory and occupies certain amount of OCMC memory that is not available for application to use during booting.

Refer to the map file for the boot loader to check for latest information on the memory utilization in the boot loader.

Location of linker command file:

BASE_DIR\binary\bootloader\bin\<platform>\gcc

After SBL execution is complete, this region can be used as per application requirement.

  • Configuring entry point for SBL

The three files that help setup the entry point in the bootloader build are "PDK_INSTALL_PATH\packages\ti\starterware\soc\armv7a\gcc\sbl_init.S" and the linker command file "PDK_INSTALL_PATH\packages\ti\starterware\examples\gcc\<device>_boot.lds". The global symbol Entry is used to provide the entry point to the bootloader. The Base address of the memory section OCMCRAM (starts at 1K offset in OCMC RAM as defined in TRM) is then used by the tiimage or GPHEader tool to provide RBL the guidance to find the entry point to pass control. After MLO is created check the TI image format file( _ti.bin) to confirm that the entry point matches the location of Entry symbol in the .map file.

NOTE

The object file created by sbl_init.S should always be the first object file in the link order for the symbol Entry to be placed at the BASE address of the memory section SBL_MEM
  • Boot image creation tools generates a large boot image if load sections are fragmented

Please note that when using objcopy the compiler generates a contiguous binary that gets loaded by the bootloader at the location specified in the header appended by TIIMAGE boot utility. IF you have some code sections in OCMC or SRAM and some section in DDR the compiler will generates a binary that spans across full memory range which would be in order of MB or even GB size so it is recommended that you create compact binaries that can be loaded into memory or implement a ELF parser to bootloader memory sections that may be fragmented in the address space. you can also load separate binaries for OCMC sections and DDR memory and load the sections separately

  • Removing Heap section from application binary to speed up boot times

A common issue reported with the ARM GCC compiler is that it appends Heap section associated with the binary to the binary image used to boot. The Heap section is usually filled with zeros so can cause significant delay in boot times. Essentially the bootloader will be writing a bunch of zeros in memory so is inefficient. Following work around has been used to circumvent the issue

Option 1: Eliminate the heap by using the compiler option "--remove-section" as described in the E2E post below:

Refer: E2E post to configure Heap in ARM application binary by adding "--remove-section"

Example BIOS configuration:

var heap1 = HeapMem.create();
heap1.size = 256 * 1024 * 1024;
heap1.sectionName = ".stack";
Memory.defaultHeapInstance = heap1;

Compiler Setting : --remove-section=.stack

Option 2 Configure Segment type to be "NO LOAD" in .cfg and use excludeSections

SYSBIOS Memory map configurations allows user to specify the section name, length and type. by configuring the section type to "NOLOAD" and using excludeSection option the heap memory can be eliminated from the final binary.

Example BIOS configuration:

Program.sectMap[".biosheap"] = new Program.SectionSpec();
Program.sectMap[".biosheap"].runSegment = "DDR2"
Program.sectMap[".biosheap"].type = "NOLOAD";
Program.sectionsExclude = ".biosheap"

Alternate approach using linker command file:

 .ddr3Heap (NOLOAD):
   {
       *(.ddr3Heap)
   } > HOST_DDR3
NOTE

The approach described above helps improve boot times but Users are recommended to initialize the HEAP sections to zeros post boot during initialization to avoid any undesired behavior during normal operation of the app

Debugging application boot

Steps to debug application boot using Processor SDK RTOS bootloader are discussed in the article Common steps to debug application boot