Processor SDK RTOS BOOT AM57x

From Texas Instruments Wiki
Jump to: navigation, search


RTOS Software Developer Guide BOOT AM57x



Overview

User Interface

Application

Debug


Overview

The Secondary Bootloader (SBL) for AM57xx device initializes the execution environment for multi-core application and this can be used to demonstrate an out-of-box experience.The section covers additional details including execution sequence, tools and additional flashing instructions.

Bootloader Execution Sequence

  • Power On Reset
  • ROM Bootloader (RBL)
    • Software pre-programmed in ROM memory starts executing
    • Checks Sysboot pins and choose booting device
    • If no valid bootloader found on booting device, RBL checks for next booting device.
    • Platform configuration and initialization.
    • Configures DPLL and clock settings for MPU, and boot media like I2C, MMCSD, SD/MMC, SPI, QSPI, Ethernet etc for reliable boot.
    • The sequence depends on RBL execution flow and Sysboot pins.
    • RBL gets image size and load address by checking TI Image Header appended on bootloader binary(.bin). Check binary formats.
    • Loads the binary to internal memory at the Load address fetched from TI Image Header
    • Passes control to Secondary Bootloader(SBL)
NOTE

Detailed description of ROM bootloader is provided in Initialization Chapter in AM57xx Technical Reference manual
  • Secondary bootloader(SBL)
    • User level secondary bootloader(SBL) begins execution from internal memory by running basic initialization routines like setting up Stack, BSS and then jumps to main() to begin Board Initialization.
    • Board Initialization is done by a call to Board_init() API.For additional details refer Processor SDK Board Support.
    • It includes setting up PLLs, enabling clocks to all interfaces and modules, performing pinmux and setting up UART console.
    • Once Board Initialization is complete, it enables clocks to the slave cores like C66x/DSP, IPU, etc and brings them out of reset.
    • Parses Multicore Application image located in memory device and copies it to DDR memory based on load address for different sections.
    • Once copy is successful it transfers control to application.
  • Application then starts executing from DDR.
NOTE

  • RBL requires boot loader to be in a special format with a header appended to the binary image. The header shall contain the load address of the bootloader and size of the bootloader image.
  • For more information on the TI header refer TRM document

Directory structure

Makefiles:

  • PDK_INSTALL_PATH/ti\boot\sbl\board\<EVAL_BOARD>\build: Makefile for bootloader that provides list of source files and library and compiler options to create bootloader binary.

Source Files:

  • PDK_INSTALL_PATH/ti\boot\sbl\board\<EVAL_BOARD>: Source to SBL main function that consolidates all features
  • PDK_INSTALL_PATH/ti\boot\sbl\soc: Source to SOC specific initialization used in the SBL.
  • PDK_INSTALL_PATH/ti\boot\sbl\src: Source to boot media specific initialization used in the SBL.


Tools and Binary Formats

This section lists out the various tools and scripts used by SBL for different boot modes and those required to create a bootable application image.

SBL/MLO image format:

To generate the MLO, SBL uses tiImageGen tool to prepend the sbl.bin image with the TI header information. The image format has been described in detail in the Image Format Section of theAM57xx Technical Reference manual

Application image format:

A bootable application image can be created by using the Am57xImageGen script provided under tools folder as part of sbl. It can be located at <PDK_INSTALL_DIR>\packages\ti\boot\sbl\tools\scripts folder.

The Am57xImageGen script uses out2rprc and multicoreImageGen format conversion tools to create the final application image. Graphical view of the multicore application image is provided below:

Multicore app image.png

The script creates the bootable image in 2 steps

Step 1: Conversion to RPRC format conversion

  • Firstly, application executable is converted from ELF/COFF format (.out) to custom TI Rprc binary image using out2rprc tool. This tool strips out the initialized sections from the executable file (i.e. *.out) and places them in a compact format that the SBL can understand. The output (bin) file is typically much smaller than the original executable (out) file.
  • The rprc files are intermediate files in a format that is consumed by MulticoreImageGen tool that generates the final binary.

RPRC File Header Format

Offset Binary value
0x00000000 Magic Word(43525052)
0x00000004 Entry Point (Location)
0x00000008 Reserved Addr
0x0000000C Section Count
0x00000010 Version

RPRC Section Header Format

Offset Binary value
0x00000000 Section start Address
0x00000004 Reserved Addr
0x00000008 Size
0x0000000C Reserved CRC
0x00000010 Reserved


Step 2: Multicore Image file generation

  • RPRC files for each cores is combined into a single multicore bootable application image.

Multicore boot image format

Meta Header Start

Offset Binary value
0x00000000 Magic String (0x5254534D)
0x00000004 Number of Files
0x00000008 Device ID
0x0000000C Reserved

Meta Header per Core

Offset Binary value
0x00000000 Core ID
0x00000004 Image Offset

Core ID and Device ID for specific devices can be located in the file sbl_slave_core_boot.h in the boot/sbl/soc/<SOC_NAME> folder

Refer section App Image Creation for more details on usage of this script and application image creation.

Flashing Tools

SBL provides a CCS based qspi flash writer utility to flash image and multicore AppImage from a SD card to onboard QSPI device. It is located at <PDK_INSTALL_DIR>\packages\ti\boot\sbl\tools\flashWriter\qspi

Building the SBL

Pre-requisites to Building

  • Set your environment using pdksetupenv.bat or pdksetupenv.sh. Refer to the Processor SDK RTOS Building page for information on setting up your build environment
  • The SBL has following dependencies and will need the following libraries built
    • Board
    • UART
    • I2C
    • SPI
    • CSL
    • OSAL
    • MMCSD
    • PM
NOTE

Refer to the makefile for the board you are using for the latest driver dependency. These libraries should come pre-built with any fresh installation of the Processor SDK RTOS but may be removed if a gmake clean is invoked

Compiling the SBL Components

To build the SBL components:

  1. cd <PDK>/packages/ti/board/diag
  2. make all BOARD=<BOARD_NAME> SOC=<SOC_NAME> BOOTMODE=<BOOTMEDIA>
  • BOARD_NAME : idkAM572x, idkAM571x, evmAM572x, idkAM574x
  • SOC_NAME : AM572x, AM571x, AM574x

This will make the SBL for a specific $BOARD and $BOOT_MEDIA. Output files will be located in: <PDK>/packages/ti/boot/sbl/binary/<BOARD>

NOTE

Refer <PDK>/packages/ti/boot/sbl/sbl_<DEVICE>.sh for more build options

Building SBL using CCS project

The SBL build in the Processor SDK RTOS is designed to be built using Makefile. Users can also choose to create a CCS project for the bootloader if they prefer the IDE environment by converting the make file based build to CCS project by linking the appropriate source files to the project and using the same compiler options.

Example: The wiki article "Creating_a_CCS_Project_for_SBL_on_AM572x_GP_EVM" demonstrates creation of SBL in CCS for AM572x GP EVM.


Boot Modes

This Release of SBL supports MMCSD and QSPI Boot modes. The different boot modes supported for all the boards is tabulated in the table below.


MMCSD QSPI
AM572x GPEVM YES NO
AM572x IDKEVM YES YES
AM571x IDKEVM YES YES
AM574x IDKEVM YES YES


Booting Via SD Card

  1. Preparing the SD card.
  2. Booting the target.

Preparing the SD card 

  1. To boot the target the SD card should be bootable. Follow the steps at Creating bootable SD card in windows or Creating bootable SD card in Linux.
  2. Delete the "MLO" and "app" in the bootable SD card which are created in the process of making the SD bootable.
  3. Copy the sbl binary(MLO) to the SD card.
  4. Copy the Application image(app) generated using the Script to the SD card.

Booting the target

  1. Insert micro SD card into the SD card slot of the board.
  2. Open a serial communication terminal like TeraTerm, MiniCom on host PC and connect to the UART console port
  3. Do a power reset of the board to boot the appliation from the SD card.

Booting Via QSPI

Booting from QSPI flash involves two steps-

  1. Flashing bootloader and app image to QSPI flash.
  2. Booting the target.

Preparing Flash Device

Use the CCS based qspi_flash_writer.out utility provided in <TI_PDK_INSTALL_DIR>\packages\ti\boot\sbl\tools\flashwriter\qspi\<Board>' to flash the SBL image at offset 0 and application image at offset 0x80000 to the QSPI device.

QSPI device Memory Map:

Offset 0x00 SBL
Offset 0x80000 Application Multicore Image

The images can be flashed into QSPI flash by following steps given below.

  1. Copy QSPI mode SBL image TI_PDK_INSTALL_DIR\packages\ti\boot\sbl\binary\<BoardName>\qspi\bin\MLO and application image(app) generated using the Script into the SD card.
    Rename the bootloader file to 'boot' and application image to 'app' with no extensions. 
  2. Copy 'config' file into the SD card, the config file should contain names of the image to be flashed and the offset.
    A sample config file can be found at TI_PDK_INSTALL_DIR\packages\ti\boot\sbl\tools\flashWriter\qspi\config. Do not change the name of the config file.
    NOTE: "config" file can be used without any modifications if bootloader and application images are renamed to "boot" and "app".
    NOTE: Do not rename the bootloader to be copied to SD card as "MLO", as MMCSD bootloader expects "MLO" and "app" to boot.
  3. Now SD card contains 3 files 1)boot 2)app 3)config files.
    config file contains the address of boot image as 0x0 and app image as 0x80000.
    Insert it into the SD card slot.
  4. Connect the board with CCS and and load the prebuilt qspi flash writer application from $(TI_PDK_INSTALL_DIR)\packages\ti\boot\sbl\tools\flashWriter\qspi\bin\<BoardName>\
  5. Run the QSPI flash writer application. You will see the following logs on the EVM's UART console.
  6. After the images have been flashed to the QSPI device disconnect from CCS and do a power reset to boot from the QSPI memory. 
PDK QSPI Flash Writer!!
Copying boot to QSPI Flash
Copying app to QSPI Flash
Changing read to quad mode
Read mode has been changed to Quad mode
SUCCESS!!!
Flashing completed
NOTE

  • The file names have to be renamed in such a way that the length of name is less than 9 characters. Any file name less than 9 characters can be used.
  • This application will flash the image at required offset without taking into consideration any overwriting to previously flashed image.
  • It is the responsibility of the user to provide proper offsets.


Test Application

SBL provides a test application to demonstrate booting of multicore application image on A15 and DSP cores.The multicore sample application uses mailbox for inter-processor communication. It is used to validate the multi-core boot-up use case.

Master application sends wake-up message to the DSP slave cores & waits for acknowledgement message from the slave cores in an infinite loop.Each slave DSP core waits for wake-up message from the master core  responds back with an acknowledgement message.

Application Image Creation

Application Image creation involves two steps.

  1. Generating the .outs of applications for individual cores
  2. Combining the .outs of individual cores to create a bootable multicore image

The steps to create the bootable image in Linux and Windows environment are listed below.

NOTE

  • Valid SOC settings are AM571x/AM572x
  • Valid BOARD settings are evmAM572x/idkAM571x/idkAM572x

Linux Environment:

Command to build the test application.

Go to cd (TI_PDK_INSTALL_DIR)\packages\ti\boot\sbl

make example BOARD=<BOARD> SOC=<SOC> to build the application
make example_clean BOARD=<BOARD>

Example:

make example BOARD=idkAM572x SOC=AM572x

To create the final bootable application image use the AM57xImageGen script and follow these steps

1. Set the following environment variable in the shell.  BIN_PATH: Pointing to the path where the AppImage needs to be generated

Ex: export BIN_PATH=$(TI_PDK_INSTALL_DIR)/packages/ti/boot/sbl/binary 

2. Edit the script file to point to the application elf files by setting the input application variables. 

 App_MPU_CPU0: Point to the path where the application .out for A15 MPU is located
 App_DSP1: Point to the path where the dsp core 1 application is located
 App_DSP2: Point to the path where the dsp core 2 application is located

export APP_MPU_CPU0=$(TI_PDK_INSTALL_DIR)/packages/ti/boot/sbl/binary/idkAM572x/example/armv7/bin/sbl_app.out

export APP_DSP1=$(TI_PDK_INSTALL_DIR)/packages/ti/boot/sbl/binary/idkAM572x/example/c66/dsp1/bin/sbl_app.xe66

export APP_DSP2=$(TI_PDK_INSTALL_DIR)/packages/ti/boot/sbl/binary/idkAM572x/example/c66/dsp2/bin/sbl_app.xe663

export APP_IPU1_CPU0=$(TI_PDK_INSTALL_DIR)/packages/ti/boot/sbl/binary/idkAM572x/example/m4/ipu1/bin/sbl_app.xem4

export APP_IPU1_CPU0=$(TI_PDK_INSTALL_DIR)/packages/ti/boot/sbl/binary/idkAM572x/example/m4/ipu2/bin/sbl_app.xem4

3. If it is not required to load an application on specific core leave the variable blank.

4. Run the script file

5. An application image by name app is created in the path pointed by BIN_PATH variable

6. Copy the Bootlaoder image(MLO) and application(app) in the SD card to boot using MMCSD boot mode.

NOTE

  • The AM57xImageGen.sh script depends on tools like mono to execute the out2rprc.exe.
  • The linux host environment needs to have this tool installed to execute this script.
  • Refer this link to download the mono tool

Windows environment:

Command to build the test application.

Go to cd (TI_PDK_INSTALL_DIR)\packages\ti\boot\sbl

gmake example BOARD=<BOARD> SOC=<SOC> to build the application 
gmake example_clean BOARD=<BOARD>

Example:

gmake example BOARD=idkAM572x SOC=AM572x

To create the final bootable application image use the AM57xImageGen script and follow these steps

1. Set the following environment variable in windows command prompt

BIN_PATH: Pointing to the path where the AppImage needs to be generated 

Ex:  set BIN_PATH=%TI_PDK_INSTALL_DIR%\packages\ti\boot\sbl\binary 

2. Edit the batch file to point to the application elf files by setting the input application variables.

  App_MPU_CPU0: Point to the path where the application .out for A15 MPU is located
  App_DSP1: Point to the path where the dsp core 1 application is located
  App_DSP2: Point to the path where the dsp core 2 application is located

set App_MPU_CPU0=%TI_PDK_INSTALL_DIR%\packages\ti\boot\sbl\binary\idkAM572x\example\armv7\bin\sbl_app.out

set App_DSP1=%TI_PDK_INSTALL_DIR%\packages\ti\boot\sbl\binary\idkAM572x\example\c66\dsp1\bin\sbl_app.xe66

set App_DSP2=%TI_PDK_INSTALL_DIR%\packages\ti\boot\sbl\binary\idkAM572x\example\c66\dsp2\bin\sbl_app.xe66

set App_IPU1_CPU0=%TI_PDK_INSTALL_DIR%\packages\ti\boot\sbl\binary\idkAM572x\example\m4\ipu1\bin\sbl_app.xem4

set App_IPU2_CPU0=%TI_PDK_INSTALL_DIR%\packages\ti\boot\sbl\binary\idkAM572x\example\m4\ipu2\bin\sbl_app.xem4 

3. If it is not required to load an application on specific core leave the variable blank.

4. Run the batch file

5. Follow the steps 4 to 6 listed above for Linux environment.

Setup Requirements

For information on board specific requirements like power supply, UART console port connections refer the Hardware User guide of the respective boards.

The configurations needed to setup UART console through a serial terminal application on host PC are listed in the next section.

UART Console Setup

PDK SBL prints messages on the UART Serial Console running on the host. Hence, a serial terminal application (like Tera Term/HyperTerminal/minicom) should be running on the host.

The host serial port must be configured at 115200 baud, no parity, 1 stop bit and no flow control.
Please ensure that the local echo setting for the terminal is turned off.

Loading the test application

Follow these steps to load the test application using a SD card on the target

copy the MLO to your SD card (located at %TI_PDK_INSTALL_DIR%\packages\ti\boot\sbl\binary\[BOARD]\mmcsd)

  1. copy the example app located at path pointed to by BIN_PATH to your SD card
  2. insert your SD card into your board and power on your board
  3. open teraterm to connect to the board's UART console
  4. press the "Hard Reset" button on your board

On Successful bootup you should see the following logs on the UART console for a AM572x based board.

 Sbl example.jpg

NOTE

MPU Core 0 example does a sequential check of mailbox messages sent from the other cores. On rare occasions, the check happens before the message is sent - the "<core> boot-up Successful" message might not be displayed even though the core(s) were booted successfully.

Application Integration

Memory Map

Table indicated below provides memory map details for SBL image in OCMC_RAM1.  For more details on pinmux and IO delay requirements refer this link Processor SDK Board Support

We recommend that users should refer to the linker command file and the map file for the boot loader to check for latest information on the memory utilization in the boot loader.

Location of linker command file: <PDK_INSTALL_PATH>\packages\ti\boot\sbl\board\<BOARD>\build

The SBL memory map is shown below

SBL memory map.png

NOTE

  • After the application boots and is running on the SOC, it is free to use the SBL_MEM region.
  • The pinmux data from the board library and MMU Table are part of the SBL_MEM region indicated in the figure above. If pinmux data needs to be placed at a specific location then users can update the SBL linker command file to add the BOARD_IO_DELAY_CODE and BOARD_IO_DELAY_DATA as described in Application Integration of board library for AM5x



SBL Customization

Changing boot media offsets

The location at which SBL resides on the flash is predefined by the ROM bootloader spec and so these defaults can`t be changed. However the SBL is a user defined bootloader so many of the defaults can easily be modified to meet application requirements. For example the flash offset location from which the bootloader reads the application is configured in the source files located under PDK_INSTALL_PATH\packages\ti\boot\sbl\src\<BOOT_MEDIA>

Examples of customization that can be changed:

  • QSPI/SPI flash offsets: These offsets are configured in sbl_qspi.c and sbl_spi.c
  • MMCSD: The name of the application is hard coded as app in function SBL_MMCBootImage in the sbl_mmcsd.c


Speeding up boot by increasing speed of the boot interface

The SBL for AM57xx devices uses LLD drivers to read and write from boot media supported. The SBL uses the default SOC configuration of the drivers and the speeds setup. For example, the SPI driver default SPI bitrate is 1 MHz (Refer PDK_INSTALL_PATH\packages\ti\drv\spi\src\SPI_drv.c) so if you wish to speed up boot you can update the SPI parameter in the SBL as shown below:

 SPI_Params_init(&spiParams);
 spiParams.bitRate = 24000000U;

The configuration of the driver is usually done in the boot/sbl/soc/<device>/sbl_soc.c file.

  • For SD/MMC: You can configure higher speed and change bus width using MMCSD_v1_HwAttrs_s or MMCSD_v0_HwAttrs_s
  • For QSPI: 2 pin and 4 pin mode, and input frequency is configured using QSPI_HwAttrs in the QSPI driver. Check driver for defaults.

Also, check to see if the CACHE and MMU settings for the ARM core are setup to enable fast boot.

NOTE

SYSBOOT settings for AM57xx

The SYSBOOT configuration in your hardware using Sitara devices (AM3/AM4/AM5) can play a big role in the time required to boot successfully. On these devices the boot pins configure a boot sequence for the ROM bootloader to check for valid boot image so if you have a preferred boot mode designers are required to use SYSBOOT setup such that the preferred boot media is first in the boot sequence. If the preferred boot media occurs later boot sequence, the boot is likely to add the time required by RBL to check other boot media for an valid image. For example if QSPI is the preferred boot media on your AM57xx hardware then you should have system configure SYSBOOT to boot of QSPI first using SYSBOOT setting for QSPI_1 or QSPI4 for Memory preferred booting or Production booting (Refer: Initialization chapter in TRM).Incorrect SYSBOOT configuration can causes long delays especially if peripheral boot is configured to be one of the preferred boot modes in the boot order

Reducing size of SBL and application

Another way to optimize boot times is to reduce the size of the binary that needs to be loaded by the bootloader by building the app with optimization for code size using -Os (GNU GCC) and for -O<level> when using TI compilers.

Other than compiler based optimizations developers can actively shutdown non-essential modules and features to reduce code size. For example if UART logging is not required or DDR memory is not connected in the system, the initialization functions can be removed to reduce code size.

Usage Notes

  • SBL AVS and ABB setup

AVS and ABB configuration is mandated for normal operation of AM57xx devices. All Processor SDK RTOS releases v3.3 and later contain SBL that sets up AVS and ABB configuration features using PM LLD APIs The complete details of PMIC configuration and AVS and ABB configuration required by the chip for different OPP has been implemented in the file:

PDK_INSTALL_PATH\packages\ti\boot\sbl\board\src\sbl_avs_config.c If you are using the same PMIC as GP EVM or IDK platform then you can reuse the settings as is in SBL for your custom platform

  • Configuring entry point for SBL

The two key files that help setup the entry point in the SBL build are "sbl/soc/<SOC_NAME>/sbl_init.S" and the linker command file "sbl/soc/<SOC_NAME>/linker.cmd". The global symbol Entry is used to provide the entry point to the SBL. The Base address of the memory section SBL_MEM is then used by the tiimage and GP Header tool to provide RBL the guidance to find the entry point to pass control. After MLO is created check the TI image format file(MLO or _ti.bin) or the GP Header file to confirm that the entry point matches the location of Entry symbol in the sbl.map

NOTE

The object file created by sbl_init.S should always be the first object file in the link order for the symbol Entry to be placed at the BASE address of the memory section SBL_MEM


Debugging application boot

Steps to debug application boot using Processor SDK RTOS bootloader are discussed in the article Common steps to debug application boot