Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS BOOT K2G

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide BOOT K2G



Overview

User Interface

Application

Debug


Overview

The Secondary Bootloader (SBL) for K2G does basic hardware initialization for the board to load and run applications.

Bootloader Execution Sequence

  • Power On Reset occurs
  • ROM Bootloader (RBL) executes. It checks for bootmode and attempts to load+run the SBL from that bootmode.
  • SBL begins execution from internal memory (MSMC RAM)
    • Board Initialization is done by a call to Board_init() API. For additional details refer to Processor SDK Board Support.
    • SBL setup includes configuring Pinmux, enable peripheral clocks, set up PLLs, and configure EMIF for DDR.
  • SBL finishes setup and looks for "app" to execute next. This user-modifiable application may reside in SD card or QSPI memory depending on the bootmode chosen.
  • Once located, app will be loaded into memory and execution will be branched to the application's entry address

Tools and Binary Formats

Making Bootable SBL image (MLO)

RBL loads and runs "MLO", which is a .out executable formatted by TI tools. To make a .out, such as SBL, bootable by ROM, you must follow these steps:

  1. armhex [.out file] [.rmd file]
    • .out file is the file you want to boot, such as sbl.out
    • .rmd file is an input file to specify sections information. An example can be found in: <PDK_INSTALL_DIR>/packages/ti/boot/sbl/board/evmK2G/build/sbl.rmd
    • armhex is a tool in TI ARM CGT compiler. This generates a [hex file], name of which is specified by the .rmd file
  2. b2ccs [hex file] [ccs file]
    • hex file is the output from the previous step
    • ccs file can be name of your choosing
  3. ccsAddGphdr -infile [ccs file] -outfile [gphdr file] -headerEndian BE
    • gphdr file can be the name of your choosing
  4. ccsAddGptlr -infile [gphdr file] -outfile [gptlr file]
    • gptlr file can be the name of your choosing
  5. byteswapccs [gptlr file] [MLO ccs file]
    • MLO ccs file can be the name of your choosing
  6. ccs2bin -swap [MLO ccs file] MLO
    • MLO will be created after this step

Armhex is part of TI ARM CGT, in <CCS_INSTALL_DIR>/tools/compiler/ti-cgt-arm_x.x.x/bin. The rest of the tools can be found in: <PDK_INSTALL_DIR>/packages/ti/boot/sbl/tools

Making Loadable User Application image (app)

For converting the compiled .out files to a format loadable by TI's Secondary Boot Loader (SBL), you must follow these two steps:

  1. out2rprc.exe [.out file] [rprc output]
  2. MulticoreImageGen.exe LE 55 [output name] 0 [rprc output]

Out2rprc.exe and MulticoreImageGen.exe are tools supplied by TI and can be located in the <PDK_INSTALL_DIR>/packages/ti/boot/sbl/tools folder. "rprc output" can be any spare name of your choosing. "output name" can also be any name of your choosing.

The '0' used in step 2 refers to the Core ID to boot. By default, '0' is MPU (Cortex A15) core 0. You can input a different value to boot to other cores. Valid values are:

Core Value
MPU Core 0 0
DSP Core 0 5

If MPU SMP is chosen, the same boot image and entry will be used for all MPU cores. SBL can also parse multiple boot images that are concatenated together. Simply use MulticoreImageGen as such:

MulticoreImageGen.exe LE 55 [output name] [Core ID a] [rprc output a] [Core ID b] [rprc output b] [Core ID c] [rprc output c] ...

Boot Modes

This release of SBL supports MMCSD and QSPI boot modes.

MMCSD Boot Mode

Preparing the SD card

  1. To boot the target, the SD card needs to be bootable. Follow the steps at Creating bootable SD card in windows or Creating bootable SD card in Linux.
  2. Copy "MLO" and "app" to your SD card.
    • MLO is the SBL formatted by the aforementioned tools. A pre-built MLO can be found at: <PDK_INSTALL_DIR>/packages/ti/boot/sbl/binary/evmK2G/mmcsd/bin
    • app is the target application to be booted and also formatted by the aforementioned tools. (Note that the tools for making the bootable MLO and the loadable app are different).

Booting via SD Card

  1. Insert micro SD card into the SD card slot of the board
  2. Set the board to MMC/SD bootmode by configuring the DIP switches to '0111'. Verify the bootmode on the LCD display on your board
  3. Open a serial communication terminal (such as TeraTerm, MiniCom, etc.) on host PC and connect to the UART console port
  4. Power on the board

Below is an example of K2G SBL successfully booting the diagnostic application:
K2g boot diag.jpg

QSPI Boot Mode

Preparing QSPI Flash

MLO and app needs to be flashed into QSPI memory so that they can be booted. MLO will reside at offset 0 and app will reside at offset 0x80000. QSPI flash memory map:

Offset 0x0 MLO
Offset 0x80000 app

The images can be flashed into QSPI flash by following steps given below:

  1. Copy MLO, app, and config to SD card
    • MLO is the SBL formatted by the aforementioned tools. A pre-built MLO can be found at: <PDK_INSTALL_DIR>/packages/ti/boot/sbl/binary/evmK2G/qspi/bin
    • app is the target application to be booted and also formatted by the aforementioned tools. (Note that the tools for making the bootable MLO and the loadable app are different).
    • config helps specify the memory map. The default config file can be found at: <PDK_INSTALL_DIR>/packages/ti/boot/sbl/tools/flashWriter/qspi. This config file may be altered to custom user settings if needed.
  2. In the SD card, rename MLO to "boot". This is the default name specified by the config file.
  3. Insert the SD card into the SD card slot on the board
  4. Connect to the board with CCS. Launch target configuration and connect to the ARM A15 core. GEL file will run on-connect and do basic board-level initialization
  5. Load the flash writer, qspi_flash_writer.out, to the connected core
    • A pre-built qspi_flash_writer.out can be found at: <PDK_INSTALL_DIR>/packages/ti/boot/sbl/tools/flashWriter/qspi/bin/evmK2G
  6. Run the QSPI flash writer application. You will see the following logs on the EVM's UART console:
 *** PDK QSPI Flash Writer ***
 Copying 'boot' to local memory
 Begin flashing 'boot' into QSPI
 Finished flashing 'boot' with size 20010 at offset 0
 Copying 'app' to local memory
 Begin flashing 'app' into QSPI
 Finished flashing 'app' with size 19398 at offset 80000
 Flashing completed!
NOTE

This application will flash the image at required offset without taking into consideration any overwriting to previously flashed image.

Booting via QSPI

  1. Set the board to QSPI-48 bootmode by configuring the DIP switches to '1111'. Verify the bootmode on the LCD display on your board
  2. Open a serial communication terminal (such as TeraTerm, MiniCom, etc.) on host PC and connect to the UART console port
  3. Power on the board

Memory Usage

SBL uses the last 0x40000 memory from MSMC RAM memory.

The SBL memory map is shown below:

SBL mem k2g.jpg

NOTE

app should not have loadable sections residing in SBL memory region to prevent overwriting SBL during load time. It is, however, free to use SBL memory after it is loaded and running.