Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS Building The SDK

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide Building The SDK



Helpful tips image.jpg

Useful Tip

(1) Go to RTOS SDK directory; (2) Enter "setupenv"; (3) Enter "gmake/make" for Windows/Linux host

Overview

The Processor SDK comes with pre-built libraries for everything you need to start writing an application. However, you may want to customize and rebuild from source. Inside the SDK there is a top-level Makefile that can be used to build some of the sub-components found within the SDK. Prior to calling this Makefile, run the provided script/batch file to setup your host environment variables. For components not covered by this top-level Makefile, please see guides within the respective component for build instructions.

The Makefile and environment setup script are found in the RTOS SDK directory:

 [SDK Install Path]/processor_sdk_rtos_[soc]_[version]/

The default SDK Install Path is C:\ti for Windows and /home/[user]/ti for Linux.

The pre-requisite compilers are provided in Code Compose Studio, see the CCS installation section of the Getting Started Guide.

NOTE

If you have installed the SDK and/or CCS in non-default locations follow the steps outlined in the article Processor_SDK_RTOS_Install_In_Custom_Path to build the SDK from the toplevel Makefile.


Setup Environment

Command

The SDK build environment can be configured on Windows and Linux by running an environment setup script located in the top-level RTOS SDK folder.

Windows

From the RTOS SDK directory, enter

 C:\ti\processor_sdk_rtos_[soc]_[version]> setupenv.bat

which will configure the Windows command shell environment for the installed RTOS SDK.

NOTE

  • You must re-run this batch file any time you open a new terminal.
  • Script also sets CCS installation path using TOOLS_INSTALL_PATH variable so set the variable if you are not using default CCS install path
 C:\ti\processor_sdk_rtos_[soc]_[version]>setupenv.bat
 Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
 REQUIRED for xdc release build
 Example: set CG_XML_BIN_INSTALL_PATH=C:/ti/cg_xml/bin
 Optional parameter not configured : DOXYGEN_INSTALL_PATH
 REQUIRED for xdc release build
 Example: set DOXYGEN_INSTALL_PATH=C:/ti/Doxygen/doxygen/1.5.1-p1/bin
 **************************************************************************
 Environment Configuration:
     PDK Directory             : /ti/PDK_AM~3/packages/
     CGTOOL INSTALL Directory  : C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_[version]
     TOOLCHAIN A15 Directory   : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
     TOOLCHAIN A8 Directory    : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
     TOOLCHAIN A9 Directory    : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
     TOOLCHAIN M4 Directory    : C:/ti/ccsv6/tools/compiler/ti-cgt-arm_[version]
     FPULIB_PATH               : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]/lib/gcc/arm-none-eabi/[version]/fpu
     CROSS_TOOL_PRFX           : arm-none-eabi-
     XDC_INSTALL_PATH          : C:/ti/xdctools_[version]_core
     BIOS_INSTALL_PATH         : C:/ti/bios_[version]
     IPC_INSTALL_PATH          : C:/ti/ipc_[version]
     EDMA3LLD_BIOS6_INSTALLDIR : C:/ti/edma3_lld_[version]
     NDK_INSTALL_PATH          : C:/ti/ndk_[version]
     IMGLIB_INSTALL_PATH       : C:/ti/imglib_c66x_[version]
     UIA_INSTALL_PATH          : C:/ti/uia_[version]
     PROC_SDK_INSTALL_PATH     : C:/ti/processor_sdk_rtos_[soc]_[version]
 **************************************************************************
 Changing to short name to support directory names containing spaces
 current directory: C:/ti/processor_sdk_rtos_[soc]_[version]
 PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
 **************************************************************************
NOTE

The warnings of optional parameters not configured can be ignored since we are only rebuilding the libraries and not generating a release package.

Linux

From the RTOS SDK directory, enter

 ~/ti/processor_sdk_rtos_[soc]_[version]$ source setupenv.sh

which will configure the Linux shell environment for the installed RTOS SDK.

 ~/ti/processor_sdk_rtos_[soc>]_[version]$ source setupenv.sh
 Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
 REQUIRED for xdc release build
 Example: export CG_XML_BIN_INSTALL_PATH="~/ti/cg_xml/bin"
 Optional parameter not configured : DOXYGEN_INSTALL_PATH
 REQUIRED for xdc release build
 Example: export DOXYGEN_INSTALL_PATH="~/ti/Doxygen/doxygen/1.5.1-p1/bin"
 **************************************************************************
 Environment Configuration:
     PDK Directory             : /home/[user]/ti/pdk_[soc]_[version]/packages
     CGTOOL INSTALL Directory  : /home/[user]/ti/ccsv6/tools/compiler/ti-cgt-c6000_[version]
     TOOLCHAIN A15 Directory   : /home/[user]/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
     TOOLCHAIN A8 Directory    : /home/[user]/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
     TOOLCHAIN A9 Directory    : /home/[user]/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
     TOOLCHAIN M4 Directory    : /home/[user]/ti/ccsv6/tools/compiler/ti-cgt-arm_[version]
     FPULIB_PATH               : /home/[user]/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]/lib/gcc/arm-none-eabi/[version]/fpu
     CROSS_TOOL_PRFX           : arm-none-eabi-
     XDC_INSTALL_PATH          : /home/[user]/ti/xdctools_[version]_core
     BIOS_INSTALL_PATH         : /home/[user]/ti/bios_[version]
     IPC_INSTALL_PATH          : /home/[user]/ti/ipc_[version]
     EDMA3LLD_BIOS6_INSTALLDIR : /home/[user]/ti/edma3_lld_[version]
     NDK_INSTALL_PATH          : /home/[user]/ti/ndk_[version]
     IMGLIB_INSTALL_PATH       : /home/[user]/ti/imglib_c66x_[version]
     UIA_INSTALL_PATH          : /home/[user]/ti/uia_[version]
     PROC_SDK_INSTALL_PATH     : /home/[user]/ti/processor_sdk_rtos_[soc]_[version]
 
 PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
 *******************************************************************************
NOTE

The warnings of optional parameters not configured can be ignored since we are only rebuilding the libraries and not generating a release package.


Top-Level Makefile

The SDK level makefile can be used to compile SDK sub-components after the build environment has been configured. The following sections cover the Makefile found in the top-level of the Processor SDK for RTOS.

Target Types

For each of the targets discussed below the following target type are defined:

  • <target> - This is the build target which will compile the release version of the component
  • <target>_clean - This target will clean the component

Top-Level Targets

The Processor SDK for RTOS provides the following targets by default which will invoke the corresponding component targets:

  • help - This will print target information defined in the Makefile
  • all - This will call the build target for each component defined in the Makefile
  • clean - This will call the clean target for each component defined in the Makefile
NOTE

Invoking build using "all" option in SDK top level for multicore SOC parts can take up to several hours to rebuild as the components need to be built for all cores (e.g., A15, C66x, M4). Please rebuild individual components in the PDK package for these devices to avoid long build times.

Common Targets

The following targets are common to all Processor SDKs for RTOS:

  • pdk - Builds the Platform Development Kit that includes CSL and low level drivers

Additional Targets

You can find the list of all the targets by invoking help target as described above. Depending on the capabilities and software available for a given device additional targets may also be defined:

  • demo - Builds demonstrations provided in the SDK
  • ipc_bios - Builds the IPC component provided in the SDK
  • ipc_examples - Builds the IPC examples provided in the IPC component


Usage Examples

The following examples demonstrate how to use the top-level Makefile for some common tasks. All of the examples below assume that you are calling the Makefile from the top-level of the SDK.

Windows

  • Build all
 C:\ti\processor_sdk_rtos_[soc]_[version]> gmake
  • Clean all
 C:\ti\processor_sdk_rtos_[soc]_[version]> gmake clean

Linux

  • Build all
 ~/ti/processor_sdk_rtos_[soc]_[version]$ make
  • Clean all
 ~/ti/processor_sdk_rtos_[soc]_[version]$ make clean


Rebuilding Components

Instructions for rebuilding sub-components can be found in documentation within the component. Here are a collection of useful pages:

  • Rebuild IPC (Starting in Release 3.0, IPC build has been integrated into the top-level SDK Makefile.)