Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS CCLINK

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide Networking



Overview

User Interface

Application

Debug


Introduction

CC-Link is an open-architecture network that was originally developed by the Mitsubishi Electric Corporation.It have been widely used in Process control, building automation etc. CLPA (CC-Link Partner Association) maintains the network technology and support many manufacturer supporting the application. CC-Link is available in multiple flavours i.e. CC-Link, CC-Link LT, CC-Link Safety, CC-Link IE (Industrial Ethernet) - Control and CC-Link IE Field. For further details regarding CCLink and its flavours please refer the CLPA website.[1]

Protocol Overview

The implementation will demonstrate how to create, run and test CC-Link IE Field Network Basic examples on TI platforms. The following shows the CC-Link IE Field Network Basic Overview:

  • 1 Gbit/s Ethernet based network
  • Ethernet physical layer (Cat5e cable & RJ45 connectors)
  • 254 stations per network
  • 100 meters between stations
  • Completely deterministic without using switches

Code Organization

The Directory structure for CC-Link IE Field Network Basic source code and examples for both NIMU and NIMU_ICSS is shown in the following table.

CCLink for CPSW i.e. NIMU
Master Station Source code $(TI_PDK_INSTALL_DIR)/packages/ti/transport/ndk/nimu/example/CCLink/cclink_master
SLave Station Source code $(TI_PDK_INSTALL_DIR)/packages/ti/transport/ndk/nimu/example/CCLink/cclink_slave
Test Examples script $(TI_PDK_INSTALL_DIR)/packages/ti/transport/ndk/nimu/example/CCLink/<SOC>
Test Examples main code $(TI_PDK_INSTALL_DIR)/packages/ti/transport/ndk/nimu/example/CCLink/src


CCLink for ICSS i.e. NIMU_ICSS
Master Station Source code $(TI_PDK_INSTALL_DIR)/packages/ti/transport/ndk/nimu_icss/example/CCLink/cclink_master
SLave Station Source code $(TI_PDK_INSTALL_DIR)/packages/ti/transport/ndk/nimu_icss/example/CCLink/cclink_slave
Test Examples script $(TI_PDK_INSTALL_DIR)/packages/ti/transport/ndk/nimu_icss/example/CCLink/<SOC>
Test Examples main code $(TI_PDK_INSTALL_DIR)/packages/ti/transport/ndk/nimu_icss/example/CCLink/src


Building the Examples

Use pdkProjectCreate.sh for Linux environment or pdkProjectCreate.bat for Windows.
This can be found under the <PDK>/packages folder. The only modification to these scripts, if any, is to update the CCS_INSTALL_PATH variable to point to CCS location if its not in the c:\ti\ccsv6 directory . Please refer to Rebuilding PDK for details of example project creation and how to run the example projects using CCS.

CC-Link IE Field Network Basic Example Description

For each EVM Type supported, there is a cclink example which demonstates cyclic data communication between master and slave station. Once the application is loaded via CCS and run, you will be able to see master sending cyclic data packets and slave receiving the packet. For example, the config file for NIMU for CPSW for idkAM572x, can be found in ti/transport/ndk/nimu/example/CCLink/am572x/armv7/bios/cclink_idkAM572x.cfg. The default IP address for master is 192.168.3.100 and for slave it is 192.168.3.4. If you wish to re-configure the IP address of the CPSW interface you will need to modify the following configuration parameters. make sure master and slave are in same network.

  • Ip.address = "new ip address"
  • Ip.mask = "new ip mask"
  • Ip.gatewayIpAddr = "new gatewayIpAddr"

If you do change these settings, you will be required to re-build the Example Project using CCS.

Name
Description
EVM Configuration
NIMU_CCLinkMaster_<evm/idk>XXXX_<arm/c66x/m4>Exampleproject.txt

Example demonstrates CCLink master station sending cyclic packet to slave.

icev2AM335x: Jumpers J18 and J19 need to be set properly to select CPSW or ICSS mode.

Pin2 and Pin3 need to be connected for ICSS mode and Pin1 and Pin2 for CPSW mode.

Update *.cfg file with static IP to test. NIMU for CPSW test Tests requires connection of configured Ethernet port under test to external PC on same subnet.

NIMU_CCLinkSlave_<evm/idk>XXXX_<arm/c66x/m4>Exampleproject.txt

Example demonstrates CCLink slave station receiving cyclic packet from master and sending a response back.

icev2AM335x: Jumpers J18 and J19 need to be set properly to select CPSW or ICSS mode.

Pin2 and Pin3 need to be connected for ICSS mode and Pin1 and Pin2 for CPSW mode.

Update *.cfg file with static IP to test. NIMU for CPSW test Tests requires connection of configured PRU-ICSS Ethernet port under test to external PC on same subnet.

NIMU_ICSS_CCLinkMaster_<evm/idk>XXXX_<arm/c66x/m4>Exampleproject.txt

Example demonstrates CCLink master station sending cyclic packet to slave.

icev2AM335x: Jumpers J18 and J19 need to be set properly to select CPSW or ICSS mode.

Pin2 and Pin3 need to be connected for ICSS mode and Pin1 and Pin2 for CPSW mode.

Update *.cfg file with static IP to test. NIMU for CPSW test Tests requires connection of configured Ethernet port under test to external PC on same subnet.

NIMU_ICSS_CCLinkSlave_<evm/idk>XXXX_<arm/c66x/m4>Exampleproject.txt

Example demonstrates CCLink slave station receiving cyclic packet from master and sending a response back.

icev2AM335x: Jumpers J18 and J19 need to be set properly to select CPSW or ICSS mode.

Pin2 and Pin3 need to be connected for ICSS mode and Pin1 and Pin2 for CPSW mode.

Update *.cfg file with static IP to test. NIMU for CPSW test Tests requires connection of configured PRU-ICSS Ethernet port under test to external PC on same subnet.


Running CC-Link IE Field Network Basic example

The following is the test setup needed to run the example for CCLink demonstration on TI platform. Connect the tested eth port of the evm to a switch for master station. Do the same connection for slave station to same switch.

Cclink setup pic.PNG


Once the connection is done, load master and slave station code on both evm and run them simultaneously. You would see following output on uart port of master station.

Cclink master screeshot.png

You would see following output on uart port of slave station.

Cclink slave screenshot.png