Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS CMB AddOn

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide CMB Addon




Introduction

This page describes the Circular Microphone Board (CMB) Addon library and the unit test provided in the Processor-SDK for RTOS.

The key functions in the CMB Addon library include:

  • Initialize the board connects to the CMB
  • Initialize/configure the McASP, EDMA, I2C and GPIO
  • Set up the CMB and on-board audio codec to the correct sample rate and format

The unit test demo utilizes other Processor SDK features/components:

  • SYS/BIOS application utilizing TI-RTOS features for DSP-C66x core
  • UIA for instrumentation logging

Currently, the following devices and EVMs are supported:


Requirements

The following materials are required to run this add-on unit test:

Hardware

  • TI EVMs (see list above)
  • Circular Microphone Array Board (CMB)
  • OMAP-L137 Prototype Board (for OMAP-L137 EVM only)

Software

  • Processor-SDK RTOS (4.0 or greater)
  • Code Composer Studio 6.1.3 and up


Software Design

Framework for Unit Test

The current framework is based on SYS/BIOS. The following are the overall steps:

  • The McASP/EDMA will generate interrupt every 10ms (approximately)
  • The EDMA ISR will prepare the audio frame buffer pointers (McASP/EDMA RX buffer) for further processing
  • The EDMA ISR will also send a semaphore to wake up the main task
  • When woke up, the main thread will perform the audio de-interleaving to separate the channels
  • The main thread will also output two of eight channels to McASP/EDMA TX buffer
  • The McASP/EDMA will send the TX buffer to the on-board audio codec

How to Build the CMB Library and Unit Test

K2G EVM

For Linux:

  • Under pdk_k2g_1_x_x/packages directory, run the following commands:
  source ./pdksetupenv.sh
  make cmb_clean
  make cmb
  the libraries will be in 
     pdk_k2g_1_x_x/packages/ti/addon/cmb/lib/k2g/c66/release
  the OUT file (audioAnalogLoopbackTest.out) for DSP will be built at 
     pdk_k2g_1_x_x/packages/ti/addon/cmb/test/evmK2G/analog/loopback/build/make

For Windows:

  • Under pdk_k2g_1_x_x/packages directory, run the following commands:
  pdksetupenv.bat
  gmake cmb_clean
  gmake cmb
  the libraries will be in 
     pdk_k2g_1_x_x\packages\ti\addon\cmb\lib\k2g\c66\release
  the OUT file (audioAnalogLoopbackTest.out) for DSP will be built at 
     pdk_k2g_1_x_x\packages\ti\addon\cmb\test\evmK2G\analog\loopback\build\make

OMAP-L137 EVM

For Linux:

  • Under pdk_omapl137_1_x_x/packages directory, run the following commands:
  source ./pdksetupenv.sh
  make cmb_clean
  make cmb
  the libraries will be in 
     pdk_omapl137_1_x_x/packages/ti/addon/cmb/lib/omapl137/c674/release
  the OUT file (audioAnalogLoopbackTest.out) for DSP will be built at 
     pdk_omapl137_1_x_x/packages/ti/addon/cmb/test/evmOMAPL137/analog/loopback/build/make

For Windows:

  • Under pdk_omapl137_1_x_x\packages directory, run the following commands:
  pdksetupenv.bat
  gmake cmb_clean
  gmake cmb
  the libraries will be in 
     pdk_omapl137_1_x_x\packages\ti\addon\cmb\lib\omapl137\c674\release
  the OUT file (audioAnalogLoopbackTest.out) for DSP will be built at 
     pdk_omapl137_1_x_x\packages\ti\addon\cmb\test\evmOMAPL137\analog\loopback\build\make


How to Run the Unit Test

The unit test will be loaded onto the target using JTAG. After running the unit test, the 2 out of 8 input audio channels from CMB will be output to the line-out of the on-board audio codec.

The following sections provide detailed steps for each EVM.

K2G EVM

  • Follow this link (http://processors.wiki.ti.com/index.php/Processor_SDK_RTOS_Setup_CCS) to get target configuration setup correctly.
  • Connect to the on board emulator (J1 on K2G EVM) to your PC USB
  • Plug power adaptor(12V) into the K2G EVM and power on the EVM
  • Launch the ccxml created above using "Launch Selected Configuration" from CCS 6.1.3
  • Then "Connect to C66xx_DSP"
  • Load the audioAnalogLoopbackTest.out from pdk_k2g_1_x_x/packages/ti/addon/cmb/test/evmK2G/analog/loopback/build/make
  • Run the program (loaded previously) by pressing F8
  • The program will run the unit test forever, taking the input from CMB and output to the on-board line-out


OMAP-L137 EVM

  • Follow this link (http://processors.wiki.ti.com/index.php/Processor_SDK_RTOS_Setup_CCS) to get target configuration setup correctly.
  • Connect to the on board emulator (J201 on OMAP-L137 EVM) to your PC USB
  • Plug power adaptor(5V) into the OMAP-L137 EVM and power on the EVM
  • Launch the ccxml created above using "Launch Selected Configuration" from CCS 6.1.3
  • Then "Connect to C674X_0"
  • Load the audioAnalogLoopbackTest.out from pdk_omapl137_1_x_x/packages/ti/addon/cmb/test/evmOMAPL137/analog/loopback/build/make
  • Run the program (loaded previously) by pressing F8
  • The program will run the unit test forever, taking the input from CMB and output to the on-board line-out