Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS CPPI

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide CPPI



Overview

User Interface

Application

Debug

Overview

CPPI offers developers a common way of handling different protocol interfaces that may require multiple priorities and multiple channels on a single port. CPPI defines the register set, data structures, interrupts and buffer handling for all peripherals, regardless of protocol.

CPPI is based on a buffer scatter/gather scheme, in which individual packets are broken up and then stored into small buffers, from which they are retrieved and reassembled (as opposed to using buffers that are located contiguously in memory). When protocol translation is required, a packet header can be appended in a small buffer, saving the CPU from having to rewrite the entire packet and header by performing a copy from one large buffer to another. The considerable savings in CPU cycles that result make buffer scatter/gathering the most efficient scheme for bridging and routing.

The LLD provides resource management for descriptors, receive/transmit channels and receive flows.

Driver Configuration

The driver configures the CPPI subsystem using cppiGblCfgParams(system configuration) structure. The default global configuration per device is present under cppi_device.c file provided per device.

For details about individual fields of this structure, see the Doxygen help by opening PDK_INSTALL_DIR\CPPIckages\ti\drv\CPPI\docs\doxygen\html\index.html.

APIs

API reference for application:

#include <ti/drv/CPPI/CPPI_drv.h>

Example

Name
Description
Expected Results
CPPI_Example application

Example demonstrating sample test use case. Reference example for developers

User observes the output printed over the CCS console

CPPI_UnitTestApplication

Unit Test application to test all APIs

User observes the output printed over the CCS console

Sample Example output

This came from k2k example:

**************************************************
*************** CPPI LLD usage example ***********
**************************************************
**************************************************
*************** CPPI LLD usage example ***********
**************************************************
**************************************************
**************************************************
*************** CPPI LLD usage example ***********
*************** CPPI LLD usage example ***********
**************************************************
**************************************************
*******Test running on Core 1 *******************
*******Test running on Core 0 *******************
*******Test running on Core 2 *******************
*******Test running on Core 3 *******************
Core 0 : L1D cache size 4. L2 cache size 0.
Core 2 : Starting BIOS...
Core 3 : Starting BIOS...
Core 0 : Starting BIOS...
Core 1 : Starting BIOS...
Core 0 : Created RM packet heap
Core 0 : Created IPC MessageQ heap
Core 0 : Created receive Q for Client1
Core 1 : Opened RM packet heap
Core 2 : Opened RM packet heap
Core 3 : Opened RM packet heap
Core 1 : Opened IPC MessageQ heap
Core 2 : Opened IPC MessageQ heap
Core 3 : Opened IPC MessageQ heap
Core 1 : Created receive Q for Server
Core 2 : Created receive Q for Server
Core 3 : Created receive Q for Server
Core 1 : Opened Server's receive Q
Core 1 : Waiting for QMSS to be initialized...

Core 0 : Opened Client1's receive Q for Server
Core 0 : Created receive Q for Client2
Core 0 : Opened Client2's receive Q for Server
Core 0 : Created receive Q for Client3
Core 2 : Opened Server's receive Q
Core 2 : Waiting for QMSS to be initialized...

Core 0 : Opened Client3's receive Q for Server

Core 0 : QMSS initialization done


Core 3 : Opened Server's receive Q
Core 1 : QMSS initialization done
Core 2 : QMSS initialization done
Core 3 : Waiting for QMSS to be initialized...


Core 3 : QMSS initialization done


Core 0 : QMSS CPDMA Opened
Core 1 : QMSS CPDMA Opened


Core 0 : Memory region 0 inserted
Core 0 : Number of descriptors requested : 8. Number of descriptors allocated : 8 
Core 0 : Opened Rx channel : 0
Core 0 : Opened Tx channel : 0
Core 0 : Queue Number : 8192 opened
Core 0 : Queue Number : 8193 opened
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@10853b20
Receive Queue 8193 Entry Count : 1 Rx descriptor 0x@10853b20
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@10853b50
Receive Queue 8193 Entry Count : 1 Rx descriptor 0x@10853b50
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@10853b80
Receive Queue 8193 Entry Count : 1 Rx descriptor 0x@10853b80
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@10853bb0
Receive Queue 8193 Entry Count : 1 Rx descriptor 0x@10853bb0
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@10853be0
Receive Queue 8193 Entry Count : 1 Rx descriptor 0x@10853be0
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@10853c10
Receive Queue 8193 Entry Count : 1 Rx descriptor 0x@10853c10
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@10853c40
Receive Queue 8193 Entry Count : 1 Rx descriptor 0x@10853c40
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@10853c70
Receive Queue 8193 Entry Count : 1 Rx descriptor 0x@10853c70
Core 0 : Received host descriptor from Queue 897 Sucessfully
Core 0 : Tx Channel closed successfully. Ref count :0
Core 0 : Rx Channel closed successfully. Ref count :0
Core 0 : Rx queue closed successfully. Ref count :0
Core 0 : Tx queue closed successfully. Ref count :0
Core 0 : Free queue closed successfully. Ref count :0
Core 0 : Closing CPPI CPDMA Ref count : 3
Core 0 : CPPI CPDMA closed successfully
Core 1 : Memory region 1 inserted


Core 1 : Number of descriptors requested : 8. Number of descriptors allocated : 8 
Core 2 : QMSS CPDMA Opened
Core 3 : QMSS CPDMA Opened
Core 1 : Opened Rx channel : 0


Core 1 : Opened Tx channel : 0
Core 2 : Memory region 2 inserted
Core 3 : Memory region 3 inserted
Core 1 : Queue Number : 0 opened
Core 2 : Number of descriptors requested : 8. Number of descriptors allocated : 8 
Core 3 : Number of descriptors requested : 8. Number of descriptors allocated : 8 
Core 1 : Queue Number : 1 opened
Core 2 : Opened Rx channel : 1
Core 3 : Opened Rx channel : 2
Transmit Queue 0 Entry Count : 1 Tx descriptor 0x@11853b20
Core 2 : Opened Tx channel : 1
Core 3 : Opened Tx channel : 2
Receive Queue 1 Entry Count : 1 Rx descriptor 0x@11853b20
Core 2 : Queue Number : 8192 opened
Core 3 : Queue Number : 8193 opened
Transmit Queue 0 Entry Count : 1 Tx descriptor 0x@11853b50
Core 2 : Queue Number : 8194 opened
Core 3 : Queue Number : 8195 opened
Receive Queue 1 Entry Count : 1 Rx descriptor 0x@11853b50
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@12853b20
Transmit Queue 8193 Entry Count : 1 Tx descriptor 0x@13853b20
Transmit Queue 0 Entry Count : 1 Tx descriptor 0x@11853b80
Receive Queue 8194 Entry Count : 1 Rx descriptor 0x@12853b20
Receive Queue 8195 Entry Count : 1 Rx descriptor 0x@13853b20
Receive Queue 1 Entry Count : 1 Rx descriptor 0x@11853b80
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@12853b50
Transmit Queue 8193 Entry Count : 1 Tx descriptor 0x@13853b50
Transmit Queue 0 Entry Count : 1 Tx descriptor 0x@11853bb0
Receive Queue 8194 Entry Count : 1 Rx descriptor 0x@12853b50
Receive Queue 8195 Entry Count : 1 Rx descriptor 0x@13853b50
Receive Queue 1 Entry Count : 1 Rx descriptor 0x@11853bb0
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@12853b80
Transmit Queue 8193 Entry Count : 1 Tx descriptor 0x@13853b80
Transmit Queue 0 Entry Count : 1 Tx descriptor 0x@11853be0
Receive Queue 8194 Entry Count : 1 Rx descriptor 0x@12853b80
Receive Queue 8195 Entry Count : 1 Rx descriptor 0x@13853b80
Receive Queue 1 Entry Count : 1 Rx descriptor 0x@11853be0
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@12853bb0
Transmit Queue 8193 Entry Count : 1 Tx descriptor 0x@13853bb0
Transmit Queue 0 Entry Count : 1 Tx descriptor 0x@11853c10
Receive Queue 8194 Entry Count : 1 Rx descriptor 0x@12853bb0
Receive Queue 8195 Entry Count : 1 Rx descriptor 0x@13853bb0
Receive Queue 1 Entry Count : 1 Rx descriptor 0x@11853c10
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@12853be0
Transmit Queue 8193 Entry Count : 1 Tx descriptor 0x@13853be0
Transmit Queue 0 Entry Count : 1 Tx descriptor 0x@11853c40
Receive Queue 8194 Entry Count : 1 Rx descriptor 0x@12853be0
Receive Queue 8195 Entry Count : 1 Rx descriptor 0x@13853be0
Receive Queue 1 Entry Count : 1 Rx descriptor 0x@11853c40
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@12853c10
Transmit Queue 8193 Entry Count : 1 Tx descriptor 0x@13853c10
Transmit Queue 0 Entry Count : 1 Tx descriptor 0x@11853c70
Receive Queue 8194 Entry Count : 1 Rx descriptor 0x@12853c10
Receive Queue 8195 Entry Count : 1 Rx descriptor 0x@13853c10
Receive Queue 1 Entry Count : 1 Rx descriptor 0x@11853c70
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@12853c40
Transmit Queue 8193 Entry Count : 1 Tx descriptor 0x@13853c40
Core 1 : Received host descriptor from Queue 896 Sucessfully
Receive Queue 8194 Entry Count : 1 Rx descriptor 0x@12853c40
Receive Queue 8195 Entry Count : 1 Rx descriptor 0x@13853c40
Core 1 : Tx Channel closed successfully. Ref count :0
Transmit Queue 8192 Entry Count : 1 Tx descriptor 0x@12853c70
Transmit Queue 8193 Entry Count : 1 Tx descriptor 0x@13853c70
Core 1 : Rx Channel closed successfully. Ref count :0
Receive Queue 8194 Entry Count : 1 Rx descriptor 0x@12853c70
Receive Queue 8195 Entry Count : 1 Rx descriptor 0x@13853c70
Core 1 : Rx queue closed successfully. Ref count :0
Core 2 : Received host descriptor from Queue 9026 Sucessfully
Core 3 : Received host descriptor from Queue 898 Sucessfully
Core 1 : Tx queue closed successfully. Ref count :0
Core 2 : Tx Channel closed successfully. Ref count :0
Core 3 : Tx Channel closed successfully. Ref count :0
Core 1 : Free queue closed successfully. Ref count :0
Core 2 : Rx Channel closed successfully. Ref count :0
Core 3 : Rx Channel closed successfully. Ref count :0
Core 1 : Closing CPPI CPDMA Ref count : 2
Core 2 : Rx queue closed successfully. Ref count :0
Core 3 : Rx queue closed successfully. Ref count :0
Core 1 : CPPI CPDMA closed successfully
Core 2 : Tx queue closed successfully. Ref count :0
Core 3 : Tx queue closed successfully. Ref count :0
Core 2 : Free queue closed successfully. Ref count :0
Core 3 : Free queue closed successfully. Ref count :0
Core 2 : Closing CPPI CPDMA Ref count : 1
Core 3 : CPPI CPDMA closed successfully
Core 2 : CPPI CPDMA closed successfully
Core 2 : CPPI exit successful
*******************************************************
*************** CPPI LLD usage example Done ***********
*******************************************************
Core 1 : CPPI exit successful
Core 3 : CPPI exit successful
*******************************************************
*******************************************************
*************** CPPI LLD usage example Done ***********
*************** CPPI LLD usage example Done ***********
*******************************************************
*******************************************************
Core 0 : CPPI exit successful
Core 0: exit QMSS
Instance name: RM_Server
Handle: 0x00849ee8
Type:   Server

Resource Status:

Core 0 : All resources freed successfully
*******************************************************
*************** CPPI LLD usage example Done ***********
*******************************************************

Debug FAQ

  1. CPPI Lockup
    1. CPPI can lock up if any pointer or length, including hint bits, are wrong. Use the User Guide (TRM) referenced below to verify every pointer and length in the descriptor. Also verify the hint bits (low 4 bits of each descriptor) which represents size of descriptor (not data) in 16-byte units. When using CPPI it should be at least 1 (32 bytes) if no extensions are used, or 2 (48 bytes) if some extensions are used. 0 (16 bytes) is likely to cause lock up!!
  2. See QMSS Debug FAQ for more.

Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\CPPI\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\CPPI\docs\ReleaseNotes_CPPI_LLD.pdf
Hardware Userguide/TRM UG TRM PDF
QMSS LLD (Navigator/Queueing HW component) QMSS LLD