Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS CSL

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide CSL



Overview

User Interface

Application

Debug



Overview

The Chip Support Library constitutes a set of well-defined APIs that abstract low-level details of the underlying SoC device so that a user can configure, control (start/stop, etc.) and have read/write access to peripherals without having to worry about register bit-field details. The CSL services are implemented as distinct modules that correspond with the underlying SoC device modules themselves. By design, CSL APIs follow a consistent style, uniformly across Processor Instruction Set Architecture and are independent of the OS. This helps in improving portability of code written using the CSL.

CSL is realized as twin-layer – a basic register-layer and a more abstracted functional-layer. The lower register layer comprises of a very basic set of macros and type definitions. The upper functional layer comprises of “C” functions that provide an increased degree of abstraction, but intended to provide “directed” control of underlying hardware.

It is important to note that CSL does not manage data-movement over underlying h/w devices. Such functionality is considered a prerogative of a device-driver and serious effort is made to not blur the boundary between device-driver and CSL services in this regard.

CSL does not model the device state machine. However, should there exist a mandatory (hardware dictated) sequence (possibly atomically executed) of register reads/writes to setup the device in chosen “operating modes” as per the device data sheet, then CSL does indeed support services for such operations.

The CSL services are decomposed into modules, each following the twin-layer of abstraction described above. The APIs of each such module are completely orthogonal (one module’s API does not internally call API of another module) and do not allocate memory dynamically from within. This is key to keeping CSL scalable to fit the specific usage scenarios and ease the effort to ROM a CSL based application.

In general for application recommended interfaces to be used will be driver API. CSL Functional layer APIs could be used for low-level access when required. CSL Register layer memory map is available for being used under rare cases in application when required.

The source code of the CSL is located under $(TI_PDK_INSTALL_DIR)\packages\ti\csl directory.

AM335x/AM437x

The CSL component of AM335x/AM437x Processor SDK is referred as StarterWare in the legacy baseline releases.To maintain backward compatibility for existing applications on AM335x/AM437x SOCs, StarterWare low level package is retained. Customers are recommended to use driver interfaces for ease of migration of application software across SOCs.

Chip Support Library/DAL Summary
Component Type Library
Install Package PDK
Install Directory pdk_AMX_<version>\packages\ti\starterware
Endian Support Little
Linker Path PDK_INSTALL_DIR\packages\ti\starterware\binary
Include Paths PDK_INSTALL_DIR\packages\ti\starterware\include


AM57x/K2x/C66x/C674x

Application Integration

CSL is common package supporting multiple devices.Software layer using CSL source would need to pass compile time define -DSOC_XXX. Refer ti\csl\soc.h for list of devices/SOC's

Refer list of APIs/interfaces available under <PDK_INSTALL_DIR\packages\ti\csl> directory

Chip Support Library Summary
Component Type Library
Install Package PDK
Install Directory PDK_INSTALL_DIR\packages\ti\csl
Endian Support Little
Linker Path PDK_INSTALL_DIR\packages\ti\csl
Include Paths $(TI_PDK_INSTALL_DIR)\packages\
Reference Guides See docs under Install Directory


CSL-FL EXAMPLES

These are example projects to test the functionality of API in CSL-FL layers. The following is the list of CSL-FL test examples which are supported with the CSL library:

  • DCAN
  • EDMA
  • GPIO
  • MAILBOX
  • I2C
  • QSPI
  • WDTIMER
  • MMCSD
  • MMU
  • SPINLOCK
  • UART
  • ECC : Limited to applicable SOC's/Boards:idkAM574x

In order build the projects:

  • Navigate to pdk_[soc]_[version]\packages
  • Run pdksetupenv.bat (windows) OR pdksetupenv.sh (linux).
  • Navigate to pdk_[soc]_[version]\packages\ti\csl

All CSL-FL examples can be cleaned and rebuilt with the following commands on windows:

C:\ti\pdk_[soc]_[version]\packages\ti\csl>gmake app_clean
C:\ti\pdk_[soc]_[version]\packages\ti\csl>gmake apps

All CSL-FL examples can be cleaned and rebuilt with the following commands on linux:

~/ti/pdk_[soc]_[version]/packages/ti/csl$ make app_clean
~/ti/pdk_[soc]_[version]/packages/ti/csl$ make apps
  • All the output binary files will be generated in common location i.e. pdk_[soc]_[version]\packages\ti\binary\[EXAMPLE]\bin\[BOARD]\
  • DCAN RTOS example

TI RTOS support is available for CSL DCAN example on AM572x platform. Refer to the readme document at below path for more details.

<PDK Root>/packages/ti/csl/example/dcan/dcanLoopback