Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS EDMA3

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide EDMA3



Overview

User Interface

Application

Debug



Introduction

EDMA3 Low Level Driver is targeted to device drivers and applications for submitting and synchronizing EDMA3-based DMA transfers.

EDMA3 is a peripheral that supports data transfers between two memory mapped devices. It supports EDMA as well as QDMA channels for data transfer.

The EDMA3 LLD consists of an EDMA3 Driver and EDMA3 Resource Manager. The EDMA3 Driver provides functionality that allows device drivers and applications for submitting and synchronizing with EDMA3 based DMA transfers. In order to simplify the usage, this component internally uses the services of the EDMA3 Resource Manager and provides one consistent interface for applications or device drivers.

Driver Configuration

EDMA3 peripheral IP is re-used in different SoCs with only a few configuration changes:

  • Number of DMA and QDMA channels supported
  • Number of PARAM sets available
  • Number of event queues and transfer controllers etc.

The EDMA3 peripheral is used by other peripherals for their DMA needs thus the EDMA3 Driver needs to cater to the requirements of device drivers of these peripherals as well as other application software that may need to use DMA services. Resources for EDMA driver is managed through RM sub module within driver.

APIs

API reference for EDMA3 driver

#include <ti/sdo/edma3/drv/edma3_drv.h>

API reference for EDMA3 Resource Management layer

#include <ti/sdo/edma3/rm/edma3_rm.h>

Additional References

EDMA3 Driver Summary
Component Type Library
Install Package EDMA3 Low level drivers
Install Directory <root_install_dir>/edma3_lld_xx_xx_xx_xx
Project Type N/A
Endian Support Little and Big
Library Name edma3_lld_drv.ae66 (little endian), edma3_lld_drv.ae66e (big endian),edma3_lld_drv.aa15fg (A15),edma3_lld_drv.aem4 (M4)
Linker Path

<ti/sdo/edma3/drv/lib/[cpu]>
<ti/sdo/edma3/rm/lib/[soc-evm]>

Include Paths <ti/sdo/edma3/drv>
<ti/sdo/edma3/rm>
Reference Guides See docs under install directory
Additional Resources Programming the EDMA3 using the Low-Level Driver (LLD)
License BSD

EDMA3 sample libs

EDMA3 Driver Sample Summary
Component Type Library
Install Package EDMA3 Low level drivers
Install Directory <root_install_dir>/edma3_lld_xx_xx_xx_xx
Project Type N/A
Endian Support Little and Big
Library Name

edma3_lld_drv_sample.ae66 (little endian), edma3_lld_drv_sample.ae66e (big endian), edma3_lld_drv_sample.aa15fg (A15), edma3_lld_drv_sample.aem4 (M4)

edma3_lld_rm_sample.ae66 (little endian), edma3_lld_rm_sample.ae66e (big endian), edma3_lld_rm_sample.aa15fg (A15), edma3_lld_rm_sample.aem4 (M4)

Linker Path

<ti/sdo/edma3/drv/sample/lib/[soc-evm]/[cpu]>
<ti/sdo/edma3/rm/sample/lib/[soc-evm]/[cpu]>

Include Paths <ti/sdo/edma3/drv>
<ti/sdo/edma3/rm>
Reference Guides See docs under install directory
Additional Resources Programming the EDMA3 using the Low-Level Driver (LLD)
License BSD