Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS EMAC

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide EMAC



Overview

User Interface

Application

Debug


Introduction

EMAC driver provides a well defined API layer which allows applications to use the EMAC peripheral to control the flow of packet data from the processor to the PHY and the MDIO module to control PHY configuration and status monitoring.

Driver Configuration

Board Specific Configuration

All the board specific configurations eg:enabling and pin-mux of RGMII/MDIO pins should be performed before calling any driver APIs.By default Board_Init() API supports all initialization sequence for TI supported EVMs.Refer Processor SDK RTOS Board Support for additional details.

Once the board specific configuration is complete driver API emac_open() can be called to initialize driver

EMAC Configuration Structure

The EMAC_soc.c file binds driver with hardware attributes on the board through EMAC_Cfg structure. This structure must be provided to EMAC driver. It must be initialized before the emac_open() function is called. Prior to calling emac_open, the address of the descriptor region base to be inserted into the QMSS memory region MUST be provided by the user application and updated into the EMAC_HwAttrs_V1 structure which is part of the EMAC_Cfg. EMAC_socGetInitCfg() can be invoked to get the EMAC initial configuration and EMAC_socSetInitCfg to update the configuration as illustrated below.

   EMAC_socGetInitCfg(0, &emac_cfg);
   /* Need to update the descriptor base address */
   emac_cfg.p_desc_base = &gHostDesc;
   /* Now set the config after updating desc base address */
   EMAC_socSetInitCfg(0, &emac_cfg);

For details about individual fields of this structure, see the Doxygen help by opening PDK_INSTALL_DIR\packages\ti\drv\uart\docs\doxygen\html\index.html.

APIs

API reference for application:

#include <ti/drv/emac/emac_drv.h>
EMAC Open

API to allow the calling application to supply a valid port number and open configuration data. Note that providing a descriptor base address is the code snippet below is only required for Keystone devices (at this time only EVMK2G is supported) which is required to set up the Host descriptor memory region in the QMSS sub-system.

...
Board_init(boardCfg);
EMAC_socGetInitCfg(0, &emac_cfg);
/* Need to update the descriptor base address */
emac_cfg.p_desc_base = &gHostDesc;
/* Now set the config after updating desc base address */
EMAC_socSetInitCfg(0, &emac_cfg);
port_num = 0;
/* Need to populate open_cfg structure with application specific configuration */
openReturn = emac_open([port_num, &open_cfg))


EMAC Config

API to allow the calling application to provide RX filter configuration. This API is currently only supported for C6657 & OMAPL13x SOCs.

/* fill in cfg_info structure */
configReturn = emac_config(port_num, &cfg_info);

At this point EMAC driver is ready to send and receive packets.


EMAC Close

API to allow user application to close an opened EMAC port. This API will release all resources allocated during the call to emac_open().

EMAC Get Statistics

API to allow user application to retrieve statistics for specified port

emac_get_statistics(port_num, * p_stats)


EMAC Receive Packet Poll

API (emac_pkt_poll) to provide a while(1) loop to receive packets. This API must be called within a task context as it is blocking API. Internally, this API will PEND on a semaphore until it it POSTED by the Hwi Interrupt Handler. The Hwi interrupt handling is setup during the call to the emac_open API at which time the user application, as part of the open, configures a receive packet callback. Once there is a received packet, the emac_pkt_poll function will invoke this callback to provide the packet to the user application and resume PENDING on a semaphore until there is another packet to receive. This API will not return to the user application.


EMAC Send

API to allow user application to send packet on opened EMAC port.

retVal = emac_send(port_num, pkt_desc);


EMAC Poll

API to allow user application to poll the status of opened EMAC port. Status info will be returned in the link_info structure.

emac_poll(port_number, &link_info);


Example

Name
Description
Expected Results
EMAC_BasicExample_evmK2G

EMAC Loopback test at CPSW switch interface. Reference example for developers

Example demonstrates loopback capability by sending dummy broadcast packet to CPSW switch. Unit test registers receive packet callback routine with LLD to be called for RX packet. Call back routine will extract packet received, perform simple memory comparison against packet sent for integrity check. Unit test will iterate over configured packet count for packet transmission and reception check.

Unit Test will print "All tests have passed" via UART console.

EMACLoopback_testProject (for DRA7xx, C6657, OMAPL137 & OMAPL138)

EMAC Loopback test at CPSW switch interface. Reference example for developers

Example demonstrates loopback capability by sending dummy broadcast packet to CPSW switch. Unit test registers receive packet callback routine with LLD to be called for RX packet. Call back routine will extract packet received, perform simple memory comparison against packet sent for integrity check. Unit test will iterate over configured packet count for packet transmission and reception check.

This example needs to be run on the OMAPL137 and OMAPL138 platforms using external loopback cable. OMAPL137 EVM is having two Ethernet ports. Connect the loopback cable to the port 1 (ENET-P1) while running the loopback example.

Unit Test will print "Loopback Test completed successfully on core 0" via CCS console for C6657 and on UART serial console for OMAPL13x.

EMAC_PktInspectionExample (for all DRA7xx devices)

This demonstrates how to write an application to filter Ethernet packets based on IP address

Prerequisites:

  • Install the packETH utility (v 1.8.1) on a Linux PC. The packETH tool is available for Windows as well, but not all features are supported
  • Download the test PCAP files and update the source and dest MAC address of the PC and EVM to be used in the test. The tcprewrite utility can be used to set the new MAC addresses (i.e. tcprewrite --enet-smac=<PC-MAC-address> --enet-dmac=<EVM-MAC-address> -i ./ip1_test.pcap -o ./ip1_test.pcap)

Steps:

  • Launch the packETH utility on the Linux PC with root permissions
  • Go to the "Gen-S" tab of the packETH utility and select the PCAP files to be used
  • Set the transfer rate for each PCAP file (i.e. 200 Mbit/s and 150 Mbit/s)
  • Set the total packets to transfer to 500000
  • Load and run the EMAC packet inspection application to the IPU1 core
  • Hit the "Send" button on the packETH utility to start streaming
  • The packet streaming should last for few seconds

Pass criteria:

  • The total packet sent for each stream is shown at the bottom of the packETH widow. The packet stream statistics must match the packet statistics printed by the DUT via serial port
  • The packet inspection utility periodically prints the EMAC statistics, which include DMA overruns, underruns and other error. No errors should be seen during the transfer.

Fail criteria:

  • Packet count mismatch between packETH utility and counters from the IPU1 application
  • Any EMAC errors reported by the IPU1 application

Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\emac\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\emac\docs\ReleaseNotes_EMAC_LLD.pdf