Processor SDK RTOS Examples

From Texas Instruments Wiki
Jump to: navigation, search


RTOS Software Developer Guide Getting Started with RTOS Examples




Overview

The SYS/BIOS examples gets user started with development of code using a real-time operating system. These are simple examples that does not get into details of software components provided in the SDK.

NOTE

All instructions on this wiki have been created using CCSv6 but should apply to CCSv7. Please report any issues by posting on E2E forums

ARM Cortex-A15

The hello example serves as a basic sanity check program for SYS/BIOS. It demonstrates how to print the string 'hello world' to stdout. As a sample we will use the AM572x device to describe the steps. The same steps can be used for create hello world examples for A15 cores in Keystone 2 family of devices.

NOTE

1. Create a work space folder (\ti\am_572x_hello_workspace) under ti folder to be used for Hello Example project, and start CCS. You may be prompted with New Products Discovered, so select all and click on Finish

2. On CCS click View --> Resource Explorer (Examples).

3. On SYS/BIOS scroll down to AM572X --> Cortex A --> Generic Example --> click on Hello Example.

Sys bios hello example screen 1.jpg

4. To import Hello Example, on the right window click on step 1. Import The Example to CCS Project.

5. On New CCS Project window enter project name and then click Next.

Sys bios hello example screen 2.jpg

6. On RSTC window select platform name: ti.platforms.evmAM572X and check that the target is set to gnu.targets.arm.A15F

7. Click Finish. Your project should show up on Project Explorer window.

8. To get log message to print on console add this variable to hello.cfg file:

var SemiHostSupport = xdc.useModule('ti.sysbios.rts.gnu.SemiHostSupport');

Note: You also need to replace the nosys library in linker with rdimon which is the Semi-Hosting enabled BSP library.

Right click on project --> Show Build Settings... --> Build --> GNU Linker --> Libraries

9. Build Hello Example project by Right click on Hello Project and click Build project.

10. Create new target configuration (if one doesn`t exist) as described in here.

11. Right click on the target configuration and Launch target configurations.

11. Right click CortexA15_0 and connect target.

12. Load and run Hello Example out file. You should see Hello World string displayed on console window.



ARM Cortex-A9

The hello example serves as a basic sanity check program for SYS/BIOS. It demonstrates how to print the string 'hello world' to stdout.

1. Create a work space folder (\ti\am_437x_hello_workspace) under ti folder to be used for Hello Example project, and start CCS. You may be prompted with New Products Discovered, so select all and click on Finish

2. On CCS click View --> Resource Explorer (Examples).

3. On SYS/BIOS scroll down to AM4378 --> Cortex A --> Generic Example --> click on Hello Example.

RTOS CortexA9 HelloWorld.png

4. To import Hello Example, on the right window click on step 1. Import The Example to CCS Project.

5. On New CCS Project window enter project name and then click Next.

HelloWorld cortexA9.png HelloWorld cortexA9 rtscConfig.png

6. On RSTC window select platform name: ti.platforms.evmAM437X and check that the target is set to gnu.targets.arm.A9F

7. Click Finish. Your project should show up on Project Explorer window.

8. To get log message to print on console add this variable to hello.cfg file:

var SemiHostSupport = xdc.useModule('ti.sysbios.rts.gnu.SemiHostSupport');

Note: You also need to replace the nosys library in linker with rdimon which is the Semi-Hosting enabled BSP library.

Right click on project --> Show Build Settings... --> Build --> GNU Linker --> Libraries

9. Build Hello Example project by Right click on Hello Project and click Build project.

10. Create new target configuration (if one doesn`t exist) as described here.

11. Right click on the target configuration and Launch target configurations.

11. Right click CortexA9_0 and connect target.

12. Load and run Hello Example out file. You should see Hello World string displayed on console window.


ARM Cortex-A8

The hello example serves as a basic sanity check program for SYS/BIOS. It demonstrates how to print the string 'hello world' to stdout.

1. Create a work space folder (\ti\am_335x_hello_workspace) under ti folder to be used for Hello Example project, and start CCS. You may be prompted with New Products Discovered, so select all and click on Finish

2. On CCS click View --> Resource Explorer (Examples).

3. On SYS/BIOS scroll down to AM3352 --> Cortex A --> Generic Example --> click on Hello Example.

RTOS CortexA8 HelloWorld.png

4. To import Hello Example, on the right window click on step 1. Import The Example to CCS Project.

5. On New CCS Project window enter project name and then click Next.

HelloWorld cortexA8.png HelloWorld cortexA8 rtscConfig.png

6. On RSTC window select platform name: ti.platforms.evmAM335X and check that the target is set to gnu.targets.arm.A8F

7. Click Finish. Your project should show up on Project Explorer window.

8. To get log message to print on console add this variable to hello.cfg file:

var SemiHostSupport = xdc.useModule('ti.sysbios.rts.gnu.SemiHostSupport');

Note: You also need to replace the nosys library in linker with rdimon which is the Semi-Hosting enabled BSP library.

Right click on project --> Show Build Settings... --> Build --> GNU Linker --> Libraries

9. Build Hello Example project by Right click on Hello Project and click Build project.

10. Create new target configuration (if one doesn`t exist) as described here.

11. Right click on the target configuration and Launch target configurations.

11. Right click CortexA8_0 and connect target.

12. Load and run Hello Example out file. You should see Hello World string displayed on console window.


ARM Cortex-M4

The hello example serves as a basic sanity check program for SYS/BIOS. It demonstrates how to print the string 'hello world' to stdout.

1. Create a work space folder (\ti\am_572x_hello_workspace) under ti folder to be used for Hello Example project, and start CCS. You may be prompted with New Products Discovered, so select all and click on Finish

2. On CCS click View --> Resource Explorer (Examples).

3. on SYS/BIOS scroll down to AM572X --> Cortex M --> Generic Example --> click on Hello Example.

SYSBIOS hello world M4 template.jpg

4. To import Hello Example, on the right window click on step 1. Import The Example to CCS Project.

5. On New CCS Project window enter project name and then click Next.

SYSBIOS M4 platformSelect.jpg

6. On RSTC window select platform name: ti.platforms.evmAM572X and check that the target is set to gnu.targets.arm.elf.M4

7. Click Finish. Your project should show up on Project Explorer window.

8. Build Hello Example project by Right click on Hello Project and click Build project.

9. Launch target configurations using appropriate emulator to connect to AM572X EVM.

10. Right click CortexA15_0 and connect target. From the Scripts menu select AM572x Multicore Initialization->IPU1SSClkEnable_API.

11. Connect to the Cortex_M4_IPU1_C0. Load and run Hello Example out file. You should see Hello World string displayed on console window.


DSP C66x

The hello example serves as a basic sanity check program for SYS/BIOS. It demonstrates how to print the string 'hello world' to stdout. As a sample we will use the AM572x device to describe the steps but the same steps can be used for create hello world examples for C66x cores in Keystone I and Keystone 2 family of devices.

NOTE

  • The C66x examples corresponding Keystone I devices can be located under C66x Multi-core DSP devies in the Resource Explorer. Refer Screenshot for Keystone I devices

1. Create a work space folder (\ti\am_572x_hello_workspace) under ti folder to be used for Hello Example project, and start CCS. You may be prompted with New Products Discovered, so select all and click on Finish

2. On CCS click View --> Resource Explorer (Examples).

3. on SYS/BIOS scroll down to AM572X --> C66x --> Generic Example --> click on Hello Example.

SYSBIOS hello world dsp template.jpg

4. To import Hello Example, on the right window click on step 1. Import The Example to CCS Project.

5. On New CCS Project window enter project name and then click Next.

SYSBIOS DSP platformSelect.jpg

6. On RSTC window select platform name: ti.platforms.evmAM572X and check that the target is set to ti.targets.elf.C66 (Auto populated)

7. Click Finish. Your project should show up on Project Explorer window.

8. Build Hello Example project by Right click on Hello Project and click Build project.

10. Create new target configuration (if one doesn`t exist) as described here.

11. Right click on the target configuration and Launch target configurations.

12. Right click CortexA15_0 and connect target. From the Scripts menu select AM572x Multicore Initialization->DSP1SSClkEnable_API.

13. Route the GPTimer5 suspend ctrl signal to the DSP using the Scripts menu GP timer Suspend Ctrl -> GPTimer5SuspendCtl_DSP1SS_BIOS as described here.

14. Connect to C66x_DSP1 Load and run Hello Example out file. You should see Hello World string displayed on console window.

DSP C674x

The hello example serves as a basic sanity check program for SYS/BIOS. It demonstrates how to print the string 'hello world' to stdout. As a sample we will use the C6748 device to describe the steps but the same steps can be used for create hello world examples for C674x cores in OMAPL1x/DA8x family of devices.

NOTE

  • Locate the appropriate device that you are using to make sure the correct SYSBIOS platform definiition gets used in the build

1. Create a work space folder ( Eg. tirtos_hello_workspace) that can be used for Hello Example project, and start CCS. You may be prompted with New Products Discovered, so select all and click on Finish Note: at this stage the version of SYSBIOS and corresponding dependencies are assumed to be discovered by CCS. If not please follow the steps described here: Discovering_SDK_products

2. On CCS click View --> Resource Explorer Classic (Examples).

3. on SYS/BIOS scroll down to C6748 /OMAPL1x and select --> C674x --> Generic Example --> click on Hello Example.

OMAPL138 SYSBIOS TI RTOS CCSv7.png

4. To import Hello Example, on the right window click on step 1. Import The Example to CCS Project.

5. On New CCS Project window enter project name and then click Next.

Create Project Step1.png

6. On RSTC window select platform name: ti.platforms.evmc6748 and check that the target is set to ti.targets.elf.C674 (Auto populated)

Create Project Step2.png

7. Click Finish. Your project should show up on Project Explorer window.

8. Build Hello Example project by Right click on Hello Project and click Build project.

10. Create new target configuration (if one doesn`t exist) as described here.

11. Right click on the target configuration and Launch target configurations.

12. Developers can Connect to the C674x on OMAPL137/C6747/C6748 can connect directly to the DSP. For OMAPL138 device, you will need to connect to the ARM as this is ARM master boot device and ARM needs to power up the DSP You should see the following log in the Console

C674X_0: Output: 	Target Connected.
C674X_0: Output: 	---------------------------------------------
C674X_0: Output: 	Memory Map Cleared.
C674X_0: Output: 	---------------------------------------------
C674X_0: Output: 	Memory Map Setup Complete.
C674X_0: Output: 	---------------------------------------------
C674X_0: Output: 	PSC Enable Complete.
C674X_0: Output: 	---------------------------------------------
C674X_0: Output: 	PLL0 init done for Core:300MHz, EMIFA:25MHz
C674X_0: Output: 	DDR initialization is in progress....
C674X_0: Output: 	PLL1 init done for DDR:150MHz
C674X_0: Output: 	Using DDR2 settings
C674X_0: Output: 	DDR2 init for 150 MHz is done
C674X_0: Output: 	---------------------------------------------

14. Connect to C674x_DSP1 Load and run Hello Example out file. You should see Hello World string displayed on console window.

Hello world dsp674x rtos.png



Usage Notes

After execution of the hello world examples on the core, the CCS Editor may report "Can't find a source file" error messages when you pause or the application exits/aborts after completion. This occurs due to source files from SYSBIOS or XDC packages not being in the default search path of the CCS Editor. when you run into this issue, you can navigate to the file using Locate file option in the Editor. Once you provide the location the CCS Editor will be able to locate all the other required files from that package based on relative path.

For example, when running SYS/BIOS Hello Example using AM57x-GP EVM if you see the message

 Can't find a source file at "/db/ztree/library/trees/xdctargets/xdctargets-i02/src/gnu/targets    /arm/rtsv7A/syscalls.c"
 Locate the file or edit the source lookup path to include its location. The above file is located  under file path ${PROC_SDK_DIR}\bios_6_42_02_29\packages\gnu\targets\arm\rtsv7A

You can also prevent these issues by adding the Processor SDK components to file search path under Windows->Preferences options in CCS GUI.


Known Issues

  • SYS/BIOS examples for Cortex-A15 generate linker errors due to the FPU related flags

Some versions of CCS are impacted by linker setting used in CCS RTOS templates and may need some manual modification to set the correct -mfpu, -mcpu and -march. If you are seeing VFP errors in the link step, you are most likely running into this issue. To correct this issue please check the resolution here: https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/539973



Useful Resources