Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS Flashing Bootable Images

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide Flashing Bootable Images



Overview

The Processor SDK RTOS for C6657, C6678, K2H, K2E, and K2L EVMs includes a script in the directory

 [SDK Install Path]/processor_sdk_rtos_<platform>_<version>/bin

named program_evm.js. The purpose of this script is to automatically flash bootable images onto your EVM.

The following sections will describe how to use this script and the default flashable binaries in the Processor SDK RTOS.

Requirements

  • A Windows or Linux PC
  • Processor SDK RTOS installed on your PC. The version to install must match the SOC you plan to use
  • Code Composer Studio installed on your PC
  • An USB connection to your EVM emulator
NOTE

Your board should be set to NO-BOOT mode. Please refer to the boot mode dip switch settings for different boot modes on your EVM Hardware User Guide. See this page for a link to all supported EVM information.

Directory Structure

The files used are in the Processor SDK RTOS directory. Expanded below are the relevant files and directories for flashing the bootable images for C667x, but a similar structure is used for C665x.

├── bin
│   ├── configs
│   │   └── evm6678l
│   │       ├── evm6678l.ccxml
│   │       ├── evm6678le.ccxml
│   │       ├── evm6678le-linuxhost.ccxml
│   │       └── evm6678l-linuxhost.ccxml
│   ├── logs
│   └── program_evm.js
└── prebuilt-images
    ├── eeprom50.bin
    ├── eeprom51.bin
    ├── eepromwriter_evm6678l.out
    ├── eepromwriter_input50.txt
    ├── eepromwriter_input51.txt
    ├── eepromwriter_input.txt
    ├── nandwriter_evm6678l.out
    ├── nand_writer_input.txt
    ├── norwriter_evm6678l.out
    └── nor_writer_input.txt

Below is the expanded tree for K2H. Similarly, this also applies to K2E and K2L EVMs.

├── bin
│   ├── configs
│   │   └── evmk2h
│   │       ├── evmk2h.ccxml
│   │       ├── evmk2h-linuxhost.ccxml
│   │       └── program_evm_config
│   ├── logs
│   └── program_evm.js
└── prebuilt-images
    ├── app
    ├── config
    ├── MLO
    └── spi_flash_writer.out

Default Binaries and Setup

Processor SDK RTOS provides the basic CCXML files to connect to your SOC. There is a separate CCXML file for each SOC, emulator, and host OS combination. These CCXML files are located in:

 [SDK Install Path]/processor_sdk_rtos_<platform>_<version>/bin/config/<SOC>

Users can choose to use their own CCXML file by setting the environment variable, PROGRAM_EVM_TARGET_CONFIG_FILE, to point to their CCXML file in their terminal or command prompt.

You can create your own CCXML file by opening CCSv6 --> View --> Target Configurations, and right-clicking on the Target Configuration pane to select New Target Configuration. After selecting your SOC and emulator, remember to set the appropriate GEL file in the advance options for Core 0. The GEL file is used to do basic SOC initialization upon connecting to the core.

Processor SDK RTOS also provides the basic binaries needed to perform flashing. These are separated into two categories - flashwriters and flash images.

Flashwriters

  • [C66x] eepromwriter_<SOC>.out - writes content to your EVM EEPROM flash memory
  • [C66x] norwriter_<SOC>.out - writes content to your EVM NOR flash memory
  • [C66x] nandwriter_<SOC>.out - writes content to your EVM NAND flash memory
  • [K2H/E/L] spi_flash_writer.out - writes multiple images to your NOR flash memory

Flash images

  • [C66x] eeprom50.bin - eeprom binary for address 0x50. The default for C66x is the POST application.
  • [C66x] eeprom51.bin - eeprom binary for address 0x51. The default for C66x is the Intermediate Boot Loader (IBL).
  • [C66x] nor.bin - nor binary to be used for NOR boot. May not be provided for every EVM or release version.
  • [C66x] nand.bin - nand binary to be used for NAND boot. May not be provided for every EVM or release version.
  • [K2H/K2E/K2L] app - NOR binary to be booted by Secondary Bootloader. The default for Keystone 2 is the POST application
  • [K2H/K2E/K2L] MLO - Secondary Bootloader. The default flash location is in SPI NOR flash memory at offset 0.

Usage

For Windows users:

 > cd [SDK Install Path]\processor_sdk_rtos_<platform>_<version>\bin
 > set DSS_SCRIPT_DIR=[CCS Install Path]\ccsv6\ccs_base\scripting\bin
 > %DSS_SCRIPT_DIR%\dss.bat program_evm.js [tmdx|tmds]evm(6678|6657|k2h|k2e|k2l)[l|le|ls][-le|-be]

For Linux users:

 > cd [SDK Install Path]/processor_sdk_rtos_<platform>_<version>/bin
 > export DSS_SCRIPT_DIR=[CCS Install Path]/ccsv6/ccs_base/scripting/bin
 > $DSS_SCRIPT_DIR/dss.sh program_evm.js [tmdx|tmds]evm(6678|6657|k2h|k2e|k2l)[l|le|ls][-le|-be]

The last argument depends on the SOC that you have, concatenated with the options to select emulator and endianness:

  • l: EVM uses XDS100 on-board Emulator
  • le: EVM uses 560 Mezzanine Emulator daughter card
  • ls: EVM uses XDS200 Emulator card
  • -le: Little Endian
  • -be: Big Endian
NOTE

  • By default, the images provided are little endian.
  • Also by default, Keystone 2 EVMs are expected to only use the XDS2xx Emulator. You do not have to supply the emulator in the parameter for K2H/K2E/K2L.

Some examples are:

TMDXEVM6678LE little endian

  > $DSS_SCRIPT_DIR/dss.sh program_evm.js tmdxevm6678le-le

TMDSEVM6657LS little endian

  > $DSS_SCRIPT_DIR/dss.sh program_evm.js tmdxevm6657ls-le

EVMK2H little endian

  > $DSS_SCRIPT_DIR/dss.sh program_evm.js tmdsevmk2h

EVMK2E little endian

  > $DSS_SCRIPT_DIR/dss.sh program_evm.js tmdsevmk2e

Sample Output

C:\ti\processor_sdk_rtos_c665x_2_00_01_07\bin>%DSS_SCRIPT_DIR%\dss.bat program_evm.js tmdxevm6657ls-le
board: evm6657l
endian: Little
emulation: XDS200 emulator
binaries: ../prebuilt-images/
ccxml: C:\ti\processor_sdk_rtos_c665x_2_00_01_07\bin/configs/evm6657l/evm6657ls.ccxml
C66xx_0: GEL Output:
Connecting Target...

C66xx_0: GEL Output: DSP core #0

C66xx_0: GEL Output: C6657L GEL file Ver is 1.006

C66xx_0: GEL Output: Global Default Setup...

C66xx_0: GEL Output: Setup Cache...

C66xx_0: GEL Output: L1P = 32K

C66xx_0: GEL Output: L1D = 32K

C66xx_0: GEL Output: L2 = ALL SRAM

C66xx_0: GEL Output: Setup Cache... Done.

C66xx_0: GEL Output: Main PLL (PLL1) Setup ...

C66xx_0: GEL Output: PLL in Bypass ...

C66xx_0: GEL Output: PLL1 Setup for DSP @ 1000.0 MHz.

C66xx_0: GEL Output:            SYSCLK2 = 333.3333 MHz, SYSCLK5 = 200.0 MHz.

C66xx_0: GEL Output:            SYSCLK8 = 15.625 MHz.

C66xx_0: GEL Output: PLL1 Setup... Done.

C66xx_0: GEL Output: Power on all PSC modules and DSP domains...

C66xx_0: GEL Output: Set_PSC_State... Timeout Error #03 pd=12, md=4!

C66xx_0: GEL Output: Power on all PSC modules and DSP domains... Done.

C66xx_0: GEL Output: DDR3 PLL (PLL2) Setup ...

C66xx_0: GEL Output: DDR3 PLL Setup... Done.

C66xx_0: GEL Output: DDR3 Init begin (1333 auto)

C66xx_0: GEL Output: XMC Setup ... Done

C66xx_0: GEL Output: IFRDY bit is SET: DDR3 Interface Ready

C66xx_0: GEL Output:
DDR3 initialization is complete.

C66xx_0: GEL Output: DDR3 Init done

C66xx_0: GEL Output: DDR3 memory test... Started

C66xx_0: GEL Output: DDR3 memory test... Passed

C66xx_0: GEL Output: PLL and DDR3 Initialization completed(0) ...

C66xx_0: GEL Output: configSGMIISerdes Setup... Begin

C66xx_0: GEL Output: SGMII SERDES has been configured.

C66xx_0: GEL Output: Enabling EDC ...

C66xx_0: GEL Output: L1P error detection logic is enabled.

C66xx_0: GEL Output: L2 error detection/correction logic is enabled.

C66xx_0: GEL Output: MSMC error detection/correction logic is enabled.

C66xx_0: GEL Output: Enabling EDC ...Done

C66xx_0: GEL Output: Global Default Setup... Done.

Start writing eeprom50
Writer:../prebuilt-images/eepromwriter_evm6657l.out

Image:../prebuilt-images/eeprom50.bin

C66xx_0: GEL Output: Invalidate All Cache...

C66xx_0: GEL Output: Invalidate All Cache... Done.

C66xx_0: GEL Output: GEL Reset...

C66xx_0: GEL Output: GEL Reset... Done.

C66xx_0: GEL Output: Disable all EDMA3 interrupts and events.

EEPROM Writer Utility Version 01.00.00.05

Writing 57432 bytes from DSP memory address 0x0c000000 to EEPROM bus address 0x0050 starting from device address 0x0000
...
Reading 57432 bytes from EEPROM bus address 0x0050 to DSP memory address 0x0c010000 starting from device address 0x0000
...
Verifying data read ...
EEPROM programming completed successfully
Start writing eeprom51
Writer:../prebuilt-images/eepromwriter_evm6657l.out

Image:../prebuilt-images/eeprom51.bin

C66xx_0: GEL Output: Invalidate All Cache...

C66xx_0: GEL Output: Invalidate All Cache... Done.

C66xx_0: GEL Output: GEL Reset...

C66xx_0: GEL Output: GEL Reset... Done.

C66xx_0: GEL Output: Disable all EDMA3 interrupts and events.

EEPROM Writer Utility Version 01.00.00.05

Writing 47888 bytes from DSP memory address 0x0c000000 to EEPROM bus address 0x0051 starting from device address 0x0000
...
Reading 47888 bytes from EEPROM bus address 0x0051 to DSP memory address 0x0c010000 starting from device address 0x0000
...
Verifying data read ...
EEPROM programming completed successfully
Writer:../prebuilt-images/nandwriter_evm6657l.out

NAND:../prebuilt-images/nand.bin

Required NAND files does not exist in ../prebuilt-images/

Writer:../prebuilt-images/norwriter_evm6657l.out

NOR:../prebuilt-images/nor.bin

Required NOR files does not exist in ../prebuilt-images/

In the above example, nothing was flashed to NAND or NOR since there were no nand.bin or nor.bin binaries to flash.