Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS GPMC

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide GPMC



Overview

User Interface

Application

Debug

Introduction

The general-purpose memory controller (GPMC) is an unified memory controller dedicated to interfacing external memory devices:

  • Asynchronous SRAM-like memories and application-specific integrated circuit (ASIC) devices
  • Asynchronous, synchronous, and page mode (only available in non-multiplexed mode) burst NOR flash devices
  • NAND Flash

Driver supports two types of transfers with data path to external memory device configured to be 16- or 8-bit:

  • Read
  • Write

In addition driver supports following modes of operation:

  • GPMC_MODE_BLOCKING: By default, driver operates in blocking mode. In blocking mode, a Task’s code execution is blocked until transaction is complete. This ensures only one transaction operates at a given time. Driver supports both interrupt or non-interrupt based blocking modes.
  • GPMC_MODE_CALLBACK In callback mode, an GPMC transaction functions asynchronously, which means that it does not block a Task’s code execution. After an GPMC transaction is complete, GPMC driver calls a user-provided hook function. Only interrupt based callback is supported.

In NAND flash mode, driver supports following ECC algorithms:

  • BCH code 8-bit
  • HAMMING code 1-bit

Driver Configuration

Board Specific Configuration

All the board specific configurations eg:enabling and pin-mux of GPMC pins should be performed before calling any driver APIs.By default Board_Init() API supports all initialization sequence for TI supported EVMs.Refer Processor SDK RTOS Board Support for additional details.

Once the board specific configuration is complete driver API GPMC_init() can be called to initialize driver

GPMC Configuration Structure

GPMC_soc.c file binds driver with hardware attributes on the board through GPMC_config structure. This structure must be provided to GPMC driver. It must be initialized before the GPMC_init() function is called and cannot be changed afterwards. For details about the individual fields of this structure, see the Doxygen help by opening PDK_INSTALL_DIR\packages\ti\drv\gpmc\docs\doxygen\html\index.html.

APIs

API reference for application:

#include <ti/drv/gpmc/GPMC.h>

 Sample code for initiating GPMC transaction:

...
Board_init(boardCfg);
...
...
gpmc = GPMC_open(peripheralNum, &gpmcParams);
...
...

/* Initiate GPMC transfers. Refer Example for details
*/
transferOK = GPMC_transfer(gpmc, &gpmcTransaction);
if (!transferOK) {
/* GPMC transaction failed */
} 

Examples

Refer Release Note for GPMC support across different EVMs

Name
Description
Expected Results
GPMC NOR/NAND Read Example Application

Simple example to read data from GPMC NOR/NAND flash on board.

Following prints will come on console based on pass/fail criteria:

Pass criteria:

GPMC flash device ID: 0x##, manufacturer ID: 0x##

GPMC flash read test passed.

All tests have passed.

GPMC NOR/NAND test application

Driver Unit Test application to test GPMC NOR/NAND flash read/erase/write

Following prints will come on console based on pass/fail criteria:

Pass criteria:

GPMC flash device ID: 0x##, manufacturer ID: 0x##

GPMC flash block erase test passed.

GPMC flash write test passed.

GPMC flash read test passed.

All tests have passed.



NOTE

1. GPMC Test Application supports write test, by default write test is disabled, user can enable the write test by defining TEST_GPMC_FLASH_WRITE in test/src/GPMC_board.h.
2. In GPMC_Test_icev2AM335x, J5 pin2 & 3 should be shorted on iceV2AM335x board in order to test GPMC NOR flash.

3. In GPMC_Test_evmAM437x, J2 pin1 & 2 should NOT be shorted on evmAM437x board in order to test GPMC NAND flash.

Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\gpmc\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\gpmc\docs\ReleaseNotes_GPMC_LLD.pdf