Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS HYPLNK

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide HYPLNK



Overview

User Interface

Application

Debug


Overview

Hyperlink is a point-to-point peripheral. Each device has equal capability to operate on the address space of the other device. This also means that there is no complex enumeration in order to get started.

Modes of Operation

The LLD is intended to bring up the Hyperlink peripheral and open memory mappings.

Interrupts

There is an interrupt generation example (in PDK_INSTALL_DIR/packages/ti/drv/hyplnk/example/cicInterruptExample) which maps and pokes the other device's CIC (Chip/SOC level interrupt controller) to generate interrupts for data transfers.

The PDK_INSTALL_DIR/packages/ti/drv/hyplnk/example/common/hyplnkIsr.c monitors local interrupts to detect fatal errors. It can also be used for IO interrupts, but there is only one output event that has to be demuxed. Thus for multicore orthogonality, the cicInterruptExample is often better example (because each destination core can have completely independent interrupts).

Driver Configuration

The driver itself is entirely configured via API at runtime. However, the examples are configured using compiler flags that are in hyplnkPlatCfg.h and hyplnkLLDCfg.h.

Hyperlink configuration structure

The hyplnk_device.c binds the driver to the hardware on the board. It is passed into the driver via the call to Hyplnk_init().

API Call Flow

The API call flow is covered in example\memoryMappedExample\src\hyplnkExample.

They key parts are:

  1. Initialize the LLD via Hyplnk_init().
  2. Configure PLL, PSC and memories via hyplnkExampleSysSetup() which is all example code
  3. Install ISR(s)
  4. Enable the peripheral using sequence in hyplnkExamplePeriphSetup()
  5. Open memory maps using hyplnkExampleAddrMap() as a guide
  6. Exchange data with memcpy or EDMA using mapped address (returned from hyplnkExampleAddrMap).


Examples

Hyperlink/hyplnk is supported only on Keystone devices. It is available on 6678, 6657, K2H, K2K, K2E. All examples can be used in either loopback (on any EVM without any special cables or breakout cards) or with two boards. For 6678 or 6657, the required cable is HL5CABLE. For K2H/K2K/K2E, the breakout card is RTM-BOCRT, and the cable is also required. Below is a picture showing how a K2H EVM is connected to a 6678 EVM via breakout card and cable.

Name
Description
EVM Configuration
Expected Results
memoryMappedExample

Memory mapped data exchange with loopback or 2 devices

Loopback runs without any extra hardware. See below for details on configuring board-to-board.

Link is established and data is exchanged.

cicInterruptExample

CIC-based interrupt exchange.

Loopback runs without any extra hardware. See below for details on configuring board-to-board.

Interrupts are sent between ARM Linux Userspace and DSPs.

Setup of multiple EVMs with one instance of CCS

This is only needed for 2 board use cases. See Multi-Emulator_Debug_with_CCS for general configuration of multiple EVMs/emulators within one instance of CCS.

Detailed instructions to run memoryMappedExample

If running with one board, enable loopback via uncommenting hyplnk_EXAMPLE_LOOPBACK in PDK_INSTALL_DIR/packages/ti/drv/hyplnk/example/common/hyplnkLLDCfg.h.

Compile the project for the specific device/evm in use.

For loopback: Load the example with hyplnk_EXAMPLE_LOOPBACK definined onto one board and run. The results should be as below.

For 2 board: Make sure the both boards configuration match each other by checking PDK_INSTALL_DIR/packages/ti/drv/hyplnk/example/common/hyplnkLLDCfg.h:

hyplnk_EXAMPLE_PORT --> which port to use for K2H/K2K/K2E
hyplnk_EXAMPLE_ALLOW_x_LANES --> 0, 1 or 4 lanes
hyplnk_EXAMPLE_SERRATE_xxpxxx --> serdes rate setup

Load the same example on both boards. It is fulling symmetric. No special configuration is needed to distinguish side A and side B. Each side should generate output similar to below.

Detailed instructions to run cicInterruptExample

This only works on devices with A15 running Linux (K2H, K2K, K2E). See PDK_INSTALL_DIR/packages/ti/drv/hyplnk/example/cicInterruptExample/Readme.txt for instructions.

Sample example output

This came from k2h device running in loopback.

Version #: 0x02010005; string HYPLNK LLD Revision: 02.01.00.05:Dec 24 2015:17:48:28
About to do system setup (PLL, PSC, and DDR)
Power domain is already enabled.  You probably re-ran without device reset (which is OK)
Constructed SERDES configs: PLL=0x00000228; RX=0x0046c495; TX=0x000ccf95
system setup worked
About to set up HyperLink Peripheral
============================Hyperlink Testing Port 0 
========================================== begin registers before initialization ===========
Revision register contents:
  Raw    = 0x4e902101
Status register contents:
  Raw        = 0x00003004
Link status register contents:
  Raw       = 0x00000000
Control register contents:
  Raw             = 0x00000000
Control register contents:
  Raw        = 0x00000000
============== end registers before initialization ===========
Hyperlink Serdes Common Init Complete
Hyperlink Serdes Lane 0 Init Complete
Hyperlink Serdes Lane 1 Init Complete
Hyperlink Serdes Lane 2 Init Complete
Hyperlink Serdes Lane 3 Init Complete
============== begin registers after initialization ===========
Status register contents:
  Raw        = 0x04402005
Link status register contents:
  Raw       = 0xfdf0bdf0
Control register contents:
  Raw             = 0x00006206
============== end registers after initialization ===========
Waiting 5 seconds to check link stability
Precursors 1 
Postcursors: 19 
Link seems stable
About to try to read remote registers
============== begin REMOTE registers after initialization ===========
Status register contents:
  Raw        = 0x0440080f
Link status register contents:
  Raw       = 0xfdf0bdf0
Control register contents:
  Raw             = 0x00006202
============== end REMOTE registers after initialization ===========
Peripheral setup worked
About to read/write once
Single write test passed
About to pass 65536 tokens; iteration = 0
=== this is not an optimized example ===
Link Speed is 4 * 3.125 Gbps
Passed 65536 tokens round trip (read+write through hyplnk) in 16829 Mcycles
Approximately 256799 cycles per round-trip
=== this is not an optimized example ===
Checking statistics
About to pass 65536 tokens; iteration = 1
=== this is not an optimized example ===
Link Speed is 4 * 3.125 Gbps
Passed 65536 tokens round trip (read+write through hyplnk) in 16829 Mcycles
Approximately 256799 cycles per round-trip
=== this is not an optimized example ===
Checking statistics
About to pass 65536 tokens; iteration = 2
.
.
.

Debug FAQ

  1. If it seems to not work, check for lError and rError in the status register (hyplnkStatusReg_s). If these appear, it means double ecc error occurred and the link is non functional. This is fatal error. Next look at hyplnkECCErrorReg_s for single (corrected) bit errors. After startup these should increment slowly (order of minutes, hours, days, not seconds or less). If they are incrementing quickly (several times per minute or second), then it means the SERDES coefficients should be calibrated by following the Keystone SERDES UG. See references section.
  2. Note that if the link goes down (uncorrectable ECC error) it is possible for the entire interconnect to lock up. If this occurs, it will not be possible to access any memory even through the JTAG interface (CCS will return errors instead of reading memory, and often disconnect the target). Thus the primary cause of this lockup should be avoided by carefully following the shutdown/reset requirement in section 2.9 of the Hyperlink UG (which is to invoke serial stop, and wait for it to take effect before resetting either endpoint).
  3. Another workaround for ECC single errors is to lower link rate and/or reduce to 1 lane. This can be done by adjusting the commented defines in PDK_INSTALL_DIR/packages/ti/drv/hyplnk/example/common/hyplnkLLDCfg.h.

Additional References

Additional documentation can be found in:

Document Location
Hardware Peripheral Hyperlink Users Guide User Guide
Serdes Users Guide User Guide
CIC Peripheral Users Guide CIC User Guide
API Reference Manual

$(TI_PDK_INSTALL_DIR)\packages\ti\drv\hyplnk\docs\doxygen\html\index.html

Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\hyplnk\docs\ReleaseNotes_HYPLNK_LLD.pdf