Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS ICSS-EMAC(DRIVER,FIRMWARE)

From Texas Instruments Wiki
Jump to: navigation, search


RTOS Software Developer Guide ICSS-EMAC



Overview

User Interface

Application

Debug


Driver Overview

The ICSS_EMAC (industrial communications subsystem Ethernet Media Access Controller) driver provide APIs to transmit and receive packets with a firmware based Ethernet switch that has been implemented on TI’s PRU-ICSS (Programmable Real-Time Unit Subsystem and Industrial Communication SubSystem) 32-bit RISC cores.


Software Architecture

The ICSS EMAC low level driver can be partitioned into the following:

  • Driver software running on the host processor, provides a well defined set of APIs to configure the driver, send packets to the firmware and receive packet from the firmware.
  • Firmware which implements a 2 port ethernet switch supporting 802.1d @100 Mbps. This runs on the TI-PRU-ICSS cores.


Driver Features

ICSS_EMAC LLD implements following:

  • Rx - Copying packet received from firmware and providing it to TCP/IP stack
  • Tx - Providing packet from TCP/IP stack to firmware
  • Learning/Forwarding Data Base
  • Storm Prevention implementation
  • Host Statistics implementation
  • TCP/IP stack related initialization
  • Configuring IP address
  • ARM interrupt management


For details of the driver, please refer to [1]


Driver Configuration

Board Specific Configuration
All the board specific configurations eg: enabling clock and pin-mux for GPIO/MDIP/IEP pins should be performed before calling any driver APIs. By default Board_Init() API supports all initialization sequence for TI supported EVMs. In addition it initializes UART instance for Console/STDIO.Refer Processor SDK RTOS Board Support for additional details.Once board specific configuration is complete  driver APIS can be invoked.


ICSS_EMAC Configuration Structure
The icss_emacSoc.c file contains the declaration of the hardware attributes corresponding to the ICSS_EMAC subsystem. Hardware attributes includes base address of various sub-subsystems required by the the ICSS_EMAC LLD. This configuration is required and needs to be passed in as part of the ICSS_EMAC Handle when calling the icss_emacInit API. For details about individual fields of this structure, see the Doxygen help by opening PDK_INSTALL_DIR\packages\ti\drv\icss_emac\docs\doxygen\html\index.html.


APIs

API reference for application:

#include <ti/drv/icss_emac/icss_emacDrv.h>

API Call Flow

The below sequence indicates the calling sequence of ICSS_EMAC driver APIs for a use case of an EMAC example which implements single Ethernet MAC using PRU-ICSS Instance 2, ETH0. For additional details refer example inside package

 ...
 Board_init(cfg);
 
 /* Create handle for PRUICSS instance 2*/
 ICSS_EMAC_testPruIcssHandle2= PRUICSS_create(pruss_config,PRUICCSS_INSTANCE_TWO);
 
 /* Setup crossbar configuration to receive PRU-ICSS interrupts and map them to A15 (illustration for PRU2ETH0) */
 CSL_xbarDspIrqConfigure(..);  /* Link ISR */
 CSL_xbarDspIrqConfigure(..);  /* RX PKT ISR */
 CSL_xbarDspIrqConfigure(..);  /* TX PKT ISR */
 
 /*Initialize driver */
 ...
 ICSS_EmacInit(..);
 
 /* Register callbacks for RX/TX, Link Interrupts, these are called in context of ISR */
 ICSS_EmacRegisterPort0ISRCallback(..);
 ICSS_EmacRegisterHwIntRx(..);
 ICSS_EmacRegisterHwIntTx(..);
 
/* Create TASK contexts for handling RX/TX, Link Interrupt events, the pend on semaphores waiting
   to be posed by ISR */
 Task_create((ti_sysbios_knl_Task_FuncPtr)ICSS_EMacOsRxTaskFnc,  &taskParams, NULL);
 Task_create((ti_sysbios_knl_Task_FuncPtr)ICSS_EMacOsTxTaskFnc, &taskParams, NULL);
 Task_create((ti_sysbios_knl_Task_FuncPtr)ICSS_EMacOsLinkTaskFnc, &taskParams, NULL);
 
 /* Register Interrupts RX/TX/Link*/
 ICSS_EMAC_testInterruptInit(ICSS_EMAC_testHandle2);
 
 /* Enable Interrupts RX/TX/Link*/
 ICSS_EMAC_testInterruptEnable(ICSS_EMAC_testHandle2);
 
 /* At this point, ICSS_EMAC LLD APIs can be called */

Firmware

TI PRU-ICSS cores (Programmable Real-Time Unit Industrial Communication Subsystem) is firmware programmable and can take on various personalities. Examples include an SORTE, ethernet Switch, Industrial protocol switch. Please refer to ICSS-EMAC Firmwares for further explanation.


Examples

Refer “ICSS_EMAC_<Basic/Switch>Example_<SOC>_<CPU>Testproject” for additional reference. Refer Release Note for ICSS_EMAC supported on different EVMs.


Name
Description
EVM Configuration
Expected Results
ICSS_EMAC_BasicExample

EMAC Loopback test at PRU-ICSS EMAC PHY.

Example demonstrates loopback capability by sending dummy broadcast packet to PRU-ICSS instance 2, ethernet port 0 (PRU ETH0). Unit test registers receive packet callback routine with LLD to be called for RX packet. Call back routine will extract packet received, perform simple memory comparison against packet sent for integrity check. Unit test will iterate 10 times for packet transmission and reception check.

10/100 Mb/s loopback cable

Unit Test will print "All tests have passed" via UART console.

ICSS_EMAC_SwitchExample

Switch Loopback test at PRU-ICSS EMAC PHY.

Example demonstrates switch learning loopback capability by sending dummy broadcast packet to PRU-ICSS instance, ethernet port. Unit test registers receive packet callback routine with LLD to be called for RX packet. Call back routine will extract packet received, perform simple memory comparison against packet sent for integrity check. As with switch for every 1 transmitted packet, firmware will respond back with 2 recieved packets. Unit test will iterate 10 times for packet transmission and reception check.

100 Mb/s loopback cable

Unit Test will print "All tests have passed" via UART console.


Additional documentation reference

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\icss_emac\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\icss_emac\docs\ReleaseNotes_ICSS_EMAC_LLD.pdf
ICSS-EMAC LLD Details [2]