Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS IPC Transports

From Texas Instruments Wiki
Jump to: navigation, search


RTOS Software Developer Guide IPC Transports



Overview

User Interface

Application

Debug


Introduction

IPC transports are the underlying configurable data paths over shared memory and hardware resources, which implement the IPC MessageQ APIs. MessageQ provides a common IPC interface between processors within a system containing a single or multiple KeyStone devices. Communication between the processors is enabled through the use of IPC transports. The transports supplied with the IPC component are shared memory based, capable of intra-device communication. Additional transports, utilizing the QMSS and SRIO LLDs, are supplied via Yocto/bitbake for ARMv7 Linux IPC and PROCSDK PDK for SYS/BIOS DSP IPC, enabling intra-SoC and inter-SoC communication, respectively.

The below table gives an overview of the transport offerings, their location, and the communication path they enable.

Transport MessageQ Interface Type Location Communication Route Enabled Communication Path Special Considerations
TransportShm... MessageQ (priority based) IPC component - SYS/BIOS subdirectories Shared memory SYS/BIOS DSP to DSP There are multiple implementations of TransportShm delivered within the IPC component. Please see the IPC documentation provided with the component for more information on these shared memory transport implementations.
TransportRpmsg MessageQ (priority based)
  • IPC component - ARMv7 Linux subdirectories
  • IPC component - SYS/BIOS subdirectories
  • Yocto/bitbake ti-ipc recipe
Shared memory
  • ARMv7 Linux to/from SYS/BIOS DSP
MessageQ messages sent over TransportRpmsg traveling from/to ARMv7 user space go through the Linux kernel before reaching the DSP. This provides clean partitioning between user memory and DSP memory. However, TransportRpmsg is considered a slow path since the user space MessageQ messages must be copied from/to DSP memory by kernel and DSP.
SYS/BIOS DSP TransportSrio Network PROCSDK RTOS PDK SRIO LLD
  • SYS/BIOS DSP to/from SYS/BIOS DSP (intra- and inter-device)
  • SYS/BIOS DSP to/from ARMv7 Linux (intra- and inter-device)
  • TransportSrio can send MessageQ messages to ARMv7 and DSP processors on remote devices in a multiple device system. IPC MultiProc must be configured to be aware of all processors existing on all devices and all devices must be connected over a SRIO interconnect.
  • The main purpose of TransportSrio is for multi-device communication over MessageQ. The transmission latency is greater for this transport due to the latter capability. Therefore, it is recommended a shared memory or other LLD-based transport is used for intra-device communication due to their lower latency costs.
ARMv7 Linux TransportSrio Network Yocto/bitbake ti-transport-srio recipe SRIO LLD
  • ARMv7 Linux to/from ARMv7 Linux (intra- and inter-device)
  • SYS/BIOS DSP to/from ARMv7 Linux (intra- and inter-device)
  • TransportSrio can send MessageQ messages to ARMv7 and DSP processors on remote devices in a multiple device system. IPC MultiProc must be configured to be aware of all processors existing on all devices and all devices must be connected over a SRIO interconnect.
  • The main purpose of TransportSrio is for multi-device communication over MessageQ. The transmission latency is greater for this transport due to the latter capability. Therefore, it is recommended a shared memory or other LLD-based transport is used for intra-device communication due to their lower latency costs.
SYS/BIOS DSP TransportQmss Network QMSS LLD
  • SYS/BIOS DSP to/from SYS/BIOS DSP
  • SYS/BIOS DSP to/from ARMv7 Linux
ARMv7 Linux TransportQmss Network Yocto/bitbake ti-transport-qmss recipe QMSS LLD
  • ARMv7 Linux process to process
  • ARMv7 Linux to/from SYS/BIOS DSP

The IPC component (ARMv7 and SYS/BIOS) is available in PROCSDK RTOS and Linux installations. It will be installed in <PROCSDK RTOS or Linux install root>/ipc_#_##_##_##<version>. Additionally, the IPC component's ARMv7 source is packaged in a Yocto/bitbake recipe. A user can develop ARMv7 Linux user-space applications with IPC on Keystone I and KeyStone II devices by building the ti-ipc package in Yocto.

Modes of Operation

SYS/BIOS DSP TransportSrio

The following SRIO socket types are supported:

TransportSrio_srioSockType_TYPE_9: In this mode, the SRIO IPC transport will use Type 9 sockets to communicate with other SRIO IPC transport endpoints.

TransportSrio_srioSockType_TYPE_11: In this mode, the SRIO IPC transport will use Type 11 sockets to communicate with other SRIO IPC transport endpoints.

ARM Linux TransportSrio

The following SRIO socket types are supported:

sock_TYPE_9: In this mode, the ARM Linux SRIO IPC transport will use Type 9 sockets to communicate with other SRIO IPC transport endpoints.

sock_TYPE_11: In this mode, the ARM Linux SRIO IPC transport will use Type 11 sockets to communicate with other SRIO IPC transport endpoints.

SYS/BIOS DSP TransportQmss

The following QMSS receive queue types are supported:

TransportQmss_queueRcvType_ACCUMULATOR: In this mode, the QMSS accumulator logic is used as the reception mechanism for the QMSS Transport.

TransportQmss_queueRcvType_QPEND: In this mode, a QMSS QPEND (direct interrupt) queue is used as the reception mechanism for the QMSS Transport.

ARM Linux TransportQmss

A QMSS QPEND queue will always be used as the reception mechanism for the ARM Linux QMSS Transport.

Transport Configuration

SYS/BIOS DSP TransportSrio

SRIO SERDES and Lane Configuration

Configuration of the SRIO SERDES and lanes are required before calling any driver APIs. Examples of the initialization sequences for supported EVMs are provided in the TransportSrio example folder. The examples call the SrioDevice_init() API prior to configuring the transport. SrioDevice_init() reference:

ti/transport/ipc/c66/srio/example/src/device_srio.c

Developers can modify the configurations made in the stock device_srio.c to change SRIO endpoint IDs, routing information, lane rates, loopback modes, etc.

APIs

API reference for application:

#include <ti/transport/ipc/c66/srio/TransportSrio.h>

ARM Linux TransportSrio

SRIO SERDES and Lane Configuration

Configuration of the SRIO SERDES and lanes are required before calling any driver APIs. Examples of the initialization sequences for supported EVMs are provided in the TransportSrio test folder. The examples call the SrioDevice_init() API prior to configuring the transport. SrioDevice_init() reference from keystone-linux/ipc-transport git repository:

linux/srio/test/[consumer or producer]_device_srio.c

Developers can modify the configurations made in the stock device_srio.c to change SRIO endpoint IDs, routing information, lane rates, loopback modes, etc.

MPM Transport SRIO Configuration

TransportSrio leverages MPM Transport in order to manage configuration of the QMSS, CPPI, and SRIO LLDs. As a result, the transport's descriptor and descriptor buffer management is pushed to MPM Transport in the ARM Linux version of TransportSrio. The MPM Transport JSON configuration file can be modified to change QMSS descriptor and buffer related parameters.

The MPM Transport JSON configuration file is located in the Linux file system at /etc/mpm/mpm_config.json

APIs

API reference for application from keystone-linux/ipc-transport git repository:

#include <linux/srio/TransportSrio.h>

SYS/BIOS DSP TransportQmss

APIs

API reference for application:

#include <ti/transport/ipc/c66/qmss/TransportQmss.h>

ARM Linux TransportQmss

MPM Transport QMSS Configuration

TransportQmss leverages MPM Transport in order to manage configuration of the QMSS and CPPI LLDs. As a result, the transport's descriptor and descriptor buffer management is pushed to MPM Transport in the ARM Linux version of TransportQmss. The MPM Transport JSON configuration file can be modified to change QMSS descriptor and buffer related parameters.

The MPM Transport JSON configuration file is located in the Linux file system at /etc/mpm/mpm_config.json

APIs

API reference for application from keystone-linux/ipc-transport git repository:

#include <linux/qmss/TransportQmss.h>

Source Delivery and Recompilation

SYS/BIOS DSP TransportSrio

The SYS/BIOS DSP TransportSrio source code and examples are delivered within the PROCSDK RTOS PDK component. DSP TransportSrio can be rebuilt using the environment setup scripts provided with the PDK package. DSP TransportSrio example applications are created as part of the pdkProjectCreate scripts. They can be imported and built the same as PDK LLD example and test CCS projects.

Recompiling on Windows
  1. Open a Windows command terminal and navigate to <pdk_install_dir>/packages.
  2. Run pdksetupenv.bat
    >pdksetupenv.bat
  3. Navigate to <pdk_install_path>/packages/ti/transport/ipc/c66/srio/
  4. Build the IPC SRIO Transport library
    >gmake

Issue the following commands if the SRIO transport ever needs to be rebuilt:

>gmake clean
>gmake
Recompiling on Linux
  1. Open a Linux bash terminal and navigate to <pdk_install_dir>/packages.
  2. Run pdksetupenv.sh
    $ source pdksetupenv.sh
  3. Navigate to <pdk_install_path>/packages/ti/transport/ipc/c66/srio/
  4. Build the IPC SRIO Transport library
    $ make

Issue the following commands if the SRIO transport ever needs to be rebuilt:

$ make clean
$ make

ARM Linux TransportSrio Source Delivery and Recompilation

The ARM Linux TransportSrio source code can be downloaded and built two ways. The transport source code is delivered and built as part of Yocto/bitbake. The source code can also be downloaded and built directly from the GIT repository.

Recompiling Through Yocto/bitbake
  1. Follow the instructions in the Exploring section of the user guide to configure the Yocto build environment. The tisdk-server-rootfs-image does not need to be built. Instead look at the section for building other components
  2. Build the TransportSrio libraries, ipc-transport-srio recipe, and user-space tests, ipc-transport-srio-test recipe:
    $ MACHINE=k2hk-evm TOOLCHAIN_BRAND=linaro ARAGO_BRAND=mcsdk bitbake ipc-transport-srio
    $ MACHINE=k2hk-evm TOOLCHAIN_BRAND=linaro ARAGO_BRAND=mcsdk bitbake ipc-transport-srio-test

    NoteNote: The initial build may take quite some time since the kernel is built as a dependency
    NoteNote: Building with just the ipc-transport-srio-test recipe will also build the ipc-transport-srio recipe since the test recipe depends on the library recipe.
  3. The built TransportSrio static library will be located in
    <base_path>/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/ipc-transport-srio/<tag-ver_recipe-ver>/packages-split/ipc-transport-srio-staticdev/usr/lib/libTransportSrio.a

    The built TransportSrio shared library will be located in
    <base_path>/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/ipc-transport-srio/<tag-ver_recipe-ver>/packages-split/ipc-transport-srio/usr/lib/libTransportSrio.so.1.0.0
  4. The ipc-transport-srio-test recipe will build test static and shared library executables for all supported devices. The executables will be located in
    base_path>/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/ipc-transport-srio-test/<tag-ver_recipe-ver>/packages-split/ipc-transport-srio-test/usr/bin/
Recompiling Through GIT Repository

Recompiling through the ARM Linux TransportSrio GIT repository requires that the latest PROCSDK Linux installation. The PROCSDK Linux PDK component and the Linux devkit must be installed. The Linux devkit installation script can be found in <PROCSDK Linux install root>/procsdk_linux_3_XX_YY_ZZ/linux-devkit/

  1. Clone the keystone-linux/ipc-transport repository from git.ti.com
    $ git clone git://git.ti.com/keystone-linux/ipc-transport.git
  2. Navigate to the PROCSDK Linux installation of pdk_3_XX_YY_ZZ/packages and source armv7setupenv.sh.
    NoteNote: The armv7setupenv.sh script must be modified to point to the linaro toolchain and installed devkit path
    $ source armv7setupenv.sh
  3. Navigate back to the SRIO transport directory in the ipc-transport GIT repository
    $ cd <repo_root_path>/ipc-transport/linus/srio
  4. Build the TransportSrio library and user-space test executables:
    $ make lib
    $ make tests
  5. The TransportSrio static and shared libraries will be copied directly into the Linux devkit's /usr/lib folder as long as the devkit install path was setup correctly prior to running the armv7setupenv.sh script
  6. The test executables will be generated in the <base_repo_path>/ipc-transport/bin/<k2 device>/test/ folder. Only the device specified in the armv7setupenv.sh will be built.
    NoteNote: Setting the USEDYNAMIC_LIB environment variable to "yes" will generate the shared library test executables
    $ export USEDYNAMIC_LIB=yes

SYS/BIOS DSP TransportQmss Source Delivery and Recompilation

The SYS/BIOS DSP TransportQmss source code and examples are delivered within the PROCSDK RTOS PDK component. DSP TransportQmss can be rebuilt using the environment setup scripts provided with the PDK package. DSP TransportQmss example applications are created as part of the pdkProjectCreate scripts. They can be imported and built the same as PDK LLD example and test CCS projects.

Recompiling on Windows
  1. Open a Windows command terminal and navigate to <pdk_install_dir>/packages.
  2. Run pdksetupenv.bat
    >pdksetupenv.bat
  3. Navigate to <pdk_install_path>/packages/ti/transport/ipc/c66/qmss/
  4. Build the IPC QMSS Transport library
    >gmake

Issue the following commands if the QMSS transport ever needs to be rebuilt:

>gmake clean
>gmake
Recompiling on Linux
  1. Open a Linux bash terminal and navigate to <pdk_install_dir>/packages.
  2. Run pdksetupenv.sh
    $ source pdksetupenv.sh
  3. Navigate to <pdk_install_path>/packages/ti/transport/ipc/c66/qmss/
  4. Build the IPC QMSS Transport library
    $ make

Issue the following commands if the QMSS transport ever needs to be rebuilt:

$ make clean
$ make

ARM Linux TransportQmss Source Delivery and Recompilation

The ARM Linux TransportQmss source code can be downloaded and built two ways. The transport source code is delivered and built as part of Yocto/bitbake. The source code can also be downloaded and built directly from the GIT repository.

Recompiling Through Yocto/bitbake
  1. Follow the instructions in the Exploring section of the user guide to configure the Yocto build environment. The tisdk-server-rootfs-image does not need to be built. Instead look at the section for building other components
  2. Build the TransportQmss libraries, ipc-transport-qmss recipe, and user-space tests, ipc-transport-qmss-test recipe:
    $ MACHINE=k2hk-evm TOOLCHAIN_BRAND=linaro ARAGO_BRAND=mcsdk bitbake ipc-transport-qmss
    $ MACHINE=k2hk-evm TOOLCHAIN_BRAND=linaro ARAGO_BRAND=mcsdk bitbake ipc-transport-qmss-test

    NoteNote: The initial build may take quite some time since the kernel is built as a dependency
    NoteNote: Building with just the ipc-transport-qmss-test recipe will also build the ipc-transport-qmss recipe since the test recipe depends on the library recipe.
  3. The built TransportQmss static library will be located in
    <base_path>/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/ipc-transport-qmss/<tag-ver_recipe-ver>/packages-split/ipc-transport-qmss-staticdev/usr/lib/libTransportQmss.a

    The built TransportQmss shared library will be located in
    <base_path>/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/ipc-transport-qmss/<tag-ver_recipe-ver>/packages-split/ipc-transport-qmss/usr/lib/libTransportQmss.so.1.0.0
  4. The ipc-transport-qmss-test recipe will build test static and shared library executables for all supported devices. The executables will be located in
    base_path>/oe-layersetup/build/arago-tmp-external-linaro-toolchain/work/cortexa15hf-vfp-neon-3.8-oe-linux-gnueabi/ipc-transport-qmss-test/<tag-ver_recipe-ver>/packages-split/ipc-transport-qmss-test/usr/bin/
Recompiling Through GIT Repository

Recompiling through the ARMv7 Linux TransportQmss GIT repository requires that the latest PROCSDK Linux installation. The PROCSDK Linux PDK component and the Linux devkit must be installed. The Linux devkit installation script can be found in <PROCSDK Linux install root>/processor_sdk_linux_3_XX_YY_ZZ/linux-devkit/

  1. Clone the keystone-linux/ipc-transport repository from git.ti.com
    $ git clone git://git.ti.com/keystone-linux/ipc-transport.git
  2. Navigate to the PROCSDK Linux installation of pdk_3_XX_YY_ZZ/packages and source armv7setupenv.sh.
    NoteNote: The armv7setupenv.sh script must be modified build for the correct K2 device, and to point to the linaro toolchain and installed devkit path
    $ source armv7setupenv.sh
  3. Navigate back to the QMSS transport directory in the ipc-transport GIT repository
    $ cd <repo_root_path>/ipc-transport/linus/qmss
  4. Build the TransportQmss library and user-space test executables:
    $ make lib
    $ make tests
  5. The TransportQmss static and shared libraries will be copied directly into the Linux devkit's /usr/lib folder as long as the devkit install path was setup correctly prior to running the armv7setupenv.sh script
  6. The test executables will be generated in the <base_repo_path>/ipc-transport/bin/<k2 device>/test/ folder. Only the device specified in the armv7setupenv.sh will be built.
    NoteNote: Setting the USEDYNAMIC_LIB environment variable to "yes" will generate the shared library test executables
    $ export USEDYNAMIC_LIB=yes

Tests & Examples

SYS/BIOS DSP TransportSrio

Name
Description
Expected Results
SYS/BIOS DSP TransportSrio Benchmark Example

Example demonstrating intra-SoC, DSP to DSP, transport over SRIO use while also measuring latency and throughput performance. The example consists of multiple iterations where each iteration runs SRIO with different lane configurations. Reference example for developers

Successful completion on two DSP cores for all example iterations.

SYS/BIOS DSP TransportSrio Producer/Consumer Example

Example demonstrates inter-SoC, DSP to DSP, transport over SRIO. The example consists of multiple iterations where each iteration runs SRIO with different lane configurations.

Successful completion for all example iterations on two DSP cores per producer and consumer devices.

ARM Linux TransportSrio

Name
Description
Expected Results
ARM Linux TransportSrio Producer/Consumer Example

Example demonstrates inter-SoC, ARM Linux to ARM Linux, transport over SRIO. The example consists of multiple iterations where each iteration runs SRIO with different lane configurations.

Successful completion for all example iterations on two Linux processes per producer and consumer devices.

SYS/BIOS DSP TransportQmss

Name
Description
Expected Results
SYS/BIOS DSP TransportQmss Benchmark Example

Example demonstrating intra-SoC, DSP to DSP, transport over QMSS use while also measuring latency and throughput performance. The example consists of multiple iterations where each iteration runs QMSS with different reception mechanisms (accumulator or QPEND queue). Reference example for developers

Successful completion on two DSP cores for all example iterations.

SYS/BIOS DSP TransportQmss DSP-Side of Heterogeneous Processor Test

Tests inter-SoC, ARM Linux to DSP, transport over QMSS. Reference test for developers

Successful completion on two DSP cores and two Linux processes.

ARM Linux TransportQmss

Name
Description
Expected Results
ARM Linux TransportQmss Multi-Process Test

Tests Linux inter-process communication via IPC transport over QMSS. Reference test for developers

Successful completion on four Linux processes.

ARM Linux TransportQmss Linux-Side of Heterogeneous Processor Test

Tests inter-SoC, ARM Linux to DSP, transport over QMSS. Reference test for developers

Successful completion on two DSP cores and two Linux processes.

Additional References

Document Location
TransportQmss API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\transport\ipc\c66\qmss\docs\doxygen\html\index.html
TransportQmss Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\transport\ipc\c66\qmss\docs\ReleaseNotes_TransportQmss.pdf
TransportSrio API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\transport\ipc\c66\srio\docs\doxygen\html\index.html
TransportSrio Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\transport\ipc\c66\srio\docs\ReleaseNotes_TransportSrio.pdf