Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS Install In Custom Path

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide Installation in Custom Path




Overview

This page will provide configuration information if the SDK is installed in a custom path.

Helpful tips image.jpg

Useful Tip

To avoid changing environment variable for each new shell, modify environment variable file directly. This file is the setupenv file located in the SDK root directory.


Changes to CCS Configuration

Installing the SDK in a folder other than where CCS is installed will require modifications to CCS to be able to discover the SDK. See the Setup CCS How To page explaining how to update CCS configuration.


Rebuilding the SDK RTOS

Installing the SDK in a folder other than the default (C:\TI for Windows, /home/[user]/ti for Linux) requires modifications to SDK RTOS scripts in order for recompilation and example/test creation to work properly.

In all the commands below, replace [version] with the appropriate version of the software/tool.

CCS in Custom Path and SDK RTOS in Default Path

CCS installation and toolchain paths can be customized by setting the TOOLS_INSTALL_PATH environment variable prior to running the SDK level setupenv script. This feature is used if CCS and the toolchains are installed somewhere other than the default C:\ti location.

For example, environment configuration assuming CCS is installed to [os_base]\ti_temp and SDK RTOS has been installed to default path, [os_base]\ti :

  • Windows
C:\> set TOOLS_INSTALL_PATH=C:\ti_temp
C:\> cd C:\ti\processor_sdk_rtos_[soc]_[version]
C:\ti\processor_sdk_rtos_[soc]_[version]> setupenv.bat

Gives the output:

Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: set CG_XML_BIN_INSTALL_PATH=C:/ti/cg_xml/bin
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: set DOXYGEN_INSTALL_PATH=C:/ti/Doxygen/doxygen/1.5.1-p1/bin
**************************************************************************
Environment Configuration:
    PDK Directory             : /ti/PDK_AM~3/packages/
    CGTOOL INSTALL Directory  : C:/ti_temp/ccsv6/tools/compiler/ti-cgt-c6000_[version]
    TOOLCHAIN A15 Directory   : C:/ti_temp/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A8 Directory    : C:/ti_temp/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A9 Directory    : C:/ti_temp/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN M4 Directory    : C:/ti_temp/ccsv6/tools/compiler/ti-cgt-arm_[version]
    FPULIB_PATH               : C:/ti_temp/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]/lib/gcc/arm-none-eabi/[version]/fpu
    CROSS_TOOL_PRFX           : arm-none-eabi-
    XDC_INSTALL_PATH          : C:/ti/xdctools_[version]_core
    BIOS_INSTALL_PATH         : C:/ti/bios_[version]
    IPC_INSTALL_PATH          : C:/ti/ipc_[version]
    EDMA3LLD_BIOS6_INSTALLDIR : C:/ti/edma3_lld_[version]
    NDK_INSTALL_PATH          : C:/ti/ndk_[version]
    IMGLIB_INSTALL_PATH       : C:/ti/imglib_c66x_[version]
    UIA_INSTALL_PATH          : C:/ti/uia_[version]
    PROC_SDK_INSTALL_PATH     : C:/ti/processor_sdk_rtos_[soc]_[version]
**************************************************************************
Changing to short name to support directory names containing spaces
current directory: C:/ti/processor_sdk_rtos_[soc]_[version]
PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
**************************************************************************
  • Linux
$ export TOOLS_INSTALL_PATH=~/ti_temp
$ cd ~/ti/processor_sdk_rtos_[soc]_[version]/
~/ti/processor_sdk_rtos_[soc]_[version]$ source setupenv.sh

Gives the output:

Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: export CG_XML_BIN_INSTALL_PATH="~/ti/cg_xml/bin"
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: export DOXYGEN_INSTALL_PATH="~/ti/Doxygen/doxygen/1.5.1-p1/bin"
**************************************************************************
Environment Configuration:
    PDK Directory             : /home/[user]/ti/pdk_[soc]_[version]/packages
    CGTOOL INSTALL Directory  : /home/[user]/ti_temp/ccsv6/tools/compiler/ti-cgt-c6000_[version]
    TOOLCHAIN A15 Directory   : /home/[user]/ti_temp/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A8 Directory    : /home/[user]/ti_temp/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A9 Directory    : /home/[user]/ti_temp/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN M4 Directory    : /home/[user]/ti_temp/ccsv6/tools/compiler/ti-cgt-arm_[version]
    FPULIB_PATH               : /home/[user]/ti_temp/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]/lib/gcc/arm-none-eabi/[version]/fpu
    CROSS_TOOL_PRFX           : arm-none-eabi-
    XDC_INSTALL_PATH          : /home/[user]/ti/xdctools_[version]_core
    BIOS_INSTALL_PATH         : /home/[user]/ti/bios_[version]
    IPC_INSTALL_PATH          : /home/[user]/ti/ipc_[version]
    EDMA3LLD_BIOS6_INSTALLDIR : /home/[user]/ti/edma3_lld_[version]
    NDK_INSTALL_PATH          : /home/[user]/ti/ndk_[version]
    IMGLIB_INSTALL_PATH       : /home/[user]/ti/imglib_c66x_[version]
    UIA_INSTALL_PATH          : /home/[user]/ti/uia_[version]
    PROC_SDK_INSTALL_PATH     : /home/[user]/ti/processor_sdk_rtos_[soc]_[version]

PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
*******************************************************************************

The RTOS SDK top level Makefile can now be used to rebuild SDK RTOS components with CCS and toolchains installed in a custom installation path.

CCS in Default Path and SDK RTOS in Custom Path

SDK RTOS component installation paths can be customized by setting the SDK_INSTALL_PATH variable prior to running the SDK level setupenv script. This feature is used if the SDK is installed somewhere other than the default C:\ti location.

For example, environment configuration assuming CCS is installed to the default path, [os_base]\ti and SDK RTOS has been installed to [os_base]\ti_temp:

  • Windows
C:\> set SDK_INSTALL_PATH=C:/ti_temp
C:\> cd C:\ti_temp\processor_sdk_rtos_[soc]_[version]
C:\ti_temp\processor_sdk_rtos_[soc]_[version]> setupenv.bat

Gives the output:

Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: set CG_XML_BIN_INSTALL_PATH=C:/ti/cg_xml/bin
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: set DOXYGEN_INSTALL_PATH=C:/ti/Doxygen/doxygen/1.5.1-p1/bin
**************************************************************************
Environment Configuration:
    PDK Directory             : /ti_temp/PDK_AM~3/packages/
    CGTOOL INSTALL Directory  : C:/ti/ccsv6/tools/compiler/ti-cgt-c6000_[version]
    TOOLCHAIN A15 Directory   : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A8 Directory    : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A9 Directory    : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN M4 Directory    : C:/ti/ccsv6/tools/compiler/ti-cgt-arm_[version]
    FPULIB_PATH               : C:/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]/lib/gcc/arm-none-eabi/[version]/fpu
    CROSS_TOOL_PRFX           : arm-none-eabi-
    XDC_INSTALL_PATH          : C:/ti_temp/xdctools_[version]_core
    BIOS_INSTALL_PATH         : C:/ti_temp/bios_[version]
    IPC_INSTALL_PATH          : C:/ti_temp/ipc_[version]
    EDMA3LLD_BIOS6_INSTALLDIR : C:/ti_temp/edma3_lld_[version]
    NDK_INSTALL_PATH          : C:/ti_temp/ndk_[version]
    IMGLIB_INSTALL_PATH       : C:/ti_temp/imglib_c66x_[version]
    UIA_INSTALL_PATH          : C:/ti_temp/uia_[version]
    PROC_SDK_INSTALL_PATH     : C:/ti_temp/processor_sdk_rtos_[soc]_[version]
**************************************************************************
Changing to short name to support directory names containing spaces
current directory: C:/ti_temp/processor_sdk_rtos_[soc]_[version]
PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
**************************************************************************
  • Linux
$ export SDK_INSTALL_PATH=~/ti_temp
$ cd ~/ti_temp/processor_sdk_rtos_[soc]_[version]/
~/ti_temp/processor_sdk_rtos_[soc]_[version]$ source setupenv.sh

Gives the output:

Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: export CG_XML_BIN_INSTALL_PATH="~/ti/cg_xml/bin"
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: export DOXYGEN_INSTALL_PATH="~/ti/Doxygen/doxygen/1.5.1-p1/bin"
**************************************************************************
Environment Configuration:
    PDK Directory             : /home/[user]/ti_temp/pdk_[soc]_[version]/packages
    CGTOOL INSTALL Directory  : /home/[user]/ti/ccsv6/tools/compiler/ti-cgt-c6000_[version]
    TOOLCHAIN A15 Directory   : /home/[user]/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A8 Directory    : /home/[user]/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A9 Directory    : /home/[user]/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN M4 Directory    : /home/[user]/ti/ccsv6/tools/compiler/ti-cgt-arm_[version]
    FPULIB_PATH               : /home/[user]/ti/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]/lib/gcc/arm-none-eabi/[version]/fpu
    CROSS_TOOL_PRFX           : arm-none-eabi-
    XDC_INSTALL_PATH          : /home/[user]/ti_temp/xdctools_[version]_core
    BIOS_INSTALL_PATH         : /home/[user]/ti_temp/bios_[version]
    IPC_INSTALL_PATH          : /home/[user]/ti_temp/ipc_[version]
    EDMA3LLD_BIOS6_INSTALLDIR : /home/[user]/ti_temp/edma3_lld_[version]
    NDK_INSTALL_PATH          : /home/[user]/ti_temp/ndk_[version]
    IMGLIB_INSTALL_PATH       : /home/[user]/ti_temp/imglib_c66x_[version]
    UIA_INSTALL_PATH          : /home/[user]/ti_temp/uia_[version]
    PROC_SDK_INSTALL_PATH     : /home/[user]/ti_temp/processor_sdk_rtos_[soc]_[version]

PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
*******************************************************************************

The RTOS SDK top level Makefile can now be used to rebuild SDK RTOS components installed in the custom installation path.

NOTE

The following known issue impacts this step:

PRSDK-1263: PDK AM437x: Make fails on Windows if CCS is installed in custom path. Workaround: Edit the UTILS_INSTALL_DIR variable in <pdk_root_dir>/packages/ti/starterware/Rules.make to point to the CCS installation on your Windows PC.

CCS and SDK RTOS in Custom Path

When CCS and the SDK RTOS are both installed to custom paths the SDK can be rebuilt by setting the SDK_INSTALL_PATH and TOOLS_INSTALL_PATH variables prior to running the SDK RTOS top level environment setup script. The Windows and Linux environment setup scripts can be found in the following locations, respectively:

  • Windows - C:\custom\install\path\processor_sdk_rtos_[soc]_[version]\setupenv.bat
  • Linux - /home/[user]/custom/install/path/processor_sdk_rtos_[soc]_[version]/setupenv.sh

The SDK_INSTALL_PATH and TOOLS_INSTALL_PATH environment variables must be set to the custom install path prior to running the environment setup script.

For example, environment configuration assuming CCS and the SDK have been installed to [os_base]\new_sdk_release\ :

  • Windows
C:\> set SDK_INSTALL_PATH=C:\new_sdk_release
C:\> set TOOLS_INSTALL_PATH=C:\new_sdk_release
C:\> cd C:\new_sdk_release\processor_sdk_rtos_[soc]_[version]
C:\new_sdk_release\processor_sdk_rtos_[soc]_[version]> setupenv.bat

Gives the output:

Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: set CG_XML_BIN_INSTALL_PATH=C:/ti/cg_xml/bin
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: set DOXYGEN_INSTALL_PATH=C:/ti/Doxygen/doxygen/1.5.1-p1/bin
**************************************************************************
Environment Configuration:
    PDK Directory             : /NEW_SD~1/PDK_AM~1/packages/
    CGTOOL INSTALL Directory  : C:/new_sdk_release/ccsv6/tools/compiler/ti-cgt-c6000_[version]
    TOOLCHAIN A15 Directory   : C:/new_sdk_release/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A8 Directory    : C:/new_sdk_release/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A9 Directory    : C:/new_sdk_release/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN M4 Directory    : C:/new_sdk_release/ccsv6/tools/compiler/ti-cgt-arm_[version]
    FPULIB_PATH               : C:/new_sdk_release/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]/lib/gcc/arm-none-eabi/[version]/fpu
    CROSS_TOOL_PRFX           : arm-none-eabi-
    XDC_INSTALL_PATH          : C:/new_sdk_release/xdctools_[version]_core
    BIOS_INSTALL_PATH         : C:/new_sdk_release/bios_[version]
    IPC_INSTALL_PATH          : C:/new_sdk_release/ipc_[version]
    EDMA3LLD_BIOS6_INSTALLDIR : C:/new_sdk_release/edma3_lld_[version]
    NDK_INSTALL_PATH          : C:/new_sdk_release/ndk_[version]
    IMGLIB_INSTALL_PATH       : C:/new_sdk_release/imglib_c66x_[version]
    UIA_INSTALL_PATH          : C:/new_sdk_release/uia_[version]
    PROC_SDK_INSTALL_PATH     : C:/new_sdk_release/processor_sdk_rtos_[soc]_[version]
**************************************************************************
Changing to short name to support directory names containing spaces
current directory: C:/new_sdk_release/processor_sdk_rtos_[soc]_[version]
PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
**************************************************************************
  • Linux
$ export SDK_INSTALL_PATH=~/new_sdk_release
$ export TOOLS_INSTALL_PATH=~/new_sdk_release
$ cd ~/new_sdk_release/processor_sdk_rtos_[soc]_[version]/
~/new_sdk_release/processor_sdk_rtos_[soc]_[version]$ source setupenv.sh

Gives the output:

Optional parameter not configured : CG_XML_BIN_INSTALL_PATH
REQUIRED for xdc release build
Example: export CG_XML_BIN_INSTALL_PATH="~/ti/cg_xml/bin"
Optional parameter not configured : DOXYGEN_INSTALL_PATH
REQUIRED for xdc release build
Example: export DOXYGEN_INSTALL_PATH="~/ti/Doxygen/doxygen/1.5.1-p1/bin"
**************************************************************************
Environment Configuration:
    PDK Directory             : /home/[user]/new_sdk_release/pdk_[soc]_[version]/packages
    CGTOOL INSTALL Directory  : /home/[user]/new_sdk_release/ccsv6/tools/compiler/ti-cgt-c6000_[version]
    TOOLCHAIN A15 Directory   : /home/[user]/new_sdk_release/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A8 Directory    : /home/[user]/new_sdk_release/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN A9 Directory    : /home/[user]/new_sdk_release/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]
    TOOLCHAIN M4 Directory    : /home/[user]/new_sdk_release/ccsv6/tools/compiler/ti-cgt-arm_[version]
    FPULIB_PATH               : /home/[user]/new_sdk_release/ccsv6/tools/compiler/gcc-arm-none-eabi-[version]/lib/gcc/arm-none-eabi/[version]/fpu
    CROSS_TOOL_PRFX           : arm-none-eabi-
    XDC_INSTALL_PATH          : /home/[user]/new_sdk_release/xdctools_[version]_core
    BIOS_INSTALL_PATH         : /home/[user]/new_sdk_release/bios_[version]
    IPC_INSTALL_PATH          : /home/[user]/new_sdk_release/ipc_[version]
    EDMA3LLD_BIOS6_INSTALLDIR : /home/[user]/new_sdk_release/edma3_lld_[version]
    NDK_INSTALL_PATH          : /home/[user]/new_sdk_release/ndk_[version]
    IMGLIB_INSTALL_PATH       : /home/[user]/new_sdk_release/imglib_c66x_[version]
    UIA_INSTALL_PATH          : /home/[user]/new_sdk_release/uia_[version]
    PROC_SDK_INSTALL_PATH     : /home/[user]/new_sdk_release/processor_sdk_rtos_[soc]_[version]

PROCESSOR SDK BUILD ENVIRONMENT CONFIGURED
*******************************************************************************

The RTOS SDK top level Makefile can now be used to rebuild SDK RTOS components installed in the custom installation path using CCS and toolchains installed in a custom path as well.


Rebuilding the PDK

Installing the PDK in a folder other than the default (C:\TI for Windows, /home/[user]/ti for Linux) requires modifications to PDK scripts in order for recompilation and example/test creation to work properly.

CCS in Custom Path and PDK in Default Path

The instructions provided in the CCS in Custom Path and SDK RTOS in Default Path section can be used to rebuild components at the PDK level. The only difference is the PDK level setup script should be used instead of the SDK RTOS level setup script. The PDK level setup scripts are found in the following locations on Windows and Linux, respectively:

  • Windows - C:\custom\install\path\pdk_[soc]_[version]\packages\pdksetupenv.bat
  • Linux - /home/[user]/custom/install/path/pdk_[soc]_[version]/packages/pdksetupenv.sh

CCS in Default Path and PDK in Custom Path

The instructions provided in the CCS in Default Path and SDK RTOS in Custom Path section can be used to rebuild components at the PDK level. The only difference is the PDK level setup script should be used instead of the SDK RTOS level setup script. The PDK level setup scripts are found in the following locations on Windows and Linux, respectively:

  • Windows - C:\custom\install\path\pdk_[soc]_[version]\packages\pdksetupenv.bat
  • Linux - /home/[user]/custom/install/path/pdk_[soc]_[version]/packages/pdksetupenv.sh

CCS and PDK in Custom Path

The instructions provided in the CCS and SDK RTOS in Custom Path section can be used to rebuild components at the PDK level. The only difference is the PDK level setup script should be used instead of the SDK RTOS level setup script. The PDK level setup scripts are found in the following locations on Windows and Linux, respectively:

  • Windows - C:\custom\install\path\pdk_[soc]_[version]\packages\pdksetupenv.bat
  • Linux - /home/[user]/custom/install/path/pdk_[soc]_[version]/packages/pdksetupenv.sh


Creating PDK Example/Test Projects When CCS is Installed to Custom Path

The pdkProjectCreate scripts must be modified in order to build PDK example and test projects only if CCS has been installed to a custom path. The modification is the same for both Windows and Linux. Inside the pdkProjectCreate scripts is a CCS_INSTALL_PATH variable which points to the Code Composer Studio root directory. This variable must be redefined to the new location of the CCS root directory if CCS is installed to a custom path.

  • Windows
REM Install Location for CCS
set CCS_INSTALL_PATH="C:\ti\ccsv6"
  • Linux
# Install Location for CCS
export CCS_INSTALL_PATH=~/ti/ccsv6
NOTE

Prior to invoking the pdkProjectCreate script, make sure to start CCS and register the SDK RTOS components installed. Project creation will fail if the RTOS SDK components installed to the custom path have not been registered with CCS. Please see CCS and SDK installed in different directories for instructions on how to register SDK RTOS components installed to a custom path with CCS