Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS OSAL

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide OSAL



Overview

User Interface

Application

Debug


Overview

The OSAL library provides operating system abstraction layer API sample implementations that are required for processor SDK drivers. Scope of APIs supported in the module is limited to support OS services required for RTOS or bare metal drivers

  • Supported Operating Systems
    • TIRTOS
    • NONOS
  • Supported SOCs
    • Please refer to component release notes

Operating System Extension

APIs
Porting of OSAL component will enable extending PDK components to additional OS environment. Reference top level API header file  includes:

#include <ti/osal/osal.h>

Application Integration Details

Baremetal or No-OS Use case

Reference library path to be included in application build environment:

 <ti/osal/lib/nonos/[soc]/[[cpu]/>
  

SysBIOS based application

Any RTSC application that needs to use osal library, should have below RTSC configuration lines before any other processor sdk components (e.g., board, gpio, uart etc).


 /* set the operating system type, 
  * supported types are "tirtos" and "nonos" 
  */
 var osType           = "tirtos";

 /* set the soc type
  * (applicable only when osTYpe 
  *  is "nonos" only)
 */
 var socType           = "am572x";

 /* Setup the OSAL Library */
 var Osal = xdc.loadPackage('ti.osal');
 Osal.Settings.osType  = osType;
 Osal.Settings.socType = socType;

   


Example

Sysbios Example

This sysbios example OSAL_BasicExample_<board>_<coretype>TestProject tests Hwi, Timer, Delay, Semaphores etc and prints output on UART console.

Introduction

This sysbios based example tests Hwi, Timer, Semaphores etc.

Supported platforms
evmAM335x 
evmAM437x 
idkAM571x 
idkAM574x 
evmAM572x 
evmK2G
evmK2H
evmOMAPL137
lcdkOMAPL138
Build instructions
Run pdkProjectCreate to create the OSAL_BasicExample_<evm>_<device>TestProject
Load the project on to CCS and build the same.
Build the example
Load the OSAL_BasicExample_<evm>_<device>TestProject
Run the example
Testing the example

The output for each of the tests (Hwi, Timer, Delay, Semaphores etc) can be seen on the UART console. After a successful run, "All tests have PASSED" will be displayed on the screen.

Baremetal Example

Introduction

This baremetal example 'osal_baremetal_test' tests Hwi, Timer, Semaphores etc and prints output on UART console.

Supported platforms
evmAM572x 
evmAM335x 
evmAM437x 
evmDRA72x 
evmDRA75x 
evmDRA78x 
iceK2G 
idkAM574x 
idkAM572x 
idkAM571x 
idkAM437x
Build instructions

OSAL tests are built using makefiles. The below steps are used to build the baremetal test binaries.

cd pdk_<ver>/packages/
Run pdksetupenv.bat 
Run "make osal"
Find the executable at ti/<pdk>/packages/ti/binary/osal_baremetal_test/bin
Load the executable on the board
Before running the executable, please make sure you have the UART connected and notice the test output on the UART console. Osal prints out the results there.
Testing the example

The output for each of the tests (Hwi, Timer, Delay, Semaphores, etc) can be seen on the UART console. After a successful run, "All tests have passed" will be displayed on the screen.

Output

The output of osal example looks like below. The below sample output is from idkAM571x on the UART console.

HWI tests have passed.
TimerTestLog: got 100 ticks from timer id = 1
TimerTestLog: got 100 ticks from timer id = 2
Timer tests have passed.
Running Osal_Delay test:..........
Osal_Delay tests have passed.
Clock tests have passed.
Semaphore tests have passed.
Semaphore Statistics:
PeakSemObjs = 5,
numMaxSemObjs = 100,
numFreeSemObjs = 97
Hwi Statistics:
PeakHwiObjs = 3,
numMaxHwiObjs = 100,
numFreeHwiObjs = 98
Timer Statistics:
PeakTimerObjs = 2,
numMaxTimerObjs = 100,
numFreeTimerObjs = 99
All tests have passed.

Additional References

Operating System Abstraction Layer Library Summary
Component Type Library
Install Package PDK
Install Directory pdk_AMX_<version>\packages\ti\osal
Project Type Eclipse RTSC
Endian Support Little
Linker Path $(TI_PDK_INSTALL_DIR)\packages\ti\osal
Linker Sections .vecs , .switch, .args, .cio
Include Paths $(TI_PDK_INSTALL_DIR)\packages\ti\osal
Reference Guides $(TI_PDK_INSTALL_DIR)\packages\ti\osal\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\osal\docs\ReleaseNotes_OSAL.pdf