Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS PA

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide PA



Overview

User Interface

Application

Debug

Introduction

The packet accelerator (PA) is one of the main components of the network coprocessor (NETCP) peripheral in KeyStone devices, including C6678, K2H/K/E/L. The PA works together with the security accelerator (SA) and the gigabit Ethernet switch subsystem to form a network processing solution. The purpose of PA in the NETCP is to perform packet processing operations such as packet header classification, checksum generation, and multi-queue routing.

Driver Configuration

The driver configures the PASS subsystem using Pa_config_t structure. This structure must be initialized before the Pa_create() function is called and cannot be changed afterwards. Also, there are bunch of system/global configurations and per entry configurations for PA. For details about individual fields of this structure and other configuration API structures, see the Doxygen help by opening PDK_INSTALL_DIR\packages\ti\drv\PA\docs\doxygen\html\index.html.

APIs

API reference for application can be found in below file:

#include <ti/drv/PA/PA.h>

Example

Name
Description
Expected Results
PA_Example application

Example demonstrating simple emac loopback use case. Reference example for developers

User observes the output printed over the CCS console

PA_UnitTestApplication

Unit Test application to test all APIs

User observes the output printed over the CCS console

PA_PktCapTestApplication

Packet Capture Unit Test application.

User observes the output printed over the CCS console

FAQ

What is the difference between internal loopback and external loopback?

  • CPSW_LOOPBACK_INTERNAL (default): The transmitted packet is loopbacked at the SGMII through SGMII internal loopback
  • CPSW_LOOPBACK_EXTERNAL: The transmitted packet should be loopbacked by an application outside of the SOC, e.g., PC, PHY.

How to test PA EMAC example with a PC?

The EVM has to be connected to PC via RJ-45 port. By default, the PA example uses the internal loopback mode, please change code: int cpswLpbkMode = CPSW_LOOPBACK_INTERNAL to CPSW_LOOPBACK_EXTERNAL.

To test the egress path (from SOC to PC):

  • Rebuilt the CCS project, load and run.
  • The PC should receive 10 identical UDP packets sending out by the PA example, the packet is defined by an array pktMatch[] in the code.

To test the ingress direction (from PC to SOC): The PC needs a tool to send out packets with controlled MAC address, IP address and UDP port matching the PA layer 2, 3 and 4 classifications, defined by the following functions:

  • Add_MACAddress(): ethInfo.dst
  • Add_IPAddress(): ipInfo.dst
  • Add_Port (): ports

How to use PA EMAC example to test other Ethernet ports than default?

The Keystone devices may have multiple Ethernet ports, connected through an internal GbE switch with a host port. There is a pre-defined symbol "NUM_PORTS" in the text file when creating the PA project. This controls how many ports used in loopback mode test. In non-loopback case, the port number may be hardcoded by gNum_Mac_Ports. This has to be changed for the test. On EVMs, those additional Ethernet ports may be accessed by various ways: Rear-Transition Module – Breakout Card (RTM-BOC) or Advanced Mezzanine Card – Breakout Card (AMC-BOC), or AMC backplane, they are EVM hardware dependent. For example, K2E has 8 SGMII ports. In the K2E EVM, two Ethernet PHYs (PHY1 and PHY2) are connected to SoC SGMII 0 and 1 respectively, to provide a copper interface and routed to a Gigabit RJ-45 connector. The SGMII 2 and 3 of SoC are routed to Port 0 and 1 of the AMC edge connector backplane interface. The SGMII 4 to 7 are routed to RTM connector which can be accessed by RTM BOC. The PA EMAC example by default tests all 8 ports in loopback. To test additional ports in non-loopback, check/modify the gNum_Mac_Ports defined to include the SGMII testing port.

Can PA be used to forward all incoming packets to host?

The design of PA is to use firmware to offload host for classifying packets, the PA has layer 2, 3 and 4 classifications. PA LLD supports two APIs to add MAC LUT1 classification and routing. The application can call either the first generation API Pa_addMac() or the second generation Pa_addMac2() APIs. When using the first API, initialize all the elements of paEthInfo_t with zero and update the routing info paRouteInfo_t with pa_DEST_HOST. When using the second generation API, paEthInfo2_t with validBitMap = 0 and paRouteInfo2_t (in paParamDesc) with pa_DEST_HOST can be passed. Please refer to Pa_addMac and Pa_addMac2() API explanations as provided under the doxygen folder of PA (Or refer to Pa.h interface header file).

Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\PA\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\PA\docs\ReleaseNotes_PA_LLD.pdf