Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS PM

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide PM



Overview

User Interface

Application

Debug

Introduction

The Power Management (PM) low level driver provide power and thermal management capabilities for RTOS applications.

Supported Devices

Device A15 A8 A9 C66x M4 Tested On
AM57xx X X X AM572x GP EVM, AM571x GP EVM
AM335x X AM335x GP EVM
AM437x X AM437x GP EVM
K2G X X K2G EVM

Driver Configuration

Board Specific Configuration

The following board-specific actions must take place prior to calling any PM Power APIs:

  • A board-specific I2C implementation must be registered with the PM HAL layer
  • The PMIC Ops structure matching the executing device's PMIC must be registered with PM HAL layer
  • Device clock rates must be initialized through the PM LIB layer

For working examples of how to implement the listed items, see the "main" functions of any PM example in [PDK_INSTALL_DIR]\packages\ti\drv\pm\examples.

PM Configuration Structure

The pm\src\pmrtos\prcm\PowerDevice.c file configures the PM driver through the PowerDevice_config structure. This structure must be provided to PM driver. The structure is a global defined within PowerDevice.c and must be initialized prior to calling Power_init(). The structure cannot be changed after calling Power_init(). For details about individual fields of this structure, see the Doxygen help by opening [PDK_INSTALL_DIR]\packages\ti\drv\pm\docs\doxygen\html\index.html.

APIs

The following lists the main application interfaces; see the end of this page for a link to the API Reference Manual with full details.

PM TI RTOS base API reference for applications can be found in below file:

#include <ti/drv/pm/Power.h>  /* Contains the core TI RTOS Power implementation APIs */

PM TI RTOS extended API reference for applications can be found in the below file:

#include <ti/drv/pm/PowerExtended.h>  /* Contains TI RTOS Power API extensions such as thermal management */

PM TI RTOS device-specific API reference for applications can be found in the below file:

#include <ti/drv/pm/PowerDevice.h>  /* Contains device-specific TI RTOS Power API definitions and structures */


Example

Name
Description
Expected Results
PM RTOS Application

Example demonstrating power management use cases. Reference example for developers

Application cycles the processor running the application through various power states using the PM APIs. User observes the output printed over the device's UART connection.
Note: The example should be run in "Free Run" mode when loaded and executed in Code Composer Studio in order to prevent sleep API testing interruptions from the JTAG.

Use the following steps to execute the application on the AM57xx's M4 and C66 processors in Code Composer Studio:

  • Connect to CortexA15_0 waiting until the GEL file initialization completes
  • Run the GEL: Scripts-->AM572x MULTICORE Initialization-->AM572x_MULTICORE_EnableAllCores
  • Connect to M4_IPU1_C0 or the C66xx_DSP1
  • Load the PM RTOS application's M4 or c66 executable
  • Free run the M4_IPU1_C0 or the C66xx_DSP1
PM RTOS Thermal Application

Example demonstrating thermal management use case. Reference example for developers

Application sets high and low thermal set points using the PM APIs. The set points are triggered by internally heating up the processor. User observes the output printed over the device's UART connection.

Use the following steps to execute the application on the AM57xx's M4 and C66 processors in Code Composer Studio:

  • Connect to CortexA15_0 waiting until the GEL file initialization completes
  • Run the GEL: Scripts-->AM572x MULTICORE Initialization-->AM572x_MULTICORE_EnableAllCores
  • Connect to M4_IPU1_C0 or the C66xx_DSP1
  • Load the PM RTOS Thermal application's M4 or c66 executable
  • Run the M4_IPU1_C0 or the C66xx_DSP1
PM Measurement Application

Menu-based application allowing selection of processor OPPs and benchmark tests.

Application allows the user to control the processor's OPP settings via the PM driver. The application also allows the user to select execution of the Dhrystone benchmark for performance and power profiling under different OPP settings. The application's menu is printed over the device's UART connection.
Note: The measurement application is only supported on the AM335x device at the moment.

Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\pm\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\pm\docs\ReleaseNotes_PM_LLD.pdf