Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS QMSS

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide QMSS



Overview

User Interface

Application

Debug


Introduction

The Queue Manager Sub System (QMSS) low level driver provides the interface to Queue Manager Subsystem hardware which is part of the Multicore Navigator functional unit for a keystone device. QMSS provides hardware assisted queue system and implements fundamental operations such as en-queue and de-queue, descriptor management, accumulator functionality and configuration of infrastructure DMA mode. The LLD provides APIs to get full entitlement of supported hardware functionality.

The LLD also includes accumulation and QoS (Quality of Service) firmware. QoS enables restriction of data rates in bytes per second or packets per second, weighted round robin queue selection, and selective descriptor dropping for oversubscribed queues. Accumulation The APIs are provided through the LLD. The API documentation for both QoS and Accumulator is available in the API Reference manual below. The capabilities of the QoS firmware are documented in their design documents. The capabilities of the accumulator are documented in the Hardware Peripheral User Guide.

Modes of Operation

QMSS library (ti.drv.qm) supports below modes

Joint Mode: In this mode, only linkingRAM0Base, linkingRAM0Size, and linkingRAM1Base are used to configure all QM groups simultaneously. For all existing devices (K2H, K2K) this is only mode that should be used. For the rest of the devices such as K2L, K2E, 6678 and 6657, this is the only mode available.

Split Mode: This mode shouldn't be used as it doesn't support all peripherals on the device.

Driver Configuration

The driver configures the QMSSSS subsystem using Qmss_GlobalConfigGroupRegs(system configuration) structure. The default global configuration per device is present under qmss_device.c file provided per device.

For details about individual fields of this structure, see the Doxygen help by opening PDK_INSTALL_DIR\QMSSckages\ti\drv\QMSS\docs\doxygen\html\index.html.

APIs

API header for application:

#include <ti/drv/QMSS/QMSS_drv.h>

Please see the doxygen in "API Reference Manual" below for details.


Example

Name
Description
Expected Results
QMSS_Example application

Example demonstrating infra DMA, interrupt test use case. Reference example for developers

User observes the output printed over the CCS console

QMSS_UnitTestApplication

Unit Test application to test all APIs

User observes the output printed over the CCS console

Sample Example Output

This came from K2K multicore example:

**************************************************
************ QMSS Multicore Example **************
**************************************************
**************************************************
************ QMSS Multicore Example **************
**************************************************
**************************************************
**************************************************
************ QMSS Multicore Example **************
************ QMSS Multicore Example **************
**************************************************
**************************************************
Core 1 : Starting BIOS...
Core 2 : Starting BIOS...
Core 3 : Starting BIOS...
Core 0 : Starting BIOS...
Core 0 : Created RM packet heap
Core 0 : Created IPC MessageQ heap
Core 0 : Created receive Q for Client1
Core 1 : Opened RM packet heap
Core 2 : Opened RM packet heap
Core 3 : Opened RM packet heap
Core 1 : Opened IPC MessageQ heap
Core 2 : Opened IPC MessageQ heap
Core 3 : Opened IPC MessageQ heap
Core 1 : Created receive Q for Server
Core 2 : Created receive Q for Server
Core 3 : Created receive Q for Server
Core 1 : Opened Server's receive Q
Core 1 : Waiting for QMSS to be initialized...

Core 0 : Opened Client1's receive Q for Server
Core 0 : Created receive Q for Client2
Core 0 : Opened Client2's receive Q for Server
Core 0 : Created receive Q for Client3
Core 2 : Opened Server's receive Q
Core 2 : Waiting for QMSS to be initialized...

Core 0 : Opened Client3's receive Q for Server

-----------------------Initializing---------------------------
Core 0 : L1D cache size 4. L2 cache size 0.
Core 0 : Memory region 0 inserted
Core 0 : Memory region 1 inserted
Core 0 : Tx Completion Queue Number     : 897 opened
Core 0 : Number of Tx descriptors requested : 32. Number of descriptors allocated : 32 
Core 0 : Number of Rx descriptors requested : 32. Number of descriptors allocated : 32 
Core 0 : Number of Sync free descriptors requested : 32. Number of descriptors allocated : 32 
Core 0 : Sync Queue Number              : 9025 opened
Core 0 : Sync Cfg Queue Number          : 9026 opened
Core 0 : Sync Free Queue Number         : 898 opened
Core 0 : Receive Free Queue Number      : 736 opened
Core 0 : Transmit Free Queue Number     : 8928 opened
Core 0 : System initialization completed: 8928
Core 0 : Publishing RM nameserver names for shared queues

--------------------Queue status CORE 0----------------------
                    After Initialization

Tx Free Queue 8928 Entry Count            : 32 
Rx Free Queue 736 Entry Count            : 32 
Tx completion Queue 897 Entry Count     : 0 
Sync Queue 9025 Entry Count              : 0 
Sync free Queue 898 Entry Count         : 32 
Sync Cfg Queue 9026 Entry Count          : 0 
-------------------------------------------------------------

Core 0 : Registering High Priority interrupt channel : 0 eventId : 48 queue Number : 704


Core 3 : Opened Server's receive Q
Core 1 : QMSS initialization done.
Core 2 : QMSS initialization done.
Core 3 : Waiting for QMSS to be initialized...




Core 3 : QMSS initialization done.

Core 1 : Rx Free Queue Number       : 736 opened
Core 2 : Rx Free Queue Number       : 736 opened
Core 3 : Rx Free Queue Number       : 736 opened
Core 1 : Tx Free Queue Number       : 8928 opened
Core 2 : Tx Free Queue Number       : 8928 opened
Core 3 : Tx Free Queue Number       : 8928 opened
Core 1 : Tx Completion Queue Number : 897 opened
Core 2 : Tx Completion Queue Number : 897 opened
Core 3 : Tx Completion Queue Number : 897 opened
Core 1 : Sync Queue Number          : 9025 opened
Core 2 : Sync Queue Number          : 9025 opened
Core 3 : Sync Queue Number          : 9025 opened
Core 1 : Sync Free Queue Number     : 898 opened
Core 2 : Sync Free Queue Number     : 898 opened
Core 3 : Sync Free Queue Number     : 898 opened
Core 1 : Sync Cfg Queue Number      : 9026 opened
Core 2 : Sync Cfg Queue Number      : 9026 opened
Core 3 : Sync Cfg Queue Number      : 9026 opened
Core 1 : Registering High Priority interrupt channel : 1 eventId : 48 queue Number : 705
Core 2 : Registering High Priority interrupt channel : 2 eventId : 48 queue Number : 706
Core 3 : Registering High Priority interrupt channel : 3 eventId : 48 queue Number : 707
Core 1 : Waiting for sync signal
Core 2 : Waiting for sync signal
Core 3 : Waiting for sync signal
Core 0 : Opened Tx channel      : 0
Core 0 : Opened Rx channel      : 0
Core 0 : Transmit Queue Number  : 800
Core 0 : Receive Queue Number   : 704
Core 0 : Opened Rx flow         : 0
Core 0 : High priority accumulator programmed for channel : 0 queue : 704

Core 0 : Transmitting 8 packets..........

*************************************************************
Core 0 : Opened Tx channel      : 0
Core 0 : Opened Rx channel      : 0
Core 0 : Transmit Queue Number  : 800
Core 0 : Receive Queue Number   : 705
Core 0 : Opened Rx flow         : 0
Core 0 : High priority accumulator programmed for channel : 1 queue : 705

Core 0 : Transmitting 8 packets..........

*************************************************************
Core 0 : Opened Tx channel      : 0
Core 0 : Opened Rx channel      : 0
Core 0 : Transmit Queue Number  : 800
Core 0 : Receive Queue Number   : 706
Core 0 : Opened Rx flow         : 0
Core 0 : High priority accumulator programmed for channel : 2 queue : 706

Core 0 : Transmitting 8 packets..........

*************************************************************
Core 0 : Opened Tx channel      : 0
Core 0 : Opened Rx channel      : 0
Core 0 : Transmit Queue Number  : 800
Core 0 : Receive Queue Number   : 707
Core 0 : Opened Rx flow         : 0
Core 0 : High priority accumulator programmed for channel : 3 queue : 707

Core 0 : Transmitting 8 packets..........

*************************************************************
Core 0 : Waiting for sync signal
Core 0 : Got sync signal
*************************************************************


--------------------Queue status CORE 0----------------------
                    After packet processing

Tx Free Queue 8928 Entry Count            : 0 
Rx Free Queue 736 Entry Count            : 32 
Tx completion Queue 897 Entry Count     : 32 
Sync Queue 9025 Entry Count              : 4 
Sync free Queue 898 Entry Count         : 27 
Sync Cfg Queue 9026 Entry Count          : 1 
-------------------------------------------------------------

Core 0 : Waiting for other cores to ack sync signal
Core 1 : Got sync signal
Core 2 : Got sync signal
Core 3 : Got sync signal
*************************************************************
*************************************************************
*************************************************************



Core 0 : acks found

--------------------Deinitializing---------------------------

--------------------Queue status CORE 0----------------------
                    Before exit

Tx Free Queue 8928 Entry Count            : 0 
Rx Free Queue 736 Entry Count            : 32 
Tx completion Queue 897 Entry Count     : 32 
Sync Queue 9025 Entry Count              : 0 
Sync free Queue 898 Entry Count         : 28 
Sync Cfg Queue 9026 Entry Count          : 4 
-------------------------------------------------------------

Core 0 : Receive free queue closed successfully. Ref count : 0
Core 0 : Transmit completion queue closed successfully. Ref count : 3
Core 0 : Transmit free queue closed successfully. Ref count : 3
Core 0 : Sync queue closed successfully. Ref count : 3
Core 0 : Sync free queue closed successfully. Ref count : 3
Core 0 : Sync queue closed successfully. Ref count : 3
Core 0 : CPPI CPDMA closed successfully
Core 0 : CPPI exit successful
Core 0: Cleaning regions
Core 0: exit QMSS
Core 1 : Receive free queue closed successfully. Ref count : 3
Core 2 : Receive free queue closed successfully. Ref count : 2
Core 3 : Receive free queue closed successfully. Ref count : 1
Core 1 : Transmit completion queue closed successfully. Ref count : 2
Core 2 : Transmit completion queue closed successfully. Ref count : 1
Core 3 : Transmit completion queue closed successfully. Ref count : 0
Core 1 : Transmit free queue closed successfully. Ref count : 2
Core 2 : Transmit free queue closed successfully. Ref count : 1
Core 3 : Transmit free queue closed successfully. Ref count : 0
Core 1 : Sync queue closed successfully. Ref count : 2
Core 2 : Sync queue closed successfully. Ref count : 1
Core 3 : Sync queue closed successfully. Ref count : 0
Core 1 : Sync free queue closed successfully. Ref count : 2
Core 2 : Sync free queue closed successfully. Ref count : 1
Core 3 : Sync free queue closed successfully. Ref count : 0
Core 1 : Sync queue closed successfully. Ref count : 2
Core 2 : Sync queue closed successfully. Ref count : 1
Core 3 : Sync queue closed successfully. Ref count : 0
*******************************************************
*******************************************************
*******************************************************
******** QMSS Multicore (1) Example Done (PASS) *******
******** QMSS Multicore (2) Example Done (PASS) *******
******** QMSS Multicore (3) Example Done (PASS) *******
*******************************************************
*******************************************************
*******************************************************
Core 0 : Deleting RM nameserver names for shared queues
Instance name: RM_Server
Handle: 0x00854578
Type:   Server

Resource Status:

Core 0 : All resources freed successfully
*******************************************************
******** QMSS Multicore (0) Example Done (PASS) *******
*******************************************************

Debug FAQ

  1. Double Push - Some queue elements lost.
    1. Pushing the same pointer twice is illegal. In hardware it does something similar to double linking the same object into two places of a software linked list. It corrupts the list, such that some items will be orphaned/lost.
  2. NULL Push - Entire queue lost
    1. Pushing NULL (0) clears the entire queue. This is intentionally done by Qmss_QueueEmpty(). However the various Qmss_QueuePush functions don't check for NULL (to save cycles). Don't push NULL (for example received when Qmss_QueuePop finds an empty queue).
  3. Hint Bits (4 low LSBs of desc pointer)
    1. These are used to tell DMAs such as CPPI the size of the descriptor. Thus, when receiving descriptors from hardware, you must use QMSS_DESC_PTR() to discard them, else unaligned memory accesses that corrupt descriptors will be generated by software.
  4. General lost descriptors
    1. Its not a bad idea to have code that can inventory all your descriptors as part of destructive debug. Iterate over all queues, and pop all descriptors. Set a bit in a large bitmap for each descriptor found. Bits that remain 0 indicate "lost" descriptors which could have happened due to double push or null push or software bugs that simply lost them. By examining the contents of descriptor(s) and buffer(s), can often determine who last used them therefore what part of code lost them.
    2. Its also good to have nondestructive debug code that can call Qmss_getQueueByteCount() and Qmss_getQueueEntryCount() for each queue. This should be able to find all but a few (~4) descriptors per hardware DMA that are in flight. If large amounts of descriptors are missing, it means there is a bug. For this debug/monitor purpose, its OK to make own Qmss_QueueHandle by casting the queue number (eg (Qmss_QueueHandle)queueNum) since its undesirable to generate accounting/management for purpose of nondestructive debug.

Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\QMSS\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\QMSS\docs\ReleaseNotes_QMSS_LLD.pdf
QoS (Weighted Round Robin and SP QoS tree) $(TI_PDK_INSTALL_DIR)\packages\ti\drv\QMSS\docs\firmware\qos_sched,qos_sched_drop_sched,qos_sched_wide.pdf
QoS (Leaky bucket and SRIO TX Scheduler) $(TI_PDK_INSTALL_DIR)\packages\ti\drv\QMSS\docs\firmware\qos.pdf
Hardware Userguide/TRM UG TRM PDF
CPPI LLD (Navigator/QMSS DMA component) CPPI LLD