Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS SA

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide SA



Overview

User Interface

Application

Debug

Introduction

The Security Accelerator (SA) also known as cp_ace (Adaptive Cryptographic Engine) is designed to provide packet security as part of IPSEC, SRTP, and 3GPP industry standards. The security accelerator low level driver (referred to as the module) provides APIs for the configuration and control of the security accelerator sub-system. The SA low level driver provides an abstraction layer between the application and the Security Accelerator Sub System (SASS). It provides both the system level interface and the channel-level interface with a set of APIs in the driver.

Modes of Operation

Security accelerator library (ti.drv.sa) supports below modes

Protocol Specific Mode: In this mode, standards such as Ipv4/Ipv6 and 3gpp protocols are supported, where command labels are created based on the protocols.

Data Mode: In this mode, user can implement a custom/proprietary protocol mode with the help of APIs provided by SA LLD

Driver Configuration

The driver configures the SASS subsystem using SA_config_t (system configuration) and Channel Configuration (Sa_ChanConfig_t) structure.

For details about individual fields of this structure and other APIs, see the Doxygen help by opening PDK_INSTALL_DIR\SAckages\ti\drv\SA\docs\doxygen\html\index.html.

APIs

API reference for application:

#include <ti/drv/SA/Salld.h>

Example

Name
Description
Expected Results
SA_Example application

Example demonstrating simple IPSec use case. Reference example for developers

User observes the output printed over the CCS console

SA_UnitTestApplication

Unit Test application to test all APIs

User observes the output printed over the CCS console

Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\sa\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\sa\docs\ReleaseNotes_SA_LLD.pdf

NoteNote: Although SASS supports 3GPP specific Ciphering and Authentication algorithms such as Kasumi F8/F9 and Snow3G F8, those algorithms are locked out in this standard SA LLD distribution. In order to access 3GPP specific functionalities, one must obtain ETSI licensing as described at http://www.etsi.org/services/security-algorithms/cellular-algorithms and then download the SASS 3GPP Enabler package from TI from the link http://software-dl.ti.com/libs/sa_3gpp_enabler/latest/index_FDS.html


Due to export control restrictions, the SA 3GPP Enabler is a seperate download from the rest of the PROCESSOR-SDK.