Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS SRIO

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide SRIO



Overview

User Interface

Application

Debug


Introduction

Driver enables the high-bandwidth system level interconnects. It is intended to offer Gigabyte per second performance levels for chip-to-chip and board-to-board communication.

Modes of Operation

Following modes of operations are supported

Direct I/O: The SRIO packet contains the specific address where the data should be stored or read in the destination device. This means that the source device must have detailed knowledge of the available memory space within the destination device.

Type 9: A destination address is not specified. Instead the Stream ID is used to map the request to a specific memory region by the local (destination) device. TI IP additionally uses Class of Service (COS) as well to further classify the mapping of a request to a memory region.

Type 11: A destination address is not specified, instead, a mailbox identifier is used within the SRIO packet. The mailbox is controlled and mapped to memory by the local (destination) device.

Driver Configuration

Board Specific Configuration

All board specific configurations eg:enabling and configuring the SRIO SERDES registers and SRIO lane configurations (communication rates, device IDs, etc) are required before calling any driver APIs. Template functions for configuring the SRIO IP and SERDES registers are provided in PDK_INSTALL_DIR\packages\ti\drv\srio\device\<device>\src\. A template function is provided for each soc that supports SRIO.

APIs

API reference for application:

#include <ti/drv/srio/srio_drv.h>

OSAL API reference for application:

#include <ti/drv/srio/srio_osal.h>
Init SRIO
Initialize QMSS and CPPI modules...
...
SrioDevice_init();
Srio_init ();
...
/* Start the application Managed SRIO Driver. Refer example/test for appCfg fields */
hAppManagedSrioDrv = Srio_start (&appCfg); 

At this point SRIO driver is ready for data transfer on specific instance identified by handle.

Send/Receive APIs

Direct IO:

Srio_sockSend_DIO(Srio_SockHandle srioSock, Srio_DrvBuffer hBuffer, uint32_t size, Srio_SockAddrInfo* to);

Type 9:

Srio_sockSend_TYPE9   (Srio_SockHandle srioSock, Srio_DrvBuffer hBuffer, uint32_t size, Srio_SockAddrInfo* to);

Type 11:

Srio_sockSend_TYPE11  (Srio_SockHandle srioSock, Srio_DrvBuffer hBuffer, uint32_t size, Srio_SockAddrInfo* to);

Receive:

Srio_sockRecv         (Srio_SockHandle srioSock, Srio_DrvBuffer* hDrvBuffer,Srio_SockAddrInfo* from);

Example

Name
Description
Expected Results
Loopback DIO ISR Example Project

The example is a demonstration of the SRIO driver running the SRIO IP Block in loopback mode. The example showcases the use of SRIO DIO sockets using LSU interrupts to indicate the completion of packet transfer.

It is shown how multiple sockets with different Source IDs can post transactions and process the pending interrupt raised by SRIO device.

The application will run through a set of DIO tests. Upon successful completion the following string will be printed "DIO with Interrupts example completed successfully."

Multicore Loopback Example Project

The example is a demonstration of the SRIO driver while operating in a Multicore environment by running the SRIO IP Block in loopback mode. The test case here showcases the SRIO Driver API being multicore safe and using the SRIO IP peripheral to exchange messages between different cores running on the same device.

In this test case each core performs the role of a producer and consumer. The test starts with Core 1 sending data to Core 2. Core 2 receives and validates the data and sends another data message to Core3; which receives and validates the data and sends another different data message to Core 0. Core 0 then sends a message to Core 1 which is received and validated.

The application will run through a set of tests sending and receiving data between two cores over SRIO. Upon successful completion the following string will be printed "Multicore Test Passed" from each DSP core.

Loopback Test

Unit Test application to test all APIs

The application will run through a set of tests to verify all SRIO LLD APIS. Upon successful completion the following string will be printed "Unit Testing completed successfully." from each DSP core.

SRIO Benchmarking Test

The SRIO benchmarking example code is created to allow customers to run benchmarks on their own TI EVMs with code that utilizes the SRIO LLD APIs. The benchmarking example code allows the user to run core to core in loopback mode (internal or external) on a single EVM, or board to board using the external interface between two EVMs. This document’s purpose is to explain how measurements are obtained and how to configure the example code for different test scenarios. SRIO physical connectivity or external SRIO switch configuration is beyond the scope of this document.

Review the SRIO Benchmarking Example documentation located in PDK_INSTALL_DIR\packages\ti\drv\srio\test\tput_benchmarking\docs\SRIO_Benchmarking_Example_Code_Guide.doc for more information on the tests pass/fail criteria.


Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\srio\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\drv\srio\docs\ReleaseNotes_SRIODriver.pdf