Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK RTOS TF

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:



RTOS Software Developer Guide TF



Overview

User Interface

Application

Debug


Overview

In a multicore environment there would be data generated by a producer in one core and would need to be consumed by multiple consumers in other cores/same core. For example, a target log information to be consumed by ARM and CCS System Analyzer.

The trace framework (TF) provides a mechanism to send the information to multiple consumers for a given producer. In trace framework, Producer populates the associated Ring buffer. Consumers consume the ring buffer and send the data to external actual consumers (like System Analyzer in CCS). The hand shake between producers and consumers happen using shared memory area known as contract memory between producers and consumers.

It is upto the consumer application to either send the data to final consumers (using ethernet for System Analyzer) or local consuption for any OAM (Operations and maintenance) features on ARM.

Driver Configuration

Traceframework requires Producer, Consumer and Contract shared memory to be configured using tf_contractInit(), tf_contractCreate(), tf_prodCreate() and tf_consCreate() functions. For details about individual fields of this structure, see the Doxygen help by opening PDK_INSTALL_DIR\Traceframeworkckages\ti\drv\Traceframework\docs\doxygen\html\index.html.

APIs

API reference for application:

#include <ti/instrumentation/traceframework/traceframework.h>


Example

Name
Description
Expected Results
Traceframework_UnitTestApplication

Unit Test application to test all APIs

User observes the output printed over the CCS console

Application Integration Details

Sys BIOS DSP (C66) Use case

Reference library path to be included in application build environment:

 <ti/instrumentation/traceframework/lib/c66>
  

SysBIOS based application

Any RTSC application that needs to use trace framework library, should have a RTSC configuration file. Please refer to <ti/instrumentation/traceframework/test/TFUnitTest/<soc>/c66/bios/tfw_Uia_utest.cfg> sample RTSC cfg file for reference.


Additional References

Traceframework Library Summary
Component Type Library
Install Package PDK
Install Directory pdk_keystone_<version>\packages\ti\instrumentation\traceframework
Project Type Eclipse RTSC
Endian Support Little
Linker Path $(TI_PDK_INSTALL_DIR)\packages\ti\instrumentation\traceframework
Linker Sections .vecs , .switch, .args, .cio
Include Paths $(TI_PDK_INSTALL_DIR)\packages\ti\instrumentation\traceframework
Reference Guides $(TI_PDK_INSTALL_DIR)\packages\ti\instrumentation\traceframework\docs\doxygen\html\index.html
Release Notes $(TI_PDK_INSTALL_DIR)\packages\ti\instrumentation\traceframework\docs\ReleaseNotes_traceframework.pdf