Processor SDK RTOS VPS DRIVERS

From Texas Instruments Wiki
Jump to: navigation, search


RTOS Software Developer Guide VPS_DRIVERS



Overview

User Interface

Application

Debug


Introduction

VPS (Video Processing SubSystem) video Drivers allow users to make use of all video hardware features like 1080P capture, HDMI/LCD/SDTV display, deinterlacing, scaling. A user can use the drivers in many different ways like multi-channel capture, memory to memory processing, display and so on. This document has detailed API description that user's can use to make use of the VPS drivers.

VPS consists of following modules

  • Video Input Port (VIP) - for video capture functions for the device
  • Video Processing Engine (VPE)- for video operations such as color space convertion, deinterlacing, scaling and chroma upsampling features.
  • Display SubSystem (DSS) - for LCD outputs on three parallel interfaces (DPI1, DPI2, and DPI3) and HDMI

Driver Configuration

Board Specific Configuration

All board specific configurations eg:enabling clock and pin-mux for UART/display/vip pins are required before calling any driver APIs. The board specific configurations are implemented under <pdk>/ti/drv/vps/src/boards/src folder.

VPS Configuration Structure

For details about individual fields of VPS library structure, see the Doxygen help by opening PDK_INSTALL_DIR\packages\ti\drv\vps\docs\doxygen\html\index.html.

APIs

The VPS driver API can be broadly divided into the following categories

  • FVID2 API - API used to create, control and use the different VPS drivers
  • VPS (Video Processing Sub-system) API - API for all video drivers
  • VPS Control Driver API
  • VPS Capture API - API for video capture drivers
  • VPS VIP Capture API - API specific to VIP capture driver
  • VPS DSSWB Capture API - API specific to DSS WB capture driver
  • VPS Display API - API for video display drivers
  • VPS Display Controller API - API for controlling and configuring VENCs in the display subsystem
  • VPS Memory to Memory (M2M) API - API for memory to memory drivers
  • M2M VPE API - API specific to VPE M2M driver
  • External Device API - API for controlling external video devices like video decoders, video encoders, video filters, IO expanders, Ultra-sonic sensors
  • Platform Specific API - API for platform/board specific control, like setting pin muxes, clocks etc
  • Board Specific API - API for board specific features.

In addition to above drivers the VPS package also includes many sample examples which show how to use the drivers in different ways. Many of these sample examples use a common set of APIs which a user may find useful to refer to for use in their final application.

API reference for application:

#include <ti/drv/vps/include/vps_<func>.h>

Example

Name
Description
Expected Results
Display Dss application

Example demonstrating simple display yuyv or bgr frames to the LCD use case. Reference example for developers

Application prompts user to select the test case input in CCS console.

Display Dss application (Bare Metal)

Example demonstrating simple display yuyv or bgr frames to the LCD use case for bare metal use cases. Reference bare metal example for developers

Application prompts user to select the test case input in CCS console.

Display Dss WB application

Example demonstrating simple display Write Back (WB) yuyv or bgr frames to the LCD use case. Reference example for developers

Application prompts user to select the test case input in CCS console.

Loopback application (Capture and Display application)

Example demonstrating simple capture and display yuyv frames from camera to the LCD use case. Reference example for developers

Application prompts user to select the test case input in CCS console, please select ov2659 camera for idkAM57x and OV1063x for evmAM572x test cases.

Loopback application Bare metal(Capture and Display application)

Example demonstrating simple capture and display yuyv frames from camera to the LCD use case for bare metal. Bare Metal reference example for developers

Application prompts user to select the test case input in CCS console, please select ov2659 camera for idkAM57x and OV1063x for evmAM572x test cases.

NoteNote:

 * Starting from Processor SDK 4.2 release, idkAM574x support is added for VPS.
 * Starting from Processor SDK 4.2 release, oV1063x camera part support is added for AM572x - GP evm.
 * Starting from Processor SDK 3.2 release, osd101t2587 lcd panel is supported (new part) along with osd101t2045 lcd panel (old part) on idkAM572x 
   and idkAM571x boards for all display subsystem examples.
 * The bare metal examples are added starting from Processor SDK 4.0 release
 * Some of the clocks such as 32KHz Sync clock are directly tied to A15 core and need that core to be running. Hence while testing the code on other cores 
   such as DSP/IPU, please make sure to disconnect the ARM core after connecting the ARM core & running the GEL files to enable the other cores and before 
   loading the executable on that core.

Additional References

Document Location
API Reference Manual $(TI_PDK_INSTALL_DIR)\packages\ti\drv\vps\docs\doxygen\html\index.html

Building VPS examples

  • VPS examples and dependent libraries are built from the top level pdk makefile after the environment setup is done using the pdksetupenv.sh(bat) file.
  • cd <pdk>/packages
  • pdksetupenv.bat (sh)
  • make vps  : to build vps examples under <pdk>/ti/packages/binary folder
  • make vps_clean : to clean the vps and vps examples.

VPS examples

Display DSS Example

Description

The example exploits the DISPC (Display Controller) and LCD/HDMI outputs available in the SoC. When run, the test outputs multiple options to select between to demonstrate the various capacity of the display subsystem. There is also option to select "Auto Run", when selected runs all the tests in sequential manner. The example works on outputing a pre-loaded video frames of YUV422I and BGR888 formats to DP1, DP2 and DP3 parallel interfaces and also to HDMI output observed on TV set, from VID1, VID2, VID3 and GFX pipelines. The example also demonstrates displaying videos combined from GFX and other VID pipelines to DPI1 LCD output. The example is also enhanced to show the display controler scaling features. Test that exploits the scalar unit to show all possible allowed scaling. Maximum scaling ratio supported is the ratio of the dss functional clock / pixel clk. Please refer to section "11.2.4.10.4.2 DISPC Scaling limitations" of AM57x Technical Reference manual for minimum ratio allowed when using the scalar unit.


Running the Display DSS example

Configuring Display:

  • Make sure the LCD panel is connected to the base EVM before running the example binary.
  • Make sure the HDMI is connected to TV from the EVM for HDMI display options.

CCS connection:

  • Load the generated executable file in CCS
  • Run the application, Select any of the option and load the buffer as suggested.
  • Content will be displayed on the LCD panel or HDMI TV connected to EVM for test options

NoteNote:

  • Test Input files for Display Sample application will be in "<pdk>\drv\vps\docs\test_inputs\DisplayInput.rar"

The rar file can be unrar-ed to get the test files using utilities such as http://www.7-zip.org Please download the latest version of 7-zip from this website. The command to unrar is: 7z x {file_to_unrar}

When the test program expects the yuyv422 file, please load display_yuyv422_prog_packed_1920_1080.tigf file and when the test program expects the bgr888 file, please load display_gbr888_prog_packed_1920_1080.tigf file.

The test runs bunch of test cases as shown in the test example menu.

Warning : Due to A15 MMU protection, memory load while CPU is running is not possible. Hence below workaround needs to be done for loading the test files.

  1. Power up the board
  2. Connect to A15 Core
  3. Load both tigf files into memory
  4. Do a CPU reset on A15
  5. Load example code for core type
  6. Run example code

Display DSS WB example

Description

The WB pipeline allows the use of the hardware processing available inside the DISPC, such as color space conversion, rescaling, and compositing to perform memory-to-memory transfer with data processing or capturing a displayed frame.

Running Display DSS WB example

The test connection and procedure for this example is very much same as the running the Display DSS example. In this example, the display output that is sent to the output is captured and sent to the WriteBack pipeline.

Loopback (Capture and Display) example

Description

This is the capture and display example that demonstrates the VIP captures functions for the devices. VIP incorporates a multi-channel raw video parser, various video processing blocks, and a flexible Video Port Direct Memory Access (VPDMA)engine to store incoming video in various formats. This example demonstrates the video capture of 720P, YUY422 format from the camera sensor (OV2659 for idkAM57x and OV1063x for evmAM572x) to DPI1 LCD output.

Running Loopback example
  • Make sure OV sensor and LCD Panel is connected to to the board before running the binary.

CCS connection:

  1. Power up the board
  2. Connect to the Core
  3. Run the application, Select any of the option.
  4. Captured Content will be displayed on the LCD panel connected to EVM

NoteNote: The camera driver support is not added for evmAM572x boards (GP AM572x EVM) - and hence all the tests related to camera are skipped for evmAM572x board.