Please note as of Wednesday, August 15th, 2018 this wiki has been set to read only. If you are a TI Employee and require Edit ability please contact x0211426 from the company directory.

Processor SDK TIOVX

From Texas Instruments Wiki
Jump to: navigation, search

Starting in v4.3, Processor SDK documentation is no longer hosted on processors wiki.

Please bookmark the new links:


Ti stk 1c rev rgb png.png


OpenVX

OpenVX is an open, Khronos (https://www.khronos.org/openvx/) defined standard for cross platform acceleration of computer vision applications. OpenVX enables performance and power-optimized computer vision processing, with emphasis on embedded and real-time use cases:

  • advanced driver assistance systems (ADAS)
  • face, body and gesture tracking
  • smart video surveillance
  • object and scene reconstruction
  • augmented reality
  • visual inspection
  • robotics and more.

Though originally intended for vision only embedded applications, it may be extended in future to non-vision applications suitable for data flow representation.

TIOVX

TIOVX is TI's implementation of OpenVX Standard.

TIOVX allows users to create vision and compute applications using OpenVX API. These OpenVX applications can be executed on TI SoCs like AM57xx (including A15 and C66 cores), following OpenVX 1.1 standard. TIOVX also provides optimized OpenVX kernels for C66x DSP. An extension API allows users to integrate their own natively developed custom kernels and call them using OpenVX APIs.

Tiovx.PNG


TIOVX software

Module/Block Description
OpenVX API OpenVX API as defined by Khronos
TIOVX API TI extensions and additional APIs in order to efficiently use OpenVX on TI platforms
TIOVX Framework TI's implementation of OpenVX spec. This layer is agnostic of underlying SoC, OS platform
TIOVX Platform This layer binds TIOVX framework to a specific platform. Ex, Processor Linux SDK for AM57xx SOCs. This layer also binds TIOVX framework to a specific OS like Linux or TI-RTOS
TIOVX Kernel Wrapper

Kernel wrappers allow TI and customers to integrate a natively implemented kernel into the TIOVX framework.

TIOVX Conformance tests

OpenVX conformance test from Khronos to make sure an implementation implements OpenVX according to specification.

There are two versions of VXLIB kernels: without BAM framework, and with BAM framework. BAM is a low level framework representing directed acyclic graph, where EDMA transfers are heavily utilized to bring 2D memory objects to higher speed L2 memory, thus improving performance almost twofold.
Current release has kernels with BAM framework. This framework achieves higher performance via heavy use of EDMA, which brings blocks of data from remote DDR memory to local L2, while DSP does the processing. List of these kernels can be checked in https://git.ti.com/processor-sdk/tiovx/trees/master/kernels/openvx-core/c66x/bam.

TIOVX DSP Kernels (in VXLIB)

There are 44 kernels in current release of VXLIB (typically there are multiple implementations for different data types).
Here is complete list of DSP kernel wrappers (wrappers are part of TIOVX):

  • AbsDiff
  • AccumulateSquare
  • Accumulate
  • AccumulateWeighted
  • Add
  • BitwiseAnd
  • BitwiseNot
  • BitwiseOr
  • BitwiseXor
  • Box3x3
  • CannyEd
  • ChannelCombine
  • ChannelExtract
  • ColorConvert
  • ConvertDepth
  • Convolve
  • Dilate3x3
  • EqHist
  • Erode3x3
  • Gaussian3x3
  • HalfscaleGaussian
  • HarrisCorners
  • Histogram
  • IntegralImage
  • Lut
  • Magnitude
  • MeanStdDev
  • Median3x3
  • MinMaxLoc
  • Multiply
  • NonLinearFilter
  • Phase
  • Sobel3x3
  • Subtract
  • Threshold


TIOVX in Processor Linux SDK on AM57xx EVM

Following TIOVX components are present in EVM filesystem:

Type
File path
Description
application
/usr/bin/tiovx-app_host
Statically linked Linux application running several thousands test cases, with all available kernels and using different test vectors
DSP firmware

/lib/firmware/dra7-dsp1-fw.xe66.openvx,

/lib/firmware/dra7-dsp2-fw.xe66.openvx

DSP firmware including DSP side of TIOVX framwork implementation, IPC implementation, DSP kernels (part of VXLIB DSP library) - for DSP1. This firmware is loaded at boot time, or using procedure mentioned below (to switch from OCL firmware to TIOVX firmware)

TIOVX release 1.0.0.0 runs exclusively wrt OpenCL, as both firmwares use common resources DSP cores and CMEM memory. That is: application can be either TIOVX-based, or OpenCL -based. Future releases may remove this limitation and use static split in resources (between OpenCL and OpenVX). TIOVX needs CMEM memory with two blocks: block 0 is big DDR block for exchange of big buffers (>100MB) and block 1 (~1MB) which is used as shared memory visible from all cores to exchange shared data objects (typically in OCMC)

Switch from OpenCL to OpenVX firmware:

pkill ti-mctd                            # Kill CMEM multi-process daemon. This releases all CMEM memory used by OpenCL memory allocation
cd /sys/bus/platform/drivers/omap-rproc/ # Prepare to send commands for remoteproc
echo 40800000.dsp > unbind               # Release DSP1
echo 41000000.dsp > unbind               # Release DSP2
rm /lib/firmware/dra7-dsp1-fw.xe66       # 
ln -s /lib/firmware/dra7-dsp1-fw.xe66.openvx /lib/firmware/dra7-dsp1-fw.xe66 # Link TIOVX firmware for DSP1
rm /lib/firmware/dra7-dsp2-fw.xe66       # 
ln -s /lib/firmware/dra7-dsp2-fw.xe66.openvx /lib/firmware/dra7-dsp2-fw.xe66  # Link TIOVX firmware for DSP2
echo 40800000.dsp > bind                 # Load new DSP1 firmware (now, for OpenVX, as set in previous steps)
echo 41000000.dsp > bind                 # Load new DSP2 firmware (now, for OpenVX, as set in previous steps)
cd -                                     # Return to original folder


Switch from OpenVX, back to OpenCL firmware:

ti-mctd                               # Start OpenCL CMEM memory allocation daemon
cd /sys/bus/platform/drivers/omap-rproc/   # Prepare for remoteproc operations
echo 40800000.dsp > unbind            # Release DSP1
echo 41000000.dsp > unbind            # Release DSP2
rm /lib/firmware/dra7-dsp1-fw.xe66    #
ln -s /lib/firmware/dra7-dsp1-fw.xe66.opencl-monitor  /lib/firmware/dra7-dsp1-fw.xe66  # Set new DSP1 firmware (OpenCL DSP firmware)
rm /lib/firmware/dra7-dsp2-fw.xe66    #
ln -s /lib/firmware/dra7-dsp2-fw.xe66.opencl-monitor  /lib/firmware/dra7-dsp2-fw.xe66  # Set new DSP2 firmware (OpenCL DSP firmware)
echo 40800000.dsp > bind              # Load new DSP1 firmware
echo 41000000.dsp > bind              # Load new DSP2 firmware
cd -                                  # Return to original folder

Run TIOVX test application

First, it is necessary to copy test vectors from https://git.ti.com/processor-sdk/tiovx/trees/master/conformance_tests/test_data to EVM filesystem (e.g. ~/tiovx/test_data).Then run following commands:

export VX_TEST_DATA_PATH=/home/root/tiovx/test_data  # Set environment variable to point to location of test vectors on EVM
tiovx-app_host 2>&1 | tee log.txt                    # Run test application, and log output to log.txt

At the end of test (taking roughly 24mins) you can expect report like this:

...
[ N7 ] Execution time for    307200 pixels (avg =    3.584000 ms, min =    3.584000 ms, max =    3.584000 ms)
[ N8 ] Execution time for    307200 pixels (avg =  171.797000 ms, min =  171.797000 ms, max =  171.797000 ms)
[ N9 ] Execution time for    307200 pixels (avg =  366.952000 ms, min =  366.952000 ms, max =  366.952000 ms)
[ G4 ] Execution time for    307200 pixels (avg =  500.146000 ms, min =  500.146000 ms, max =  500.146000 ms)
[ N1 ] Execution time for       256 pixels (avg =    0.278000 ms, min =    0.278000 ms, max =    0.278000 ms)
[ N2 ] Execution time for       256 pixels (avg =    0.230000 ms, min =    0.230000 ms, max =    0.230000 ms)
[ N3 ] Execution time for       256 pixels (avg =    0.281000 ms, min =    0.281000 ms, max =    0.281000 ms)
[ N4 ] Execution time for       256 pixels (avg =    0.303000 ms, min =    0.303000 ms, max =    0.303000 ms)
[ N5 ] Execution time for       256 pixels (avg =    0.285000 ms, min =    0.285000 ms, max =    0.285000 ms)
[ G5 ] Execution time for       256 pixels (avg =    2.169000 ms, min =    2.169000 ms, max =    2.169000 ms)
[ N1 ] Execution time for       256 pixels (avg =    0.243000 ms, min =    0.243000 ms, max =    0.243000 ms)
[ N2 ] Execution time for       256 pixels (avg =    0.301000 ms, min =    0.301000 ms, max =    0.301000 ms)
[ G6 ] Execution time for       256 pixels (avg =    0.871000 ms, min =    0.871000 ms, max =    0.871000 ms)
[ N1 ] Execution time for       256 pixels (avg =    0.352000 ms, min =    0.352000 ms, max =    0.352000 ms)
[ N2 ] Execution time for       256 pixels (avg =    0.246000 ms, min =    0.246000 ms, max =    0.246000 ms)
[ N2 ] Execution time for       256 pixels (avg =    0.324000 ms, min =    0.324000 ms, max =    0.324000 ms)
[ G7 ] Execution time for       256 pixels (avg =    1.502000 ms, min =    1.502000 ms, max =    1.502000 ms)
[ N1 ] Execution time for       256 pixels (avg =   75.37000  ms, min =   75.37000  ms, max =   75.37000  ms)
[ G8 ] Execution time for       256 pixels (avg =   60.474000 ms, min =   60.474000 ms, max =   60.474000 ms)
[     DONE ] tivxMaxNodes.MaxNodes/0/few_strong_corners/MIN_DISTANCE=3.0/SENSITIVITY=0.10/GRADIENT_SIZE=3/BLOCK_SIZE=5/k=3/VX_INTERPOLATION_NEAREST_NEIGHBOR
[ -------- ] 1 tests from test case tivxMaxNodes

[ ======== ]
[ ALL DONE ] 6217 test(s) from 110 test case(s) ran
[ PASSED   ] 6217 test(s)
[ FAILED   ] 0 test(s)
[ DISABLED ] 7397 test(s)

To be conformant 6217 required test(s) must pass. Disabled 7397 test(s) are optional.

#REPORT: 20170927134830 ALL 13614 7397 6217 6217 6217 0 (version 1.1-20170301)
<-- main:

Please note that last ~3000 lines of test log include performance data (execution time and number of pixels processed) useful for further evaluation.


Recompile TIOVX (using Yocto build)

TIOVX framework implementation is available at https://git.ti.com/processor-sdk/tiovx/trees/master
TIOVX sample application including IPC implementation based on standard MessageQ, as well as application running conformance tests, can be found at https://git.ti.com/processor-sdk/tiovx-app/trees/master
Additional documentation can be found at https://git.ti.com/processor-sdk/tiovx/trees/master/docs

TIOVX framework and TIOVX-APP can be recompiled like any other component, as described in http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK. Optionally you can do full rebuild with:

MACHINE=am57xx-evm bitbake arago-core-tisdk-image

For modifying individual components in PLSDK, please refer to: to http://processors.wiki.ti.com/index.php/Processor_SDK_Building_The_SDK#Recipes
If there is a need to modify source code of TIOVX host library (framework) files (A15 side), please do that in: tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/tiovx-lib-host/01.00.00.00-r1/git/ folder.
For example, to modify list of tests executed: update file ./tiovx/conformance_tests/test_tiovx/test_main.h, or ./tiovx/conformance_tests/test_conformance/test_main.h
After the source modification, force compile the Library (Linux host side), and rebuild the package using:

MACHINE=am57xx-evm bitbake tiovx-lib-host  -f -c compile
MACHINE=am57xx-evm bitbake tiovx-lib-host

Similarly application code can be modified in: ./tisdk/build/arago-tmp-external-linaro-toolchain/work/am57xx_evm-linux-gnueabi/tiovx-app-host/01.00.00.00-r1/git, and then force-recompiled and rebuilt using:

MACHINE=am57xx-evm bitbake tiovx-app-host -f -c compile
MACHINE=am57xx-evm bitbake tiovx-app-host