Put CRAMFS Image to Flash
From Texas Instruments Embedded Processors Wiki
Contents |
Prerequisites
- A CRAMFS file system image.
- For information on creating a CRAMFS file system image see the Create a CRAMFS Target Image page
- A terminal application for communicating with the DVEVM. i.e. minicom or hyperterminal
- A copy of the U-Boot bootloader running on the target
- If you do not have U-Boot running on the target please see the RBL, UBL and host program article for how to get the U-Boot bootloader installed on your board first
- A kernel with CRAMFS support enabled
- For details on how to enable CRAMFS support in the TI kernel see the CRAMFS kernel configuration page
- A tftp server for loading the kernel image used in this example.
- NOTE: You can also write the kernel image to Flash rather than using tftp boot but this is outside the scope of this document.
Writing the CRAMFS Image to Flash
This section details how to write the CRAMFS image to NOR and NAND Flash. For both types of flash you should follow the steps in the common section and then proceed to the section for your Flash device.
Common
These steps are common to both NOR and NAND flash and should be done before proceeding to the individual Flash sections.
The following steps are performed on the host Linux workstation.
- Copy the kernel image with CRAMFS support to the tftp root directory
These steps assume that the kernel compiled with CRAMFS support is located at /home/user/workdir/ti-davinci and that the tftp root is /tftpboot
host$ cp /home/user/workdir/ti-davinci/arch/arm/boot/uImage /tftpboot
- Copy the CRAMFS file system image to the tftp root directory
host$ cp <path to cramfs image>/cramfs.image /tftpboot
The following steps are performed at the u-boot prompt on the target board
- Download the CRAMFS file system image via TFTP
DVEVM# setenv serverip <tftp server ip> DVEVM# setenv bootfile cramfs.image DVEVM# dhcp
The dhcp command will cause the file specified by "bootfile" to be downloaded to address 0x80700000 from the tftp server specified by the "serverip" variable. You should see output similar to:
DVEVM # dhcp
BOOTP broadcast 1
DHCP client bound to address <board ip>
TFTP from server <server ip>; our IP address is <board ip>
Filename 'cramfs.image'.
Load address: 0x80700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#####
done
Bytes transferred = 2686976 (290000 hex)
Take note of the Load address (0x80700000) and the Bytes transferred (0x290000) as these are needed in the following steps.
You may now proceed to the appropriate section for your Flash device depending on if you are using NOR Flash or NAND Flash
NOR Flash
This section will detail how to write the CRAMFS image to NOR Flash
- Determine the location in Flash to store the CRAMFS image
DVEVM# flinfo
Bank # 1: INTEL 28F128P30T
Size: 16 MB in 131 Sectors
Sector Start Addresses:
02000000 02020000 02040000 E 02060000 (RO) 02080000
....
NOTE: U-Boot resides in the first 5 sectors of flash so do not write the image in that location. Likewise be sure that if you are writting your kernel in flash you leave enough room between the end of U-Boot and the begining of the CRAMFS image for the kernel. For this example we will use address 0x2140000
- Erase the NOR Flash
DVEVM# protect off 0x2140000 +0x290000
Un-Protected 21 sectors
DVEVM# erase 0x2140000 +0x290000
Erasing sector 10 ... done.
Erasing sector 11 ... done.
Erasing sector 12 ... done.
.
.
Erase Operation Completed.
Erased 21 sectors
- Copy the CRAMFS image from RAM into Flash
DVEVM# cp.b 0x80700000 0x2140000 0x290000 Copy to Flash...\done
- Protect the CRAMFS image in NOR (optional)
DVEVM# protect on 0x2140000 +0x290000
NAND Flash
This section will detail how to write the CRAMFS image to NAND Flash
- Determine the sectore size of your NAND Flash and round the CRAMFS image size up to a multiple of sectore size
DVEVM# nand info Device 0: NAND 64MiB 1,8V 8-bit, sector size 16 KiB
Note the sector size listed at the end of the output from the nand info command. Since the NAND flash requires that I/O operations be done in increments of sector size you must round up the size of your CRAMFS image to the next full sector in order for the erase and write commands to work.
In this example the sector size is 16KB which is 0x4000 so the following calculation can be done
CRAMFS image size = 0x290000 Num sectors = 0x290000 / 0x4000 = A4 which does not need rounding Rounded size = Num sectors * 0x4000 = A4 * 0x4000 = 0x290000
- Erase the NAND Flash
NOTE: U-Boot resides in the first 5 sectors of flash so do not write the image in that location. Likewise be sure that if you are writting your kernel in flash you leave enough room between the end of U-Boot and the begining of the CRAMFS image for the kernel. For this example we will use offset 0x130000.
DVEVM# nand erase 0x130000 0x290000 NAND erase: device 0 offset 0x130000, size 0x290000 Erasing at 0x3bc000 -- 100% complete. OK
- Copy the CRAMFS image from RAM to NAND
DVEVM# nand write 0x80700000 0x130000 0x290000
NAND write: device 0 offset 0x130000, size 0x290000
2686976 bytes written: OK
Boot CRAMFS Image
This section covers the bootargs that need to be set to boot the Linux kernel using a CRAMFS file system. In this example the kernel is loaded via tftp and the CRAMFS file system is stored in Flash. You will need to replace the offsets and sizes used here with the ones for your file system.
- Set the bootargs to use CRAMFS
DVEVM# setenv bootargs 'console=ttyS0,115200n8 ip=dhcp root=/dev/ram0 rw initrd=0x85000000,6M mem=120M'
Here we are using the CRAMFS image that was placed in memory at address 0x85000000 by the bootcmd.
- Set the bootcmd to copy the CRAMFS image to DDR and boot the kernel (if using tftp be sure to reset the bootfile variable to the kernel image)
- For NAND Flash use:
DVEVM# setenv bootcmd 'nand read 85000000 130000 290000; dhcp; bootm'
- For NOR Flash use:
DVEVM# setenv bootcmd 'cp.b 0x2140000 0x85000000 0x290000; dhcp; bootm'
- Boot the board.
DVEVM# saveenv DVEVM# boot
You should see output similar to:
DVEVM # boot
NAND read: device 0 offset 0x130000, size 0x290000
2686976 bytes read: OK
BOOTP broadcast 1
DHCP client bound to address <board ip>
TFTP from server <server ip>; our IP address is <board ip>
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#########################################
done
Bytes transferred = 1538588 (177a1c hex)
## Booting image at 80700000 ...
Image Name: Linux-2.6.10_mvl401
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1538524 Bytes = 1.5 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
OK
Starting kernel ...
<kernel output removed here>
RAMDISK: cramfs filesystem found at block 0
RAMDISK: Loading 2624KiB [1 disk] into ram disk... done.
VFS: Mounted root (cramfs filesystem) readonly.
<kernel output removed here>
Hello World!!!
INIT: Entering runlevel: 3
Starting internet superserver: inetd.
MontaVista(R) Linux(R) Professional Edition 4.0.1 (0502020)
login:
Leave a Comment