RN 3 01 00 06

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Release Notes for release 3.01.00.06

Introduction

This release includes the Linux graphics drivers for the OMAP35x/AM35x/37xx family of chipsets. The Graphics SDK contains documentation, demo programs and tools.


Important Note:

AM/DM37x support is included for internal development only.


Requirements, Pre-requisites and demo instructions

For software setup and pre-requisites and other instructions, refer to the main pages at,

OMAP35x_Graphics_SDK_Getting_Started_Guide


Features in this release


Kernel, Toolchain used for validation

The kernel was taken from the below tree (Feb/Mar 2010),

http://arago-project.org/git/projects/?p=linux-omap3.git;a=summary

The release has also been tested with PSP release PSP-SDK-03.00.00.04 version.


What is supported

Khronos API support

Window Systems

The following Window Systems are supported, on Linux:

Buffer Swap modes

The following modes of buffer swapping are supported,

Selection of these modes is done via entries in /etc/init.d/powervr.ini. Please refer to Online GSG (Main page).

Extensions



What is not supported


Additional Packages

Demonstration packages for Texture streaming extension are available at the below link,

Benchmarking packages for SGX functionalities and APIs are available at,


Fixed in this Release


Limitations/ Known Issues


Installation and Usage

Please look for detailed installation and usage instructions in the Getting Started Guide (Main page).


Contents

The folders in the installed package contain binaries for several family of devices containing the SGX530 core. Brief description of these folders is below.


Graphics SDK folder contents
Folder Name Description Used by
1 gfx_dbg_es2.x / gfx_rel_es2.x Debug/Release binaries for platforms having SGX core revision 1.0.3 (OMAP35x ES version 2.0) How to check?
2 gfx_dbg_es3.x / gfx_rel_es3.x Debug/Release binaries for platforms having SGX core revision 1.2.1 (OMAP35x ES version 3.1) How to check?
3 gfx_dbg_es5.x / gfx_rel_es5.x Debug/Release binaries for platforms having SGX core revision 1.2.5 (AM37xx/DM37xx) How to check?
4 GFX_Linux_KM Source for Graphics Kernel Modules Contains kernel dependent code, changes depending on Linux kernel used
5 GFX_Linux_SDK Demos, Training courses, PVR Tools,classes and header files Used for building new applications (Available only in the SDK package, not in the BIN package)
6 include Contains updated header file for GL extensions, specifically the buffer class streaming extension Useful for video texturing applications involving bufferclass driver
7 tools Contains devmem2, and other packages Useful for running/debugging/benchmarking of Graphics SDK
Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox