RTSC Codec And Server Package Wizards

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents

Introduction

The RTSC Codec Package Wizard and RTSC Server Package Wizard are utilities designed to rapidly create XDC Codec Packages and Codec Engine compatible test servers (containing a single codec).

Both utilities run on Windows and Linux with both GUI and command line options. They are provided with the ceutils (see below)

Note that as of Codec Engine 2.20 the GenServer Wizard is now available. It is provided with the Codec Engine and NOT part of ceutils. Customers should migrate to GenServer. For consistency/migration many of the same options were preserved. This server wizard is now deprecated, however because GenServer requires >= CE 2.20, this server wizard will still be necessary for customers using e.g. >= CE 1.20.02.

Note that the same applies to the codec package wizard in ceutils - it is now deprecated as the GenCodecPkg Wizard is now provided and supported as part of Codec Engine.

Download

Prerequisites

The RTSC Package Wizards recommend the following components be installed:

Without Codec Engine and either Codec Engine's CE Tools or xDAIS, the RTSC Codec Package Wizard and RTSC Server Package Wizard will not run at all. Without CG_XML and Code Gen Tools, the RTSC Codec Package Wizard will not be able to determine stack size, section information, or the names of xDAIS functions. Without DSP/BIOS, the server that results from building the output of the RTSC Server Package Wizard cannot be created.

Wizard Instructions

Other Wizard Documents

XDAIS for Codecs

The new QualiTI XDAIS compliance tool is now available in XDAIS 6.10.

References

E2e.jpg For technical support please post your questions at http://e2e.ti.com. Please post only comments about the article RTSC Codec And Server Package Wizards here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox