SCI-TPA2038-MVK MAVRK Module

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

MAVRK Banner.png

MAVRK is no longer an active TI evaluation platform. Please contact TI application support if you need further information on TI products or support.


Construction Icon small.png This page is currently under construction. The content of this page is due to change quite frequently and thus the quality and accuracy are not guaranteed until this message has been removed. Please feel free to contribute to this page while construction is in progress.



Coming Soon.png

Board Status: Level Test

Contents

Purpose of this Wiki Page

This page explains the Signal Conditioning Interface (SCI) TPA2038 Modular and Versatile Reference Kit (MAVRK) module in detail. For more information on the MAVRK system, referring to the MAVRK Introduction page is good start. After reading this guide, a developer should understand the features of the SCI-TPA2038-MVK MAVRK module.

EVM Overview

The SCI-TPA2038-MVK module highlights a pair of TPA2038D1 3.2W Mono Channel Class D amplifier, a device which is commonly used in battery or low power audio applications. The SCI-TPA2038-MVK can be used with the MAVRK Pro Motherboard if coupled with the AFE-BREAKOUT-MVK MAVRK module.


EVM Description

SCI-TPA2038-MVK MAVRK Module

The SCI-TPA2038-MVK is a dual 3.4W Class D Audio system that can can typically drive 1.4W in 8Ohm and 2.5W in 4Ohm speakers with a 1% Total Harmonic Distortion (THD) utilizing a 5V power rail.

This EVM utilizes the four SCI GPIOs to control Gain and Shutdown functions of both amplifiers.

Included with the SCI-TPA2038-MVK is a pair of breakout boards that allow either filtering or pass through of the amplifier output. The spec of this breakout card also allows active filters to be designed for this board as well.



Figure 1: SCI-DRV8814-MVK Dual Motor Control System

Features

TPA2038D1 Features

SCI-TPA2038-MVK Features

Highlighted Products

The SCI-TPA2038_MVK MAVRK Module features the following devices:

Feature Applications

The SCI-TPA2038-MVK MAVRK module can be used to demonstrate the following applications:

Block Diagram

SCI-TPA2038 Block Diagram.png


Figure 2. SCI-TPA2038-MVK Block Diagram

EVM Wiki

The most up-to-date information on this module can be found at the SCI-TPA2038-MVK MAVRK module wiki page.

EVM Landing Page

Ordering information and availability of this module can be found at the SCI-TPA2038-MVK MAVRK module tool folder.

Hardware Description

Power Requirements

The SCI-TPA2038-MVK utilizes either the 5.5VDC from the Pro Motherboard or an external 2.5 to 5.5V DC power source.

If the Pro Motherboard power rail is utilized by itself, the maximum current draw from the 5.5V rail is limited to 200ma.

If an external source is utilized, a 5.5V, 2A DC power supply is recommended. The maximum short circuit current for each TPA2038D1 is 2Amps @ 3.6 Volts.

The SCI-TPA2038-MVK module is supported by the MAVRK AppMonitor and AppSelect tools. For more information on these tools and how to install them, refer to the How to get the MAVRK Software link below.

The preferred method for working with this EVM is through the use of the MAVRK Pro Motherboard.

SCI-TPA2038-MVK Safe Module.png

The motherboard will provide the digital control for this EVM. Power can be supplied by the Pro Motherboard or an external 5V, 2A DC supply. The software demo uses MAVRK_SCI4 as the image in Figure 4 shows, however (with a small change in software) it is also possible to insert the SCI-TPA2038-MVK into any of the other 3 SCI slots are retain full functionally. Also in the picture is the AFE-BREAKOUT-MVK in MAVRK_AFE4 which provides pass through of the digital signals to the SCI-TPA2038-MVK.

The power source for the Pro Motherboard in this demo shown in Figure 4 is the USB cable. It should be noted that when any board on the MAVRK board is installed or removed, all power sources should be moved first by pressing the Standby button and the SCI-DRV8814-MVK power source MUST be off as well to prevent possible damage to the boards.

Typical installation of the module is as follows:

   1. Plug in the USB.  
     a.  The Standby button should be blue, which effectively removes all power from the modules on the mother board. 
   2. Run the MAVRK AppSelect tool 
   3. Install all modules required for the demo
     a. An MCU module to initialize the motherboard and to communicate to the SCI-DRV8814-MVK.
     b. At least one AFE-BREAKOUT-MVK module.  It should be noted multiple AFE's can be installed.
     c. At least one SCI-TPA2038-MVK module in the slot below the AFE Breakout module. 
   3. Install one of the Filter or Passthrough modules in the output filter stage of the TPA2038. 
   4. Install the JTAG debugger if a C Compiler is used to download code into the MCU.  Otherwise the QT tool will use the USB connection to download the code.
   5. Press the Standby button to provide power to the motherboard modules.
   6. Activate power source to the SCI-DRV8814-MVK.


Figure 4: SCI-TPA2038-MVK Demo Setup in Standby Mode

EVM Connectors, Fuses, and Switches

The SCI-TPA2038-MVK has two common modes for operation, a stand-alone mode, where one of the analog input jacks is tied to the input of the TPA2038 and a second mode where an Audio Codec is used in the AFE slot to route audio to the TPA2038.

Stand Alone Mode

Figure 5 shows the Stand Alone mode. Left and Right analog speakers are connected in the P1 SPKR_OUT screw terminal.

Jumper JP03 IN SEL will need to be removed to re-route the audio from IN1 Audio Jack J1.


SCI-TPA2038-MVK in Standalone mode.png


Figure 5. Standalone Mode for the SCI-TPA2038-MVK

Audio Codec Mode

Figure 6 shows the installation of JP03 IN SEL to disable the routing of the Audio from J1 IN1 to the TPA2038.

In this mode, J1 IN1 and J2 IN2, shown in Figure 6, and J3 HPOUT shown in Figure 7 are routed to the AFE Slot above the SCI-TPA2038-MVK.

The input of the TPA2038 Amplifiers are also tied to the AFE Slot above the SCI--TPA2038-MVK.

SCI-TPA2038-MVK in Audio Codec mode - Front.png


Figure 6. Audio Codec Mode for the SCI-TPA2038-MVK Top View

SCI-TPA2038-MVK in Audio Codec mode - Back.png


Figure 7. Audio Codec Mode for the SCI-TPA2038-MVK Bottom View

MIC1 and MIC2, when jumpered, routes the MIC Bias channels into the AFE Slot above the SCI-TPA2038-MVK.

SCI-TPA2038-MVK in Audio Codec mode - MIC BIAS.png


Figure 8. MIC Bias Enable for the SCI-TPA2038-MVK Top View

I2C Signal Access

The figure below shows the location of the I2C signals from the MAVRK Pro Motherboard.

These through holes can be used to connect I2C peripherals (volume control for example) to the SCI-TPA2038-MVK.

SCI-TPA2038-MVK I2C Connection.png


Figure 9. I2C Connections for the SCI-TPA2038-MVK

Audio Filter Board

At the output stage of the TPA2038 is a output filter module incorporating a pair of 6 pin single row headers as shown in the figure below.

This filter is keyed to prevent the board to be plugged incorrectly.

SCI-TPA2038-MVK Filter Board.png


Figure 10. Filter Board on the SCI-TPA2038-MVK


Audio Filter Pinout
Pin #
P3
P4
Pin 1 OUTL+ SPKL+
Pin 2 OUTL+ SPKL-
Pin 3 ANLG_VDD_5.5V KEY
Pin 4 OUTR+ SPKR+
Pin 5 OUTR+ SPKR-
Pin 5 Ground Ground


Figure 11 shows the Passthrough board Installed on the SCI-TPA2038-MVK

SCI-TPA2038-MVK Filter Board Installed.png


Figure 11. Filter Board Installed on the SCI-TPA2038-MVK

EVM Test Points

SCI TPA2038 MAVRK Ground Test Points.png

Several test points exist on the SCI-TPA2038-MVK.

The figure below shows two ground test points. These test points can be used to ground scope or volt meter probes.

The AVDD_5.5V test point can be used to monitor the supply into the SCI-TPA2038-MVK.

There are also two test points for the Left and Right channel. These test points can be used to view the signals going into the TPA2038's.


Figure 11. Ground Test Points for the SCI-TPA2038-MVK

EVM LEDs

MAVRK SCI TPA2038 LEDs.png

The figure below shows the only LED on the TPA2038. This LED, signalling an over current condition, is red and during normal operation is not lit (off). If the Over Current LED is lit, the 200ma barrier has been reached on the Pro Motherboard's supply voltage of 5.5V. If this LED remains lit, the best solution is to drop the gain of the TPA2038 or power the SCI-TPA2038-MVK with an external 5V DC power supply.


Figure 12. Fault LEDs on the SCI-DRV8814-MVK

Software Installation

MAVRK Software Minimum Requirements

How to get the MAVRK Software

This module is supported with the MAVRK AppSelect tool and the MAVRK AppMonitor tool

To download and install the MAVRK AppSelect and AppMonitor tools, refer to the Software Installation Guide.

Where do I find the MAVRK Qt Demo Application?

An application to visual packet information from the embedded system can be found in the mavrk_qt_tool software repository under the Released Version - QT Demo Application directory. Please see Software Installation Guide for instructions on cloning the QT Tool project.

If you desire to create your own Qt demonstration, please reference the following resources:

Where do I find the Demo and Test Code?

MAVRK TPA2038 Demo Application?

Demonstrating the TPA2038 MAVRK Module

Board Files

Download a PDF of the bill of materials.

SCI-TPA2038-MVK Bill of Materials

SCI-TPA2038-MVK BOM.png

Layout (PDF)

Download a PDF of additional board layers.

SCI-TPA2038-MVK Board Top Silkscreen

6542606 SCI-TPA2038-MVK WIKI A.png

Schematics (PDF)

Download a PDF of all schematics.

SCI-TPA2038-MVK Schematics

SCI-TPA2038-MVK Schematic.png

Fabrication Drawings (PDF)

Download a PDF of the fabrication drawing.

SCI-TPA2038-MVK Fabrication Drawing

SCI-DRV8814-MVK Fab Drawing.png

Gerber Files

Download a ZIP of the Gerber files.

SCI-TPA2038-MVK Gerber Files

6542606 SCI-TPA2038-MVK A1 GERBER.png

Cadence Schematic and Board Files

Download a ZIP of the Cadence schematic and board files.

SCI-TPA2038-MVK Cadence Schematic and Board Files

6542606 SCI-TPA2038-MVK A1 Cadence.png

MAVRK Links

I want more info on MAVRK

Visit the MAVRK wiki pages to get comprehensive information on MAVRK.

I have MAVRK Questions

Post your questions on the MAVRK Forum and get an answer from the MAVRK team.

(Recommended):


I want more Technical Info on MAVRK Hardware

Read through some of the hardware wiki pages below.


I want more Technical Info on MAVRK Software

Read through some of the software wiki pages below.


I want to get a MAVRK board

You can order a MAVRK Starter kit from the MAVRK Starter Kit tool folder page. To order other modules, search for them by name on TI's Web site to find their tool folder pages.

Important Notices

(NOTE: EDIT THIS SECTION AFTER THE BOARD MEETS FCC/IECS COMPLIANCE. FIX THE FCC AND ICES PDF LINKS AND CHANGE {{MAVRK Imporatant Notices}} to {{MAVRK Important Notices Complies FCC}}. Please hide this paragraph with < nowiki ></ nowiki > tags when you produce a guide from this template.)

ESD Precautions

The following guidelines should be followed in order to avoid ESD damage to the board components:

Certifications

(Insert links to the PDFs of the FCC and ICES standard reports above the other certifications. The will look like the first two links below.)

FCC standard EMC test report for the <Insert Module Name> aboard the MAVRK Pro Motherboard

ICES standard EMC test report for the <Insert Module Name> aboard the MAVRK Pro Motherboard

Eco-Info & Lead-Free Home

RoHS Compliant Solutions

Statement on Registration, Evaluation, Authorization of Chemicals (REACh)

Evaluation Board/Kit/Module (EVM) Additional Terms

Texas Instruments (TI) provides the enclosed Evaluation Board/Kit/Module (EVM) under the following conditions:

The user assumes all responsibility and liability for proper and safe handling of the goods. Further, the user indemnifies TI from all claims arising from the handling or use of the goods.

Should this evaluation board/kit not meet the specifications indicated in the User’s Guide, the board/ kit may be returned within 30 days from the date of delivery for a full refund. THE FOREGOING LIMITED WARRANTY IS THE EXCLUSIVE WARRANTY MADE BY SELLER TO BUYER AND IS IN LIEU OF ALL OTHER WARRANTIES, EXPRESSED, IMPLIED, OR STATUTORY, INCLUDING ANY WARRANTY OF MERCHANTABILITY OR FITNESS FOR ANY PARTICULAR PURPOSE. EXCEPT TO THE EXTENT OF THE INDEMNITY SET FORTH ABOVE, NEITHER PARTY SHALL BE LIABLE TO THE OTHER FOR ANY INDIRECT, SPECIAL, INCIDENTAL, OR CONSEQUENTIAL DAMAGES.

Please read the User's Guide and, specifically, the Warnings and Restrictions notice in the User's Guide prior to handling the product. This notice contains important safety information about temperatures and voltages. For additional information on TI's environmental and/or safety programs, please visit www.ti.com/esh or contact TI.

No license is granted under any patent right or other intellectual property right of TI covering or relating to any machine, process, or combination in which such TI products or services might be or are used. TI currently deals with a variety of customers for products, and therefore our arrangement with the user is not exclusive. TI assumes no liability for applications assistance, customer product design, software performance, or infringement of patents or services described herein.

Regulatory Compliance Information

As noted in the EVM User’s Guide and/or EVM itself, this EVM and/or accompanying hardware may or may not be subject to the Federal Communications Commission (FCC) and Industry Canada (IC) rules.

For EVMs not subject to the above rules, this evaluation board/kit/module is intended for use for ENGINEERING DEVELOPMENT, DEMONSTRATION OR EVALUATION PURPOSES ONLY and is not considered by TI to be a finished end product fit for general consumer use. It generates, uses, and can radiate radio frequency energy and has not been tested for compliance with the limits of computing devices pursuant to part 15 of FCC or ICES-003 rules, which are designed to provide reasonable protection against radio frequency interference. Operation of the equipment may cause interference with radio communications, in which case the user at his own expense will be required to take whatever measures may be required to correct this interference.

General Statement for EVMs including a radio

User Power/Frequency Use Obligations: This radio is intended for development/professional use only in legally allocated frequency and power limits. Any use of radio frequencies and/or power availability of this EVM and its development application(s) must comply with local laws governing radio spectrum allocation and power limits for this evaluation module. It is the user’s sole responsibility to only operate this radio in legally acceptable frequency space and within legally mandated power limitations. Any exceptions to this is strictly prohibited and unauthorized by Texas Instruments unless user has obtained appropriate experimental/development licenses from local regulatory authorities, which is responsibility of user including its acceptable authorization.

For EVMs annotated as FCC – FEDERAL COMMUNICATIONS COMMISSION Part 15 Compliant

Caution

This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions: (1) This device may not cause harmful interference, and (2) this device must accept any interference received, including interference that may cause undesired operation. Changes or modifications not expressly approved by the party responsible for compliance could void the user's authority to operate the equipment.

FCC Interference Statement for Class A EVM devices

This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when the equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. Operation of this equipment in a residential area is likely to cause harmful interference in which case the user will be required to correct the interference at his own expense.

FCC Interference Statement for Class B EVM devices

This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a residential installation. This equipment generates, uses and can radiate radio frequency energy and, if not installed and used in accordance with the instructions, may cause harmful interference to radio communications. However, there is no guarantee that interference will not occur in a particular installation. If this equipment does cause harmful interference to radio or television reception, which can be determined by turning the equipment off and on, the user is encouraged to try to correct the interference by one or more of the following measures:

For EVMs annotated as IC – INDUSTRY CANADA Compliant

This Class A or B digital apparatus complies with Canadian ICES-003.

Changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.

Concerning EVMs including radio transmitters

This device complies with Industry Canada licence-exempt RSS standard(s). Operation is subject to the following two conditions: (1) this device may not cause interference, and (2) this device must accept any interference, including interference that may cause undesired operation of the device.

Concerning EVMs including detachable antennas

Under Industry Canada regulations, this radio transmitter may only operate using an antenna of a type and maximum (or lesser) gain approved for the transmitter by Industry Canada. To reduce potential radio interference to other users, the antenna type and its gain should be so chosen that the equivalent isotropically radiated power (e.i.r.p.) is not more than that necessary for successful communication. This radio transmitter has been approved by Industry Canada to operate with the antenna types listed in the user guide with the maximum permissible gain and required antenna impedance for each antenna type indicated. Antenna types not included in this list, having a gain greater than the maximum gain indicated for that type, are strictly prohibited for use with this device.

~

Cet appareil numérique de la classe A ou B est conforme à la norme NMB-003 du Canada.

Les changements ou les modifications pas expressément approuvés par la partie responsable de la conformité ont pu vider l’autorité de l'utilisateur pour actionner l'équipement.

Concernant les EVMs avec appareils radio

Le présent appareil est conforme aux CNR d'Industrie Canada applicables aux appareils radio exempts de licence. L'exploitation est autorisée aux deux conditions suivantes : (1) l'appareil ne doit pas produire de brouillage, et (2) l'utilisateur de l'appareil doit accepter tout brouillage radioélectrique subi, même si le brouillage est susceptible d'en compromettre le fonctionnement.

Concernant les EVMs avec antennes détachables

Conformément à la réglementation d'Industrie Canada, le présent émetteur radio peut fonctionner avec une antenne d'un type et d'un gain maximal (ou inférieur) approuvé pour l'émetteur par Industrie Canada. Dans le but de réduire les risques de brouillage radioélectrique à l'intention des autres utilisateurs, il faut choisir le type d'antenne et son gain de sorte que la puissance isotrope rayonnée équivalente (p.i.r.e.) ne dépasse pas l'intensité nécessaire à l'établissement d'une communication satisfaisante.

Le présent émetteur radio a été approuvé par Industrie Canada pour fonctionner avec les types d'antenne énumérés dans le manuel d’usage et ayant un gain admissible maximal et l'impédance requise pour chaque type d'antenne. Les types d'antenne non inclus dans cette liste, ou dont le gain est supérieur au gain maximal indiqué, sont strictement interdits pour l'exploitation de l'émetteur.

Important Notice for Users of this Product in Japan

This development kit is NOT certified as Confirming to Technical Regulations of Radio Law of Japan! If you use this product in Japan, you are required by Radio Law of Japan to follow the instructions below with respect to this product:

  1. Use this product in a shielded room or any other test facility as defined in the notification #173 issued by Ministry of Internal Affairs and Communications on March 28, 2006, based on Sub-section 1.1 of Article 6 of the Ministry’s Rule for Enforcement of Radio Law of Japan,
  2. Use this product only after you obtained the license of Test Radio Station as provided in Radio Law of Japan with respect to this product, or
  3. Use of this product only after you obtained the Technical Regulations Conformity Certification as provided in Radio Law of Japan with respect to this product.

Also, please do not transfer this product, unless you give the same notice above to the transferee. Please note that if you could not follow the instructions above, you will be subject to penalties of Radio Law of Japan.

Texas Instruments Japan Limited (address) 24-1, Nishi-Shinjuku 6 chome, Shinjukku-ku, Tokyo, Japan

http://www.tij.co.jp

【ご使用にあたっての注意】

本開発キットは技術基準適合証明を受けておりません。

本製品のご使用に際しては、電波法遵守のため、以下のいずれかの措置を取っていただく必要がありますのでご注意ください。

(1)電波法施行規則第6条第1項第1号に基づく平成18年3月28日総務省告示第173号で定められた電波暗室等の試験設備でご使用いただく。

(2)実験局の免許を取得後ご使用いただく。

(3)技術基準適合証明を取得後ご使用いただく。

なお、本製品は、上記の「ご使用にあたっての注意」を譲渡先、移転先に通知しない限り、譲渡、移転できないものとします。

上記を遵守頂けない場合は、電波法の罰則が適用される可能性があることをご留意ください。

日本テキサス・インスツルメンツ株式会社

東京都新宿区西新宿6丁目24番1号

西新宿三井ビル

http://www.tij.co.jp

EVALUATION BOARD/KIT/MODULE (EVM) WARNINGS, RESTRICTIONS AND DISCLAIMERS

For Feasibility Evaluation Only, in Laboratory/Development Environments

Unless otherwise indicated, this EVM is not a finished electrical equipment and not intended for consumer use. It is intended solely for use for preliminary feasibility evaluation in laboratory/development environments by technically qualified electronics experts who are familiar with the dangers and application risks associated with handling electrical mechanical components, systems and subsystems. It should not be used as all or part of a finished end product.

Your Sole Responsibility and Risk

You acknowledge, represent and agree that:

  1. You have unique knowledge concerning Federal, State and local regulatory requirements (including but not limited to Food and Drug Administration regulations, if applicable) which relate to your products and which relate to your use (and/or that of your employees, affiliates, contractors or designees) of the EVM for evaluation, testing and other purposes.
  2. You have full and exclusive responsibility to assure the safety and compliance of your products with all such laws and other applicable regulatory requirements, and also to assure the safety of any activities to be conducted by you and/or your employees, affiliates, contractors or designees, using the EVM. Further, you are responsible to assure that any interfaces (electronic and/or mechanical) between the EVM and any human body are designed with suitable isolation and means to safely limit accessible leakage currents to minimize the risk of electrical shock hazard.
  3. You will employ reasonable safeguards to ensure that your use of the EVM will not result in any property damage, injury or death, even if the EVM should fail to perform as described or expected.
  4. You will take care of proper disposal and recycling of the EVM’s electronic components and packing materials.

Certain Instructions

It is important to operate this EVM within TI’s recommended specifications and environmental considerations per the user guidelines. Exceeding the specified EVM ratings (including but not limited to input and output voltage, current, power, and environmental ranges) may cause property damage, personal injury or death. If there are questions concerning these ratings please contact a TI field representative prior to connecting interface electronics including input power and intended loads. Any loads applied outside of the specified output range may result in unintended and/or inaccurate operation and/or possible permanent damage to the EVM and/or interface electronics. Please consult the EVM User's Guide prior to connecting any load to the EVM output. If there is uncertainty as to the load specification, please contact a TI field representative. During normal operation, some circuit components may have case temperatures greater than 60°C as long as the input and output are maintained at a normal ambient operating temperature. These components include but are not limited to linear regulators, switching transistors, pass transistors, and current sense resistors which can be identified using the EVM schematic located in the EVM User's Guide. When placing measurement probes near these devices during normal operation, please be aware that these devices may be very warm to the touch. As with all electronic evaluation tools, only qualified personnel knowledgeable in electronic measurement and diagnostics normally found in development environments should use these EVMs.

Agreement to Defend, Indemnify and Hold Harmless

You agree to defend, indemnify and hold TI, its licensors and their representatives harmless from and against any and all claims, damages, losses, expenses, costs and liabilities (collectively, "Claims") arising out of or in connection with any use of the EVM that is not in accordance with the terms of the agreement. This obligation shall apply whether Claims arise under law of tort or contract or any other legal theory, and even if the EVM fails to perform as described or expected.

Safety-Critical or Life-Critical Applications

If you intend to evaluate the components for possible use in safety critical applications (such as life support) where a failure of the TI product would reasonably be expected to cause severe personal injury or death, such as devices which are classified as FDA Class III or similar classification, then you must specifically notify TI of such intent and enter into a separate Assurance and Indemnity Agreement.

Leave a Comment
Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox