Secondary Bootloaders on OMAP-L1x

From Texas Instruments Embedded Processors Wiki

Jump to: navigation, search
Translate this page to   

Contents


NOR Legacy

This topic describes the development of a secondary bootloader used for NOR legacy boot on an OMAP-L1x or C674x device. The NOR legacy boot mode forgoes the more sophisticated Application Image Script (AIS) boot system to simplify boot. A NOR legacy image consists of a single block of program data stored at the head of NOR (EMIFA chip select 2, or address 0x60000000). At boot, the bootloader copies this block to L2RAM and jumps directly into the copied code starting at address 0x11800004.

No integrated tool exists to prepare NOR legacy boot images, so this topic provides step-by-step instructions. Please note that boot modes and implementations vary between devices. This topic applies only to OMAP-L1x and C674x devices.

NOR Configuration Word

OMAP-L1x and C674x devices have three separate NOR bootmodes, but all three share the same boot pin selection values. The bootloader distinguishes between the three boot modes by reading the first 32-bit word of NOR. This word is called the NOR Configuration Word. For NOR Legacy boot, the configuration word should look like this:

Bit Field Value Description
31-12 Reserved 0 Reserved
11-8 COPY 0x0 1 KB

0x1 2 KB

...

0xE 15 KB

0xF 16 KB

Length of data to copy from the base of the NOR Flash to the base of the digital signal processor

(DSP) L2 RAM. This value is used only for the Legacy NOR boot method.

7-6 Reserved 0 Reserved
5-4 METHOD 0 Legacy NOR boot
3-1 Reserved 0 Reserved
0 ACCESS EMIFA 0x0 8-bit access

0x1 16-bit access

access mode

To summarize: the NOR Configuration word takes the form 0x00000X0Y, where (X + 1) is the size in KB of the NOR legacy boot image and Y selects either 8- or 16-bit NOR access.

The first step in building a secondary bootloader application is to determine how much space the appliation data will occupy in memory. Using this, determine the necessary value of the NOR configuration word. Note that 16 KB is the largest possible application size for NOR legacy boot. Larger application sizes may require the use of an alternate boot mode.

Building the Secondary Bootloader Application

Once the configuration word is finalized, the application source and linker command files are next. The linker must not place any program data or initialization sections in memory outside the first 16 KB (or smaller, depending on your NOR configuration word) of L2RAM. Furthermore, the very first word of L2RAM must be reserved for the NOR configuration word. An example linker command file may have the following form:

Linker Command File (DSP) Linker Command File (ARM)
-stack 0x1000
-heap  0x1000

MEMORY {
    CFG_L2RAM:    o = 0x11800000  l = 0x00000020
    PROG_L2RAM:   o = 0x11800020  l = 0x00003FE0
}

SECTIONS {
    .entryPoint >       PROG_L2RAM
    .text	> PROG_L2RAM
    .data	> PROG_L2RAM
    .const	> PROG_L2RAM
    .far	> PROG_L2RAM
    .switch	> PROG_L2RAM
    .cinit	> PROG_L2RAM
    .bss	> PROG_L2RAM
    .cio	> PROG_L2RAM
    .stack	> PROG_L2RAM
    .sysmem	> PROG_L2RAM
    .nor_cfg_word > CFG_L2RAM
}
-stack 0x1000
-heap  0x1000

MEMORY {
    CFG_L3RAM:    o = 0x80000000  l = 0x00000020
    PROG_L3RAM:   o = 0x80000020  l = 0x00003FE0
}

SECTIONS {
    .entryPoint >       PROG_L3RAM
    .text	> PROG_L3RAM
    .data	> PROG_L3RAM
    .const	> PROG_L3RAM
    .far	> PROG_L3RAM
    .switch	> PROG_L3RAM
    .cinit	> PROG_L3RAM
    .bss	> PROG_L3RAM
    .cio	> PROG_L3RAM
    .stack	> PROG_L3RAM
    .sysmem	> PROG_L3RAM
    .nor_cfg_word > CFG_L3RAM
}

Note that a 32-byte section is set aside for the exclusive use of the configuration word. This is the minimum allowed section size in some cases, and it is a safe value to use.

The NOR configuration word must now be inserted into the secondary bootloader's source code. This can be done using a simple assembly source file:

    .global _c_int00
    .sect ".nor_config_word"
config_word:
    .word 0x00000F01
    B _c_int00
    NOP
    NOP
    NOP
    NOP
    NOP
    NOP


At boot, the bootloader will jump to address 0x11800004 (0x80000004 on ARM), then branch from there to the secondary bootloader's actual entrypoint. Note that this assumes that the standard RTS library entrypoint, _c_int00, is used. To use an alternate entrypoint, the branch (B) instruction argument must be changed.

With the NOR configuration word placed at 0x11800000 and the program data confined to the first 16 KB of L2 RAM, the secondary bootloader should now be ready to build (for DSP - for ARM, the NOR configuration word placed at 0x80000000 and the program data is confined to the first 16 KB of L3 RAM). Compile and link the application.

Extracting the Binary Image

The application executable (.out) must now be converted to a raw binary image. TI's code generation tools include utilities to do this, but it is a complicated task. Locate the hex utility in your code gen tools' bin folder. (The DSP version should be named hex6x.exe, and the ARM version should be hex470.exe.)

Next, create a utility command file (.cmd) to hold the complicated parameters that will tell the utility what we want to do. The contents of this file should be as follows:

hex6x.exe Command File (DSP) hex470.exe Command File (ARM)
-b
-image
-zero
-memwidth 8
-linkerfill
-fill 0x00000000

ROMS
{
  FLASH: org = 0x11800000, len=0x4000, romwidth=8
}
-b
-image
-zero
-memwidth 8
-linkerfill
-fill 0x00000000

ROMS
{
  FLASH: org = 0x80000000, len=0x4000, romwidth=8
}

This tells the utility to extract all sections contained in the 16-KB block starting at the head of L2RAM (DSP) or L3RAM (ARM). The contents of these sections will be dumped to a binary file and fill any unoccupied space with 0-valued words. Call the script with the following command line instruction (with "secondary_bl" replaced by your actual file names):

DSP:

hex6x.exe secondary_bl.cmd -o=secondary_bl.bin secondary_bl.out

ARM:

hex470.exe secondary_bl.cmd -o=secondary_bl.bin secondary_bl.out

The resulting binary file should now be ready to flash to a NOR device. Use a hex editor to double-check that the binary file contents seem correct. The first word in the binary file should be the NOR configuration word in little-endian order.

NOR Direct

Preparing an image for NOR Legacy boot mode is similar to NOR legacy, with a few modifications:

  1. Coming soon

See Also

Application Note: Using the D800K001 Bootloader

Application Note: Using the OMAP-L1x8 Bootloader

E2e.jpg For technical support on OMAP please post your questions on The OMAP Forum. Please post only comments about the article Secondary Bootloaders on OMAP-L1x here.
Hyperlink blue.png Links
ARM Microcontroller MCU ARM Processor Digital Media Processor Digital Signal Processing Microcontroller MCU Multi Core Processor
Ultra Low Power DSP 8 bit Microcontroller MCU 16 bit Microcontroller MCU 32 bit Microcontroller MCU

Leave a Comment

Comments

Comments on Secondary Bootloaders on OMAP-L1x


Tlorenz said ...

This wiki page can confuse customers by thinking hex6x.exe and hex470.exe allows to create bootable images OMAP-L1x boot ROM can execute. This is not the case. OMAP-L138 follows the AIS protocol standard from TI which is not supported by such tools. The chapter "See Also" points to the documents dedicated for non secondary boot. Using secondary boot customers need to have a clear understanding of the output of the hex tools to make sure the secondary boot code is compatible.

--Tlorenz 13:42, 16 May 2011 (CDT)

Rg-bm said ...

To boot directly from the NOR flash (tested on C6748 eval board):

  • make sure you DO NOT initialize the EMIF(A) when running directly from Nor flash!
  • assembly:

.word 0x00000011

  • linker command file:

-stack 0x1000 -heap 0x1000

MEMORY {

   CFG_NOR:      o = 0x60000000  l = 0x00000020
   PROG_NOR:     o = 0x60000020  l = 0x00003FE0
   PROG_L2RAM:   o = 0x11800000  l = 0x00002000

}

SECTIONS {

   .entryPoint > PROG_NOR
   .text	> PROG_NOR
   .const	> PROG_NOR
   .switch	> PROG_NOR
   .cinit	> PROG_NOR
   
   .far	> PROG_L2RAM
   .data	> PROG_L2RAM
   .bss	> PROG_L2RAM
   .cio	> PROG_L2RAM
   .stack	> PROG_L2RAM
   .sysmem	> PROG_L2RAM
   .nor_cfg_word > CFG_NOR

}


--Rg-bm 02:58, 8 September 2011 (CDT)

Personal tools
Namespaces
Variants
Actions
Navigation
Print/export
Toolbox